![]() |
MCUSW
|
The EthTrcv Driver MCAL provides low level access to Ethernet transceiver present on Jacinto 7 device family EVMs.
The EthTrcv Driver implements a standardized interface specified in the AUTOSAR_SWS_EthernetTransceiverDriver document.
The EthTrcv Driver is part of the Communication Stack in the AUTOSAR Basic Software (BSW).
Sub Modules | |
| EthTrcv Configuration | |
Functions | |
| void | EthTrcv_Init (const EthTrcv_ConfigType *CfgPtr) |
| This function initializes the Ethernet Transceiver controller. All the required initialization for the transceiver driver is performed in this function. More... | |
| Std_ReturnType | EthTrcv_TransceiverInit (uint8 TrcvIdx) |
| This function initializes the Ethernet Transceiver controller. All the required initialization for the transceiver driver is performed in this function. More... | |
| Std_ReturnType | EthTrcv_SetTransceiverMode (uint8 TrcvIdx, EthTrcv_ModeType CtrlMode) |
| This function enables / disables the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_GetTransceiverMode (uint8 TrcvIdx, EthTrcv_ModeType *TrcvModePtr) |
| This function obtains the state of the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_StartAutoNegotiation (uint8 TrcvIdx) |
| This function restarts the negotiation of the transmission parameters used by the indexed. More... | |
| Std_ReturnType | EthTrcv_GetLinkState (uint8 TrcvIdx, EthTrcv_LinkStateType *LinkStatePtr) |
| This function obtains the link state of the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_GetBaudRate (uint8 TrcvIdx, EthTrcv_BaudRateType *BaudRatePtr) |
| This function obtains the baud rate of the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_GetDuplexMode (uint8 TrcvIdx, EthTrcv_DuplexModeType *DuplexModePtr) |
| This function obtains the duplex mode of the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_SetPhyTestMode (uint8 TrcvIdx, EthTrcv_PhyTestModeType Mode) |
| This function Activates a given test mode. More... | |
| Std_ReturnType | EthTrcv_SetPhyLoopbackMode (uint8 TrcvIdx, EthTrcv_PhyLoopbackModeType Mode) |
| This function Activates a given loopback mode. More... | |
| Std_ReturnType | EthTrcv_GetPhySignalQuality (uint8 TrcvIdx, uint32 *SignalQualityPtr) |
| This function Obtains the current signal quality of the link of the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_SetPhyTxMode (uint8 TrcvIdx, EthTrcv_PhyTxModeType Mode) |
| This function Activates a given transmission mode. More... | |
| Std_ReturnType | EthTrcv_GetCableDiagnosticsResult (uint8 TrcvIdx, EthTrcv_CableDiagResultType *ResultPtr) |
| This function Retrieves the cable diagnostics result of a given transceiver. More... | |
| Std_ReturnType Std_ReturnType | EthTrcv_GetPhyIdentifier (uint8 TrcvIdx, uint32 *OrgUniqueIdPtr, uint8 *ModelNrPtr, uint8 *RevisionNrPtr) |
| This function Obtains the PHY identifier of the Ethernet Transceiver according to IEEE 802.3-2015 chapter 22.2.4.3.1 PHY Identifer. More... | |
| void | EthTrcv_GetVersionInfo (Std_VersionInfoType *VersionInfoPtr) |
| Function returns the version information of this module. More... | |
| void | EthTrcv_ReadMiiIndication (uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegIdx, uint16 RegVal) |
| This function is called when information has been read out via MII interface. Triggered by previous Eth_ReadMii call. It can directly be called within Eth_ReadMii. More... | |
| void | EthTrcv_WriteMiiIndication (uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegId) |
| This function is called when information has been written via MII interface. Triggered by previous Eth_WriteMii call. It can directly be called within Eth_WriteMii. More... | |
| void | EthTrcv_MainFunction (void) |
| This function is used for polling state changes and wakeup reasons. It calls EthIf_TrcvModeIndication when the transceiver mode changed. It stores wakeup events if EthTrcvWakeUpSupport is set to ETHTRCV_WAKEUP_BY_POLLING. More... | |
EthTrcv Driver Module SW Version Info | |
Defines for ETHTRCV Driver version used for compatibility checks | |
| #define | ETHTRCV_SW_MAJOR_VERSION (9U) |
| Driver Implementation Major Version. More... | |
| #define | ETHTRCV_SW_MINOR_VERSION (2U) |
| Driver Implementation Minor Version. More... | |
| #define | ETHTRCV_SW_PATCH_VERSION (0U) |
| Driver Implementation Patch Version. More... | |
EthTrcv Driver Module AUTOSAR Version Info | |
Defines for ETHTRCV Driver AUTOSAR version used for compatibility checks | |
| #define | ETHTRCV_AR_RELEASE_MAJOR_VERSION (4U) |
| AUTOSAR Major Version implemented. More... | |
| #define | ETHTRCV_AR_RELEASE_MINOR_VERSION (3U) |
| AUTOSAR Minor Version implemented. More... | |
| #define | ETHTRCV_AR_RELEASE_REVISION_VERSION (1U) |
| AUTOSAR patch Version implemented. More... | |
EthTrcv Driver ID Info | |
| #define | ETHTRCV_VENDOR_ID (44U) |
| Texas Instruments Vendor ID. More... | |
| #define | ETHTRCV_MODULE_ID (73U) |
| EthTrcv Driver ID. More... | |
| #define | ETHTRCV_INSTANCE_ID (0U) |
| EthTrcv Instace ID. More... | |
EthTrcv Error Codes | |
| #define | ETHTRCV_E_INV_TRCV_IDX ((uint8) 0x01U) |
| Invalid transceiver index. More... | |
| #define | ETHTRCV_E_UNINIT ((uint8) 0x02U) |
| EthTrcv module was not initialized. More... | |
| #define | ETHTRCV_E_PARAM_POINTER ((uint8) 0x03U) |
| #define | ETHTRCV_E_INIT_FAILED ((uint8) 0x04U) |
| #define ETHTRCV_SW_MAJOR_VERSION (9U) |
Driver Implementation Major Version.
| #define ETHTRCV_SW_MINOR_VERSION (2U) |
Driver Implementation Minor Version.
| #define ETHTRCV_SW_PATCH_VERSION (0U) |
Driver Implementation Patch Version.
| #define ETHTRCV_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major Version implemented.
| #define ETHTRCV_AR_RELEASE_MINOR_VERSION (3U) |
AUTOSAR Minor Version implemented.
| #define ETHTRCV_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR patch Version implemented.
| #define ETHTRCV_VENDOR_ID (44U) |
Texas Instruments Vendor ID.
| #define ETHTRCV_MODULE_ID (73U) |
EthTrcv Driver ID.
| #define ETHTRCV_INSTANCE_ID (0U) |
EthTrcv Instace ID.
| #define ETHTRCV_E_INV_TRCV_IDX ((uint8) 0x01U) |
Invalid transceiver index.
| #define ETHTRCV_E_UNINIT ((uint8) 0x02U) |
EthTrcv module was not initialized.
brief Invalid pointer in parameter list
| #define ETHTRCV_E_PARAM_POINTER ((uint8) 0x03U) |
brief Initialization failure
| #define ETHTRCV_E_INIT_FAILED ((uint8) 0x04U) |
| void EthTrcv_Init | ( | const EthTrcv_ConfigType * | CfgPtr | ) |
This function initializes the Ethernet Transceiver controller. All the required initialization for the transceiver driver is performed in this function.
* Service name : EthTrcv_Init * Syntax : void EthTrcv_Init( * const EthTrcv_ConfigType* ConfigPtr * ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x01 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : CfgPtr. Points to the implementation specific structure * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : Initializes the Ethernet Transceiver Driver. *
| Std_ReturnType EthTrcv_TransceiverInit | ( | uint8 | TrcvIdx | ) |
This function initializes the Ethernet Transceiver controller. All the required initialization for the transceiver driver is performed in this function.
* Service name : EthTrcv_Init * Syntax : void EthTrcv_TransceiverInit( * uint8 TrcvIdx * ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x02 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : TrcvIdx tranceiver controller index * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: Service accepted * E_NOT_OK: Service denied * Description : Initializes the Ethernet Transceiver Driver. *
| Std_ReturnType EthTrcv_SetTransceiverMode | ( | uint8 | TrcvIdx, |
| EthTrcv_ModeType | CtrlMode | ||
| ) |
This function enables / disables the indexed transceiver.
* Service name : EthTrcv_SetTransceiverMode * Syntax : Std_ReturnType EthTrcv_SetTransceiverMode( * uint8 TrcvIdx, * EthTrcv_ModeType CtrlMode * ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x03 * Sync/Async : Asynchronous * Reentrancy : Non Reentrant * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * CtrlMode * ETHTRCV_MODE_DOWN: disable the transceiver * ETHTRCV_MODE_ACTIVE: enable the transceiver * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: Service accepted * E_NOT_OK: Service denied * Description : Enables / disables the indexed transceiver. *
| Std_ReturnType EthTrcv_GetTransceiverMode | ( | uint8 | TrcvIdx, |
| EthTrcv_ModeType * | TrcvModePtr | ||
| ) |
This function obtains the state of the indexed transceiver.
* Service name : EthTrcv_GetTransceiverMode * Syntax : Std_ReturnType EthTrcv_GetTransceiverMode( * uint8 TrcvIdx, * EthTrcv_ModeType* TrcvModePtr * ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x04 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: transceiver could not be initialized * Description : Obtains the state of the indexed transceiver. *
| Std_ReturnType EthTrcv_StartAutoNegotiation | ( | uint8 | TrcvIdx | ) |
This function restarts the negotiation of the transmission parameters used by the indexed.
* Service name : EthTrcv_StartAutoNegotiation * Syntax : Std_ReturnType EthTrcv_StartAutoNegotiation( * uint8 TrcvIdx * ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x05 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: transceiver could not be initialized * Description : Restarts the negotiation of the transmission parameters * used by the indexed. *
| Std_ReturnType EthTrcv_GetLinkState | ( | uint8 | TrcvIdx, |
| EthTrcv_LinkStateType * | LinkStatePtr | ||
| ) |
This function obtains the link state of the indexed transceiver.
* Service name : EthTrcv_GetLinkState * Syntax : Std_ReturnType EthTrcv_GetLinkState( * uint8 TrcvIdx, * EthTrcv_LinkStateType* LinkStatePtr * ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x06 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * Parameters (inout): None * Parameters (out) : LinkStatePtr * ETHTRCV_LINK_STATE_DOWN: transceiver is disconnected * ETHTRCV_LINK_STATE_ACTIVE: transceiver is connected * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: transceiver could not be initialized * Description : Obtains the link state of the indexed transceiver. *
| Std_ReturnType EthTrcv_GetBaudRate | ( | uint8 | TrcvIdx, |
| EthTrcv_BaudRateType * | BaudRatePtr | ||
| ) |
This function obtains the baud rate of the indexed transceiver.
* Service name : EthTrcv_GetBaudRate * Syntax : Std_ReturnType EthTrcv_GetBaudRate( * uint8 TrcvIdx, * EthTrcv_BaudRateType* BaudRatePtr * ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x07 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * Parameters (inout): None * Parameters (out) : BaudRatePtr * ETHTRCV_BAUD_RATE_10MBIT: 10MBit connection * ETHTRCV_BAUD_RATE_100MBIT: 100MBit connection * ETHTRCV_BAUD_RATE_1000MBIT: 1000MBit connection * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: transceiver could not be initialized * Description : Obtains the baud rate of the indexed transceiver. *
| Std_ReturnType EthTrcv_GetDuplexMode | ( | uint8 | TrcvIdx, |
| EthTrcv_DuplexModeType * | DuplexModePtr | ||
| ) |
This function obtains the duplex mode of the indexed transceiver.
* Service name : EthTrcv_GetDuplexMode * Syntax : Std_ReturnType EthTrcv_GetDuplexMode( * uint8 TrcvIdx, * EthTrcv_DuplexModeType* DuplexModePtr * ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x08 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * Parameters (inout): None * Parameters (out) : DuplexModePtr * ETHTRCV_DUPLEX_MODE_HALF: half duplex connections * ETHTRCV_DUPLEX_MODE_FULL: full duplex connection * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: transceiver could not be initialized * Description : Obtains the duplex mode of the indexed transceiver. *
| Std_ReturnType EthTrcv_SetPhyTestMode | ( | uint8 | TrcvIdx, |
| EthTrcv_PhyTestModeType | Mode | ||
| ) |
This function Activates a given test mode.
* Service name : EthTrcv_SetPhyTestMode * Syntax : Std_ReturnType EthTrcv_SetPhyTestMode( * uint8 TrcvIdx, * EthTrcv_PhyTestModeType Mode) * * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] :0x11 * Sync/Async : Synchronous * Reentrancy : Reentrant for different TrcvIdx. Non reentrant for the same TrcvIdx * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * Parameters (in) : Mode. Test mode to be activated. Refer to the \ref EthTrcv_PhyTestModeType. * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: transceiver could not be initialized * Description : Activates a given test mode *
| Std_ReturnType EthTrcv_SetPhyLoopbackMode | ( | uint8 | TrcvIdx, |
| EthTrcv_PhyLoopbackModeType | Mode | ||
| ) |
This function Activates a given loopback mode.
* Service name : EthTrcv_SetPhyLoopbackMode * Syntax : Std_ReturnType EthTrcv_SetPhyLoopbackMode( * uint8 TrcvIdx, * EthTrcv_PhyLoopbackModeType Mode * ) * * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] :0x12 * Sync/Async : Synchronous * Reentrancy : Reentrant for different TrcvIdx. Non reentrant for the same TrcvIdx * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * Parameters (in) : Mode. Refer to the \ref EthTrcv_PhyLoopbackModeType. * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: transceiver could not be initialized * Description : Activates a given loopback mode. *
| Std_ReturnType EthTrcv_GetPhySignalQuality | ( | uint8 | TrcvIdx, |
| uint32 * | SignalQualityPtr | ||
| ) |
This function Obtains the current signal quality of the link of the indexed transceiver.
* Service name : EthTrcv_GetPhySignalQuality * Syntax : Std_ReturnType EthTrcv_GetPhySignalQuality( * uint8 TrcvIdx, * uint32* SignalQualityPtr * ) * * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] :0x12 * Sync/Async : Synchronous * Reentrancy : Reentrant for different TrcvIdx. Non reentrant for the same TrcvIdx * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * Parameters (Out) : SignalQualityPtr Pointer to the memory where the signal * quality shall be stored. * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: transceiver could not be initialized * Description : Obtains the current signal quality of the link of the indexed transceiver. *
| Std_ReturnType EthTrcv_SetPhyTxMode | ( | uint8 | TrcvIdx, |
| EthTrcv_PhyTxModeType | Mode | ||
| ) |
This function Activates a given transmission mode.
* Service name : EthTrcv_SetPhyTxMode * Syntax : Std_ReturnType EthTrcv_SetPhyTxMode( * uint8 TrcvIdx, * EthTrcv_PhyTxModeType Mode * ) * * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] :0x13 * Sync/Async : Synchronous * Reentrancy : Reentrant for different TrcvIdx. Non reentrant for the same TrcvIdx * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * Parameters (in) : Mode Transmission mode to be activated. Refer to \ref EthTrcv_PhyTxModeType * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: transceiver could not be initialized * Description : Activates a given transmission mode. *
| Std_ReturnType EthTrcv_GetCableDiagnosticsResult | ( | uint8 | TrcvIdx, |
| EthTrcv_CableDiagResultType * | ResultPtr | ||
| ) |
This function Retrieves the cable diagnostics result of a given transceiver.
* Service name : EthTrcv_GetCableDiagnosticsResult * Syntax : Std_ReturnType EthTrcv_GetCableDiagnosticsResult( * uint8 TrcvIdx, * EthTrcv_CableDiagResultType* ResultPtr * ) * * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] :0x14 * Sync/Async : Synchronous * Reentrancy : Reentrant for different TrcvIdx. Non reentrant for the same TrcvIdx * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * Parameters (out) : ResultPtr. Transmission mode to be activated. Refer to \ref * EthTrcv_CableDiagResultType * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: transceiver could not be initialized * Description : Retrieves the cable diagnostics result of a given transceiver.. *
| Std_ReturnType Std_ReturnType EthTrcv_GetPhyIdentifier | ( | uint8 | TrcvIdx, |
| uint32 * | OrgUniqueIdPtr, | ||
| uint8 * | ModelNrPtr, | ||
| uint8 * | RevisionNrPtr | ||
| ) |
This function Obtains the PHY identifier of the Ethernet Transceiver according to IEEE 802.3-2015 chapter 22.2.4.3.1 PHY Identifer.
* Service name : EthTrcv_GetPhyIdentifier * Syntax : Std_ReturnType EthTrcv_GetPhyIdentifier( * uint8 TrcvIdx, * uint32* OrgUniqueIdPtr, * uint8* ModelNrPtr, * uint8* RevisionNrPtr * ) * * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x15 * Sync/Async : Synchronous * Reentrancy : Reentrant for different TrcvIdx. Non reentrant for the same TrcvIdx * Parameters (in) : TrcvIdx. Index of the transceiver within the context * of the Ethernet Transceiver Driver * Parameters (in) : OrgUniqueIdPtr Pointer to the memory where the Organizationally Unique * Identifier shall be stored. * Parameters (in) : ModelNrPtr Pointer to the memory where the Manufacturer's Model * Number shall be stored. * Parameters (in) : RevisionNrPtr Pointer to the memory where the Revision Number * shall be stored. * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: transceiver could not be initialized * Description : Obtains the PHY identifier of the Ethernet Transceiver according to * IEEE 802.3-2015 chapter 22.2.4.3.1 PHY Identifer.. *
| void EthTrcv_GetVersionInfo | ( | Std_VersionInfoType * | VersionInfoPtr | ) |
Function returns the version information of this module.
* Service name : EthTrcv_GetVersionInfo * Syntax : void EthTrcv_GetVersionInfo( * Std_VersionInfoType* versioninfo * ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x07 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : VersionInfoPtr. Pointer to where to store the version * information of this module. * Return value : None * Description : This function returns the version information of this * module *
| void EthTrcv_ReadMiiIndication | ( | uint8 | CtrlIdx, |
| uint8 | TrcvIdx, | ||
| uint8 | RegIdx, | ||
| uint16 | RegVal | ||
| ) |
This function is called when information has been read out via MII interface. Triggered by previous Eth_ReadMii call. It can directly be called within Eth_ReadMii.
* Service name : EthTrcv_ReadMiiIndication * Syntax : void EthTrcv_ReadMiiIndication( * uint8 CtrlIdx, * uint8 TrcvIdx, * uint8 RegIdx, * uint8 RegVal * ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x09 * Sync/Async : Synchronous * Reentrancy : Non Reentrant for the same CtrlIdx, reentrant for * different * Parameters (in) : CtrlIdx. Index of the controller within the context * of the Ethernet Driver * TrcvIdx. Index of the transceiver on the MII * RegIdx. Index of the transceiver register on the MII * RegVal. Value contained in the indexed register * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : Called when information has been read out via MII interface. * Triggered by previous Eth_ReadMii call. Can directly be * called within Eth_ReadMii. *
| void EthTrcv_WriteMiiIndication | ( | uint8 | CtrlIdx, |
| uint8 | TrcvIdx, | ||
| uint8 | RegId | ||
| ) |
This function is called when information has been written via MII interface. Triggered by previous Eth_WriteMii call. It can directly be called within Eth_WriteMii.
* Service name : EthTrcv_WriteMiiIndication * Syntax : void EthTrcv_WriteMiiIndication( * uint8 CtrlIdx, * uint8 TrcvIdx, * uint8 RegId * ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0a * Sync/Async : Synchronous * Reentrancy : Non Reentrant for the same CtrlIdx, reentrant for * different * Parameters (in) : CtrlIdx. Index of the controller within the context * of the Ethernet Driver * TrcvIdx. Index of the transceiver on the MII * RegIdx. Index of the transceiver register on the MII * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : Called when information has been written via MII interface. * Triggered by previous Eth_WriteMii call. Can directly be * called within Eth_WriteMii. *
| void EthTrcv_MainFunction | ( | void | ) |
This function is used for polling state changes and wakeup reasons. It calls EthIf_TrcvModeIndication when the transceiver mode changed. It stores wakeup events if EthTrcvWakeUpSupport is set to ETHTRCV_WAKEUP_BY_POLLING.
* Service name : EthTrcv_MainFunction * Syntax : void EthTrcv_MainFunction( * void * ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0c * Description : Used for polling state changes and wakeup reasons. Calls * EthIf_TrcvModeIndication when the transceiver mode * changed. Stores wakeup events if EthTrcvWakeUpSupport is * set to ETHTRCV_WAKEUP_BY_POLLING. *