![]() |
MCUSW
|
This file contains ISR function declaration for CDD IPC Driver.
Go to the source code of this file.
CDD Driver ISR category level | |
|
This file provides ISR API's that is used to receive and process events from remote cores
Defines for CDD Driver ISR ISR category level | |
| #define | CDD_IPC_ISR_VOID (0x00U) |
| void ISR type More... | |
| #define | CDD_IPC_ISR_CAT1 (0x01U) |
| Category 1 ISR type. More... | |
| #define | CDD_IPC_ISR_CAT2 (0x02U) |
| Category 2 ISR type. More... | |
| void | Cdd_IpcIrq_Fun (uint32 srcProcId) |
| A Mailbox can raise multiple interrupts. In this implementation, the Mailbox new message interrupt is used determine presence of data from the remote core in the vring. More... | |
| #define CDD_IPC_ISR_VOID (0x00U) |
void ISR type
| #define CDD_IPC_ISR_CAT1 (0x01U) |
Category 1 ISR type.
| #define CDD_IPC_ISR_CAT2 (0x02U) |
Category 2 ISR type.
| void Cdd_IpcIrq_Fun | ( | uint32 | srcProcId | ) |
A Mailbox can raise multiple interrupts. In this implementation, the Mailbox new message interrupt is used determine presence of data from the remote core in the vring.
Typically, we would have 1 interrupt for each remote core. Due to system resource needs, multiple remote cores could use a single interrupt.
Depending on the SoC variant, the isr to registered with interrupt will change. Please refer CDD IPC example application to associate right ISR with interrupt.ISR for New Message