113#include "Std_Types.h"
135#define CDD_IPC_SW_MAJOR_VERSION (11U)
137#define CDD_IPC_SW_MINOR_VERSION (0U)
139#define CDD_IPC_SW_PATCH_VERSION (0U)
149#define CDD_IPC_AR_RELEASE_MAJOR_VERSION (4U)
151#define CDD_IPC_AR_RELEASE_MINOR_VERSION (3U)
153#define CDD_IPC_AR_RELEASE_REVISION_VERSION (1U)
166#define CDD_IPC_MODULE_ID ((uint16) 255U)
168#define CDD_IPC_VENDOR_ID ((uint16) 44U)
170#define CDD_IPC_INSTANCE_ID ((uint8) 0U)
185#define CDD_IPC_SID_GETVERSIONINFO (0x01U)
187#define CDD_IPC_SID_INIT (0x02U)
189#define CDD_IPC_SID_SEND (0x03U)
191#define CDD_IPC_SID_RECEIVE (0x04U)
193#define CDD_IPC_SID_ANNOUNCE (0x05U)
195#define CDD_IPC_SID_INTERNAL_ISR_ID (0x06U)
197#define CDD_IPC_SID_REG_READBACK (0x07U)
199#define CDD_IPC_SID_DEINIT (0x08U)
201#define CDD_IPC_SID_CTRL_RECEIVE (0x09U)
203#define CDD_IPC_SID_IS_INIT_DONE (0x0AU)
205#define CDD_IPC_SID_GET_MAX_MSG_SIZE (0x0BU)
207#define CDD_IPC_SID_MAILBOX_STATE (0x0CU)
219#define CDD_IPC_E_OK (0x00U)
221#define CDD_IPC_E_INIT_FAILED (0x01U)
223#define CDD_IPC_E_UNINIT (0x02U)
225#define CDD_IPC_E_PARAM_POINTER (0x03U)
227#define CDD_IPC_E_ALREADY_INITIALIZED (0x04U)
229#define CDD_IPC_E_INVALID_CONFIG (0x05U)
231#define CDD_IPC_E_SEND (0x06U)
233#define CDD_IPC_E_RECEIVE_RETRY (0x07U)
235#define CDD_IPC_E_NOT_SUPPORTED (0x08U)
237#define CDD_IPC_E_CALLBACK_NULL (0x09U)
243#define CDD_IPC_MAX_MSG_LEN (496U)
247#define CDD_IPC_MAX_CTRL_MSG_LEN (32U)
254#define CDD_IPC_MAX_RETRY_NOTIFY (2U)
276typedef struct Cdd_IpcMpType_s
299typedef struct Cdd_IpcVertIoType_s
320typedef struct Cdd_IpcChannelType_s
349typedef struct Cdd_IpcConfigType_s
407typedef struct Cdd_IpcChannelBufType_s
439#if (STD_ON == CDD_IPC_VERSION_INFO_API)
441 P2VAR(Std_VersionInfoType, AUTOMATIC,
442 CDD_APP_DATA) VersionInfoPtr);
482#if (STD_ON == CDD_IPC_DEINIT_API)
513 VAR(uint32, AUTOMATIC) chId,
514 P2CONST(
void, AUTOMATIC, CDD_APP_DATA) pBuf,
515 VAR(uint32, AUTOMATIC) bufLen);
546 VAR(uint32, AUTOMATIC) chId,
547 P2VAR(
void, AUTOMATIC, CDD_APP_DATA) pBuf,
548 P2VAR(uint32, AUTOMATIC, CDD_APP_DATA) bufLen);
574#if (STD_ON == CDD_IPC_ANNOUNCE_API)
576 P2CONST(UCHAR, AUTOMATIC, CDD_APP_DATA) pBuf,
577 VAR(uint32, AUTOMATIC) chId);
613#if (STD_ON == CDD_IPC_ANNOUNCE_API)
615 P2VAR (uint32, AUTOMATIC, CDD_APP_DATA) pRemoteProcId,
616 P2VAR (uint32, AUTOMATIC, CDD_APP_DATA) pRemoteEndPt,
617 P2VAR (
void, AUTOMATIC, CDD_APP_DATA) pBuf,
618 P2VAR (uint32, AUTOMATIC, CDD_APP_DATA) bufLen);
641#if (STD_ON == CDD_IPC_REGISTER_READBACK_API)
664#if (STD_ON == CDD_IPC_IS_INIT_DONE_API)
686#if (STD_ON == CDD_IPC_GET_MAX_MSG_SIZE_API)
708#if (STD_ON == CDD_IPC_SAFETY_DIAGNOSTIC_API)
This file contains generated pre compile configurations for CDD IPC MCAL driver.
uint32 reserved
Definition Cdd_Ipc.h:307
uint32 maxMsgSize
Definition Cdd_Ipc.h:332
uint32 cddipcclrsts
Definition Cdd_Ipc.h:391
uint32 cddipcenbclr
Definition Cdd_Ipc.h:393
uint32 reserved
Definition Cdd_Ipc.h:397
uint32 cddipcmsgsts
Definition Cdd_Ipc.h:387
uint32 cddipcenbset
Definition Cdd_Ipc.h:395
uint32 reserved
Definition Cdd_Ipc.h:284
uint32 remoteProcId
Definition Cdd_Ipc.h:328
uint32 reserved
Definition Cdd_Ipc.h:336
uint32 cddipcRev
Definition Cdd_Ipc.h:377
void * vertIoRingAddr
Definition Cdd_Ipc.h:301
uint32 numProcs
Definition Cdd_Ipc.h:280
uint32 vertIoObjSize
Definition Cdd_Ipc.h:305
uint32 cddipcirqrawsts
Definition Cdd_Ipc.h:389
uint32 cddipcfifosts
Definition Cdd_Ipc.h:385
uint32 reserved
Definition Cdd_Ipc.h:360
uint32 bufSize
Definition Cdd_Ipc.h:411
uint32 remoteEp
Definition Cdd_Ipc.h:326
uint32 numMsgQueued
Definition Cdd_Ipc.h:330
uint32 cddipceoi
Definition Cdd_Ipc.h:381
uint32 numRegisters
Definition Cdd_Ipc.h:373
uint32 cddipcmsg
Definition Cdd_Ipc.h:383
uint8 * pBuf
Definition Cdd_Ipc.h:409
Cdd_Ipc_NewMessage NewMessageNotify
Definition Cdd_Ipc.h:334
uint32 cddipcsyscfg
Definition Cdd_Ipc.h:379
const Cdd_IpcChannelType * pChCfg
Definition Cdd_Ipc.h:357
Cdd_IpcMpType coreIds
Definition Cdd_Ipc.h:351
uint32 localEp
Definition Cdd_Ipc.h:324
uint32 vertIoRingSize
Definition Cdd_Ipc.h:303
uint32 channelCount
Definition Cdd_Ipc.h:355
uint32 id
Definition Cdd_Ipc.h:322
uint32 ownProcID
Definition Cdd_Ipc.h:278
Cdd_IpcVertIoType vertIoCfg
Definition Cdd_Ipc.h:353
VAR(uint8, ETH_VAR_NO_INIT_128) Eth_Ctrl_0_Egress_BufferMem_0[24576U]
boolean Cdd_IpcIsInitDone(void)
Service for checking if IPC module is initialized.
void(* Cdd_Ipc_NewMessage)(void)
Definition Cdd_Ipc.h:256
Std_ReturnType Cdd_IpcReceiveCtrlMsg(uint32 *pRemoteProcId, uint32 *pRemoteEndPt, void *pBuf, uint32 *bufLen)
Service for reception of N bytes of control message from remote cores.
Std_ReturnType Cdd_IpcReceiveMsg(VAR(uint32,) chId, void *pBuf, uint32 *bufLen)
Service for reception of N bytes of data from remote cores.
void Cdd_IpcGetVersionInfo(Std_VersionInfoType *VersionInfoPtr)
Service for getting CDD version.
uint32 Cdd_IpcGetMailboxStatus(VAR(uint32,) remoteProcId)
Service to get Mailbox state is FULL or not.
void Cdd_IpcInit(void)
Service for CDD Initialization.
Std_ReturnType Cdd_IpcSendMsg(VAR(uint32,) chId, const void *pBuf, VAR(uint32,) bufLen)
Service for sending an message to remote cores.
uint32 Cdd_IpcGetMaxMsgSize(VAR(uint32,) chId)
Service for checking if IPC module is initialized.
Std_ReturnType Cdd_IpcDeinit(void)
Service for deinitializing CDD.
Std_ReturnType Cdd_IpcAnnounce(const UCHAR *pBuf, VAR(uint32,) chId)
Service for broadcasting capabilities of this core to all other cores.
Std_ReturnType Cdd_IpcRegisterReadBack(uint32 remoteProcId, Cdd_IpcRegRbValues *pRegArgs)
Service for reading the configuration registers of the MCAL modules.
#define CDD_IPC_CORE_ID_MAX
IPC maximum possible core ID.
Definition Cdd_IpcCfg.h:344
Channel RP Msg buffer type Used to hold the received buffer, before apps can pick it up.
Definition Cdd_Ipc.h:408
Defines logical communication channel between cores.
Definition Cdd_Ipc.h:321
CDD IPC Configuration type.
Definition Cdd_Ipc.h:350
Defines processor identifiers Core on which MCAL/AUTOSAR is hosted and other cores with which IPC is ...
Definition Cdd_Ipc.h:277
Defines Shared Memories for VRING and VRING OBJECT VRING is the shared memory between cores and VRING...
Definition Cdd_Ipc.h:300