MCUSW
Loading...
Searching...
No Matches
Cdd_IpcCfg.h File Reference

Introduction

This file contains generated pre compile configurations for CDD IPC MCAL driver.

Go to the source code of this file.

Communication Channel ID & Configured Buffer sizes

#define CddIpcConf_IpcComChanId_Cdd_IpcMcu20   (0U)
 
#define CDD_IPC_RPMSG_OBJ_SIZE   (256U)
 
#define CDD_IPC_CH_0_BUFF_SIZE   ((256U * (496U + 32U)) + CDD_IPC_RPMSG_OBJ_SIZE)
 
#define CDD_IPC_MAX_CHANNEL_CFG   (2U)
 
#define IPC_VRING_BUFFER_SIZE   (0x1C00000U)
 VRing Buffer Size required for all core combinations.
 
#define IPC_MPU1_0   (0U)
 Core definitions.
 
#define IPC_MCU1_0   (1U)
 
#define IPC_MCU1_1   (2U)
 
#define IPC_MCU2_0   (3U)
 
#define IPC_MCU2_1   (4U)
 
#define IPC_MCU3_0   (5U)
 
#define IPC_MCU3_1   (6U)
 
#define IPC_C66X_1   (7U)
 
#define IPC_C66X_2   (8U)
 
#define IPC_C7X_1   (9U)
 
#define IPC_MPU1_1   (10U)
 
#define IPC_MAX_PROCS   (11U)
 
#define CDD_IPC_CORE_ID_MAX   (11U)
 IPC maximum possible core ID.
 
#define IPC_MAILBOX_CLUSTER_CNT   (12U)
 
#define CDD_IPC_NEW_MSG_NTFY_FXN   Cdd_IpcNewMessageNotify
 
#define CDD_IPC_NEW_CTRL_MSG_NTFY_FXN   Cdd_IpcNewCtrlMessageNotify
 
const uint32 IPC_Mailbox_BasePhyAddr [IPC_MAILBOX_CLUSTER_CNT]
 
Ipc_ProcInfo g_Ipc_mp_procInfo [IPC_MAX_PROCS]
 Processor IDs to name mapping for all processor in Jacinto7.
 
Ipc_MailboxInfo g_IPC_MailboxInfo [IPC_MAX_PROCS][IPC_MAX_PROCS]
 
const struct Cdd_IpcConfigType_s CddIpcConfiguraions_PC
 
uint8 Cdd_IpcDrvVertIoObj [CDD_IPC_VERTIO_OBJECT_SIZE]
 Communication Channels configured.
 
void Cdd_IpcNewMessageNotify (void)
 New Message notification function.
 
void Cdd_IpcNewCtrlMessageNotify (uint32 remoteProcId)
 New Control Message notification function.
 
void Cdd_Ipc_Isr_Cdd_IpcIrqMbxFromMcu_20 (void)
 A Mailbox can raise multiple interrupts. In this implementation, the Mailbox new message interrupt is used determine presence of data from the remote core in the vring.
 

Macros

#define CDD_IPC_PRE_COMPILE_VARIANT   (STD_ON)
 Pre-Compile Build Variant flag. STD_ON for VariantPreCompile / STD_OFF for VariantPostBuild.
 
#define CDD_IPC_DEV_ERROR_DETECT   (STD_ON)
 Enable/disable CDD Ipc dev detect error.
 
#define CDD_IPC_ISR_TYPE   (CDD_IPC_ISR_CAT1)
 ISR type.
 
Pre-Compile Switches for API Services
#define CDD_IPC_VERSION_INFO_API   (STD_ON)
 Enable/disable version info API.
 
#define CDD_IPC_DEINIT_API   (STD_ON)
 Enable/disable De Initialization API.
 
#define CDD_IPC_ANNOUNCE_API   (STD_ON)
 Enable/disable Service Announcement API.
 
#define CDD_IPC_REGISTER_READBACK_API   (STD_ON)
 Enable/disable Critical Register read back API.
 
#define CDD_IPC_SAFETY_DIAGNOSTIC_API   (STD_ON)
 Enable/disable safety diagnostics API.
 
#define CDD_IPC_IS_INIT_DONE_API   (STD_ON)
 Enable/disable Cdd_IpcIsInitDone API.
 
#define CDD_IPC_GET_MAX_MSG_SIZE_API   (STD_ON)
 Enable/disable Cdd_IpcGetMaxMsgSize API.
 
Dependency configurations
#define CDD_IPC_OS_COUNTER_ID   ((CounterType)OsCounter_0)
 Counter ID for counter used to count wait ticks.
 
Cdd Ipc DEM Error codes to report

Pre-compile switches for enabling/disabling DEM events

#define DemConf_DemEventParameter_CDD_IPC_DEM_NO_EVENT   (0xFFFFU)
 
#define CDD_IPC_DEM_NO_EVENT   DemConf_DemEventParameter_CDD_IPC_DEM_NO_EVENT
 
#define CDD_IPC_E_HARDWARE_ERROR   (DemConf_DemEventParameter_CDD_IPC_E_HARDWARE_ERROR)
 Hardware failed.
 
CORE Names
#define CDD_IPC_CORE_MCU1_0   (1U)
 
#define CDD_IPC_CORE_MCU1_1   (2U)
 
#define CDD_IPC_CORE_MCU2_0   (3U)
 
#define CDD_IPC_CORE_MCU2_1   (4U)
 
#define CDD_IPC_CORE_MCU3_0   (5U)
 
#define CDD_IPC_CORE_MCU3_1   (6U)
 
#define CDD_IPC_CORE_C66X_1   (7U)
 
#define CDD_IPC_CORE_C66X_2   (8U)
 
#define CDD_IPC_CORE_C7X_1   (9U)
 
#define CDD_IPC_CORE_MAX_PROCS   (11U)
 
#define CDD_IPC_OWN_CORE_ID   (CDD_IPC_CORE_MCU1_0)
 Used core identifiers.
 
#define CDD_IPC_REMOTE_CORE_MCU2_0_USED
 
VirtIO Object
#define CDD_IPC_VERTIO_OBJECT_SIZE   (0x1000U)