MCUSW
Wdg User Guide

Introduction

This document details AUTOSAR BSW WDG module implementation

  • Supported AUTOSAR Release : 4.3.1
  • Supported Configuration Variants : Pre-Compile, Link Time and Post-build
  • Vendor ID : WDG_VENDOR_ID (44)
  • Module ID : WDG_MODULE_ID (102)

The WDG module initializes, and configures WDG hardware(RTI) to meet requirements as detailed in AUTOSAR BSW WDG Driver Specification. Following section highlights key aspects of this implementation, which would be of interest to an integrator.


Wdg Driver Architecture/Design

WDG design, which is not included as part of release


Functional Description

WDG employs built in hardware module called "RTI",RTI is a down-counter that count from non-zero value to zero and generates an interrupt to CPU or ESM which in-turn could be programmed to reset the SoC. Please refer WDG Deisgn (Wdg Design Document) for details (specifically section "Watchdog SOC Reset Functionality")

Clock Source to RTI

The clock supplied to these RTI determines the rate of count-down. For each RTI, clock source can be programmable and the frequency of the clock varies on the SoC being used.

Programming of clock source for the RTI is programmed by other software entities (such as SBL, start up code, etc...). The driver expects user of this module to programme required clock source. The example application demonstrates configuring clock sources for the RTI.

Back To Top


RTI Instance

Only one RTI instances in MCU domain is supported by this driver implementation named as MCU_RTIx where x indicates the instance of RTI.

Note: The WRTLOCK bit in mux control register(CTRLMMR_MCU_RTIx_CLKSEL Register) of the associated instance of WDG should be set.

Back To Top


Configuration

The Wdg Driver implementation supports multiple configuration variants (refer section Introduction), the driver expects generated Wdg_Cfg.h to be present at (File Structure). Please refer (Build) to specify path to generated configuration. The associated RTI configuration generated files Wdg_Cfg.c ,Wdg_Lcfg.c Wdg_PBcfg.c to be present as shown in (File Structure)

The generated configuration files should not be modified manually. The config tool Elektrobit Tresos should be used to modify the configuration files.

The following section details on the un-supported features and additional features added.


Variance / Deviation from the specification

Wdg_SetMode API

Wdg_SetMode interface API is not supported. Due to hardware limitations, Mode and Timeout can’t be modified if watchdog is already running i.e only during initialization Mode and Timeout can be set.

Back To Top


WdgOffMode

OFF-Mode is not supported.Due to hardware limitations, If watchdog is already running, it cannot be disabled or shutdown.


WdgServiceInterruptRoutine

This driver does not support routine servicing a watchdog as an interrupt routine driven by a hardware timer.


WdgExternalDriver

This driver is an internal, belongs to the Microcontroller Abstraction Layer whereas external watchdog driver belongs to the Onboard Device Abstraction Layer.So requirements w.r.o external watchdog are not implemented.


Implementation Specific Configurations

This driver implementation introduces below listed configurable options.

Back To Top


WdgDeviceVariant

Name WdgDeviceVariant
Description Used to specific family of devices, the variant of the device being used will belong to one or more family of devices. Please refer (Supported Device Families) to determine the family of device. Based on the family, the number of RTI instances module supported could vary.
Container Name WdgGeneral
Type Enumeration
Range AM62Ax
Value Configuration Class VARIANT-PRE-COMPILE

Back To Top


WdgRtiFrequency

Name WdgRtiFrequency
Description RTI Clock Frequency (Hz) used to calculate preload value during init time.Please refer RTI Integration section in TRM for clock source details.
Container Name WdgGeneral
Type Integer
Range 0 to 12500000
Value Configuration Class VARIANT-PRE-COMPILE

Back To Top


WdgRegisterReadbackApi

Name WdgRegisterReadbackApi
Description Compile switch to enable / disable the Critical Registers Readback API.
Container Name WdgGeneral
Type Boolean
Value Configuration Class VARIANT-PRE-COMPILE

Back To Top


WdgInstanceId

Name WdgInstanceId
Description Selects Watchdog HW instance id.
Container Name WdgSettingsConfig
Type Integer
Value Configuration Class VARIANT-PRE-COMPILE

Back To Top


WdgReaction

Name WdgReaction
Description Watchdog reaction for timer expiration or incorrect service.0x5 = This is the default value. The windowed watchdog will cause a reset if the watchdog is servicedoutside the time window defined by the configuration, or if the watchdog is not serviced at all. 0xA = The windowed watchdog will generate a non-maskable interrupt to the CPU if the watchdog is serviced outside the time window defined by the configuration, or ifthe watchdog is not serviced at all. Writing any other value will cause a system reset if the watchdog is serviced outside the time windowdefined by the configuration, or if the watchdog is not serviced at all.
Container Name WdgSettingsFast/WdgSettingsSlow
Type Enumeration
Range WDG_RESET_RXN : Reaction is reset WDG_INTERRUPT_RXN : Reaction is interrupt generation
Value Configuration Class VARIANT-PRE-COMPILE, VARIANT-LINK-TIME and VARIANT-POST-BUILD

Back To Top


WdgWindowSize

Name WdgWindowSize
Description Digital Windowed Watchdog Window Size. Selecting 100% enables standard watchdog (not windowed). WWDSIZE: 0x00000050 = 50%, WWDSIZE: 0x00000500 = 25%, WWDSIZE: 0x00005000 = 12.5%, WWDSIZE: 0x00050000 = 6.25%, WWDSIZE: 0x00500000 = 3.125%, WWDSIZE: Any other value = 3.125%
Container Name WdgSettingsFast/WdgSettingsSlow
Type Enumeration
Range WDG_WINDOW_100_PERCENT : 100% window WDG_WINDOW_50_PERCENT : 50% window WDG_WINDOW_25_PERCENT : 25% window WDG_WINDOW_12P5_PERCENT : 12.5% window WDG_WINDOW_6P25_PERCENT : 6.25% window WDG_WINDOW_3P125_PERCENT : 3.125% window
Value Configuration Class VARIANT-PRE-COMPILE, VARIANT-LINK-TIME and VARIANT-POST-BUILD

Back To Top


WdgTimeoutValue

Name WdgTimeoutValue
Description Watchdog timeout period in milli seconds. Watchdog generates a non-maskable interrupt or reset to the CPU if the watchdog is serviced after this timeout period.
Container Name WdgSettingsFast/WdgSettingsSlow
Type Integer
Range 0 to 65535
Value Configuration Class VARIANT-PRE-COMPILE, VARIANT-LINK-TIME and VARIANT-POST-BUILD

Back To Top


Non Standard Service APIs


Wdg_trigger

The Wdg Manager (or other entities) shall control the watchdog driver via a so called trigger condition. As long as the trigger condition is valid the Wdg Driver services the watchdog hardware, if the trigger condition becomes invalid the Wdg Driver stops triggering and the watchdog expires. API used to trigger wdg is Wdg_trigger and should be called by application periodically. If interrupt is used to call the trigger API, then the interrupt shall be a high priority periodic interrupt routine in the application. Also the trigger condition shall be set to minimum effective value depending on the application needs.

Service Name Wdg_Trigger
Syntax void Wdg_Trigger (void)
Service ID[hex] 0x05
Sync/Async Synchronous
Reentrancy Non Reentrant
Parameters (inout) None
Parameters (out) None
Return Value None
Description This function triggers the servicing of the watchdog.

Back To Top


Wdg_RegisterReadback

To protect HW from unintended reconfiguration (corruption / fault hardware), some of the critical registers are read and to be checked periodically. The values of these registers are not expected to change during normal operation. This is an optional service API, which can be turned OFF. (refer section WdgRegisterReadbackApi)

Service Name Wdg_RegisterReadback
Syntax void Wdg_RegisterReadback (Wdg_RegisterReadbackType * regRbPtr)
Service ID[hex] 0x06
Sync/Async Synchronous
Reentrancy Reentrant (but not for the same RTI channel)
Parameters (inout) regRbPtr : Pointer of type Wdg_RegisterReadbackType
Parameters (out) None
Return Value E_OK: Register read back has been done E_NOT_OK: Register read back failed (if driver is not initialized or RegRbPtr is NULL_PTR
Description Reads the important registers of the hardware unit and returns the value in the structure.

Back To Top


Power-up

The driver doesn't configure the functional clock and power for the RTI modules. It's expected that SBL power-up the required modules. Please refer SBL documentation.

Back To Top


Build and Running the Example Application

Please follow steps detailed in section (Build) to build library or example

Back To Top


Steps to run example application

Please refer (Running Examples)

Back To Top


Memory Mapping

Various objects of this implementation (e.g. variables, functions, constants) are defined under different sections. The linker command file at (Examples Linker File (Select memory location to hold example binary)) defines separate section for these objects. When the driver is integrated, its expected that these sections are created and placed in appropriate memory locations. (Locations of these objects depend on the system design and performance needs)

Section WDG_CODE WDG_VAR WDG_VAR_NOINIT WDG_VAR_CLEARED WDG_CONST WDG_CONFIG_DATA
WDG_DATA_INIT_UNSPECIFIED_SECTION USED USED
WDG_TEXT_SECTION USED
WDG_DATA_NO_INIT_UNSPECIFIED_SECTION USED
WDG_CONST_32_SECTION USED
WDG_ISR_TEXT_SECTION USED
WDG_CONFIG_SECTION USED

Back To Top


Cache

This driver implementation has been validated with cache enabled. For optimal performance it’s recommended to place (Memory Mapping) sections in cache enabled memory area.

Back To Top


Dependencies on SW Modules


ESM

RTI/WDG hardware cannot reset the SoC when WDG expires, instead a pin of the SoC can be asserted. It's expected that an external entity (such as PMIC) will monitor this pin and reset the SoC when pin is driven low. The ESM reports errors in two ways.

  • An interrupt to a processor in the device. This allows the device to analyze and try to recover from an error.
  • An external ERROR pin. This allows the system outside of the SoC to monitor for potentially fatal errors(errors that the device cannot self-recover from). the external I/O(MCU_SAFETY_ERRORn pin) will remain asserted (active low) for a minimum period of time. After that period of time, if the error has been cleared by an internal processor, the pin will go inactive (high). If it does not go inactive in that time, then an external agent should intervene, as there may be an unrecoverable error.

Please refer chapter Error Signalling Module(ESM) in TRM, item 2 of (Refer to Design Document provided in CSP) for more details.

Back To Top


DET

This implementation depends on the DET in order to report development errors and can be turned OFF. Refer section (Development Error Reporting) for detailed error codes.

Back To Top


DEM

This implementation depends on the DEM in order to report extended production errors. Refer section (Production Code Error Reporting) for detailed error codes.

Back To Top


File Structure

wdg_design_dir_detailed.png
Detailed Directory Structure
  1. Driver implemented by : Wdg.h, Wdg.c, Wdg_Priv.c and Wdg_Priv.h
  2. Example Configuration by : Wdg_Cfg.h, Wdg_Cfg.c, Wdg_Lcfg.c and Wdg_PBcfg.c
  3. Example Application by : WdgApp.c and WdgApp.h

Back To Top


Error Handling


Development Error Reporting

Development errors are reported to the DET using the service Det_ReportError(), when enabled. The driver interface (Wdg.h File Structure) lists the Error Id.

Back To Top


Error codes

Type of Error Related Error code Value (Hex)
Invalid driver state WDG_E_DRIVER_STATE 0x10
Invalid mode param WDG_E_PARAM_MODE 0x11
Invalid config param WDG_E_PARAM_CONFIG 0x12
Invalid timeout value WDG_E_PARAM_TIMEOUT 0x13
Invalid NULL ptr param WDG_E_PARAM_POINTER 0x14
Invalid configuration set selection WDG_E_INIT_FAILED 0x15

Back To Top


Production Code Error Reporting

Production error are reported to DEM via the service Dem_SetEventStatus().


DEM Error codes

Error Name Description
WDG_E_MODE_FAILED Setting watchdog mode failed
WDG_E_DISABLE_REJECTED Disabling watchdog mode failed

Back To Top


Safety Diagnostic Features

CLK5C - External Watchdog

This is for use of an external watchdog. Software necessary is defined by the External Watchdog selected by the System Integrator. This is provided by PMIC in TI solution. PMIC Watchdog driver supports this and has APIs that covers all watchdog features.

PMIC Watchdog driver can be found in this path "/PDK install PATH/pdk/packages/ti/drv/pmic"

PMIC watchdog referance example can be found in "/PDK install PATH/pdk/packages/ti/drv/pmic/test/wdg_test"

Software Readback of Static Configuration Registers

Periodic readback of configuration registers can provide a diagnostic for inadvertent writes to these registers. The WDG MCAL driver provides the API - Wdg_RegisterReadback to readback static and written configuration registers to implement this diagnostic feature.

Back To Top


API Description

Refer API Documentation for details

Back To Top


Example Application

The example application demonstrates use of the Wdg module. The configuration file is present at (File Structure)

  • Supports Link time,Post Build and Pre Compile Configuration Variants
  • Following default configuration is provided
    • RTI Instance selected is RTI0
    • RTI clock source is selected as 12.5 MHz.
    • RTI window size is set to 100%.
    • RTI reaction after expiry is set to interrupt mode.
    • RTI timeout value is set for 2sec.
    • RTI Mode selected is WDGIF_SLOW_MODE.
    • RTI will be serviced 5 times(approx 10 secs) and then it will expire in 2sec and generates an ESM interrupt.

The list below identifies key steps performed in the example.

  • Initializes “Example Run Result Status Flag”
  • WdgApp_Startup()
    • Initializes ESM
    • Registers ISR for enabled Wdg instance
    • Initializes memory section to check stack/memory corruption
  • WdgApp_PowerAndClkSrc()
    • Set up the clock sources for the enabled Wdg Instance
  • WdgApp_WdgTest()
    • Get version info.
    • On Expiry of WDG timeout, wait for user input, To generate an interrupt (via ESM) or To drive MCU_SAFETY_ERROR Pin low (via ESM) .
    • Initialize Wdg.
    • Set trigger condition i.e permission to service the Wdg for the next n milliseconds.
    • Service Wdg for n milliseconds.
    • Wait for ESM interrupt that is generated after Wdg expiry.
    • If user input selected is "To drive MCU_SAFETY_ERROR Pin low", pin muxing of MCU_SAFETY_ERRORn is done.
    • User needs to give input 1 after probing test point at 2 stages one is before Wdg expires and another after Wdg expires.
  • Checks for error status, stack corruption and prints result

Back To Top


Example Log

  • User Input : To generate an interrupt (via ESM)
        [MCU_R5FSS0_0] Starting WDG test  !!!
     
        WDG MCAL Version Info
        ---------------------
        Vendor ID           : 44
        Module ID           : 102
        SW Major Version    : 9
        SW Minor Version    : 0
        SW Patch Version    : 0
     
        On Expiry of WDG timeout Please enter :
        0 To generate an interrupt (via ESM) 
        1 To drive MCU_SAFETY_ERROR Pin low (via ESM) 
        0
        Variant - Pre Compile being used !!!
        WDG timeout is configured for 2000 millisecs
        Number of times WDG will be serviced : 5
        WDG ESM Interrupt will be generated after 2000 * 5 i.e 10000 millisecs
        WDG Elapsed and generated an event to ESM
        ESM has generated an Interrupt
        WDG App Completed as expected!!!
        Please refer user guide on usage details
        WDG Stack Usage : 2860 bytes
        WDG Test Passed!!!
    
        [MCU_R5FSS0_0] Starting WDG test  !!!
     
        WDG MCAL Version Info
        ---------------------
        Vendor ID           : 44
        Module ID           : 102
        SW Major Version    : 9
        SW Minor Version    : 0
        SW Patch Version    : 0
     
        On Expiry of WDG timeout Please enter :
        0 To generate an interrupt (via ESM) 
        1 To drive MCU_SAFETY_ERROR Pin low (via ESM) 
        1
        Test Point J9 26, 2(GND) On AM62X EVM Test (SOM Board),  and it should be Active HIGH before WDG expires
        Please enter 1 after probing on test point 
        1
        Variant - Pre Compile being used !!!
        WDG timeout is configured for 2000 millisecs
        Number of times WDG will be serviced : 5
        WDG ESM Interrupt will be generated after 2000 * 5 i.e 10000 millisecs
        WDG Elapsed and generated an event to ESM
        ESM has generated an Interrupt
         On AM62XEVM Test Point pin No 26 and 2 (GND) on J9 Tag (SOM Board) and it should be Active LOW after ESM interrupt generated
        Please enter 1 after probing for ESM Error on test point 
        1
        WDG App Completed as expected!!!
        Please refer user guide on usage details
        WDG Stack Usage : 2860 bytes
        WDG Test Passed!!!

Back To Top


References

Back To Top


Document Revision History

Revision Date Author Description Status
0.1 22 Nov 2022 Raja K First version Approved
0.2 15 Mar 2023 Raja K Updated Example Log Approved
0.3 21 July 2023 Saritha P Updated Example Log Approved
0.4 11 Sep 2023 Saritha P Updated Example Log Approved