MCUSW
Dio User Guide

Introduction

This document details AUTOSAR BSW DIO module implementation

  • Supported AUTOSAR Release : 4.3.1
  • Supported Configuration Variants : Pre-Compile & Link Time
  • Vendor ID : DIO_VENDOR_ID (44)
  • Module ID : DIO_MODULE_ID (120)

The DIO module provides interfaces to external peripherals by abstracting the input and output pins on the microcontroller device as detailed in the AUTOSAR BSW DIO Driver Specification. Following sections highlight key aspects of this implementation which would be of interest to an integrator.


Dio Driver Architecture/Design

DIO design, which is not included as part of release


Functional Description

Pin Mapping

The DIO driver provides an interface to external peripherals by abstracting the input and output pins on the microcontroller device. The DIO pins are general purpose in nature. AM62Ax have one Wakeup DIO driver instances.

32 Pins are grouped into a port and channelId corresponds to sequential number starting with 0 for wakeup domain 0 and pin 0.

AM62Ax can support up to 1 instances. These instances are generally associated with specific domain, e.g. wakeup domain. The following diagram is from the device specific TRM.

dio_design_dio_typical_app.png
DIO Typical Application:DRA80x

Pin Mapping AM62Ax

In case of AM62Ax, each Dio instance supports 9 banks of 16 DIO signals/pins or channels (1 in MCU). Please note in each instance there are some pins that are not pinned out and are reserved.
The mapping of pins in the different instances is shown in the following table. For this implementation the absolute numbering of channel ids starts from the Dio instance in the wakeup domain. Please refer TRM for more details.

Instance Pin Number ChannelId Port ID Available/Not Available
MCU_GPIO 0 0 22 0 Available

Back To Top


Configuration

The Dio Driver implementation supports multiple configuration variants (refer section Introduction), the driver expects generated Dio_Cfg.h to be present as (File Structure). Please refer (Build) to specify path to generated configuration. The associated dio driver configuration generated files Dio_Cfg.c and Dio_Lcfg.c to be present as show (File Structure)

The following section details on the un-supported features and additional features added.


Variance from the specification

Direct Read Back

As the microcontroller currently doesn't support direct read back, the AUTOSAR requirement pertaining to direct read back has not been implemented.

Back To Top


Dio_ConfigType

This structure contains all post-build configurable parameters of the DIO driver. As post-build configuration is not supported, this structure has not been used in this implementation.


Implementation Specific Configurations

This driver implementation introduces configurable options listed below

Back To Top


DioDeviceVariant

Name DioDeviceVariant
Description Used to specific family of devices, the variant of the device being used will belong one or more family of devices. Please refer (Supported Device Families) to determine the family of device. Based on the family, the number of instances of Dio module supported could vary.
Container Name DioGeneral
Type Enumeration
Range AM62Ax, etc… (new family of devices could be added in future)
Value Configuration Class VARIANT-PRE-COMPILE

Back To Top


DIO_WRITE_PORT_EVENT_ID

Name DIO_WRITE_PORT_EVENT_ID
Description This is the event ID for Dem event in the Dio_WritePort() API
Container Name DioDemEventParameterRef
Type IDENTIFIABLE
Value Configuration Class VARIANT-PRE-COMPILE

Back To Top


DIO_WRITE_CHANNEL_EVENT_ID

Name DIO_WRITE_CHANNEL_EVENT_ID
Description This is the event ID for Dem event in the Dio_WriteChannel() API.
Container Name DioDemEventParameterRef
Type IDENTIFIABLE
Value Configuration Class VARIANT-PRE-COMPILE

Back To Top


DioRegisterReadbackApi

Name DioRegisterReadbackApi
Description

Adds / Removes service API DioRegisterReadbackApi ()

Safety feature : Check some of the critical registers (corruption of which
could potentially break functionality of the Dio)

The expected usage: Periodically this service API is invoked and
checked for data-consistency. i.e. the values of the registers checked
in this API are not expected to change.

Also refer (Dio_RegisterReadback)

Container Name DioGeneral
Type Boolean
Value Configuration Class VARIANT-PRE-COMPILE

Back To Top


Non Standard Service APIs


Dio_RegisterReadback

To protect HW from un-intended re-configuration (corrupted / fault hardware), some of the critical registers are read periodically and checked. By an entity outside the driver, the values of these registers are not expected to change. This is an optional service API, which can be turned OFF (refer section DioRegisterReadbackApi)

Description Comments
Service Name Dio_RegisterReadback Can potentially be turned OFF (design_dio_desc_cfg_ti)
Syntax uint32 Dio_RegisterReadback (DIO_ChannelType ChannelId) Returns PID register of associated DIO module
Service ID NA
Sync / Async Sync
Reentrancy Non Reentrant
Parameter in ChannelId Channel Identifier
Parameters out None
Return Value Standard unsigned integer An integer value

Back To Top


Interrupt Configuration

The Driver doesn’t register any interrupts handler (ISR), it is expected that consumer of this driver registers the required interrupt handler.

Back To Top


Power-up

The driver doesn't configure the functional clock and power for the Dio modules. Its expected that SBL powers-up the required modules. Please refer SBL documentation.

Back To Top


Build and Running the Application

Please follow steps detailed in section (Build) to build library or example.

Back To Top


Steps to run example application

Please follow the steps detailed in section (Running Examples) to build and run example. Back To Top


Memory Mapping

Various objects of this implementation (e.g. variables, functions, constants) are defined under different sections. The linker command file at (Examples Linker File (Select memory location to hold example binary)) defines separate section for these objects. When the driver is integrated, its expected that these sections are created and placed in appropriate memory locations. (Locations of these objects depend on the system design and performance needs)

Section DIO_CODE DIO_CONST DIO_CONFIG
DIO_VAR_CONST_UNSPECIFIED_SECTION (.data) USED
DIO_VAR_CONST_32_SECTION (.data) USED
DIO_FUNC_TEXT_SECTION USED
DIO_CONFIG_DATA_SECTION_NON_CONST USED
DIO_CONFIG_DATA_SECTION_CONST USED

Back To Top


Cache

This driver implementation has been validated with cache enabled. For optimal performance it is recommended to place (Memory Mapping) sections in cache enabled memory area.

Back To Top


Dependencies on SW Modules


DET

This implementation depends on the DET in order to report development errors and can be turned OFF. Refer section (Development Error Reporting) for detailed error codes.

Back To Top


SchM

This implementation requires 1 level of exclusive access to guard critical sections. Invokes SchM_Enter_Dio_DIO_EXCLUSIVE_AREA_0 (), SchM_Exit_Dio_DIO_EXCLUSIVE_AREA_0 () to enter critical section and exit.

In the example implementation (File Structure SchM_Dio.c) , all the interrupts on CPU are disabled.

Back To Top


File Structure

dio_design_dir_structure.png
Detailed Directory Structure
  1. Driver implemented by : Dio.h , Dio.c, Dio_Priv.h
  2. Example Configuration by : Dio_Cfg.h , Dio_Cfg.c and Dio_Lcfg.c
  3. Example Application by : DioApp.c

Back To Top


Error Handling


Development Error Reporting

Development errors are reported to the DET using the service Det_ReportError(), when enabled. The driver interface (Dio.h File Structure) lists the SID

Back To Top


Error codes

Type of Error Related Error code Value (Hex)
Invalid channel name requested DIO_E_PARAM_INVALID_CHANNEL_ID 0x0A
Parameter is NULL Pointer DIO_E_PARAM_CONFIG 0x10
Invalid Port Nam3 DIO_E_PARAM_INVALID_PORT_ID 0x14
API parameter checking: invalid channel DIO_E_PARAM_INVALID_GROUP 0x1F
NULL Pointer DIO_E_PARAM_POINTER 0x20

Back To Top


Production Code Error Reporting

Production error are reported to DEM via the service DEM_ReportErrorStatus(). In addition to standard errors, this implementation reports "DIO_WRITE_CHANNEL_EVENT_ID" and "DIO_WRITE_PORT_EVENT_ID" for DEM events in channel and port writes.

Back To Top


API Description

The AUTOSAR BSW Dio Driver specification details the APIs required for Dio Driver. Please refer to (design_dio_low_level) for detailed API description. Also refer to (Non Standard Service APIs) for non-standard APIs which are included in this implemented.

Refer API Documentation for details Back To Top


Example Application

The example application demonstrates use of Dio module, the list below identifies key steps performed the example. The configuration file is present at (File Structure)

  • Initializes “Result Status Flag”
  • DioApp_Startup ()
    • Initial Setup of Control Module registers : Unlocking the pad configuration registers
      • In the upper and lower 32-bits for the required partitions, the write lock key must be written with the designated key value before write-protected partition registers can be modified.
      • A check is performed to ensure that the partitions are unlocked.
    • Configuration of Control Module registers : Pin multiplexing
      • As multiple pins are multiplexed, it is necessary to select the desired pin by configuring the pad config registers
      • In the specific pad configuration registers following bits need to be updated:
        • MUXMODE : This selects the correct signal for MUX selection (DIO pin)
        • PULLUDEN : This is an active low signal to enable pullup/pulldown in pad mode (Disable by selecting 1U)
        • RXACTIVE : This is to enable the receiver (Enable by selecting 1U)
        • DS_PULLUD_EN : This is an active low signal to enable pullup/pulldown in deep sleep mode(Disable by selecting 1U)
        • By writing 0x00040007U to the specific pad config registers in the control module the above registers can be updated as mentioned.
      • Further details can be found under Device Configuration > Control Module in TRM.
    • Initialize the DIO module instance and ports to be used by the example application
      • Select the required instance of DIO module
      • The following bank registers for an instance to be initialized as follows:
        • Direction Register : direction of DIO pin for LED is set as output(can be set as input(1U) or output(0U) depending on use case)
        • Set Output Drive State Register : initial value of output pin is updated with this register.
        • Clear Output Drive State Register : initial clearing value of output pin is updated with this register.
      • DIO relies on other entities to perform the above initialization steps.
  • DioApp_mainTest ()
    • Perform channel read/write confirm by checking the LED 18 ON EVM rev E2/3
    • Perform channel group read/write on initialized channel group
    • Perform port read/write on initialized ports
    • Perform flip channel on initialized channel
  • Checks for error status, stack corruption and prints result

Back To Top


Example Log

### AM62Ax {#ug_dio_eg_log_Am62Ax}

    [MCU_R5FSS0_0] 

    Sample Application - STARTS !!!
 
    DIO MCAL Version Info
    ---------------------
    Vendor ID           : 44
    Module ID           : 120
    SW Major Version    : 9
    SW Minor Version    : 0
    SW Patch Version    : 0
 
    Test A. Write and Read Channel
    ------------------------------
    Channels written
    Channel read DIO_PinLevel[0] = 0 
    Channel read DIO_PinLevel[1] = 1 
    Channel read DIO_PinLevel[2] = 0
    DIO Service API Read-back Channel Succeeds !!!
    DIO Service API Read-back Channel Succeeds for Main_GPIO_0 !!!
    DIO Service API Read-back Channel Succeeds for Main_GPIO_1 !!!

    DIO Test A :Service API: Write/Read Channel completed

    Test B. Write and Read Channel Group
    ---------------------
    DIO Service Read/Write Channel Group Read-back Succeeds !!!

    DIO Test B : Service API : Write/Read Channel Group completed

    Test C. Write and Read Port
    ---------------------
    DIO Service API Read-Back Port succeeds !!!

    DIO Test C : Service API: Write/Read Port completed

    Test D. Flip Channel 
    ----------------------
    Pin Value Before Flip: 0 
    Pin Value After Flip: 1 

    DIO Test D : Service API: Flip Channel completed
    DIO Stack Usage: 2836 bytes

    ----------------------------------

    DioApp: Sample Application - Completes successfully !!!

References

Back To Top


Document Revision History

Revision Date Author Description Status
0.1 22 Nov 2022 Dinesh Kumar C E First version Approved
0.2 15 Mar 2023 Vyankatesh D Updated Example log Approved
0.3 21 July 2023 Vyankatesh D Updated Example log Approved
0.4 11 Sep 2023 Pranathi Vadakattu Updated Example log Approved