6.12. GPT

6.12.1. Modules

Name

GPT Driver Interrupt Handlers

6.12.2. Types

Base type

Type Name

Brief

enum

Gpt_ModeType

List of process modes.

enum

Gpt_PredefTimerType

Type for GPT Predefined(free running) Timers.

enum

Gpt_ChannelMode

GPT channel mode macros.

enum

Gpt_PrescaleValueType

List of Prescale values for General purpose timer channels The timer counter is prescaled with the value 2^(PTV+1). Example: PTV = 3, counter increases value (if started) after 16 functional clock periods Note: Not applicable to GPT Predef timers.

enum

Gpt_ChannelStateType

GPT channel state GPT will be in one of this state during its lifetime.

typedef uint32

Gpt_ChannelType

Type describing the Gpt channel.

typedef uint32

Gpt_ValueType

Type describing the timeout value.

typedef uint32

Gpt_CntId

Type describing the counter block to use for GPT.

typedef void(*)(void)

Gpt_NotifyType

Notification callback function pointer.

typedef uint32

Gpt_ClockSourceType

Type for specifying source clock selection.

6.12.2.1. enum Gpt_ModeType

Enumerator

Value

Description

GPT_MODE_UNITIALIZED

0U

GPT initialized.

GPT_MODE_NORMAL

Normal operation mode of the GPT.

GPT_MODE_SLEEP

Operation for reduced power operation mode. In sleep mode only wakeup capable channels are available.

Brief: List of process modes.

6.12.2.2. enum Gpt_PredefTimerType

Enumerator

Value

Description

GPT_PREDEF_UNDEFINED

0U

GPT Predef Timer is undefined.

GPT_PREDEF_TIMER_1US_16BIT

1U

GPT Predef Timer with tick duration 1us and range 16bit.

GPT_PREDEF_TIMER_1US_24BIT

2U

GPT Predef Timer with tick duration 1us and range 24bit.

GPT_PREDEF_TIMER_1US_32BIT

3U

GPT Predef Timer with tick duration 1us and range 32bit.

GPT_PREDEF_TIMER_100US_32BIT

4U

GPT Predef Timer with tick duration 100us and range 32bit.

Brief: Type for GPT Predefined(free running) Timers.

6.12.2.3. enum Gpt_ChannelMode

Enumerator

Value

Description

GPT_CH_MODE_CONTINUOUS

0U

After reaching the target time, the timer continues running with the value “zero” again.

GPT_CH_MODE_ONESHOT

After reaching the target time, the timer stops automatically (timer expired).

GPT_CH_MODE_CONT_WAKEUP

GPT_CH_MODE_ONESHOT_WAKEUP

Brief: GPT channel mode macros.

6.12.2.4. enum Gpt_PrescaleValueType

Enumerator

Value

Description

GPT_PRESCALE_UNDEFINED

Brief: List of Prescale values for General purpose timer channels The timer counter is prescaled with the value 2^(PTV+1). Example: PTV = 3, counter increases value (if started) after 16 functional clock periods Note: Not applicable to GPT Predef timers.

6.12.2.5. enum Gpt_ChannelStateType

Enumerator

Value

Description

GPT_UNINITIALIZED

0U

GPT is uninitialized.

GPT_INITIALIZED

GPT is initialized.

GPT_RUNNING

GPT is running.

GPT_STOPPED

GPT is stopped.

GPT_EXPIRED

GPT is expired.

Brief: GPT channel state GPT will be in one of this state during its lifetime.

6.12.2.6. typedef Gpt_ChannelType

typedef uint32 Gpt_ChannelType;

Brief: Type describing the Gpt channel.

6.12.2.7. typedef Gpt_ValueType

typedef uint32 Gpt_ValueType;

Brief: Type describing the timeout value.

6.12.2.8. typedef Gpt_CntId

typedef uint32 Gpt_CntId;

Brief: Type describing the counter block to use for GPT.

6.12.2.9. typedef Gpt_NotifyType

typedef void(* Gpt_NotifyType) (void);

Brief: Notification callback function pointer.

6.12.2.10. typedef Gpt_ClockSourceType

typedef uint32 Gpt_ClockSourceType;

Brief: Type for specifying source clock selection.

6.12.3. Structures

Name

Brief

GptConfigReg

GPT register readback structure.

Gpt_ChannelConfigType

Configuration per channel.

Gpt_ConfigType

global configuration of the driver

Gpt_DriverObjType

Driver object.

6.12.4. Defines

Name

Brief

GPT_SW_MAJOR_VERSION

Driver Implementation Major Version.

GPT_SW_MINOR_VERSION

Driver Implementation Minor Version.

GPT_SW_PATCH_VERSION

Driver Implementation Patch Version.

GPT_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by GPT Driver.

GPT_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by GPT Driver.

GPT_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by GPT Driver.

GPT_VENDOR_ID

Texas Instruments Vendor ID.

GPT_MODULE_ID

GPT Driver Module ID.

GPT_INSTANCE_ID

GPT Driver Instance ID.

GPT_CH_ISR_MODE_CONTINUOUS

GPT continuous mode index.

GPT_CH_ISR_MODE_ONESHOT

GPT oneshot mode index.

GPT_CH_ISR_MODE_CONT_WAKEUP

GPT continuous wakeup mode index.

GPT_CH_ISR_MODE_ONESHOT_WAKEUP

GPT oneshot wakeup mode index.

GPT_E_UNINIT

API service used without module initialization.

GPT_E_BUSY

API service called during ongoing process (Timer is already running)

GPT_E_MODE

API service called when driver is in wrong mode.

GPT_E_ALREADY_INITIALIZED

API Gpt_Init is called but the module is already initialized.

GPT_E_INIT_FAILED

API Gpt_Init is called but the module is already initialized.

GPT_E_PARAM_CHANNEL

API called with invalid channel.

GPT_E_PARAM_VALUE

API servcie called with invalid start timer parameter.

GPT_E_PARAM_POINTER

API servcie called with invalid(Null_Ptr) data buffer pointer.

GPT_E_PARAM_PREDEF_TIMER

API service called with invalid Predef Timer.

GPT_E_PARAM_MODE

Gpt_SetMode is called with wrong mode parameter.

GPT_E_INVALID_ISR

Invalid entry to ISR.

GPT_SID_GET_VERSION_INFO

Gpt_GetVersionInfo() API Service ID.

GPT_SID_INIT

Gpt_Init() API Service ID.

GPT_SID_DEINIT

Gpt_DeInit() API Service ID.

GPT_SID_GET_TIME_ELAPSED

Gpt_GetTimeElapsed() API Service ID.

GPT_SID_GET_TIME_REMAINING

Gpt_GetTimeRemaining() API Service ID.

GPT_SID_START_TIMER

Gpt_StartTimer() API Service ID.

GPT_SID_STOP_TIMER

Gpt_StopTimer() API Service ID.

GPT_SID_ENABLE_NOTIFY

Gpt_EnableNotification() API Service ID.

GPT_SID_DISABLE_NOTIFY

Gpt_DisableNotification() API Service ID.

GPT_SID_SET_MODE

Gpt_SetMode() API Service ID.

GPT_SID_DISABLE_WAKEUP

Gpt_DisableWakeup() API Service ID.

GPT_SID_ENABLE_WAKEUP

Gpt_EnableWakeup() API Service ID.

GPT_SID_CHECK_WAKEUP

Gpt_CheckWakeup() API Service ID.

GPT_SID_GET_PREDEFTIMERVALUE

Gpt_GetPredefTimerValue() API Service ID.

GPT_SID_GET_GETHWUNITOBJ

GPT Get Hw Unit Obj API Service ID.

GPT_SID_GET_CONFIG_REG_READBACK

GPT Gpt_ConfigRegReadBack API Service ID.

GPT_DRIVER_UNINITIALIZED

Driver status UN INITIALIZED.

GPT_DRIVER_INITIALIZED

Driver status INITIALIZED.

CH_COMP_MASK

Masks the higher order bits to evaluate compare block (lsb0 and lsb1)

MAX_RESOLUTION

Maximum resolution for the timer.

SET (type, var, bit)

Set a bit.

CLEAR (type, var, bit)

Clear a bit.

6.12.5. Functions

Return type

Function Name

Brief

void

Gpt_GetVersionInfo(Std_VersionInfoType * VersionInfoPtr)

This service returns the version information of this module.

void

Gpt_Init(const Gpt_ConfigType * configPtr)

This service Initializes the GPT driver.

void

Gpt_DeInit(void )

This service deinitializes the GPT driver.

Gpt_ValueType

Gpt_GetTimeRemaining(Gpt_ChannelType channel)

This service returns the time remaining until the target time is reached.

void

Gpt_StartTimer(Gpt_ChannelType channel, Gpt_ValueType value)

This service starts a timer channel.

void

Gpt_StopTimer(Gpt_ChannelType channel)

This service stops a timer channel.

void

Gpt_EnableNotification(Gpt_ChannelType channel)

This service enables the interrupt notification for a channel (relevant in normal mode).

void

Gpt_DisableNotification(Gpt_ChannelType channel)

This service disables the interrupt notification for a channel (relevant in normal mode).

Std_ReturnType

Gpt_ConfigRegReadBack(Gpt_ChannelType channel, GptConfigReg * GptConfigReg_pt)

This function reads the important registers of the hardware unit and returns the value in the structure.

void

Gpt_CheckWakeup(EcuM_WakeupSourceType WakeupSource)

This function checks if a wakeup capable GPT channel is the source for a wakeup event and calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid GPT channel wakeup event.

void

Gpt_DisableWakeup(Gpt_ChannelType Channel)

This service disables the wakeup interrupt of a channel (relevant in sleep mode)

void

Gpt_EnableWakeup(Gpt_ChannelType Channel)

This Function enables the wakeup interrupt of a channel (relevant in sleep mode)

Std_ReturnType

Gpt_GetPredefTimerValue(Gpt_PredefTimerType PredefTimer, uint32 * TimeValuePtr)

This Function delivers the current value of the desired GPT Predef Timer.

void

Gpt_SetMode(Gpt_ModeType Mode)

This Function sets the operation mode of the GPT.

6.12.5.1. function Gpt_GetVersionInfo

void Gpt_GetVersionInfo(
    Std_VersionInfoType * VersionInfoPtr
)

Brief: This service returns the version information of this module.

Returns the version information of this module

Service ID[hex] - 0x00

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • VersionInfoPtr - Pointer to where to store the version information of this module

Returns:

  • None

Return: None

6.12.5.2. function Gpt_Init

void Gpt_Init(
    const Gpt_ConfigType * configPtr
)

Brief: This service Initializes the GPT driver.

This service initializes all the configured Gpt channels. This will set the state of the each channel to”initialized”, also set the Gpt driver state to “Normal”.

Service ID[hex] - 0x01

Sync/Async - Synchronous

Reentrancy - Non Reentrant

Parameters:

  • ConfigPtr - configuration structure for initializing the module.

Returns:

  • None

Return: None

6.12.5.3. function Gpt_DeInit

void Gpt_DeInit(
    void 
)

Brief: This service deinitializes the GPT driver.

This service deinitializes the RTI used by Gpt driver to the power on reset state. The Gpt driver state is changed to “Uninitialized” state”. All the channel registers are cleared to stop the timer channels. API will disable all interrupt notifications, wakeup interrupts.

Service ID[hex] - 0x02

Sync/Async - Synchronous

Reentrancy - Non Reentrant

Returns:

  • None

Return: None

6.12.5.4. function Gpt_GetTimeRemaining

Gpt_ValueType Gpt_GetTimeRemaining(
    Gpt_ChannelType channel
)

Brief: This service returns the time remaining until the target time is reached.

Gpt_GetTimeRemaining will return the timer value remaining until the target time will be reached next time. The remaining time is target time minus time already elapsed. In one shot mode, if the timer is in stopped state, the function will return remaining time value at the moment of stopping. If the timer is expired, the function will return 0.

Service ID[hex] - 0x04

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • Channel - ChannelId of the Gpt channel.

Returns:

  • Remaining timer value (in number of ticks)

Return: Gpt_ValueType

6.12.5.5. function Gpt_StartTimer

void Gpt_StartTimer(
    Gpt_ChannelType channel,
    Gpt_ValueType value
)

Brief: This service starts a timer channel.

Gpt_StartTimer will start the selected timer channel with defined target time. If the timer channel is enabled for interrupt notification, then interrupt notification will be triggered after expiration of the selected timer channel. In one shot mode, if the timer is expired then the channel will be stopped in interrupt subroutine. The selected channel will be moved to “Running” state after calling this function.

Service ID[hex] - 0x05

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • Channel - ChannelId of the Gpt channel.

  • value - Target time in number of ticks.

Returns:

  • None

Return: None

6.12.5.6. function Gpt_StopTimer

void Gpt_StopTimer(
    Gpt_ChannelType channel
)

Brief: This service stops a timer channel.

Gpt_StopTimer will stop the selected timer channel.This will clear all the registers corresponding to the selected channel. The state of the timer channel will be changed to “Stopped”.If the channel is in state “Initialized”,”Expired”,”Stopped” before calling this function, the function will be left without any action.

Service ID[hex] - 0x06

Sync/Async - Synchronous

Reentrancy - Reentrant(but not for the same timer channel)

Parameters:

  • Channel - Numeric identifier of the GPT channel.

Returns:

  • None

Return: None

6.12.5.7. function Gpt_EnableNotification

void Gpt_EnableNotification(
    Gpt_ChannelType channel
)

Brief: This service enables the interrupt notification for a channel (relevant in normal mode).

Gpt_EnableNotification will enable the interrupt notification for the selected channel. The SETINT bit in RTI Set interrupt register will be Set to enable the Compare interrupt. The interrupt is triggered when Free running counter value matches with compare register value.

Service ID[hex] - 0x07

Sync/Async - Synchronous

Reentrancy - Reentrant(but not for the same timer channel)

Parameters:

  • Channel - Numeric identifier of the GPT channel.

Returns:

  • None

Return: None

6.12.5.8. function Gpt_DisableNotification

void Gpt_DisableNotification(
    Gpt_ChannelType channel
)

Brief: This service disables the interrupt notification for a channel (relevant in normal mode).

Gpt_DisableNotification will disable the compare interrupt notification for the selected channel. The SETINT bit in RTI Set interrupt register will be cleared to disable the Compare interrupt. The interrupt is triggered when Free running counter value matches with compare register value.

Service ID[hex] - 0x08

Sync/Async - Synchronous

Reentrancy - Reentrant(but not for the same timer channel)

Parameters:

  • Channel - Numeric identifier of the GPT channel.

Returns:

  • None

Return: None

6.12.5.9. function Gpt_ConfigRegReadBack

Std_ReturnType Gpt_ConfigRegReadBack(
    Gpt_ChannelType channel,
    GptConfigReg * GptConfigReg_pt
)

Brief: This function reads the important registers of the hardware unit and returns the value in the structure.

This API should be called after Gpt_Init is called. Otherwise this API will return E_NOT_OK.

This API could be used to readback the register contents after Gpt_Init and then the readback value could be compared during GPT execution to check the correctness of the HW unit. Since this API is used for this purpose, the register returned are the ones which doesn’t change after init based on conv or channel config.

Service ID[hex] - 0x0F

Sync/Async - Synchronous

Reentrancy - Reentrant(but not for the same timer channel)

Parameters:

  • GptChannel - Numeric identifier of the GPT channel. If this is invalid, then the API will return E_NOT_OK.

  • RegRbPtr - Pointer to where to store the readback values. If this pointer is NULL_PTR, then the API will return E_NOT_OK.

Returns:

  • E_OK - Register read back has been done

  • E_NOT_OK - Register read back failed

Return: Std_ReturnType

6.12.5.10. function Gpt_CheckWakeup

void Gpt_CheckWakeup(
    EcuM_WakeupSourceType WakeupSource
)

Brief: This function checks if a wakeup capable GPT channel is the source for a wakeup event and calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid GPT channel wakeup event.

Service ID[hex] - 0x0C

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • WakeupSource - Information on wakeup source to be checked. The associated GPT channel can be determined from configuration data.

Returns:

  • None

Return: None

6.12.5.11. function Gpt_DisableWakeup

void Gpt_DisableWakeup(
    Gpt_ChannelType Channel
)

Brief: This service disables the wakeup interrupt of a channel (relevant in sleep mode)

Service ID[hex] - 0x0A

Sync/Async - Synchronous

Reentrancy - Reentrant(but not for the same timer channel)

Parameters:

  • Channel - Numeric Identifier of the GPT Channel

Returns:

  • None

Return: None

6.12.5.12. function Gpt_EnableWakeup

void Gpt_EnableWakeup(
    Gpt_ChannelType Channel
)

Brief: This Function enables the wakeup interrupt of a channel (relevant in sleep mode)

Service ID[hex] - 0x0B

Sync/Async - Synchronous

Reentrancy - Reentrant(but not for the same timer channel)

Parameters:

  • Channel - Numeric Identifier of the GPT Channel

Returns:

  • None

Return: None

6.12.5.13. function Gpt_GetPredefTimerValue

Std_ReturnType Gpt_GetPredefTimerValue(
    Gpt_PredefTimerType PredefTimer,
    uint32 * TimeValuePtr
)

Brief: This Function delivers the current value of the desired GPT Predef Timer.

Service ID[hex] - 0x0D

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • PredefTimer - GPT Predef Timer

  • TimeValuePtr - Pointer to time value destination data in RAM

Returns:

  • E_OK no error has been detected

  • E_NOT_OK aborted due to errors

Return: Std_ReturnType

6.12.5.14. function Gpt_SetMode

void Gpt_SetMode(
    Gpt_ModeType Mode
)

Brief: This Function sets the operation mode of the GPT.

Service ID[hex] - 0x09

Sync/Async - Synchronous

Reentrancy - Non Reentrant

Parameters:

  • Mode -GPT_MODE_NORMAL: Normal operation mode of the GPT driver. GPT_MODE_SLEEP: Sleep mode of the GPT driver (wakeup capable). See also Gpt_ModeType

  • TimeValuePtr - Pointer to time value destination data in RAM

Returns:

  • None

Return: None