title: Fls_RegEnConfig summary: FLS external flash protocol specific configuration parameters.
Fls_RegEnConfig
FLS external flash protocol specific configuration parameters.
#include <Fls.h>
Structure Members
Member Type |
Member name |
Brief |
|---|---|---|
uint8 |
isAddrReg |
Config using addressed register enable/diable. |
uint8 |
cmdRegRd |
Command to read config register. |
uint8 |
cmdRegWr |
Command to write config register. |
uint32 |
cfgReg |
Address to config register. |
uint16 |
shift |
Number of register bit shifts. |
uint16 |
mask |
Mask to config register. |
uint8 |
cfgRegBitP |
Data to be written. |