4.22. WDG Module

4.22.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

BSW

Basic Software

DET

Default Error Tracer

HW

Hardware

SW

Software

WDG

Watchdog Timer

MCU

Micro Controller Unit

OS

Operating System

4.22.2. Introduction

This document describes the functionality and configuration of the AUTOSAR BSW module Wdg.

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Pre-Compile, Post-build & Link-Time

Vendor ID

WDG_VENDOR_ID (44)

Module ID

WDG_MODULE_ID (102)

Supported Platform

AM263x

The WDG driver depends on some other modules, like DET for error handling, OSEK/AUTOSAR OS for interrupt handling and the Mcu module for system clock settings.

4.22.3. Functional Overview

4.22.3.1. WDG Driver Architecture

The Wdg driver has architecture as shown in below figure from the AUTOSAR spec

Wdg in AUTOSAR architecture

Fig. 4.96 Wdg in AUTOSAR architecture

The WDG driver provides services for handling the watch dog timer on the microcontroller.

The WDG driver performs two main tasks, which are as follows:

  1. Initialization of WDG

  2. Reset WDG expiration time (trigger)

4.22.3.2. Initialization

The initialization covers the following steps

  1. Set selected watchdog timer expiration time

  2. Set selected trigger timeout

  3. Set selected window size (Digital Windowed Watchdog)

  4. Set selected mode (Fast or slow can be selected and can be switched runtime)

4.22.3.3. States

  1. WDG_IDLE: This is indicating the module is initialized and not busy.

  2. WDG_BUSY: This is indicating the module is busy.

4.22.3.4. Assumptions

  1. The clock and PLL configuration is outside driver and should be configured for proper WDG operation.

  2. The Pin Muxing should be initialized before initializing the Wdg module.

4.22.3.5. Limitations

  1. Wdg_SetTriggerCondition(0): If “0” is passed as the parameter for Wdg_SetTriggerCondition will result in an immediate stop of the watchdog triggering and an instantaneous watchdog reset of the ECU (irrespective of whether reaction is NMI or reset).

4.22.3.6. Design overview

Please refer SITARA MCU MCAL Architecture Document and MCAL: WDG Detailed Design Document provided as part of CSP.

4.22.4. Hardware Features

4.22.4.1. Hardware Features supported

  • Setting default mode and timeout during initialization.

  • Setting window size (Digital Windowed Watchdog).

  • Enable watchdog timer.

  • Service watchdog timer.

  • Mode can be changed at runtime

4.22.4.2. Not supported Features

  • Off mode not supported

4.22.4.3. Non compliance

4.22.4.3.1. Deviations to requirements (Requirement Traceability)

4.22.4.3.1.1. Deviation of requirements against AUTOSAR specification requirements

Will be updated in next release

4.22.5. Source files

Static source C Files are defined below

📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Wdg
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Wdg.h : WDG module header file. Needs to be included by higher layers.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Wdg.c : Main part of the module functionality, implements the AUTOSAR APIs for WDG driver.
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┗ 📜Wdg_Priv.c : Platform specific internal file.
┃ ┃ ┃ ┣ 📜Wdg_Priv.h : Platform specific internal file.
┃ ┃ ┗ 📜Makefile
┃ 📂mcal_config
┃ 📂mcal_docs
┃ 📜README.txt

Plugin files are defined below in the table.

Plugin Files

Description

Wdg_Cfg.h

Contains the base addresses, Precompile switches, Macros for channels, counters etc.

Wdg_PBcfg.c

Contains all channels Post-Build Configuration parameters

Wdg_Cfg.c

Contains all channels Pre-Compile Configuration parameters

WDG header file include structure

Fig. 4.97 WDG header file include structure

4.22.6. Module requirements

Please refer Software Product Specification document provided as part of CSP.

4.22.6.1. Memory Mapping

Memory Mapping Sections

WDG_CODE

WDG_CODE_ISR

WDG_VAR_NO_INIT

WDG_VAR_ZERO_INIT

WDG_PBCFG

WDG_PBCFG_ROOT

WDG_START_SEC_VAR_INIT_UNSPECIFIED(.bss)

x

WDG _STOP_SEC_VAR_INIT_UNSPECIFIED

x

WDG _START_SEC_CODE_APPL(.text)

x

WDG _STOP_SEC_CODE_APPL

x

WDG _START_SEC_VAR_UNSPECIFIED(.data)

x

WDG _STOP_SEC_VAR_UNSPECIFIED

x

WDG _START_SEC_CODE(.text)

x

WDG _STOP_SEC_CODE

x

WDG_START_SEC_PBCFG(.data)

x

WDG_STOP_SEC_PBCFG

x

WDG_START_SEC_PBCFG_ROOT(.const)

x

WDG_STOP_SEC_PBCFG_ROOT

x

4.22.6.2. Scheduling

The Wdg module has no scheduled functions.

4.22.6.3. Error handling

4.22.6.3.1. Development Error Reporting (DET)

The errors reported to DET and DEM are described in the following table

Type of Error

Related Error code

Value (Hex)

API service used in wrong context (e.g. module not initialized).

WDG_E_DRIVER_STATE

0x10

API service called with wrong / inconsistent parameter(s)

WDG_E_PARAM_MODE

0x11

API service called with wrong / inconsistent parameter(s)

WDG_E_PARAM_CONFIG

0x12

The passed timeout value is higher than the max timeout value.

WDG_E_PARAM_TIMEOUT

0x13

API is called with wrong pointer value (e.g. NULL pointer)

WDG_E_PARAM_POINTER

0x14

4.22.6.3.2. Parameter Checking

AUTOSAR requires that API functions check the validity of their parameters. The checks are described in spec and are done as internal parameter checks of the API functions. These checks are for development error reporting and can be en/dis-abled separately. Refer to the configuration chapter where the en/dis-abling of the checks is described. En/dis-abling of single checks is an addition to the AUTOSAR standard which requires to en/dis-able the complete parameter checking via the parameter WDG_DEV_ERROR_DETECT. The following table shows which parameter checks are performed on which services:

Services

Wdg_Init

Wdg_SetMode

Wdg_SetTriggerCondition

Wdg_GetVersionInfo

Wdg_Trigger

WDG_E_DRIVER_STATE

X

X

WDG_E_PARAM_MODE

X

WDG_E_PARAM_CONFIG

WDG_E_PARAM_TIMEOUT

X

WDG_E_PARAM_POINTER

X

X

WDG_E_MODE_FAILED

X

WDG_E_DISABLE_REJECTED

X

4.22.6.3.3. Production Code Error Reporting

By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus(). The errors reported to DEM are described in the following table:

Type of Error

Related Error code

Description

Assigned by DEM

WDG_E_MODE_FAILED

This error is raised when setting the watchdog mode fails.

Assigned by DEM

WDG_E_DISABLE_REJECTED

Initialization or watchdog mode switch failed because it would disable the watchdog though this is not allowed in this configuration

Assigned by DEM

WDG_E_HARDWARE_ERROR

This error is raised when register write failure occurs (Hardware Failure)

4.22.7. Used resources

4.22.7.1. Interrupt Handling

Watchdog uses Non maskable interrupt (Interrupt Number 128) and the ISR shall be called when interrupt occurs

Interrupt Number

ISR API Mapped

RTI_WDT0_NMI

WDT_Isr

4.22.8. Integration description

4.22.8.1. Dependent modules

4.22.8.1.1. MCU

The module MCU powers up the microcontroller’s peripherals at startup time and initializes the PLL.

4.22.8.1.2. OS

An operating system can be used for task scheduling, interrupt handling, global suspend and restore of interrupts and creating of the Interrupt Vector Table. The WDG module may use AUTOSAR OS to suspend and restore global interrupts.

4.22.8.1.3. SchM

There are no exclusive areas.

4.22.8.1.4. Critical Sections

There are no critical sections.

4.22.8.1.5. DEM

By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus(). Note: Dem Event is enable only if $(Module_Name)DemEventParameterRefs is enabled.

4.22.8.1.6. DET

By default, production code related errors are reported to the DET using the service Det_ReportError(). If development error reporting is enabled (i.e. pre-compile parameter WDG_DEV_ERROR_DETECT== STD_ON). The reported service IDs identify the services which are described in 3.4.

4.22.8.1.7. Callback Notification

The WDG driver does not provide any call back functions.

4.22.8.2. Multi-core support

Not supported

4.22.9. Configuration

4.22.9.1. WdgDemEventParameterRefs

Item

Name

WdgDemEventParameterRefs

Description

Reference to the DemEventParameter which shall be issued when the error “Timeout on blocking API call occurs “ has occurred.

Post-build-variant-multiplicity

false

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Link Time

VARIANT-LINK-TIME

Pre-Compile Time

VARIANT-PRE-COMPILE

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.22.9.2. WdgGeneral

All general parameters of the watchdog driver are collected here.

4.22.9.2.1. WdgDevErrorDetect

Item

Name

WdgDevErrorDetect

Description

Compile switch to enable / disable development error detection for this module.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

true

4.22.9.2.2. WdgDisableAllowed

Item

Name

WdgDisableAllowed

Description

Compile switch to allow / forbid disabling the watchdog driver during runtime.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

false

4.22.9.2.3. WdgIndex

Item

Name

WdgIndex

Description

Represents the watchdog driver’s ID so that it can be referenced by the watchdog interface.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

0

Max-value

255

Min-value

0

4.22.9.2.4. WdgInitialTimeout

Item

Name

WdgInitialTimeout

Description

The initial timeout (seconds) for the trigger condition to be initialized during Init function. It shall be not larger than WdgMaxTimeout.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

1.0

Max-value

65.535

Min-value

0.0

4.22.9.2.5. WdgMaxTimeout

Item

Name

WdgMaxTimeout

Description

The maximum timeout (seconds) to which the watchdog trigger condition can be initialized.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

65.535

Max-value

65.535

Min-value

0.0

4.22.9.2.6. WdgWindowSize

Item

Name

WdgWindowSize

Description

The Digital Windowed Watchdog window size. Selecting 100% enables standard watchdod (not windowed)

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

WINDOW_SIZE_100_PERCENT

Range

WINDOW_SIZE_3_125_PERCENT
WINDOW_SIZE_6_25_PERCENT
WINDOW_SIZE_12_5_PERCENT
WINDOW_SIZE_25_PERCENT
WINDOW_SIZE_50_PERCENT
WINDOW_SIZE_100_PERCENT

4.22.9.2.7. WdgRunArea

Item

Name

WdgRunArea

Description

Represents the watchdog driver execution area is either from ROM(Flash) or RAM as required with the particular microcontroller.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

RAM

Range

RAM
ROM

4.22.9.2.8. WdgTriggerLocation

Item

Name

WdgTriggerLocation

Description

Location (memory address) of the watchdog trigger routine.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

NULL_PTR

4.22.9.2.9. WdgVersionInfoApi

Item

Name

WdgVersionInfoApi

Description

Compile switch to enable / disable the version information API

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

true

4.22.9.2.10. WdgRegisterReadbackApi

Item

Name

WdgRegisterReadbackApi

Description

Compile switch to enable / disable the Register Readback API

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

false

4.22.9.2.11. WdgRtiFrequency

Item

Name

WdgRtiFrequency

Description

RTI Clock Frequency (MHz)

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

200

Max-value

200

Min-value

0

4.22.9.2.12. WdgSkipForceReset

Item

Name

WdgSkipForceReset

Description

Compile switch to enable / disable skipping force reset of WDG when 0 timeout is passed in Wdg_SetTriggerCondition

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Default-value

false

4.22.10. Examples

4.22.10.1. Overview

  1. Initializes clock using Mcu_Init()

  2. Configure the interrupts for WDG using WDTApp_interruptConfig()

  3. Default Example program is configured in Non-Maskable Interrupt method (WDT will trigger interrupt when counter becomes zero).

  4. WDT window reaction can be changed to “reset” through configuration (EB Tresos).

  5. Get Watchdog version using Wdg_GetVersionInfo()

  6. Calculate and define the triggerValue and maxServiceInterval

  7. In example, service interval is 25ms and service count is 100. So, every 25ms core will service the WDT for 100 times (25*100 = 2500 ms).

  8. Initialize the timer using Gpt_Init()

  9. Initialize the Watchdog using Wdg_Init()

  10. Start the timer using API Gpt_StartTimer()

  11. Set the trigger condition using Wdg_SetTriggerCondition() along with timeout value (Timeout is defined by subtracting triggerValue with maxServiceInterval)

  12. Then after it will raise an interrupt and interrupt will run (WDT_Isr() function). In ISR function core reset will occurs and start running program again automatically.

  13. On reset, Check the reason for the reset using GetResetReason(). If reset happened due to WDT then “Test Passed”

  14. In Reset window reaction mode, after counter reaches to zero POR(Power ON Reset) happens.

4.22.10.2. Hardware Software Setup and Tools

None

4.22.10.3. Steps to build and run example

  1. WDG example application demonstrates the MCAL WDG driver features, which is referred from folder <MCAL_ROOT>/examples/WDG.

  2. This application can be built from the build folder by giving “gmake –s wdg_app PLATFORM=am263” command in command prompt.

  3. Once the build is completed we get an appimage file, which is flashed in am263x controller and executed.

  4. To Flash the appimage at the respective memory location as the SBL expects, path of the appimage file is provided in “default_sbl_qspi” file in “..<MCU_PLUS_SDK_INSTALLATION>\tools\boot\sbl_prebuilt\am263x-cc”

  5. Set the boot mode of board to UART mode.(UART boot mode: 1000)

  6. Open command prompt at the path “..<MCU_PLUS_SDK_INSTALLATION>\tools\boot” and provide command as follows: “python uart_uniflash.py -p COM<x> –cfg=sbl_prebuilt/am263x-cc/default_sbl_qspi.cfg” Here <x> depicts the COM PORT number where hardware is connected to system, which can be detected from device manager

  7. Once the appimage is flashed after the command is executed, change the boot mode of board to QSPI mode.(QSPI boot mode: 0010)

  8. Open the terminal to get the expected application log after doing hard reset on board.

  9. Verify that the application produces the correct results as expected shown below.

4.22.10.4. Example Logs


   WDG_APP: Sample Application - STARTS !!!

   WDG MCAL Version Info
   ---------------------
   Vendor ID           : 44
   Module ID           : 102
   SW Major Version    : 9
   SW Minor Version    : 1
   SW Patch Version    : 0

   ----------------------------------------------------------------------------------
   Starting WDG test  !!!
   ----------------------------------------------------------------------------------
   Service Count 100
   Service Interval 25 milliseconds
   ------------------------------------------
   Trigger Value = 2500 milliseconds
   ------------------------------------------
   Maximum Service Interval 74 milliseconds 
   Initializing channels
   Post-Build variant is being used .
   Reset Reason 2 
   Test Passed!! 
   WDG Stack Usage: 800 bytes
   ------------------------------------------

4.22.10.5. File Structure

📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Wdg
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜WdgApp.c : Contains WDG test example.
┃ ┃ ┃ ┣ 📜WdgApp.h : Contains WDG test example headers.
┃ ┃ ┃ ┣ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Wdg_Demo_Cfg
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am263
┃ ┃ ┃ ┃ ┃ ┣ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Wdg_Cfg.h : Contains the Precompile switches, Macros etc.
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Wdg_Cfg.c : Contains Pre-Compile Configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Wdg_Lcfg.c : Contains linker Configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Wdg_PBcfg.c : Contains Post-Build Configuration parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┣ 📜README.txt

4.22.11. FAQ’s

Will be updated in next release

4.22.12. References

AUTOSAR_SWS_WatchdogDriver
Technical Reference Manual