4.2. CAN Module

4.2.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

RTE

Runtime Environment

BSW

Basic Software

GPIO

General Purpose Input Output

MCAL

Micro Controller Abstraction Layer

API

Application Programming Interface

DET

Default Error Tracer

HW

Hardware

SW

Software

I/O

Input/Output

CAN

Controller Area Network

CanIf

Can Interface

L-PDU

Data Link Layer Protocol Data Unit. Consists of Identifier, Data Length and Data (SDU).

DLC

Data Length Code

OS

Operating System

4.2.2. Introduction

This document details AUTOSAR BSW CAN module implementation

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Post-build, Pre-Compile

Vendor ID

CAN_VENDOR_ID (44)

Module ID

CAN_MODULE_ID (80)

Supported Platform

AM263x

The CAN driver provides services for basic transmission and reception of CAN frames in both interrupt and polling mode. These components can be used by an application.

CAN MCAL AUTOSAR

Fig. 4.19 Can MCAL AUTOSAR

4.2.3. Functional Overview

The CAN module initializes and controls the internal CAN Controllers of the microcontroller. It provides services to write, read, and configure mailboxes of the Can controllers

4.2.3.1. Initialization

Can_Init () must be called to initialize the CAN driver at power on and sets controller independent init values. This will also set the controllers to CAN_CS_STOPPED.

4.2.3.2. States

There are 4 states in which the CAN hardware/driver can be:

  • CAN_CS_UNINT: This is the state when the Hardware is just started.

  • CAN_CS_STOPPED: This is the state in which Hardware is in when after the initialization routine is called. CAN controller be fully initialized but does not participate in the bus transactions.

  • CAN_CS_STARTED: This is the state in which hardware is in when it is fully operational i.e.., it is sending and receive messages from the bus on CAN network.

  • CAN_CS_SLEEP: This is the state in which the hardware is in when the controller is sleeping. Changing the mode via Can_SetControllerMode ().

Following modes changes are supported:

  1. CAN_CS_STARTED

  2. CAN_CS_STOPPED

  3. CAN_CS_SLEEP

The figure below taken from the AUTOSAR specification shows the state transitions for different function calls and events:

CAN channel states and state transitions

Fig. 4.20 CAN channel states and state transitions

4.2.3.3. CAN operating modes

The CAN module has a very simple state machine, with the two states CAN_UNINIT and CAN_READY. After power-up/reset, the CAN module shall be in the state CAN_UNINIT.

CAN driver modes

Fig. 4.21 CAN driver modes

4.2.3.4. Assumptions

None

4.2.3.5. Limitations

CAN Wake mode is not supported.

4.2.3.6. Design overview

Please refer SITARA MCU MCAL Architecture Document and MCAL: CAN Detailed Design Document provided as part of CSP.

4.2.4. Hardware Features

4.2.4.1. Hardware Features supported

  • Conforms with CAN Protocol 2.0 A, B and ISO 11898-1:2015

  • Full CAN FD support (up to 64 data bytes)

  • 1-Mbps nominal bit rate, 5-Mbps data bit rate

  • Loop-back mode for self-test

  • AUTOSAR and SAE J1939 support

  • Maskable interrupt (two configurable interrupt lines and clock stop or wakeup)

  • Two clock domains (CAN clock and host clock)

  • Clock stop and wakeup support

  • Up to 32 dedicated transmit buffers

  • Configurable transmit FIFO, up to 32 elements

  • Configurable transmit queue, up to 32 elements

  • Configurable transmit Event FIFO, up to 32 elements

  • Up to 64 dedicated receive buffers

  • Two configurable receive FIFOs, up to 64 elements each

  • Up to 128 filter elements

  • Parity/ECC support - Message RAM single error correction and double error detection (SECDED) mechanism.

4.2.4.2. AUTOSAR Features supported

  • 4 CAN Controllers for AM263x.

  • Supports transmission and reception of Classic.

  • Frames through CAN (CAN FD Controller).

  • Initialization of CAN controller HW.

  • Transmitting of CAN Frames and confirmation.

  • Reception of the CAN Frames.

  • Polling modes for Read / Write / BusOff confirmations.

  • Mailbox objects – Full and Basic filters for Rx.

  • Use of Software Delays according to configured timeout and number of ticks to check for timeouts.

  • Mixed Mode Operation.

  • Triggered transmission API.

  • LPDU Callback function.

4.2.4.3. Not supported Features

  • Support for pretend networking

  • CAN Wake mode is not supported.

  • Timestamp Counter.

4.2.4.4. Non compliance

4.2.4.4.1. Deviations to requirements (Requirement Traceability)

4.2.4.4.1.1. Deviation of requirements against AUTOSAR specification requirements

Will be updated in future release

4.2.5. Source files

Static source C Files are defined below

📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Can
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Can.h : Contains the API’s of the Can driver to be used by upper layers.
┃ ┃ ┃ ┣ 📜Can_Irq.h : Contains ISR function declaration.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Can.c : Contains the implementation of the API’s for Can driver.
┃ ┃ ┃ ┣ 📜Can_Irq.c : contains the implementation for Can interrupts handlers.
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┗ 📜Can_Mcan.c : Contains Internal Functions Definitions
┃ ┃ ┃ ┗ 📜Can_Priv.c : Contains Functions that support the API’s for Can driver
┃ ┃ ┃ ┣ 📜Can_Priv.h : Contains data structures and Internal function declarations.
┃ ┃ ┃ ┗ 📜mcan.c : Contains hardware Functions Definitions
┃ ┃ ┃ ┗ 📜mcan.h : Contains hardware Functions declarations and structures
┃ ┃ ┗ 📜Makefile
┃ 📂mcal_config
┃ 📂mcal_docs
┃ 📜README.txt

Plugin files are defined below in the table.

Plugin Files

Description

Can_Cfg.h

Contains the Precompile switches, Macros for CAN controllers, Hardware Objects etc.

Can_PBcfg.c

Contains all controllers Post-Build Configuration parameters

Can_Cfg.c

Contains all controllers Pre-Compile Configuration parameters

Can Header File Structure

Fig. 4.22 Can Header File Structure

4.2.6. Module requirements

Please refer Software Product Specification document provided as part of CSP.

4.2.6.1. Memory Mapping

Memory Mapping Sections

CAN_CODE

CAN_CODE_ISR

CAN_VAR_NO_INIT

CAN_VAR_ZERO_INIT

CAN_PBCFG

CAN_PBCFG_ROOT

CAN_START_SEC_VAR_INIT_UNSPECIFIED (.bss)

X

CAN_STOP_SEC_VAR_INIT_UNSPECIFIED

X

CAN_START_SEC_CODE_APPL (.text)

X

CAN_STOP_SEC_CODE_APPL

X

CAN_START_SEC_VAR_UNSPECIFIED (.bss)

x

CAN_STOP_SEC_VAR_UNSPECIFIED

x

CAN_START_SEC_CODE(.text)

x

CAN_STOP_SEC_CODE

x

CAN_START_SEC_PBCFG (.data)

X

CAN_STOP_SEC_PBCFG

X

CAN_START_SEC_PBCFG_ROOT (.const)

X

CAN_STOP_SEC_PBCFG_ROOT

X

4.2.6.2. Scheduling

Schedule Function API

Description

Can_MainFunction_Write

This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING

Can_MainFunction_Read

This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.

Can_MainFunction_BusOff

This function performs the polling of bus-off events that are configured statically as ‘to be polled’.

Can_MainFunction_Wakeup

This function performs the polling of wake-up events that are configured statically as ‘to be polled’.

Can_MainFunction_Mode

This function performs the polling of CAN controller mode transitions.

4.2.6.3. Error handling

4.2.6.3.1. Development Error Reporting

Development errors are reported to the DET using the service Det_ReportError(),when enabled. The driver interface contains the MACRO declaration of the error codes to be returned.

4.2.6.3.1.1. Error codes

Type of Error

Related Error code

Value (Hex)

API service called with wrong parameter pointer

CAN_E_PARAM_POINTER

0x01

API service called with wrong hardware handle

CAN_E_PARAM_HANDLE

0x02

API service called with wrong data length

CAN_E_PARAM_DATA_LENGTH

0x03

API service called with wrong parameter Controller

CAN_E_PARAM_CONTROLLER

0x04

API service used without initialization

CAN_E_UNINIT

0x05

Invalid transition for the current mode.

CAN_E_TRANSITION

0x06

Parameter baud rate has an invalid value.

CAN_E_PARAM_BAUDRATE

0x07

invalid ICOM configuration Id

CAN_E_ICOM_CONFIG_INVALID

0x08

Invalid Configuration set selection.

CAN_E_INIT_FAILED

0x09

4.2.6.3.1.2. Runtime Error

Type of Error

Related Error code

Value (Hex)

Received CAN message is lost

CAN_E_DATALOST

0x01

4.2.6.3.2. DEM Error

Type of Error

Related Error Code

Description

Assigned by DEM

CAN_E_HARDWARE_ERROR

This error is raised when CAN register setting timeout occurs.

4.2.7. Used resources

4.2.7.1. Interrupt Handling

The Driver doesn’t register any interrupts handler (ISR), it’s expected that consumer of this driver registers the required interrupt handler.

AUTOSAR_SWS_CANDriver section: 10 Configuration specification, details the expected behavior and control flow for ISR implementation, please refer the same.

For every CAN Instance, an ISR requires to be registered. The Interrupt number associated with instance of the CAN is detailed in TRM (also, please refer the Example application). Interrupt type should be selected in CAN plugin.

Two interrupt routines are provided by the CAN driver. The ISR’s are in the file Can_Irq.c User might edit it for adapting for the suitable OS. The current support is for the NON-OS Interrupts structure. CAN interrupts are hooked up on the Interrupt 0 line (IE0).

Following are the CAN controllers, its respective ISRs for each CAN Controller in AM263x:

Can Controllers

ISR Routines

MCAN0

Can_0_Int0ISR()

MCAN0 Error

Can_0_Int1ISR()

MCAN1

Can_1_Int0ISR()

MCAN1 Error

Can_1_Int1ISR()

MCAN2

Can_2_Int0ISR()

MCAN2 Error

Can_2_Int1ISR()

MCAN3

Can_3_Int0ISR()

MCAN3 Error

Can_3_Int1ISR()

  1. Can_0_Int0ISR For AM263x device, this ISR is called on detection of an event on interrupt line 0 for the MCAN0/MCANA controller. Transmission and reception related events including error events and ECC error events are managed in this ISR.

  2. Can_0_Int1ISR For AM263x device, This function manages the ECC related events for MCAN0/MCANA module. The ECC events for MCAN can only be configured and detected via ESM module. So, for detecting the ECC errors for the MCAN0/MCANA module, the application needs to register and configure the ESM to generate interrupt for ECC Errors. This function can then be called to manage the ECC related events. Note: MCAN0/MCANA Interrupt line 1 can only be used for ECC and is not supported for normal interrupt functionality in the configurator

  3. Can_1_Int0ISR For AM263x device, This ISR is called on detection of an event on interrupt line 0 of the MCAN1/MCANB controller. Transmission and reception related events including error events are managed in this ISR.

  4. Can_1_Int1ISR For AM263x device, This function manages the ECC related events for MCAN1/MCANB module. The ECC events for MCAN can only be configured and detected via ESM module. So, for detecting the ECC errors for the MCAN module, the application needs to register and configure the ESM to generate interrupt for ECC Errors. This function can then be called to manage the ECC related events. Note: MCAN1/MCANB Interrupt line 1 can only be used for ECC and is not supported for normal interrupt functionality in the configurator

  5. Can_2_Int0ISR For AM263x device, This ISR is called on detection of an event on interrupt line 0 of the MCAN2 controller. Transmission and reception related events including error events are managed in this ISR.

  6. Can_2_Int1ISR_Fun For AM263x device, This function manages the ECC related events for MCAN2 module. The ECC events for MCAN can only be configured and detected via ESM module. So, for detecting the ECC errors for the MCAN module, the application needs to register and configure the ESM to generate interrupt for ECC Errors (for MCAN module). This function can then be called to manage the ECC related events. Note: MCAN2 Interrupt line 1 can only be used for ECC and is not supported for normal interrupt functionality in the configurator

  7. Can_3_Int0ISR For AM263x device, This ISR is called on detection of an event on interrupt line 0 of the MCAN3 controller. Transmission and reception related events including error events are managed in this ISR.

  8. Can_3_Int1ISR_Fun For AM263x device, This function manages the ECC related events for MCAN3 module. The ECC events for MCAN can only be configured and detected via ESM module. So, for detecting the ECC errors for the MCAN module, the application needs to register and configure the ESM to generate interrupt for ECC Errors (for MCAN module). This function can then be called to manage the ECC related events. Note: MCAN3 Interrupt line 1 can only be used for ECC and is not supported for normal interrupt functionality in the configurator

4.2.8. Integration description

4.2.8.1. Dependent modules

4.2.8.1.1. MCU

The CAN Modules expects the MCU modules to enable the MCAN controller. The Clock configuration should be configured in CAN module to select the correct clock source in the parameter “ CanCpuClockRef “.

Clock Reference in MCU module

Fig. 4.23 Clock Reference in MCU module

4.2.8.1.2. Port

The CAN Modules expects that pinmux is set correctly to configure the MCAN TX/RX pins for CAN mode. This is done by the PORT driver.

4.2.8.1.3. OS

An operating system can be used for task scheduling, interrupt handling, global suspend and restore of interrupts and creating of the Interrupt Vector Table. The CAN module may use AUTOSAR OS to suspend and restore global interrupts.

4.2.8.1.4. DET

The CAN module depends on the DET (by default) to report development errors.The DET can be replaced optionally by an equivalent component which is responsible to recognize development errors, if no DET component is available.

4.2.8.1.5. DEM

By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus().

Note: Dem Event is enable only if $(Module_Name)DemEventParameterRefs is enabled.

4.2.8.1.6. Callback Notification

At its configurable interfaces the CAN defines notifications that can be mapped to callback functions provided by other modules. The mapping is not statically defined by the CAN but can be performed at configuration time. The function prototypes that can be used for the configuration have to match the appropriate function prototype signatures, which are described in the following.

Can_ErrorNotification: This is of type Can_ErrNotifyType which is defined in Can.h file. This is called to report back the ECC error status to the application when ECC error interrupt happens.

4.2.8.1.7. SchM

If multiple AUTOSAR runnables have access to the same Data Store Memory block, the exported AUTOSAR specification enforces data consistency by using an AUTOSAR exclusive area. With this specification, the runnables have mutually exclusive access to the per-instance memory global data, which prevents data corruption. Beside the OS, the BSW Scheduler provides functions that CAN module calls at begin and end of critical sections. This implementation requires 1 level of exclusive access to guard critical sections.

The data consistency mechanism that has to be applied to an ExclusiveArea might be domain, ECU or even project specific. The decision which mechanism has to be applied by RTE / Basic Software Scheduler is taken during ECU integration by setting the Exclusive Area configuration parameter RteExclusiveAreaImplMechanism. This parameter is an input for RTE generator. For CAN Module, data consistency and exclusive access to critical sections are required for the following sections as shown in the table below:

Exclusive Area Functions used

CAN Function calling Exclusive Area

Need for Exclusive Area

Recommended Exclusive Area Mapping

CAN_EXCLUSIVE_AREA_0

Can_Write_Internal
Can_SetBaudrate
Can_DisableControllerInterrupts
Can_EnableControllerInterrupts
Can_MainFunction_Write
Can_MainFunction_Read

To protect against multiple access for shared resources

ALL_INTERRUPT_BLOCKING : All interrupts should be blocked as this API’s can be called in the interrupts

4.2.8.2. Multi-core support

Not Supported

4.2.9. Configuration

The Can Driver implementation supports multiple configuration variants The driver expects generated Can_Cfg.h to be present as input file. The associated Can driver configuration generated source files are Can_Cfg.c and Can_PBcfg.c if Post-Build config variant is selected, only Can_Cfg.c if Pre-Compile variant is selected

The generated configuration files should not be modified manually. The config tool Elektrobit Tresos should be used to modify the configuration files.

Refer AUTOSAR_SWS_CANDriver section: 10 Configuration specification for configuration parameters details

4.2.9.1. CanConfigSet

This container contains the multiple configuration container and sub containers of the AUTOSAR Can module.

4.2.9.1.1. CanController

This container contains the configuration parameters of the CAN controller(s).

4.2.9.1.1.1. CanControllerId

Item

Name

CanControllerId

Description

This parameter provides the controller ID which is unique in a given CAN Driver. The value for this parameter starts with 0 and continue without any gaps.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

4.2.9.1.1.2. CanControllerInstance

Item

Name

CanControllerInstance

Description

Selects Can Controller Instance.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

MCAN0

Range

MCAN0
MCAN1
MCAN2
MCAN3

4.2.9.1.1.3. CanControllerActivation

Item

Name

CanControllerActivation

Description

Defines if a CAN controller is used in the configuration.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.2.9.1.1.4. CanControllerBaseAddress

Item

Name

CanControllerBaseAddress

Description

Specifies the CAN controller base address.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

1382023168

Max-value

1382219776

Min-value

1382023168

4.2.9.1.1.5. CanErrorNotification

Item

Name

CanErrorNotification

Description

Callback function for ECC Error and Parity error in case of AM263x

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

4.2.9.1.1.6. CanBusoffProcessing

Item

Name

CanBusoffProcessing

Description

Enables / disables API Can_MainFunction_BusOff() for handling busoff events in polling mode.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

INTERRUPT

Range

INTERRUPT
POLLING

4.2.9.1.1.7. CanRxProcessing

Item

Name

CanRxProcessing

Description

Enables / disables API Can_MainFunction_Read() for handling PDU reception events in polling mode.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

INTERRUPT

Range

INTERRUPT
MIXED
POLLING

4.2.9.1.1.8. CanTxProcessing

Item

Name

CanTxProcessing

Description

Enables / disables API Can_MainFunction_Write() for handling PDU transmission events in polling mode.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

INTERRUPT

Range

INTERRUPT
MIXED
POLLING

4.2.9.1.1.9. CanWakeupFunctionalityAPI

Item

Name

CanWakeupFunctionalityAPI

Description

Adds / removes the service Can_CheckWakeup() from the code. This feature is not supported

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.2.9.1.1.10. CanDisableAutoRetranmission

Item

Name

CanDisableAutoRetranmission

Description

Disable auto retransmission on xmit error

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Post-Build-Time

VARIANT-POST-BUILD

Default-value

true

4.2.9.1.1.11. CanWakeupProcessing

Item

Name

CanWakeupProcessing

Description

Enables / disables API Can_MainFunction_Wakeup() for handling wakeup events in polling mode. This feature is not supported

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

INTERRUPT

Range

INTERRUPT
POLLING

4.2.9.1.1.12. CanWakeupSupport

Item

Name

CanWakeupSupport

Description

CAN driver support for wakeup over CAN Bus. This feature is not supported

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.2.9.1.1.13. CanControllerDefaultBaudrate

Item

Name

CanControllerDefaultBaudrate

Description

Reference to baudrate configuration container configured for the Can Controller.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.2.9.1.1.14. CanCpuClockRef

Item

Name

CanCpuClockRef

Description

Reference to the CPU clock configuration, which is set in the MCU driver configuration

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.2.9.1.1.15. CanWakeupSourceRef

Item

Name

CanWakeupSourceRef

Description

This parameter contains a reference to the Wakeup Source for this controller as defined in the ECU State Manager.

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.2.9.1.2. CanControllerBaudrateConfig

This container contains bit timing related configuration parameters of the CAN controller(s).

4.2.9.1.2.1. CanControllerBaudRate

Item

Name

CanControllerBaudRate

Description

Specifies the baudrate of the controller in kbps.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

500

Max-value

2000

Min-value

0

4.2.9.1.2.2. CanControllerBaudRateConfigID

Item

Name

CanControllerBaudRateConfigID

Description

Uniquely identifies a specific baud rate configuration. This ID is used by SetBaudrate API.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

65535

Min-value

0

4.2.9.1.2.3. CanControllerPropSeg

Item

Name

CanControllerPropSeg

Description

Specifies propagation delay in time quantas.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

8

Max-value

255

Min-value

0

4.2.9.1.2.4. CanControllerSeg1

Item

Name

CanControllerSeg1

Description

Specifies phase segment 1 in time quantas.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

5

Max-value

255

Min-value

0

4.2.9.1.2.5. CanControllerSeg2

Item

Name

CanControllerSeg2

Description

Specifies phase segment 2 in time quantas.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

4

Max-value

255

Min-value

0

4.2.9.1.2.6. CanControllerSyncJumpWidth

Item

Name

CanControllerSyncJumpWidth

Description

Specifies the synchronization jump width for the controller in time quantas.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

1

Max-value

255

Min-value

0

4.2.9.1.3. CanControllerFdBaudrateConfig

This optional container contains bit timing related configuration parameters of the CAN controller(s) for payload and CRC of a CAN FD frame. If this container exists the controller supports CAN FD frames.

4.2.9.1.3.1. CanControllerFdBaudRate

Item

Name

CanControllerFdBaudRate

Description

Specifies the data segment baud rate of the controller in kbps.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

5000

Max-value

16000

Min-value

0

4.2.9.1.3.2. CanControllerPropSeg

Item

Name

CanControllerPropSeg

Description

Specifies propagation delay in time quantas.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

2

Max-value

255

Min-value

0

4.2.9.1.3.3. CanControllerSeg1

Item

Name

CanControllerSeg1

Description

Specifies phase segment 1 in time quantas.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

2

Max-value

255

Min-value

0

4.2.9.1.3.4. CanControllerSeg2

Item

Name

CanControllerSeg2

Description

Specifies phase segment 2 in time quantas.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

3

Max-value

255

Min-value

0

4.2.9.1.3.5. CanControllerSyncJumpWidth

Item

Name

CanControllerSyncJumpWidth

Description

Specifies the synchronization jump width for the controller in time quantas.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

2

Max-value

255

Min-value

0

4.2.9.1.3.6. CanControllerTrcvDelayCompensationOffset

Item

Name

CanControllerTrcvDelayCompensationOffset

Description

Specifies the Transceiver Delay Compensation Offset in ns. If not specified Transceiver Delay Compensation is disabled.

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

180

Max-value

400

Min-value

0

4.2.9.1.3.7. CanControllerTxBitRateSwitch

Item

Name

CanControllerTxBitRateSwitch

Description

Specifies if the bit rate switching shall be used for transmissions.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.2.9.1.4. CanTTController

This container is only included and valid if TTCAN SWS is used and TTCAN is enabled.

4.2.9.1.4.1. CanTTControllerGlobalTimeFiltering

Item

Name

CanTTControllerGlobalTimeFiltering

Description

Enables/disables the global time filtering.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.2.9.1.4.2. CanTTControllerLevel2

Item

Name

CanTTControllerLevel2

Description

Defines whether Level 2 or Level 1 is used.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.2.9.1.5. CanHardwareObject

This container contains the configuration (parameters) of CAN Hardware Objects.

4.2.9.1.5.1. CanFdPaddingValue

Item

Name

CanFdPaddingValue

Description

Specifies the value which is used to pad unspecified data in CAN FD frames > 8 bytes for transmission. This is necessary due to the discrete possible values of the DLC if > 8 bytes.

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

4.2.9.1.5.2. CanHandleType

Item

Name

CanHandleType

Description

Specifies the type (Full-CAN or Basic-CAN) of a hardware object.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

FULL

Range

BASIC
FULL

4.2.9.1.5.3. CanHardwareObjectUsesPolling

Item

Name

CanHardwareObjectUsesPolling

Description

Enables polling of this hardware object.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Default-value

false

4.2.9.1.5.4. CanHwObjectCount

Item

Name

CanHwObjectCount

Description

Number of hardware objects used to implement one HOH. In case of a HRH this parameter defines the number of elements in the hardware FIFO or the number of shadow buffers, in case of a HTH it defines the number of hardware objects used for multiplexed transmission or for a hardware FIFO used by a FullCAN HTH.

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

1

Max-value

65535

Min-value

1

4.2.9.1.5.5. CanIdType

Item

Name

CanIdType

Description

Specifies whether the IdValue is of type

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

STANDARD

Range

EXTENDED
MIXED
STANDARD

4.2.9.1.5.6. CanObjectId

Item

Name

CanObjectId

Description

Holds the handle ID of HRH or HTH. The value of this parameter is unique in a given CAN Driver, and it should start with 0 and continue without any gaps.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

65535

Min-value

0

4.2.9.1.5.7. CanObjectType

Item

Name

CanObjectType

Description

Specifies if the HardwareObject is used as Transmit or as Receive object

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

TRANSMIT

Range

RECEIVE
TRANSMIT

4.2.9.1.5.8. CanTriggerTransmitEnable

Item

Name

CanTriggerTransmitEnable

Description

This parameter defines if or if not Can supports the trigger-transmit API for this handle.

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.2.9.1.5.9. CanControllerRef

Item

Name

CanControllerRef

Description

Reference to CAN Controller to which the HOH is associated to.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.2.9.1.5.10. CanMainFunctionRWPeriodRef

Item

Name

CanMainFunctionRWPeriodRef

Description

Reference to CanMainFunctionPeriod

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.2.9.1.6. CanHwFilter

This container is only valid for HRHs and contains the configuration (parameters) of one hardware filter.

4.2.9.1.6.1. CanHwFilterCode

Item

Name

CanHwFilterCode

Description

Specifies (together with the filter mask) the identifiers range that passes the hardware filter.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

4294967295

Min-value

0

4.2.9.1.6.2. CanHwFilterMask

Item

Name

CanHwFilterMask

Description

Describes a mask for hardware-based filtering of CAN identifiers. The CAN identifiers of incoming messages are masked with the appropriate CanFilterMaskValue. Bits holding a 0 mean don’t care, i.e. do not compare the message’s identifier in the respective bit position.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

4294967295

Min-value

0

4.2.9.1.7. CanTTHardwareObjectTrigger

This container is only included and valid if TTCAN SWS is used and TTCAN is enabled.

4.2.9.1.8. CanIcom

This container contains the parameters for configuring pretended networking

4.2.9.1.9. CanIcomConfig

This container contains the configuration parameters of the ICOM Configuration.

4.2.9.1.9.1. CanIcomConfigId

Item

Name

CanIcomConfigId

Description

This parameter identifies the ID of the ICOM configuration.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Max-value

255

Min-value

1

4.2.9.1.9.2. CanIcomWakeOnBusOff

Item

Name

CanIcomWakeOnBusOff

Description

This parameter defines that the MCU shall wake if the bus off is detected or not.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.2.9.1.10. CanIcomWakeupCauses

This container contains the configuration parameters of the wakeup causes to leave the power saving mode.

4.2.9.1.11. CanIcomRxMessage

This container contains the configuration parameters for the wakeup causes for matching received messages. It has to be configured as often as received messages are defined as wakeup cause.

4.2.9.1.11.1. CanIcomMessageId

Item

Name

CanIcomMessageId

Description

This parameter defines the message ID the wakeup causes of this CanIcomRxMessage are configured for. In addition a mask (CanIcomMessageIdMask) can be defined, in that case it is possible to define a range of rx messages, which can create a wakeup condition.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Max-value

536870912

Min-value

0

4.2.9.1.11.2. CanIcomPayloadLengthError

Item

Name

CanIcomPayloadLengthError

Description

This parameter defines that the MCU shall wake if a payload error occurs

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.2.9.1.12. CanIcomRxMessageSignalConfig

This container contains the configuration parameters for the wakeup causes for matching signals.

4.2.9.1.12.1. CanIcomSignalMask

Item

Name

CanIcomSignalMask

Description

This parameter shall be used to mask a signal in the payload of a CAN message.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Max-value

18446744073709551615

Min-value

0

4.2.9.1.12.2. CanIcomSignalOperation

Item

Name

CanIcomSignalOperation

Description

This parameter defines the operation, which shall be used to verify the signal value creates a wakeup condition.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Range

AND
EQUAL
GREATER
SMALLER
XOR

4.2.9.1.12.3. CanIcomSignalValue

Item

Name

CanIcomSignalValue

Description

This parameter shall be used to define a signal value which shall be compared (CanIcomSignalOperation) with the masked CanIcomSignalMask value of the received signal (CanIcomSignalRef).

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Max-value

18446744073709551615

Min-value

0

4.2.9.1.12.4. CanIcomSignalRef

Item

Name

CanIcomSignalRef

Description

This parameter defines a reference to the signal which shall be checked additional to the message id (CanIcomMessageId).

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.2.9.2. CanGeneral

This container contains the parameters related each CAN Driver Unit.

4.2.9.2.1. CanDevErrorDetect

Item

Name

CanDevErrorDetect

Description

Switches the Development Error Detection and Notification ON or OFF.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.2.9.2.2. CanDeInitApi

Item

Name

CanDeInitApi

Description

Adds / removes the service Can_DeInit() from the code.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.2.9.2.3. CanIndex

Item

Name

CanIndex

Description

Specifies the InstanceId of this module instance. If only one instance is present it shall have the Id 0.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

4.2.9.2.4. CanLPduReceiveCalloutFunction

Item

Name

CanLPduReceiveCalloutFunction

Description

This parameter defines the existence and the name of a callout function that is called after a successful reception of a received CAN Rx L-PDU. If this parameter is omitted no callout shall take place.

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.2.9.2.5. CanMainFunctionBusoffPeriod

Item

Name

CanMainFunctionBusoffPeriod

Description

This parameter describes the period for cyclic call to Can_MainFunction_Busoff. Unit is seconds.

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

10.0

Max-value

65.535

Min-value

0.001

4.2.9.2.6. CanMainFunctionModePeriod

Item

Name

CanMainFunctionModePeriod

Description

This parameter describes the period for cyclic call to Can_MainFunction_Mode. Unit is seconds.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

10.0

Max-value

65.535

Min-value

0.001

4.2.9.2.7. CanMainFunctionReadPeriod

Item

Name

CanMainFunctionReadPeriod

Description

This parameter describes the period for cyclic call to Can_MainFunction_Read. Unit is seconds.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Max-value

65.535

Min-value

0.001

4.2.9.2.8. CanMainFunctionWritePeriod

Item

Name

CanMainFunctionWritePeriod

Description

This parameter describes the period for cyclic call to Can_MainFunction_Write. Unit is seconds.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Max-value

65.535

Min-value

0.001

4.2.9.2.9. CanSetBaudrateApi

Item

Name

CanSetBaudrateApi

Description

The support of the Can_SetBaudrate API is optional.If this parameter is set to true the Can_SetBaudrate API shall be supported. Otherwise the API is not supported.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.2.9.2.10. CanTimeoutDuration

Item

Name

CanTimeoutDuration

Description

Specifies the maximum time for blocking function until a timeout is detected. Unit is in clock ticks. Configure the timeout according to r5f clock frequency(200MHz/400MHz)

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

10.0

Max-value

65.535

Min-value

0.001

4.2.9.2.11. CanDefaultOSCounterId

Item

Name

CanDefaultOSCounterId

Description

Default Os Counter Id if node reference to OsCounter ref CanOsCounterRef is not set

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

16

Min-value

0

4.2.9.2.12. CanVersionInfoApi

Item

Name

CanVersionInfoApi

Description

Switches the Can_GetVersionInfo() API ON or OFF.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.2.9.2.13. CanMaxNrOfTxObjects

Item

Name

CanMaxNrOfTxObjects

Description

Number of Transmit Objects

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

3

Max-value

3

Min-value

0

4.2.9.2.14. CanTypeofInterruptFunction

Item

Name

CanTypeofInterruptFunction

Description

Type of ISR function

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CAN_ISR_CAT2

Range

CAN_ISR_VOID
CAN_ISR_CAT1
CAN_ISR_CAT2

4.2.9.2.15. CanRegisterReadbackAPI

Item

Name

CanRegisterReadbackAPI

Description

Enable/Disable configuration readback safe TI API.If this parameter is set to true the readback API shall be supported. Otherwise the API is not supported.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.2.9.2.16. CanLoopBackTest_Enable

Item

Name

CanLoopBackTest_Enable

Description

Enable/Disable LoopBack test API.If this parameter is set to true the LoopBack mode shall be supported which is used for internal testing. Otherwise the API is not supported.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.2.9.2.17. CanOsCounterRef

Item

Name

CanOsCounterRef

Description

This parameter contains a reference to the OsCounter, which is used by the CAN driver.

Multiplicity-Configuration-Class

–

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.2.9.2.18. CanSupportTTCANRef

Item

Name

CanSupportTTCANRef

Description

The parameter refers to CanIfSupportTTCAN parameter in the CAN Interface Module configuration.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.2.9.2.19. CanIcomGeneral

This container contains the general configuration parameters of the ICOM Configuration.

4.2.9.2.19.1. CanIcomVariant

Item

Name

CanIcomVariant

Description

Defines the variant, which is supported by this CanController

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CAN_ICOM_VARIANT_NONE

Range

CAN_ICOM_VARIANT_HW
CAN_ICOM_VARIANT_NONE
CAN_ICOM_VARIANT_SW

4.2.9.2.20. CanMainFunctionRWPeriods

This container contains the parameter for configuring the period for cyclic call to Can_MainFunction_Read or Can_MainFunction_Write depending on the referring item.

4.2.9.2.20.1. CanMainFunctionPeriod

Item

Name

CanMainFunctionPeriod

Description

This parameter describes the period for cyclic call to Can_MainFunction_Read or Can_MainFunction_Write depending on the referring item. Unit is seconds

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0.001

Max-value

65.535

Min-value

0.001

4.2.9.3. Steps To Configure Can Module

  1. Open EB Tresos configurator tool and load Port, Mcu and Can modules

  2. Open PORT module plugin and configure required pins as CAN-TX, CAN-RX

  3. Open CAN module plugin, Select the Config Variant (Pre-compile/Link-Time)

  4. In CAN module plugin configure required parameters.

  5. Save the configuration and generate the configuration.

4.2.10. Examples

4.2.10.1. Overview

  1. By default, the CAN example runs in Loop Back mode.

  2. For AM263x:

    • All 4 CAN Controllers transmit the data and then receive it through the Interrupt Service Routine (ISR).

    • After receiving the data, it is compared with the transmitted data.

  3. If the received data mismatches the transmitted data, then the application fails.

  4. External Loop back mode can be enabled by setting “CAN_LOOPBACK_ENABLE” in Can_Cfg.h to STD_OFF.

  5. In External Loop Back mode, CAN communication can be tested using the PCAN debugger.

  6. For AM263x “PROC110E2A” board:

    • MCAN1 pins are popped out, and MCAN1 is configured with a 1Mbps nominal bit-rate and 5 Mbps data bit-rate.

  7. While running the example code in External Loop back mode:

    • First, it asks to select the CAN instance, where “m” corresponds to MCAN1/MCANB.

    • Then it asks to select the interrupt or polling method.

    • If interrupts are enabled for the instance in Can_PBcfg.c, then select the interrupt (“i”) method; otherwise, choose the Polling (“p”) method.

    • After selecting the method, options for transmission and reception will appear.

    • If the user chooses the transmit option, they are further prompted to select between standard and extended frames.

    • Selecting the standard option transmits a Standard CAN frame, while choosing the extended option transmits an extended frame to PCAN.

  8. In receive mode, the controller is ready to receive CAN frames from PCAN.

4.2.10.2. Hardware Software Setup and Tools

  1. Locate the CAN-H and CAN-L pins on both the PCAN device and the board. Refer to the documentation or user manual for both the PCAN device and the board to find the correct pins.

  2. Select appropriate cables with the necessary connectors to connect between the PCAN device and the board. Ensure the cables have the correct connectors to fit securely into both the PCAN device and board’s connectors.

CAN Hardware Connectivity with PCAN USB

Fig. 4.24 CAN Hardware Connectivity with PCAN USB

  1. Connect the CAN-H pin from the PCAN device to the corresponding CAN-H pin on the board using the chosen cable.

  2. Connect the CAN-L pin from the PCAN device to the corresponding CAN-L pin on the board using the chosen cable.

  3. Place a 120-ohm resistor between the CAN-H and CAN-L lines at the board end.

  4. The resistor should be connected in parallel between the CAN-H and CAN-L lines, creating a termination point.

  5. Open the PCAN configuration software on your PC. The software is usually provided by the manufacturer of the PCAN device.

  6. Locate the settings for bit rate configuration.

  7. Set the nominal bit rate to 1 Mbps and the data bit rate to 5 Mbps.

  8. Apply the changes and save the configuration.

  9. Ensure all connections are secure and properly plugged into their respective connectors on both the PCAN device and the board.

  10. Before powering on the system, double-check all connections to ensure they are correctly made, and there are no loose or improperly connected cables.

  11. After making the connections and configuring the PCAN device, power on both the board and the PCAN device.

  12. Once the system is powered on, verify that the CAN communication is established between the board and the PCAN device.

4.2.10.3. Steps to build and run example

  1. CAN example application demonstrating the MCAL CAN driver features is in folder <MCAL_ROOT>/examples/Can.

  2. This application can be built from the build folder by giving “gmake –s can_app PLATFORM=am263.”

  3. Once the build is completed we get a binary file, which is loaded in our controller and executed.

4.2.10.4. Configuration used to test this example

  1. All 4 Instances of CAN are configured.

  2. All CAN controllers are configured with 1Mbps Arbitration bit rate and 5 Mbps of Data bit rate.

  3. In total 16 Hardware Objects are configured, For each CAN controller 2 HTH and 2 HRH.

  4. In Default example for Reception 0xC1 ID filter is configured for Polling Mode and 0xC0 ID filter is configured for Interrupt mode.

  5. Please refer configuration parameters in below images for baudrate update

For 1Mbps and 5Mpbs:

../_images/can_image9.png
../_images/can_image10.png

For 500Kbps and 2.5Mpbs:

../_images/can_image11.png
../_images/can_image12.png

4.2.10.5. Example Logs


    CanApp: Sample Application - STARTS !!!
    CanAppgCanAppMcuClockConfig[0].Mcu_ClockSourceId = 4 gCanAppMcuClockConfig[0].Mcu_ClockDiv = 4  
    CanApp: CAN Loopback test 
    CanApp: Can Controller: MCAN0
    CanAppCalling Can_Write 
    CanAppCan_Write ok 
    CanApp: Test Passed
    CanApp: Can Controller: MCAN1
    CanAppCalling Can_Write 
    CanAppCan_Write ok 
    CanApp: Test Passed
    CanApp: Can Controller: MCAN2
    CanAppCalling Can_Write 
    CanAppCan_Write ok 
    CanApp: Test Passed
    CanApp: Can Controller: MCAN3
    CanAppCalling Can_Write 
    CanAppCan_Write ok 
    CanApp: Test Passed
    CAN Stack Usage: 764 bytes
    CAN Test Passed!!!


4.2.10.6. File Structure

📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Can
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜CanApp.c : Contains CAN test example.
┃ ┃ ┃ ┣ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Can_Demo_Cfg
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am263
┃ ┃ ┃ ┃ ┃ ┣ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Can_Cfg.h : Contains the Precompile switches, Macros for CAN controllers, Hardware Objects etc.
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Can_Cfg.c : Contains all controllers Pre-Compile Configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Can_PBcfg.c : Contains all controllers Post-Build Configuration parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┣ 📜README.txt

Note

Can_PBcfg.c and Can_Cfg.c will be present if Post-Build config variant is selected, only Can_Cfg.c will be present if Pre-Compile variant is selected

4.2.11. FAQ’s

Bit rate Calculation

4.2.12. References

AUTOSAR_SWS_CANDriver
Technical Reference Manual