4.18. PORT Module
4.18.1. Acronyms and Definitions
Abbreviation/Term |
Explanation |
|---|---|
AUTOSAR |
Automotive Open System Architecture |
RTE |
Runtime Environment |
BSW |
Basic Software |
GPIO |
General Purpose Input Output |
ADC |
Analogue Digital Converter |
MCU |
Micro Controller Unit |
OS |
Operating System |
API |
Application Programming Interface |
HW |
Hardware |
SW |
Software |
4.18.2. Introduction
This document describes MCAL PORT Driver functionality, its application interfaces and configuration details as per AUTOSAR version 4.3.1
Supported AUTOSAR Release |
4.3.1 |
Supported Configuration Variants |
Pre-Compile, Post-build |
Vendor ID |
PORT_VENDOR_ID (44) |
Module ID |
PORT_MODULE_ID (124) |
Supported Platform |
AM263x |
4.18.3. Functional Overview
The Port driver module is an I/O driver in AUTOSAR Basic Software (BSW) layer. PORT driver provide the services for initializing the whole PORT structure of the microcontroller. It is used to assign various functionalities to Port and port pins (e.g. GPIOs, ADC, SPI and other peripheral modes)
4.18.3.1. PORT Driver Architecture
The following figure shows where the PORT is located in the AUTOSAR architecture
Fig. 4.82 PORT in AUTOSAR architecture
4.18.3.2. Initialization
Port_Init API initializes the PORT driver and does pin configuration of specified PORT PIN Id’s. Port_Init also enables all pins for specified module selected in the config structure passed to Port_Init.
4.18.3.3. States
No state is maintained in the PORT driver.
4.18.3.4. Assumptions
None
4.18.3.5. Limitations
The Pins which are configured as GPIO, the parameter “PortInputOverrideCtrl” and “PortOutputOverrideCtrl” should be as disabled.
Fig. 4.83 Configuration settings
4.18.3.6. Design overview
Please refer SITARA MCU MCAL Architecture Document and AM26x MCAL: PORT Detailed Design Document provided as part of CSP.
4.18.4. Hardware Features
4.18.4.1. IP Supported Features
Configuring the pins for rising and/or falling edge, specified for each GPIO pin.
Configuring the GPIO signal conditioning chain
Invert/Non-invert
Signal Qualification:
Asynchronous input
Synchronize to SYSCLK
Qualification using sampling window
Enabling all pins of specified peripheral for given mode of operation. This option provides a way configuring all pins for a peripheral for required mode of operation.
GPIO Channel/Bank Interrupt notification is supported for Rising, Falling and Both edge interrupts.
4.18.4.2. AUTOSAR Supported Features
The PORT Driver module shall initialize the whole port structure of the microcontroller.
The PORT Driver module shall allow the configuration of different functionality for each port and port pin. e.g. ADC, SPI, DIO etc.
The PORT Driver module shall provide additional configurations for the MCU port/port pins:
Pin direction (input/output)
Pin level initial value
Pin direction changeable during runtime (yes/no)
Port mode changeable during runtime
The PORT Driver module shall provide a number of optional configurations for the MCU ports and port pins (if supported by hardware):
Slew rate control
Activation of internal pull-ups
Type of Readback support (pin level,output register value)
4.18.4.3. Not Supported Features
None
4.18.5. Source files
Description of static files is provided below:
📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Port
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┗ 📜Port.h : Contains the API’s of the PORT driver to be used by upper layers
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┗ 📜Port.c : Contains the implementation of the API’s for PORT driver
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┣ 📜Port_Irq.h : Contains ISR function declaration
┃ ┃ ┃ ┣ 📜Port_Irq.c : Contains ISR function definitions
┃ ┃ ┃ ┣ 📜Port_Priv.c : Contains Internal functions definition of PORT driver
┃ ┃ ┃ ┗ 📜Port_Priv.h : Contains Internal functions declaration of PORT driver
┃ ┃ ┗ 📜Makefile
┣ 📂mcal_config
┣ 📂mcal_docs
┗ 📜README.txt
Description of generated files is provided below:
Plugin Files |
Descriptions |
|---|---|
Port_Cfg.h |
Contains the Precompile switches, Symbolic names of PortPin |
Port_PBcfg.c |
Contains all pins Post-Build Configured parameters |
Port_Cfg.c |
Contains all pins Pre-Compile Configured parameters |
Fig. 4.84 PORT header file include structure
4.18.6. Module requirements
Please refer Software Product Specification document provided as part of CSP.
4.18.6.1. Memory Mapping
Memory Mapping Sections |
PORT_CODE |
PORT_VAR_ZERO_INIT |
PORT_PBCFG |
|---|---|---|---|
PORT_START_SEC_VAR_INIT_UNSPECIFIED (.data) |
x |
||
PORT_STOP_SEC_VAR_INIT_UNSPECIFIED |
x |
||
PORT_START_SEC_CODE (.bss) |
x |
||
PORT_STOP_SEC_CODE |
x |
||
PORT_START_SEC_CONFIG_DATA (.data) |
x |
||
PORT_STOP_SEC_CONFIG_DATA |
x |
||
PORT_START_SEC_ISR_CODE (.bss) |
x |
||
PORT_STOP_SEC_ISR_CODE |
x |
4.18.6.2. Scheduling
4.18.6.2.1. SchM
Beside the OS the BSW Scheduler provides functions that module PORT calls at begin and end of critical sections.
4.18.6.2.2. Critical Sections
There is only one kind of critical sections in this driver. Within these sections all read /modify / write accesses to internal MCU status variables must be protected. This is handled internally in the driver by invoking SchM_Enter_Port_PORT_EXCLUSIVE_AREA_0()/SchM_Exit_Port_PORT_EXCLUSIVE_AREA_0().
4.18.6.3. Error handling
4.18.6.3.1. Development Error Reporting
The module PORT depends on the DET (by default) in order to report development errors. Detection and reporting of development errors can be enabled or disabled by the switch PORT_DEV_ERROR_DETECT = STD_ON in the Port_Cfg.h
AUTOSAR requires that API functions shall check the validity of their respective parameters. These checks are for development error reporting and can be enabled or disabled.
4.18.6.4. Error Code
4.18.6.4.1. Development Errors
The errors reported to DET module are described in the following table:
Type of Error |
Related Error code |
Value (Hex) |
|---|---|---|
Invalid Port Pin ID requested. |
PORT_E_PARAM_PIN |
0x0A |
Port Pin not configured as changeable. |
PORT_E_DIRECTION_UNCHANGEABLE |
0x0B |
API Port_Init service called with wrong parameter. |
PORT_E_INIT_FAILED |
0x0C |
API Port_SetPinMode service called when mode is unchangeable.Invalid Mode Passed |
PORT_E_PARAM_INVALID_MODE |
0x0D |
API Port_SetPinMode service called when mode is unchangeable |
PORT_E_MODE_UNCHANGEABLE |
0x0E |
API service called without module initialization. |
PORT_E_UNINIT |
0x0F |
API called with a Null Pointer. |
PORT_E_PARAM_POINTER |
0x10 |
4.18.6.4.2. DEM Errors
The extended production errors reported to DEM module are described in the following table:
Error Code |
Description |
|
|---|---|---|
Assigned by DEM |
PORT_E_HARDWARE_ERROR |
This error is raised when register write failure occurs.(Hardware Failure) |
4.18.7. Used resources
4.18.7.1. Interrupt Handling
4.18.7.1.1. GPIO Interrupts
Individual channel Interrupt can be configured with particular channel and it’s being used to detect the rising/falling/both edge occurred on configured channel.
Bank channel Interrupt are the interrupt that can be configured with particular bank and it’s being used to detect the rising/falling/both edge occurred on all channels in configured bank.
Below are the four GPIO XBAR interrupts available.
GPIO Interrupt |
|---|
GPIO XBAROUT14 INTR |
GPIO XBAROUT15 INTR |
GPIO XBAROUT16 INTR |
GPIO XBAROUT17 INTR |
The above mentioned 4 GPIO XBAR interrupts should be mapped to Software ISR’s mentioned below:
For Individual Channel Interrupt: Port_Ch<n>Isr , here <n> is between 0 to 138.
For Bank Interrupt: Port_Bnk<m>Isr , here <m> is between 0 to 8.
These all four GPIO cross bar interrupt source can be configured either Individual channel Interrupt or Bank interrupt.
Each GPIO pin is interrupt capable and can be configured in PortDioConfig container in PORT Plugins as shown below.
The PORT module depends on MCU module for the configuration of Channel/Bank Interrupt. All above 4 GPIO interrupts should be configured by MCU driver before usage. McuGpioXbarIntrConfiguration container from MCU plugins can be used to do to the same.
GPIO interrupt API’s:
APIs |
Description |
|---|---|
Port_PinEnableIntrNotification |
This function is Non- Autosar based and is used to enable bank/channel GPIO Interrupts for particular channel |
Port_PinDisableIntrNotification |
This function is Non- Autosar based and is used to disable bank/channel GPIO Interrupts for particular channel |
Port_GetInterruptStatus |
This function is Non- Autosar based and is used to collect interrupt register value for each GPIO bank |
Port_ClearInterruptStatus |
This function is Non- Autosar based and is used to clear interrupt register for each GPIO bank |
Note
Mcu Plugins should be added with Port Plugins while Port configuration files generation.
Each used channel in PortDioConfig container should be configured as a GPIO with INPUT direction.
Please refer PORT Example Application to know more about GPIO Interrupt feature configuration and its usage.
4.18.7.1.2. Hardware - Software - ISR API name mapping
For interrupt notification, ISR is provided in PORT driver. The following interrupt is generated by PORT module. The supported ISR is a part of the Port_Irq.h file.
Following are PORT module ISR’s:
For Individual Channel Interrupt: Port_Ch<\n>Isr , here <n> is between 0 to 138.
For Bank Interrupt: Port_Bnk<m>Isr , here <m> is between 0 to 8.
4.18.7.2. Hardware-Software Mapping
4.18.7.2.1. GPIO Channels Mapping
AM263x have total 139 GPIO pins available which allocated from Bank A(Bank 0) to Bank I(Bank 8). Each Bank contains 16 channels except Bank I(Bank 8).
Bank I contains the 11 channels.
GPIO Banks |
GPIO Channels |
|---|---|
BankA / Bank0 |
Channel 0 to channel 15 |
BankB / Bank1 |
Channel 16 to channel 31 |
BankC / Bank2 |
Channel 32 to channel 47 |
BankD / Bank3 |
Channel 48 to channel 63 |
BankE / Bank4 |
Channel 64 to channel 79 |
BankF / Bank5 |
Channel 80 to channel 95 |
BankG / Bank6 |
Channel 96 to channel 111 |
BankH / Bank7 |
Channel 112 to channel 127 |
BankI / Bank8 |
Channel 128 to channel 138 |
4.18.8. Integration description
4.18.8.1. Dependent modules
4.18.8.1.1. DET
This implementation depends on the DET in order to report development errors. The detection of development errors is configurable (ON / OFF). The switch PORT_DEV_ERROR_DETECT will activate or deactivate the detection of all development errors.
4.18.8.1.2. DEM
Note
Dem Event is enable only if $(Module_Name)DemEventParameterRefs is enabled.
4.18.8.1.3. Callback Notification
Notifications:
As it is a configurable interface, the PORT defines notifications that can be mapped to callback functions provided by other modules. The mapping is not statically defined by the PORT but can be performed at configuration time. The function prototypes that can be used for the configuration have to match the appropriate function prototype signatures, described below:
PortDioInterruptNotification:
This is of type Port_IsrNotificationType which is defined in Port_Cfg.h file. This is called to notify the group about the completion of the requested conversion and availability of the conversion results.
4.18.8.2. Multi-core and Resource allocator
Not Supported
4.18.9. Configuration
4.18.9.1. Configuration Variants
The PORT can be configured as Post-Build or Pre-Compile variant, using EB tresos tool.
Variants |
Generated Files |
|---|---|
PostBuild |
Port_PBcfg.c , Port_Cfg.h |
Pre-Compile |
Port_Cfg.c , Port_Cfg.h |
4.18.9.2. Parameter Description
4.18.9.2.1. Standard Configuration
Standard Parameters |
Description |
Default Value(AM263X) |
Range(AM263X) |
Unit/Datatype |
|---|---|---|---|---|
PortNumberOfPortPins |
The number of specified PortPins in this PortContainer |
NA |
1..65535 |
Integer |
PortPinId |
Pin Id of the port pin. This value will be assigned to the symbolic name derived from the port pin container short name. |
NA |
1..144 |
Integer |
PortPinDirection |
The initial direction of the pin (IN or OUT). If the direction is not changeable, the value configured here is fixed. |
PORT_PIN_DEFAULT |
PORT_PIN_IN PORT_PIN_OUT PORT_PIN_DEFAULT |
Enumeration |
PortPinDirectionChangeable |
Parameter to indicate if the direction is changeable on a port pin during runtime. |
FALSE |
TRUE/ FALSE |
Boolean |
PortPinInitialMode |
Port pin mode from mode list for use with Port_Init() function. |
NA |
1..104 |
Enumeration |
PortPinLevelValue |
Port Pin Level value from Port pin list. |
PORT_PIN_LEVEL_HIGH |
PORT_PIN_LEVEL_HIGH PORT_PIN_LEVEL_LOW |
Enumeration |
PortPinMode |
Port pin mode from mode list. |
NA |
1..104 |
Enumeration |
PortPinModeChangeable |
Parameter to indicate if the mode is changeable on a port pin during runtime. True: Port Pin mode changeable allowed. False: Port Pin mode changeable not permitted. |
FALSE |
TRUE/ FALSE |
Boolean |
PortDevErrorDetect |
Switches the Development Error Detection and Notification on or off |
TRUE |
TRUE/ FALSE |
Boolean |
PortSetPinDirectionApi |
Pre-processor switch to enable / disable the use of the function Port_SetPinDirection(). |
TRUE |
TRUE/ FALSE |
Boolean |
PortSetPinModeApi |
Pre-processor switch to enable / disable the use of the function Port_SetPinMode(). |
TRUE |
TRUE/ FALSE |
Boolean |
PortVersionInfoApi |
Pre-processor switch to enable / disable the API to read out the modules version information. |
TRUE |
TRUE/ FALSE |
Boolean |
PortRefreshPortDirectionApi |
Pre-processor switch to enable / disable the API to refresh the port direction. |
TRUE |
TRUE/ FALSE |
Boolean |
4.18.9.2.2. IP Specific Configuration
Standard Parameters |
Description |
Default Value(AM263X) |
Range(AM263X) |
Unit/Datatype |
|---|---|---|---|---|
PortPinPeripheral |
Select peripheral of interest to narron down list of pins of interest. |
NA |
List of peripherals in HW, Refer TRM for more details |
Enumeration |
PortPinPeripheralSignal |
Select specific peripheral signal pin of interest |
NA |
List of signals for each peripheral, Refer TRM for more details |
Enumeration |
PortPinName |
PAD IO name of the selected pin |
NA |
List of Port pin names, Refer TRM for more details |
Enumeration |
PortPinIdAddr |
Pin Id of the port pin. This value will be assigned to the symbolic name derived from the port pin container short name. |
NA |
NA |
String |
PortPinInhibitEnable |
The port pin inhibit enable. |
PORT_PIN_PULL_INHIBIT_DEFAULT |
PORT_PIN_PULL_INHIBIT_ENABLE PORT_PIN_PULL_INHIBIT_DISABLE PORT_PIN_PULL_INHIBIT_DEFAULT |
Enumeration |
PortPullTypeSelect |
Type of PULL U/D selection |
PORT_PIN_PULLTYPE_DEFAULT |
PORT_PIN_PULLTYPE_PULLDOWN PORT_PIN_PULLTYPE_PULLUP PORT_PIN_PULLTYPE_DEFAULT |
Enumeration |
PortSlewControlSelect |
Slew control configuration |
PORT_PIN_SLEWCONTROL_DEFAULT |
PORT_PIN_SLEWCONTROL_FAST_SLEW PORT_PIN_SLEWCONTROL_SLOW_SLEW PORT_PIN_SLEWCONTROL_DEFAULT |
Enumeration |
PortInputOverrideCtrl |
Port inputOverride control |
PORT_PIN_INPUT_RETAIN_HW_CTRL |
PORT_PIN_DISABLE_INPUT_OVERRIDE PORT_PIN_ENABLE_INPUT_OVERRIDE PORT_PIN_INPUT_RETAIN_HW_CTRL |
Enumeration |
PortOutputOverrideCtrl |
Port OutputOverride control |
PORT_PIN_OUTPUT_RETAIN_HW_CTRL |
PORT_PIN_DISABLE_OUTPUT_OVERRIDE PORT_PIN_ENABLE_OUTPUT_OVERRIDE PORT_PIN_OUTPUT_RETAIN_HW_CTRL |
Enumeration |
PortDioPinNumber |
Port GPIO Pin Number (0 to 138) |
0 |
Will be calculated |
Integer |
PortDioEdgeTrigger |
EdgeTrigger Interrupt Selection |
PORT_FALLING_EDGE |
PORT_RISING_EDGE PORT_FALLING_EDGE PORT_BOTH_EDGE |
Enumeration |
PortPinSelectInterruptType |
Select Interrupt type |
PORT_BANK_INTR |
PORT_BANK_INTR / PORT_CHANNEL_INTR |
Enumeration |
PortDioInterruptNotification |
Definition of the Callback function. |
NULL_PTR |
NA |
Function Name |
PortMcuGpioXbarReference |
Reference to the McuGpioXbarIntrConfiguration container (Each channel configuration should be linked to respective interrupt which is configured by MCU driver.) |
NULL |
It is calculated based on McuGpioXbarIntrConfiguration container data |
REFERENCE |
PortDeviceVariant |
Select SOC variant .This parameter shall be used by driver to impose device specific constraints. The user guide shall detail the device specific constraints |
AM263X |
AM263X |
Enumeration |
PortDefaultOSCounterId |
Default Os Counter Id if node reference to OsCounter ref PortOsCounterRef is not set |
0 |
0..16 |
Integer |
PortSafeTIApi |
Enable/Disable SAFETI Configuration register readback. |
TRUE |
TRUE/ FALSE |
Boolean |
PortEnableIntrApi |
Pre-processor switch to enable / disable the use of Interrupt Functionality |
TRUE |
TRUE/ FALSE |
Boolean |
PortGetIntrStatusApi |
Pre-processor switch to enable / disable the use of Port_GetInterruptStatus API |
TRUE |
TRUE/ FALSE |
Boolean |
PortClearIntrStatusApi |
Pre-processor switch to enable / disable the use of PortClearIntrStatusApi API |
TRUE |
TRUE/ FALSE |
Boolean |
PortTimeoutDuration |
PORT timeout - used in PORT busy wait |
32000 |
1..4294967295 |
Integer |
PortTypeofInterruptFunction |
Type of ISR function |
PORT_ISR_CAT1 |
PORT_ISR_VOID PORT_ISR_CAT1 PORT_ISR_CAT2 |
Enumeration |
Note
GPIO usage for the cores other than R5F0_0 If AUTOSAR MCAL is running on cores other than R5F0_0, user need to take care of following configuration
R5F CPU ownership of GPIO.
0 -> R5FSS0 Core0
1 -> R5FSS0 Core1
2 -> R5FSS1 Core0
3 -> R5FSS1 Core1
Note
PortDioConfig container is specifically used only to configure the GPIO interrupt feature parameters.
To use the GPIO interrupt feature, user should configure the required GPIO channels in PortDioConfig container.
4.18.9.3. Symbolic Names deviations
None.
4.18.9.4. Configuration rules and constraints to enable possibility checks
Will be updated in future release:
4.18.9.5. Steps To Configure Port Module
Open EB Tresos configurator tool and Select the Config Variant ( Precompile/Post-Build) and Device Variant ( Pin Package ) parameters
Go to Port Container tab and create a new container
Open the created container and go to PortPin container to create a portPin configuration. ( Multiple PortPin configurations can be created )
Open the created Port pin, and configure the pin parameters
Select the Port pin peripheral instance ( Mode ) which needs to be configured and accordingly select the Peripheral Signal. As per selected Signal, physical pin ID needs to be selected from the list
Configure the other parameters as per pin usage.
Open Port pin Mode tab and add the default port pin mode ( at least one mode is required for this field ). Other supported modes for that pin can also be configured if user needs to change the mode for the pin afterwards.
Configure the number of port pins in port container general tab
Save the configuration and generate the configuration.
4.18.10. Examples
The example application demonstrates use of Port module, the list below identifies key steps performed in the example.
4.18.10.1. Overview
Will be updated in future release:
4.18.10.2. Setup required to run example
Will be updated in future release:
4.18.10.3. How to run examples
4.18.10.3.1. Steps to build and run example
PORT example application demonstrating the MCAL PORT driver features is in folder <MCAL_ROOT>/examples/Port.
This application can be built from the root folder by giving gmake –s port_app PLATFORM=am263.
Once the build is completed we get a binary file, which is loaded in our controller and executed.
4.18.10.3.2. External set up Information
PORT module is tested using CC board (PROC111E2).
4.18.10.3.3. Configuration used to test this example
Pin configurations : Following pins are configured as a GPIO and used in example application to test.
Pin Ball Number |
Pin Signal Name |
|---|---|
C15 |
GPIOGH_120 |
B8 |
GPIOAB_21 |
4.18.10.4. Sample Log
CLANG compiled : portApp: Sample Application - STARTS !!!
Port Driver version info:9.0.1
Port Driver Module/Driver:124.44
[GPIO INTR verification] => Press SW1 switch on board to trigger the interrupt
Interrupt -- Bank Number : 1 GpioChannelNum : 255 Edge : 1
Pin Value for channel 120 : 1
Dio_FlipChannel(channel_120)
Pin Value for channel 120 : 0
Dio_FlipChannel(channel_120)
Pin Value for channel 120 : 1
Pin Value for channel 120 : 1
Dio_FlipChannel(channel_120)
Pin Value for channel 120 : 1
PORT Test Passed!!!
4.18.10.5. File Structure
📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Port
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜Portapp.c : Contains Port test example
┃ ┃ ┃ ┗ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Port_Demo_Cfg
┃ ┃ ┃ ┗ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am263
┃ ┃ ┃ ┃ ┃ ┗ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Port_Cfg.h : Contains the configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┗ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣📜Port_Cfg.c : Contains all Pre-Compile Configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣📜Port_PBcfg.c : contains all Post build configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣📜Port_PBcfg_Intr.c : Contains all Post Build Configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Port_PBcfg_UART0.c : contains all Post Build configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┗ 📜README.txt
4.18.10.6. Test Report
Please refer AM26x PORT Driver Test Case Report as part of CSP provided in the release package.