4.1. ADC Module

4.1.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

BSW

Basic Software

MCAL

Micro Controller Abstraction Layer

API

Application Programming Interface

ADC

Analogue Digital Converter

DET

Default Error Tracer

MCU

Micro Controller Unit

OS

Operating System

SW

Software

HW

Hardware

ISR

Interrupt Service Routine

SPS

Samples Per Second

SOC

Start of Conversion

EOC

End of Conversion

INT

Interrupt

4.1.2. Introduction

This document describes MCAL ADC Driver functionality, its application interfaces and configuration details as per AUTOSAR version 4.3.1 .

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Pre-Compile & Post Build

Vendor ID

ADC_VENDOR_ID (44)

Module ID

ADC_MODULE_ID (123)

Supported Platform

AM263x

4.1.3. Functional Overview

The ADC module initiates analog to digital conversion requests and provides the conversion results for external analog monitoring channels and internally connected digital temperature sensors. It provides services to start, stop and read conversion results for configurable ADC groups consisting of one or more external analog monitoring channels.

4.1.3.1. ADC Driver Architecture

The following figure shows where the ADC is located in the AUTOSAR architecture

ADC in AUTOSAR architecture

Fig. 4.1 ADC in AUTOSAR architecture

The ADC hardware module is a successive approximation (SAR) style ADC. This ADC is composed of a core and a wrapper. The core is composed of the analog circuits which include the channel select MUX, the sample-and hold (S/H) circuit, the successive approximation circuits, voltage reference circuits, and other analog support circuits. The wrapper is composed of the digital circuits that configure and control the ADC. These circuits include the logic for programmable conversions, result registers, interfaces to analog circuits, interfaces to the peripheral buses, post-processing circuits, and interfaces to other on-chip modules. Each ADC module consists of a single sample-and-hold (S/H) circuit. The ADC module is designed to be duplicated multiple times on the same chip, allowing simultaneous sampling or independent operation of multiple ADCs.

ADC Hardware Overview

Fig. 4.2 ADC Hardware Overview

System Overview

Fig. 4.3 System Overview

4.1.3.2. Initialization

Adc_Init() has to be called to initialize the ADC driver before initiating any group conversion. This will also set all the groups to ADC_IDLE state.

4.1.3.3. States

There are 4 states in which each ADC group for one shot single access mode can be:

  1. ADC_IDLE: This is the state before starting a group, no conversion request for the group has been initiated or after the conversion result of a stream completed group is read.

  2. ADC_BUSY: This is the state after a group is started but hasn’t finished i.e. conversion result for the group is not yet available.

  3. ADC_COMPLETED: This is the state after a group has finished first or more samples of ADC analog input.

  4. ADC_STREAM_COMPLETED: This is the state after a group has finished i.e., conversion result for the group is available.

ADC State Diagram - 1

Fig. 4.4 ADC State Diagram - 1

ADC State Diagram - 2

Fig. 4.5 ADC State Diagram - 2

4.1.3.4. Assumptions

Below listed are assumed to valid for this design/implementation, exceptions and other deviations are listed for each explicitly. Care should be taken to ensure these assumptions are addressed.

  1. ADC module requires system clock to be in operation.

  2. ADC module is not dependent on PORT module for Configuration of ADC Port pins.

  3. Configuration of ADC cross bar interrupts shall be configured in MCU module.

  4. ADC data buffer control for each hardware unit is handled by MCU module.

  5. For using DMA feature, driver assumes that cache initialization is done in application only and not done by the driver.

4.1.3.5. Limitations

Maximum 4 hardware triggered channel groups can be queued, when ADC Priority implementation ADC_PRIORITY_HW and ADC_PRIORITY_HW_SW.

Note

Hardware Triggered Channel Groups can be queued with ADC Priority implementation ADC_PRIORITY_HW and ADC_PRIORITY_HW_SW.

ADC Priority implementation ADC_PRIORITY_HW and ADC_PRIORITY_HW_SW requires all four Interrupts (ADC_INT1 to ADC_INT4) for conversion of ADC (In case of using queuing mechanism).

4.1.3.6. Design overview

4.1.3.6.1. ADC Hardware Description

ADC module is composed of

  1. Five Hardware units,

  2. Each Hardware unit has four ADC interrupt

  3. Each Hardware unit has Analog input channels ADCIN[0:5] ( have dedicated pins ).

  4. Each Hardware unit has 15 SOC’s (start of conversion units) for conversion of ADC channels.

SOC architecture

Fig. 4.6 SOC architecture

The analog channel which needs to be converted, needs to be placed in one of the SOC’s for conversion and result will be available is respective result register as shown in below figure. Based on trigger (either HW trigger or SW trigger), conversion shall be started for ADC HW Channel.

ADC Channel Conversion Process

Fig. 4.7 ADC Channel Conversion Process

4.1.3.6.2. Autosar ADC Design

The ADC Analog input channels are configured in container AdcChannel. The actual physical channel ID needs to be specified here.

The ADC Group consists of the combination of ADC channels. These Groups configured in container AdcHwUnit.

The below figure shows, how physical channels are mapped in Group.

ADC Channel Group Configuration

Fig. 4.8 ADC Channel Group Configuration

Since the conversion of ADC Channels is based on ADC Group in AUTOSAR, the ADC Groups are placed in SOC’s based on Group’s being called for conversion using autosar API’s:

Adc_StartGroupConversion for SW triggered groups

Adc_EnableHardwareTrigger for HW triggered groups

The below figure shows the group conversion process for AUTOSAR ADC module in ADC hardware:

ADC Channel Group Conversion Process

Fig. 4.9 ADC Channel Group Conversion Process

Here based on group priority the ADC Groups are allocated with SOC’s of Hardware unit. Lowest priority group will be at bottom of SOC and highest will be at TOP of SOC structure. If high priority group comes during execution of low priority group, the high priority Group shall be placed above the top of low priority SOC. If the priority mechanism is active, the ADC module shall handle channel group conversion requests for groups with the same priority level, in a ‘first come first served’ order.

4.1.3.6.3. Cross Bar Interrupt

There are four interrupts for each hardware unit of ADC module, which can be access through cross bar interrupt. There are 32 cross bar interrupts for AM263x, ADC modules can be mapped to any of these cross interrupts as per requirement.

The Mapping of ADC interrupts and cross bar interrupts are handled by MCU module configuration. (Refer section : MCU)

Same interrupt source number should be configured by application.

Interrupt Cross Bar List

Fig. 4.10 Interrupt Cross Bar List

4.1.3.6.4. ADC Polling Mechanism

In Polling Mechanism, we shall use the API Adc_PollingMainFunction. This API shall be responsible to change the group status and updated the group channelbuffer(which are configured as polling mode). The Function “Adc_PollingMainFunction”, shall be called periodically or else via using API “Adc_GetStatus”.

The consistency of the group channel results can be obtained via API function Adc_GetGroupStatus and Adc_ReadGroup.

Note

Cross bar Interrupts for ADC interrupt shall be configured in MCU module.

If priority mechanism is ADC_PRIORITY_NONE, only SW triggered groups can be configured and SW groups are stored in SW Queue as per priority.

Multiple HW trigger Group can be stored in SOC’s (Depending on channels configured in Group), if priority mechanism ADC_PRIORITY_HW_SW or ADC_PRIORITY_HW.

SW trigger Group are stored in SW Queue and HW triggered Group’s are allocated with SOC’s ( if group priority is higher then current executing group ).

Its recommended to disable all the ADC interrupts related of particular Hardware unit in the application, if ADC groups are configured in Polling mode.

In case of mixed mode setting is used (Polling and Interrupt mode together) then the conversion should be triggered one after the other.

4.1.4. Hardware Features

4.1.4.1. ADC IP Supported Features

  • 12-bit resolution

  • Single-ended signal conversions

  • Multiple trigger sources

  • Input multiplexer with up to 6 channels

  • 16 individually addressable result registers

  • Four flexible interrupts

  • Post-Processing Blocks:

    • Flag a high or low compare limit

4.1.4.2. AUTOSAR Supported Features

  • Software triggered one-shot conversion where the converted group consists of exactly one channel.

  • Hardware triggered one-shot conversion where the converted group consists of exactly one channel.

  • Continuous conversion where the converted group consists of exactly one channel.

  • Software triggered one-shot conversion where the converted group consists of more than one channel.

  • Hardware triggered one-shot conversion where the converted group consists of more than one channel.

  • Continuous conversion where the converted group consists of more than one channel.

  • Support for limit checking for all ADC hardware channels.

4.1.4.3. Not supported Features

ADC Hardware Features not supported:

  • Burst mode

  • External reference set by VREFHI and VREFLO pins

  • Differential mode support

  • Four post-processing blocks each with

    • Saturating offset calibration

    • Error from set-point calculation

    • Trigger-to-sample delay capture

Autosar Features not supported:

Support and management of HW low power states

4.1.5. Source files

Description of static files is provided below:

📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Adc
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┗ 📜Adc.h : Contains the API’s of the ADC driver to be used by upper layers
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┗ 📜Adc.c : Contains the implementation of the API’s for ADC driver
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┣ 📜Adc_Dbg.h : Contains debug variable declaration for ADC MCAL driver
┃ ┃ ┃ ┣ 📜Adc_Irq.c : Contains ISR function definitions
┃ ┃ ┃ ┣ 📜Adc_Irq.h : Contains ISR function declaration
┃ ┃ ┃ ┣ 📜Adc_Platform.c : Contains device specific function definition, data types and definitions
┃ ┃ ┃ ┣ 📜Adc_Platform.h : Contains device specific function definition, data types and definitions
┃ ┃ ┃ ┣ 📜Adc_Priv.c : Contains Internal functions definition of ADC driver
┃ ┃ ┃ ┣ 📜Adc_Priv.h : Contains Internal functions declaration of ADC driver
┃ ┃ ┃ ┣ 📜Adc_Reg.h : Contains definition of ADC Registers.
┃ ┃ ┃ ┣ 📜Adc_RegResult.h : Contains definition of ADC result Registers
┃ ┃ ┃ ┣ 📜Adc_Types.h : Contains the autosar data types and internal macro definitions
┃ ┃ ┃ ┣ 📜Adc_Utils.c : Utility functions implementation file. This file defines the helper functions like create, add and remove nodes
┃ ┃ ┃ ┗ 📜Adc_Utils.h : Utility functions implementation file. This file defines the helper functions like create, add and remove nodes
┃ ┃ ┗ 📜Makefile
┣ 📂mcal_config
┣ 📂mcal_docs
┗ 📜README.txt

Description of generated files is provided below:

Plugin Files

Description

Adc_Cfg.h

Contains the Precompile switches, Symbolic names of Group, channels and hardware units and Configured maximum number Groups and hardware units

Adc_PBcfg.c

Contains all channels Post-Build Configuration parameters

Adc_Cfg.c

Contains all channels Pre-Compile Configuration parameters

The below diagram shows the files structure for the ADC driver.

ADC header file include structure

Fig. 4.11 ADC header file include structure

4.1.6. Module requirements

Please refer Software Product Specification document provided as part of CSP.

4.1.6.1. Memory Mapping

Memory Mapping Sections

ADC_CODE

ADC_CODE_ISR

ADC_VAR_NO_INIT

ADC_VAR

ADC_CONST

ADC_PBCFG

ADC_START_SEC_VAR_INIT_UNSPECIFIED(.bss)

x

ADC_STOP_SEC_VAR_INIT_UNSPECIFIED

x

ADC_START_SEC_CONFIG_DATA (.const)

x

ADC_STOP_SEC_CONFIG_DATA

x

ADC_START_SEC_CODE(.text)

x

ADC_STOP_SEC_CODE

x

ADC_START_SEC_VAR_INIT_32(.bss)

x

ADC_STOP_SEC_VAR_INIT_32

x

ADC_START_SEC_VAR_NO_INIT_UNSPECIFIED(.data)

x

ADC_STOP_SEC_VAR_NO_INIT_UNSPECIFIED

x

ADC_START_SEC_ISR_CODE (.rodata)

x

ADC_STOP_SEC_ISR_CODE

x

4.1.6.2. Scheduling

4.1.6.2.1. SchM

Beside the OS the BSW Scheduler provides functions that module ADC calls at begin and end of critical sections.

4.1.6.2.2. Critical Sections

There is only one kind of critical sections in this driver. Within these sections all read /modify / write accesses to internal ADC driver data structures must be protected. Therefore switching to tasks that also access ADC has to be avoided and all ADC interrupts have to be suspended. This is handled internally by ADC Driver.

4.1.6.3. Error handling

4.1.6.3.1. Development Error Reporting

The module ADC depends on the DET (by default) in order to report development errors. The DET can be replaced optionally by an equivalent component which is responsible to recognize development errors, if no DET component is available.

The DET error is reported with Module ID.

4.1.6.4. Error codes

4.1.6.4.1. Development Errors

Type of Error

Related Error code

Value (Hex)

API service used without module initialization

ADC_E_UNINIT

0x0A

API service called during ongoing process

ADC_E_BUSY

0x0B

API service called while no conversion is ongoing

ADC_E_IDLE

0x0C

API service called ADC is already initialized

ADC_E_ALREADY_INITIALIZED

0x0D

API service called with incorrect configuration parameter

ADC_E_PARAM_CONFIG

0x0E

API service called with invalid data buffer

ADC_E_PARAM_POINTER

0x14

API service called with invalid group ID

ADC_E_PARAM_GROUP

0x15

API service called on a group with conversion mode configured as continuous

ADC_E_WRONG_CONV_MODE

0x16

API service called for group with wrong trigger source

ADC_E_WRONG_TRIGG_SRC

0x17

Enable/disable notification function for a group whose configuration set has no notification available

ADC_E_NOTIF_CAPABILITY

0x18

Conversion started and result buffer pointer is not initialized

ADC_E_BUFFER_UNINIT

0x19

One or more ADC group/channel not in IDLE state

ADC_E_NOT_DISENGAGED

0x1A

Unsupported power state request

ADC_E_POWER_STATE_NOT_SUPPORTED

0x1B

Requested power state cannot be reached directly

ADC_E_TRANSITION_NOT_POSSIBLE

0x1C

ADC not prepared for target power state

ADC_E_PERIPHERAL_NOT_PREPARED

0x1D

4.1.6.4.2. Runtime Errors

Type of Error

Related Error code

Value (Hex)

API service called during ongoing process

ADC_E_BUSY

0x0B

API service called while no conversion is ongoing

ADC_E_IDLE

0x0C

AUTOSAR requires that API functions check the validity of their parameters. The checks are described in spec and are done as internal parameter checks of the API functions. These checks are for development error reporting and can be en/dis-abled separately. Refer to the configuration chapter where the en/dis-abling of the checks is described. En/dis-abling of single checks is an addition to the AUTOSAR standard which requires to en/dis-able the complete parameter checking via the parameter ADC_DEV_ERROR_DETECT. The following table shows which parameter checks are performed on which services:

Check Services

ADC_E_UNINIT

ADC_E_BUSY

ADC_E_IDLE

ADC_E_ALREADY_INITIALIZED

ADC_E_PARAM_CONFIG

ADC_E_PARAM_POINTER

ADC_E_PARAM_GROUP

ADC_E_WRONG_TRIGG_SRC

ADC_E_NOTIF_CAPABILITY

ADC_E_BUFFER_UNINIT

Adc_Init

x

x

Adc_DeInit

x

Adc_StartGroupConversion

x

x

x

x

Adc_StopGroupConversion

x

x

x

x

Adc_ReadGroup

x

x

x

x

Adc_EnableGroupNotification

x

x

x

x

Adc_DisableGroupNotification

x

x

x

Adc_GetGroupStatus

x

x

Adc_GetVersionInfo

x

Adc_SetupResultBuffer

x

x

x

x

Adc_EnableHardwareTrigger

x

x

x

x

Adc_DisEnableHardwareTrigger

x

x

x

x

Adc_Get_StreamLastPointer

4.1.6.4.3. DEM Errors

ADC modules does not report DEM errors.

4.1.7. Used resources

4.1.7.1. Interrupt Handling

For interrupt notification, ISR’s are provided in ADC driver. There are four ISR for each ADC hardware unit. Depending on hardware unit configured, it will call group notify function. The interrupt service routines shall be mapped to the interrupt sources of the respective cross bar interrupt. The supported ISR’s are part of the Adc_Irq.h file.

Following are ADC module ISR for each hardware unit:

For interrupt notification, ISR’s are provided in ADC driver. There is one ISR for each ADC hardware unit. Depending on hardware unit configured, it will call group notify function. The interrupt service routines shall be mapped to the interrupt sources of the respective cross bar interrupt. The supported ISR’s are part of the Adc_Irq.h file.

Following are ADC module ISR for each hardware unit:

ADC HW UNIT

HW Interrupt

SW ISR for ADC module

ADC HW UNIT 0

ADC0.INT1

Adc_ADCINT1_IrqUnit0

ADC HW UNIT 0

ADC0.INT2

Adc_ADCINT2_IrqUnit0

ADC HW UNIT 0

ADC0.INT3

Adc_ADCINT3_IrqUnit0

ADC HW UNIT 0

ADC0.INT4

Adc_ADCINT4_IrqUnit0

ADC HW UNIT 1

ADC1.INT1

Adc_ADCINT1_IrqUnit1

ADC HW UNIT 1

ADC1.INT2

Adc_ADCINT2_IrqUnit1

ADC HW UNIT 1

ADC1.INT3

Adc_ADCINT3_IrqUnit1

ADC HW UNIT 1

ADC1.INT4

Adc_ADCINT4_IrqUnit1

ADC HW UNIT 2

ADC2.INT1

Adc_ADCINT1_IrqUnit2

ADC HW UNIT 2

ADC2.INT2

Adc_ADCINT2_IrqUnit2

ADC HW UNIT 2

ADC2.INT3

Adc_ADCINT3_IrqUnit2

ADC HW UNIT 2

ADC2.INT4

Adc_ADCINT4_IrqUnit2

ADC HW UNIT 3

ADC3.INT1

Adc_ADCINT1_IrqUnit3

ADC HW UNIT 3

ADC3.INT2

Adc_ADCINT2_IrqUnit3

ADC HW UNIT 3

ADC3.INT3

Adc_ADCINT3_IrqUnit3

ADC HW UNIT 3

ADC3.INT4

Adc_ADCINT4_IrqUnit3

ADC HW UNIT 4

ADC4.INT1

Adc_ADCINT1_IrqUnit4

ADC HW UNIT 4

ADC4.INT2

Adc_ADCINT2_IrqUnit4

ADC HW UNIT 4

ADC4.INT3

Adc_ADCINT3_IrqUnit4

ADC HW UNIT 4

ADC4.INT4

Adc_ADCINT4_IrqUnit4

DMA Module ISR

EDMA INT

CDD_EDMA_lld_transferCompletionMasterIsrFxn

4.1.8. Integration description

4.1.8.1. Dependent modules

4.1.8.1.1. MCU

The ADC modules expects the MCU module to be powered on. The ADC module depends on MCU module for data buffer control and crossbar interrupt mapping of ADC interrupts depending on the Hardware unit being configured.

Suppose the Hardware Unit 1 and Hardware Unit 3 are configured for ADC module:

ADC Hardware container

Fig. 4.12 ADC Hardware container

Then, the MCU module container McuAdcConfiguration should be configured as shown in below figure:

McuAdcConfiguration container

Fig. 4.13 McuAdcConfiguration container

ADC Hardware unit selection

Fig. 4.14 ADC Hardware unit selection

Similarly, the crossbar interrupts also needs to be mapped in MCU module according to HW unit and interrupts being required.

The ADC interrupts needs to be mapped to the corresponding cross bar interrupt required.

Please refer limitation section of Interrupts to be configured for ADC as per AdcPriorityImplementation.

ADC Interrupt configuration

Fig. 4.15 ADC Interrupt configuration

ADC Interrupt selection

Fig. 4.16 ADC Interrupt selection

4.1.8.1.2. DMA

The ADC Module requires DMA module to be configured, when ADC is configured in DMA mode and ADC channel Group is configured for DMA access.

  1. ADC Module Configuration:

    • The ADC module parameter AdcDMAEnable should be configured for TRUE.

    • The ADC Channel Group parameter AdcGroupDataAccessMethod should be configured with ADC_GROUP_DMA_ACCESS.

    • The ADC parameter AdcDmaChannelId in AdcChannel container represents the DMA Channel ID (0 to 63) to be configured.

    • This AdcDmaChannelId parameter should be configured sequentially.

  2. DMA module Configuration:

    • In CDD DMA module, CddDmaChannelTriggerConfiguration container should be configured w.r.t the trigger selection for ADC module.

    • ADC module is dependent on X-BAR DMA interrupts, thus we have configure the X-BAR interrupts in DMA module.

  3. The ADC Trigger source should be configured for one and many of DMA channels using following parameters, in containers

    • CddDmaDmaChannelModule represents the DMA Channel ID (0 - 63)

    • CddDmaChannelTriggerSource represents which Trigger source we should map the DMA Channel ID.

    • CddDmaDmaChannelXbar represents the DMA Cross-BAR. If the CddDmaChannelTriggerSource is selected between DMA_TRIG_XBAR_DMA_XBAR_OUT_0 to DMA_TRIG_XBAR_DMA_XBAR_OUT_15, then this parameter should be mapped to respective Cross-BAR.

    • CddDmaDmaChannelXbarMap represents the trigger source for the Cross-BAR, which can be from module like ADC, EPWM, FSI etc.

    • The ADC Trigger source should be selected according to the Interrupt Source and ADC instance configured. The ADC parameter AdcDmaChannelId in AdcChannel container and CddDmaDmaChannelModule in CddDmaChannelTriggerConfiguration container should be same.

CDD DMA configuration

Fig. 4.17 CDD DMA configuration

ADC module DMA channel ID selection

Fig. 4.18 ADC module DMA channel ID selection

4.1.8.1.3. DET

This implementation depends on the DET in order to report development errors The detection of development errors is configurable (ON / OFF).

4.1.8.1.4. Callback Functions

The ADC driver does not provide any call back functions

4.1.8.1.5. Callback Notification

Notifications:

As it is a configurable interface, the ADC defines notifications that can be mapped to callback functions provided by other modules. The mapping is not statically defined by the ADC but can be performed at configuration time. The function prototypes that can be used for the configuration have to match the appropriate function prototype signatures, which are described in the following.

Adc_GroupEndNotifyType:

This is of type Adc_GroupEndNotifyType which is defined in Adc_Types.h file. This is called to notify the group about the completion of the requested conversion and availability of the conversion results.

4.1.8.2. Multi-core and Resource allocator

Not Supported

4.1.9. Configuration

4.1.9.1. Configuration Variants

The ADC can be configured as Post-Build or Pre-Compile variant, using EB tresos tool.

Variants

Generated Files

PostBuild

Adc_PBcfg.c , Adc_Cfg.h

Pre-Compile

Adc_Cfg.c , Adc_Cfg.h

4.1.9.2. Parameter Description

4.1.9.2.1. Standard Configuration

Standard Parameters

Description

Default Value

Range

Unit/Datatype

AdcHwUnitId

Numeric ID of the HW Unit. This symbolic name allows accessing Hw Unit data. Enumeration literals are defined vendor specific.

ADC_UNIT_1

ADC_UNIT_1

ENUMERATION

AdcHwPrescale

Optional ADC module specific clock prescale factor

if supported by hardware.

ADC_CLK_DIV_1_0

ADC_CLK_DIV_2_0

ADC_CLK_DIV_2_5

ADC_CLK_DIV_3_0

ADC_CLK_DIV_3_5

ADC_CLK_DIV_4_0

ADC_CLK_DIV_4_5

ADC_CLK_DIV_5_0

ADC_CLK_DIV_5_5

ADC_CLK_DIV_6_0

ADC_CLK_DIV_6_5

ADC_CLK_DIV_7_0

ADC_CLK_DIV_7_5

ADC_CLK_DIV_8_0

ADC_CLK_DIV_8_5

ENUMERATION

AdcChannelId

This parameter defines the assignment of the channel to the physical ADC hardware channel.

0

0..1024

INTEGER

AdcChannelLimitCheck

Enables or disables limit checking for an ADC channel.

FALSE

TRUE /FALSE

BOOLEAN

AdcChannelHighLimit

High limit - used for limit checking.

4095

0..4095

INTEGER

AdcChannelLowLimit

Low limit - used for limit checking.

0

0..4096

INTEGER

AdcChannelRangeSelect

In case of active limit checking: defines which conversion values are taken into account related to the boarders defined with AdcChannelLowLimit and AdcChannelHighLimit.

NA

NA

ENUMERATION

AdcGroupAccessMode

Type of access mode to group conversion results.

ADC_ACCESS_MODE_SINGLE

ADC_ACCESS_MODE_SINGLE

ADC_ACCESS_MODE_STREAMING

ENUMERATION

AdcGroupConversionMode

Type of conversion mode supported by the driver.

ADC_CONV_MODE_CONTINUOUS

ADC_CONV_MODE_CONTINUOUS

ADC_CONV_MODE_ONESHOT

ENUMERATION

AdcGroupId

Numeric ID of the group. This parameter is the symbolic name to be used on the API. This symbolic name allows accessing Channel Group data. This value will be assigned to the symbolic name derived of the AdcGroup container shortName.

0

0..1023

INTEGER

AdcGroupPriority

Priority level of the AdcGroup.

0

0..255

INTEGER

AdcGroupAccessMode

Type of access mode to group conversion results.

ADC_ACCESS_MODE_SINGLE

ADC_ACCESS_MODE_SINGLE

ADC_ACCESS_MODE_STREAMING

ENUMERATION

AdcGroupReplacement

Replacement mechanism, which is used on ADC group level, if a group conversion is interrupted by a group which has a higher priority.

ADC_GROUP_REPL_SUSPEND_RESUME

ADC_GROUP_REPL_ABORT_RESTART

ADC_GROUP_REPL_SUSPEND_RESUME

ENUMERATION

AdcGroupTriggSrc

Type of source event that starts a group conversion.

ADC_TRIGG_SRC_SW

ADC_TRIGG_SRC_HW

ADC_TRIGG_SRC_SW

ENUMERATION

AdcHwTrigSignal

Configures on which edge of the hardware trigger signal the driver should react i.e. start the conversion (only if supported by the ADC hardware).

ADC_HW_TRIG_BOTH_EDGES

ADC_HW_TRIG_BOTH_EDGES

ADC_HW_TRIG_FALLING_EDGE

ADC_HW_TRIG_RISING_EDGE

ENUMERATION

AdcHwTrigTimer

Reload value of the ADC module embedded timer (only if supported by ADC hardware).

ADC_TRIGGER_RTI0

ADC_TRIGGER_RTI0

ADC_TRIGGER_RTI1

ADC_TRIGGER_RTI2

ADC_TRIGGER_RTI

ADC_TRIGGER_INPUT_XBAR_OUT5

ADC_TRIGGER_EPWM0_SOCA

ADC_TRIGGER_EPWM0_SOCB

ADC_TRIGGER_EPWM1_SOCA

ADC_TRIGGER_EPWM1_SOCB

ADC_TRIGGER_EPWM2_SOCA

ADC_TRIGGER_EPWM2_SOCB

ADC_TRIGGER_EPWM3_SOCA

ADC_TRIGGER_EPWM3_SOCB

ADC_TRIGGER_EPWM4_SOCA

ADC_TRIGGER_EPWM4_SOCB

ADC_TRIGGER_EPWM5_SOCA

ADC_TRIGGER_EPWM5_SOCB

ADC_TRIGGER_EPWM6_SOCA

ADC_TRIGGER_EPWM6_SOCB

ADC_TRIGGER_EPWM7_SOCA

ADC_TRIGGER_EPWM7_SOCB

ADC_TRIGGER_EPWM8_SOCA

ADC_TRIGGER_EPWM8_SOCB

ADC_TRIGGER_EPWM9_SOCA

ADC_TRIGGER_EPWM9_SOCB

ADC_TRIGGER_EPWM10_SOCA

ADC_TRIGGER_EPWM10_SOCB

ADC_TRIGGER_EPWM11_SOCA

ADC_TRIGGER_EPWM11_SOCB

ADC_TRIGGER_EPWM12_SOCA

ADC_TRIGGER_EPWM12_SOCB

ADC_TRIGGER_EPWM13_SOCA

ADC_TRIGGER_EPWM13_SOCB

ADC_TRIGGER_EPWM14_SOCA

ADC_TRIGGER_EPWM14_SOCB

ADC_TRIGGER_EPWM15_SOCA

ADC_TRIGGER_EPWM15_SOCB

ADC_TRIGGER_EPWM16_SOCA

ADC_TRIGGER_EPWM16_SOCB

ADC_TRIGGER_EPWM17_SOCA

ADC_TRIGGER_EPWM17_SOCB

ADC_TRIGGER_EPWM18_SOCA

ADC_TRIGGER_EPWM18_SOCB

ADC_TRIGGER_EPWM19_SOCA

ADC_TRIGGER_EPWM19_SOCB

ADC_TRIGGER_EPWM20_SOCA

ADC_TRIGGER_EPWM20_SOCB

ADC_TRIGGER_EPWM21_SOCA

ADC_TRIGGER_EPWM21_SOCB

ADC_TRIGGER_EPWM22_SOCA

ADC_TRIGGER_EPWM22_SOCB

ADC_TRIGGER_EPWM23_SOCA

ADC_TRIGGER_EPWM23_SOCB

ADC_TRIGGER_EPWM24_SOCA

ADC_TRIGGER_EPWM24_SOCB

ADC_TRIGGER_EPWM25_SOCA

ADC_TRIGGER_EPWM25_SOCB

ADC_TRIGGER_EPWM26_SOCA

ADC_TRIGGER_EPWM26_SOCB

ADC_TRIGGER_EPWM27_SOCA

ADC_TRIGGER_EPWM27_SOCB

ADC_TRIGGER_EPWM28_SOCA

ADC_TRIGGER_EPWM28_SOCB

ADC_TRIGGER_EPWM29_SOCA

ADC_TRIGGER_EPWM29_SOCB

ADC_TRIGGER_EPWM30_SOCA

ADC_TRIGGER_EPWM30_SOCB

ADC_TRIGGER_EPWM31_SOCA

ADC_TRIGGER_EPWM31_SOCB

ADC_TRIGGER_ECAP0

ADC_TRIGGER_ECAP1

ADC_TRIGGER_ECAP2

ADC_TRIGGER_ECAP3

ADC_TRIGGER_ECAP4

ADC_TRIGGER_ECAP5

ADC_TRIGGER_ECAP6

ADC_TRIGGER_ECAP7

ADC_TRIGGER_ECAP8

ADC_TRIGGER_ECAP9

ENUMERATION

AdcNotification

Callback function for each group

AdcApp_Group0EndNotification

NA

FUNCTION-NAME

AdcStreamingBufferMode

Configure streaming buffer as “linear buffer” (i.e. the ADC Driver stops the conversion as soon as the stream buffer is full) or as “ring buffer” (wraps around if the end of the stream buffer is reached).

ADC_STREAM_BUFFER_LINEAR

ADC_STREAM_BUFFER_CIRCULAR

ADC_STREAM_BUFFER_LINEAR

ENUMERATION

AdcStreamingNumSamples

Number of ADC values to be acquired per channel in streaming access mode.

1

1..255

INTEGER

AdcGroupDefinition

Assignment of AdcChannels to a AdcGroups.

NA

NA

REFERENCE

AdcDeInitApi

Adds / removes the service Adc_DeInit() from the code.

TRUE

TRUE /FALSE

BOOLEAN

AdcDevErrorDetect

Switches the Development Error Detection and Notification ON or OFF

TRUE

TRUE /FALSE

BOOLEAN

AdcEnableLimitCheck

Enables or disables limit checking feature in the ADC driver.

FALSE

TRUE /FALSE

BOOLEAN

AdcEnableQueuing

Determines, if the queuing mechanism is active in case of priority mechanism disabled.

Note: If priority mechanism is enabled, queuing mechanism is always active and the parameter ADC_ENABLE_QUEUING is not evaluated.

true: Enabled. false: Disabled.

TRUE

TRUE /FALSE

BOOLEAN

AdcEnableStartStopGroupApi

Adds / removes the services Adc_StartGroupConversion() and Adc_StopGroupConversion() from the code.

TRUE

TRUE /FALSE

BOOLEAN

AdcPriorityImplementation

Determines whether a priority mechanism is available for prioritization of the conversion requests and if available, the type of prioritization mechanism. The selection applies for groups with trigger source software and trigger source hardware.

ADC_PRIORITY_HW_SW

ADC_PRIORITY_HW

ADC_PRIORITY_HW_SW

ADC_PRIORITY_NONE

ENUMERATION

AdcGrpNotifCapability

Determines, if the group notification mechanism (the functions to enable and disable the notifications) is available at runtime.

TRUE

TRUE /FALSE

BOOLEAN

AdcHwTriggerApi

Adds / removes the services Adc_EnableHardwareTrigger() and Adc_DisableHardwareTrigger() from the code.

TRUE

TRUE /FALSE

BOOLEAN

AdcReadGroupApi

Adds / removes the service Adc_ReadGroup() and from the code.

TRUE

TRUE /FALSE

BOOLEAN

AdcResultAlignment

Alignment of ADC raw results in ADC result buffer (left/right alignment).

ADC_ALIGN_RIGHT

ADC_ALIGN_RIGHT

ENUMERATION

AdcVersionInfoApi

Adds / removes the service Adc_GetVersionInfo() from the code.

TRUE

TRUE /FALSE

BOOLEAN

AdcChannelValueSigned

Information whether the result value of the ADC driver has sign information (true) or not (false). If the result shall be interpreted as signed value it shall apply to C-language rules.

FALSE

TRUE /FALSE

BOOLEAN_LABEL

AdcGroupFirstChannelFixed

Information whether the first channel of an ADC Channel group can be configured (false) or is fixed (true) to a value determined by the ADC HW Unit.

FALSE

TRUE /FALSE

BOOLEAN_LABEL

AdcMaxChannelResolution

Maximum Channel resolution in bits (does not specify accuracy).

0

1..63

INTEGER_LABEL

4.1.9.2.2. IP Specific Configuration

Texas Instruments Parameters

Description

Default Value

Range

Unit

AdcExtHwTrigTimer

Configure the streaming buffer as a linear buffer

(i.e. the ADC Driver stops the conversion as soon as the stream buffer is full) or as a ring buffer (wraps around if the end of the stream buffer is reached).

ADC_TRIGGER_RTI0

ADC_TRIGGER_RTI0

ADC_TRIGGER_RTI1

ADC_TRIGGER_RTI2

ADC_TRIGGER_RTI3

ADC_TRIGGER_INPUT_XBAR_OUT5

ADC_TRIGGER_EPWM0_SOCA

ADC_TRIGGER_EPWM0_SOCB

ADC_TRIGGER_EPWM1_SOCA

ADC_TRIGGER_EPWM1_SOCB

ADC_TRIGGER_EPWM2_SOCA

ADC_TRIGGER_EPWM2_SOCB

ADC_TRIGGER_EPWM3_SOCA

ADC_TRIGGER_EPWM3_SOCB

ADC_TRIGGER_EPWM4_SOCA

ADC_TRIGGER_EPWM4_SOCB

ADC_TRIGGER_EPWM5_SOCA

ADC_TRIGGER_EPWM5_SOCB

ADC_TRIGGER_EPWM6_SOCA

ADC_TRIGGER_EPWM6_SOCB

ADC_TRIGGER_EPWM7_SOCA

ADC_TRIGGER_EPWM7_SOCB

ADC_TRIGGER_EPWM8_SOCA

ADC_TRIGGER_EPWM8_SOCB

ADC_TRIGGER_EPWM9_SOCA

ADC_TRIGGER_EPWM9_SOCB

ADC_TRIGGER_EPWM10_SOCA

ADC_TRIGGER_EPWM10_SOCB

ADC_TRIGGER_EPWM11_SOCA

ADC_TRIGGER_EPWM11_SOCB

ADC_TRIGGER_EPWM12_SOCA

ADC_TRIGGER_EPWM12_SOCB

ADC_TRIGGER_EPWM13_SOCA

ADC_TRIGGER_EPWM13_SOCB

ADC_TRIGGER_EPWM14_SOCA

ADC_TRIGGER_EPWM14_SOCB

ADC_TRIGGER_EPWM15_SOCA

ADC_TRIGGER_EPWM15_SOCB

ADC_TRIGGER_EPWM16_SOCA

ADC_TRIGGER_EPWM16_SOCB

ADC_TRIGGER_EPWM17_SOCA

ADC_TRIGGER_EPWM17_SOCB

ADC_TRIGGER_EPWM18_SOCA

ADC_TRIGGER_EPWM18_SOCB

ADC_TRIGGER_EPWM19_SOCA

ADC_TRIGGER_EPWM19_SOCB

ADC_TRIGGER_EPWM20_SOCA

ADC_TRIGGER_EPWM20_SOCB

ADC_TRIGGER_EPWM21_SOCA

ADC_TRIGGER_EPWM21_SOCB

ADC_TRIGGER_EPWM22_SOCA

ADC_TRIGGER_EPWM22_SOCB

ADC_TRIGGER_EPWM23_SOCA

ADC_TRIGGER_EPWM23_SOCB

ADC_TRIGGER_EPWM24_SOCA

ADC_TRIGGER_EPWM24_SOCB

ADC_TRIGGER_EPWM25_SOCA

ADC_TRIGGER_EPWM25_SOCB

ADC_TRIGGER_EPWM26_SOCA

ADC_TRIGGER_EPWM26_SOCB

ADC_TRIGGER_EPWM27_SOCA

ADC_TRIGGER_EPWM27_SOCB

ADC_TRIGGER_EPWM28_SOCA

ADC_TRIGGER_EPWM28_SOCB

ADC_TRIGGER_EPWM29_SOCA

ADC_TRIGGER_EPWM29_SOCB

ADC_TRIGGER_EPWM30_SOCA

ADC_TRIGGER_EPWM30_SOCB

ADC_TRIGGER_EPWM31_SOCA

ADC_TRIGGER_EPWM31_SOCB

ADC_TRIGGER_ECAP0

ADC_TRIGGER_ECAP1

ADC_TRIGGER_ECAP2

ADC_TRIGGER_ECAP3

ADC_TRIGGER_ECAP4

ADC_TRIGGER_ECAP5

ADC_TRIGGER_ECAP6

ADC_TRIGGER_ECAP7

ADC_TRIGGER_ECAP8

ADC_TRIGGER_ECAP9

ENUMERATION

AdcDmaReference

Reference to the DMA Group Channel

NA

NA

REFERENCE

AdcMaxDmaChannelId

Number of actual DMA channels. This is of type published information and not editable

63

NA

INTEGER

AdcDmaInstance

Number of actual DMA channels. This is of type published information and not editable

0

NA

INTEGER

AdcFifoErrLog

Enables/Disables ADC Fifo error logging.Useful in debugging.

TRUE

TRUE/FALSE

BOOLEAN

AdcErrLogMaxLen

Max length of error log buffer that can be used

100

0..1024

INTEGER

AdcHwUnitMonitorMode

This is the Interrupt Mode or Polling Mode for monitoring ADC conversion done status.

ADC_INTERRUPT_MODE

ADC_INTERRUPT_MODE

ADC_POLLING_MODE

ENUMERATION

AdcBufferedModeSelect

To select buffered on or off

TRUE

TRUE/FALSE

BOOLEAN

AdcDMAEnable

Enables DMA Access method for ADC Channel Group.

FALSE

TRUE/FALSE

BOOLEAN

AdcDeviceVariant

Select SOC variant .This parameter shall be used by driver to impose device specific constraints. The user guide shall detail the device specific constraints

AM263

NA

ENUMERATION

AdcMaxGroupCount

Maximum group across all hwunit

4

1..1024

INTEGER

AdcMaxHwUnitCount

Max HW unit - This should match the sum for the units ISR

1

5

INTEGER

AdcHwUnitActive

Enables Disable HW UNIT

TRUE

TRUE/FALSE

BOOLEAN

AdcTypeofInterruptFunction

Type of ISR function

ADC_ISR_CAT1

ADC_ISR_VOID

ADC_ISR_CAT1

ADC_ISR_CAT2

ENUMERATION

AdcOsCounterRef

This parameter contains a reference to the OsCounter which is used by the ADC driver.

ASPathDataOfSchema: /AUTOSAR/EcucDefs/Os/OsCounter

ASPathDataOfSchema: /AUTOSAR/EcucDefs/Os/OsCounter

REFERENCE

AdcDefaultOSCounterId

Default Os Counter Id if node reference to OsCounter ref AdcOsCounterRef is not set

0

0..16

INTEGER

AdcEnableRegisterReadbackApi

Enable API to readback ADC critical registers

FALSE

TRUE / FALSE

BOOLEAN

AdcMinRange

Minimum value of range.

0

NA

INTEGER

AdcMaxNumChannels

Number of MCAL channels - in terms of ADC HW, this represents the number of hardware steps.This is a fixed value as per the ADC module and can’t be changed

12

NA

INTEGER

AdcMinHwChannelId

Number of actual HW channels - in terms of ADC HW the actual channel input to the ADC module

0

NA

INTEGER

AdcPollingMainFunctionApi

Enable API to do the polling operation

TRUE

TRUE/FALSE

BOOLEAN

4.1.9.3. Symbolic Names deviations

None

4.1.9.4. Configuration rules and constraints to enable plausibility checks

None

4.1.10. Examples

4.1.10.1. Overview

Will be updated in future release:

4.1.10.2. External Setup required to run example

ADC module is tested using CC board (PROC111E2) and analog input is provided to ADC input channels through DC power supply (0-12V).

The ADC analog input for the AM263x ranges from 0 – 3.3V.

ADC_ANI0 is provided with 1V.

ADC_ANI1 is provided with 3.2V.

4.1.10.3. How to run examples

4.1.10.3.1. Steps to build and run example

ADC example application demonstrating the MCAL ADC driver features is in folder <MCAL_ROOT>/examples/Adc.

This application can be built from the root folder by giving gmake –s adc_app PLATFORM=am263.

Once the build is completed we get a binary file, which is loaded in our controller and executed.

4.1.10.3.2. Configuration used to test this example

The ADC module example is configured with following groups on ADC Hardware Unit 1

  1. Adc Group 0 : One Shot Conversion Software Triggered with Data Access Polling Mode.

  2. Adc Group 1 : One Shot Conversion Software Triggered with Data Access Interrupt Mode.

  3. Adc Group 2 : One Shot Conversion Software Triggered with Data Access Polling Mode.

  4. Adc Group 3 : One Shot Conversion Software Triggered with Data Access Interrupt Mode.

The ADC module example application testing procedure as follows:

HW UNIT 1 is configured

One Shot Mode Testing: (Group 0) (Group 1) (Group 2) (Group 3) (HW UNIT 1)

  1. Group is Triggered for Conversion using API Adc_StartConversion()

  2. Adc_PollingMainFunction() is called for Groups configured as Data Access Polling Mode.

  3. AdcApp_procIsr() is called through AdcApp_GroupEndNotification for Groups configured as Data Access Interrupt Mode.

  4. Wait until the conversion is completed.

  5. Conversion is stopped using API Adc_StopConversion().

  6. Check the notification message, the notification counter should be incremented with ADC results available in the ADC result buffer ( Adc_AppBuffer )

Cross bar mapping:

  1. ADC HW UNIT 1 : ADC1.INT1 is mapped to XBAR1 (147)

  2. ADC HW UNIT 3 : ADC3.INT1 is mapped to XBAR2 (148)

Refer crossbar section in MCU module to map crossbar.

4.1.10.4. Sample Log


 ADC_APP: Sample Application - STARTS !!!
 ADC_APP: GROUPs 4: HWUNIT 1: LOOP COUNT 1:!!!
  
 --------------------------------------
 Apply different voltages (between 0 - 3.3 volts) to the Six ADC channels
 --------------------------------------
  
 Press any key to start conversion

  
  ADC MCAL Version Info
  ---------------------
  Vendor ID           : 44
  Module ID           : 123
  SW Major Version    : 9
  SW Minor Version    : 1
  SW Patch Version    : 0
  
  
  Read Buffer Content
  -------------------
  ADC Group 0 Log:
  ----------------
  Channel                ADC Value       Volt
  ----------------------------------------------------
  0              0x00000cc1      1434mV
  ADC Group 1 Log:
  ----------------
  Channel                ADC Value       Volt
  ----------------------------------------------------
  0              0x00000cc1      1434mV
  ADC Group 2 Log:
  ----------------
  Channel                ADC Value       Volt
  ----------------------------------------------------
  0              0x00000cc1      1434mV
  1              0x00000000      0000mV
  2              0x00000000      0000mV
  3              0x00000000      0000mV
  ADC Group 3 Log:
  ----------------
  Channel                ADC Value       Volt
  ----------------------------------------------------
  0              0x00000cc1      1434mV
  1              0x00000000      0000mV
  ADC Test Passed!!!
  ADC_APP: Sample Application - DONE !!!

4.1.10.5. File Structure

📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Adc
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜AdcApp.c : Contains ADC test example
┃ ┃ ┃ ┣ 📜AdcApp.h : ADC example header file
┃ ┃ ┃ ┗ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Adc_Demo_Cfg
┃ ┃ ┃ ┗ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am263
┃ ┃ ┃ ┃ ┃ ┗ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Adc_Cfg.h : Contains the configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┗ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Adc_Cfg.c : Contains all Pre-Compile Configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Adc_PBcfg.c : Contains all Post-Build Configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┗ 📜README.txt

4.1.10.6. Test Report

Please refer AM26x ADC Driver Test Case Report as part of CSP provided in the release package.

4.1.11. References

AUTOSAR_SWS_ADC
Technical Reference Manual