4.18. LIN Module

4.18.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

BSW

Basic Software

MCAL

Micro Controller Abstraction Layer

DET

Default Error Tracer

HW

Hardware

SW

Software

EcuM

ECU Manager

LIN

Local Interconnect Network

MCU

Micro Controller Unit

OS

Operating System

4.18.2. Introduction

This document describes the functionality and configuration of the AUTOSAR BSW module LIN.

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Pre-Compile, Post-build

Vendor ID

LIN_VENDOR_ID (44)

Module ID

LIN_MODULE_ID (82)

Supported Platform

AM261x

The LIN module initializes and controls the Lin peripheral. It provides services to send, receive data, sleep and wakeup of the Lin peripheral.

4.18.3. Functional Overview

4.18.3.1. Initialization

Lin_Init () must be called to initialize the LIN driver at power on and sets controller independent init values. This will also set the Lin controllers to IDLE state.

4.18.3.2. States

Refer Chapter 7.3.3 State Diagrams in AUTOSAR_SWS_LINDriver for more details.

4.18.3.3. Assumptions

Only one LIN channel of an ECU is allowed to connect to a particular LIN cluster.

4.18.3.4. Limitations

  1. Abort of current ongoing transmission [SWS_Lin_00021].

  2. Automatic transmission of Goto Sleep command [SWS_Lin_00089].

4.18.3.5. Design overview

Will be updated in future release

4.18.4. Hardware Features

4.18.4.1. IP Supported Features

  • Compatibility with LIN 1.3 protocols

  • Configurable baud rate up to 20 kpbs

  • Two external pins: LINRX and LINTX.

  • Multibuffered receive and transmit units

  • Identification masks for message filtering

  • Automatic commander header generation

  • Wake up on LINRX dominant level from transceiver

  • Automatic wake up support

  • Error detection

  • 2 interrupt lines with priority encoding

  • Support for LIN 2.0 checksum

  • Enhanced baud rate generator

4.18.4.2. AUTOSAR Supported Features

  • Conformance to LIN 2.1 protocol; operation in Master Mode only.

  • Support of upto 3 Lin Channels

  • Sleep / wakeup functionality

  • Enhanced and Classic checksum model

  • Transmission / Reception of upto 8 bytes of Data

  • PDU Directions supported : LIN_MASTER_RESPONSE, LIN_SLAVE_RESPONSE, LIN_SLAVE_TO_SLAVE

  • Use of EcuM wakeup source

  • Use of Det for reporting of development errors

4.18.4.3. Not supported Features

  • Abort of ongoing transmission

  • Automatic transmission of Goto Sleep command

4.18.4.4. Non compliance

4.18.4.4.1. Deviations to requirements (Requirement Traceability)

4.18.4.4.1.1. Deviation of requirements against AUTOSAR specification requirements

Will be updated in next release

4.18.5. Source files

Static source C Files are defined below

📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Lin
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Lin.h : Contains interface header for Lin Drv functions.
┃ ┃ ┃ ┣ 📜Lin_Irq.h : Contains ISR function declarations for LIN Drv.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Lin.c : Contains interface for Lin Drv functions.
┃ ┃ ┃ ┣ 📜Lin_Irq.c : Contains Interrupt Service Routines for Lin Drv.
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┗ 📜cslr_lin.h : Contains Register definitions required for accessing Lin peripherals.
┃ ┃ ┃ ┣ 📜Lin_Priv.c : Contains controller dependent local functions and private functions to be used in Lin.c
┃ ┃ ┃ ┗ 📜Lin_Priv.h : Contains interface header for Lin private functions.
┃ ┃ ┗ 📜Makefile
┃ 📂mcal_config
┃ 📂mcal_docs
┃ 📜README.txt

Plugin files are defined below in the table.

Plugin Files

Description

Lin_Cfg.h

Contains the Precompile switches, Macros for LIN channels etc.

Lin_PBcfg.c

Contains all channels Post-Build Configuration parameters

Lin_Cfg.c

Contains all channels Pre-Compile Configuration parameters

Lin header file include structure

Fig. 4.80 Lin header file include structure

4.18.6. Module requirements

Please refer Software Product Specification document provided as part of CSP.

4.18.6.1. Memory Mapping

Memory Mapping Sections

LIN_CODE

LIN_CODE_ISR

LIN_VAR_NO_INIT

LIN_VAR

LIN_CONST

LIN_PBCFG

LIN_START_SEC_VAR_INIT_UNSPECIFIED(.bss)

x

LIN_STOP_SEC_VAR_INIT_UNSPECIFIED

x

LIN_START_SEC_CONFIG_DATA (.const)

x

LIN_STOP_SEC_CONFIG_DATA

x

LIN_START_SEC_CODE(.text)

x

LIN_STOP_SEC_CODE

x

LIN_START_SEC_VAR_INIT_32(.bss)

x

LIN_STOP_SEC_VAR_INIT_32

x

LIN_START_SEC_VAR_NO_INIT_UNSPECIFIED(.data)

x

LIN_STOP_SEC_VAR_NO_INIT_UNSPECIFIED

x

LIN_START_SEC_ISR_CODE

x

LIN_STOP_SEC_ISR_CODE

x

4.18.6.2. Scheduling

There are no scheduled functions within the LIN driver

4.18.6.3. Error handling

4.18.6.3.1. DET Errors

The errors reported to DET module are described in the following table:

Type of Error

Related Error code

Value (Hex)

API service used without module initialization

LIN_E_UNINIT

0x00

API service used with an invalid or inactive channel parameter

LIN_E_INVALID_CHANNEL

0x02

API service called with invalid configuration pointer

LIN_E_INVALID_POINTER

0x03

Invalid state transition for the current state

LIN_E_STATE_TRANSITION

0x04

API service called with a NULL pointer

LIN_E_PARAM_POINTER

0x05

4.18.6.3.2. Runtime Errors

None

4.18.7. Used resources

4.18.7.1. Interrupt Handling

The Driver doesn’t register any interrupts handler (ISR), it’s expected that consumer of this driver registers the required interrupt handler.

AUTOSAR_SWS_LINDriver section: 10 Configuration specification, details the expected behavior and control flow for ISR implementation, please refer the same.

Lin driver provides ISR for wakeup detection. The interrupt vector lines to be used is configurable in Lin driver. The interrupt category must be configured in Lin Driver and OS modules. The ISR’s are implemented in the file Lin_Irq.c.

Respective ISRs for each Lin Instances in AM261x are as follows:

Lin Instances

ISR Routines

LIN0 Wakeup Line 0 (IE0)

Lin_0_Int0ISR()

LIN0 Wakeup Line 1 (IE1)

Lin_0_Int1ISR()

LIN1 Wakeup Line 0 (IE0)

Lin_1_Int0ISR()

LIN1 Wakeup Line 1 (IE1)

Lin_1_Int1ISR()

LIN2 Wakeup Line 0 (IE0)

Lin_2_Int0ISR()

LIN2 Wakeup Line 1 (IE1)

Lin_2_Int1ISR()

  1. Lin_0_Int0ISR For AM261x device, this ISR is called on detection of wakeup event on interrupt line 0 for the LIN0 controller.

  2. Lin_0_Int1ISR For AM261x device, this ISR is called on detection of wakeup event on interrupt line 1 for the LIN0 controller.

  3. Lin_1_Int0ISR For AM261x device, this ISR is called on detection of wakeup event on interrupt line 0 for the LIN1 controller.

  4. Lin_1_Int1ISR For AM261x device, this ISR is called on detection of wakeup event on interrupt line 1 for the LIN1 controller.

  5. Lin_2_Int0ISR For AM261x device, this ISR is called on detection of wakeup event on interrupt line 0 for the LIN2 controller.

  6. Lin_2_Int1ISR For AM261x device, this ISR is called on detection of wakeup event on interrupt line 1 for the LIN2 controller.

4.18.8. Integration description

4.18.8.1. Dependent modules

4.18.8.1.1. MCU

The hardware of the internal LIN hardware unit depends on the system clock, prescaler(s) and PLL. Hence, the length of the LIN bit timing depends on the clock settings made in module MCU. The LIN driver module will not take care of setting the registers that configure the clock, prescaler(s) and PLL (e.g. switching on/off the PLL) in its init functions. The MCU module must do this.

4.18.8.1.2. PORT

The Port driver configures the port pins used for the LIN driver as input or output. Hence, the Port driver has to be initialized prior to the use of LIN functions. Otherwise, LIN driver functions will exhibit undefined behavior.

4.18.8.1.3. OS

The LIN driver uses interrupts and therefore there is a dependency on the OS, which configures the interrupt sources.

4.18.8.1.4. LIN Driver Users

The LIN Interface is the only user of the LIN driver services.

4.18.8.1.5. DET

In development mode, the Lin module reports development error through the Det_ReportError function of module DET.

AUTOSAR requires that API functions shall check the validity of their respective parameters. These checks are for development error reporting and can be enabled or disabled.

4.18.8.1.6. Callback Notification

None

4.18.8.1.7. SchM

If multiple AUTOSAR runnables have access to the same Data Store Memory block, the exported AUTOSAR specification enforces data consistency by using an AUTOSAR exclusive area. With this specification, the runnables have mutually exclusive access to the per-instance memory global data, which prevents data corruption. Beside the OS, the BSW Scheduler provides functions that LIN module calls at begin and end of critical sections. This implementation requires 1 level of exclusive access to guard critical sections.

The data consistency mechanism that has to be applied to an ExclusiveArea might be domain, ECU or even project specific. The decision which mechanism has to be applied by RTE / Basic Software Scheduler is taken during ECU integration by setting the Exclusive Area configuration parameter RteExclusiveAreaImplMechanism. This parameter is an input for RTE generator. For LIN Module, data consistency and exclusive access to critical sections are required for the following sections as shown in the table below:

Exclusive Area Functions used

LIN Function calling Exclusive Area

Need for Exclusive Area

Recommended Exclusive Area Mapping

LIN_EXCLUSIVE_AREA_0

Lin_SendFrame
Lin_GoToSleep
Lin_GoToSleepInternal
Lin_WakeupProcess
Lin_WakeupInternalProcess
Lin_GetStatus

To protect against multiple access for shared resources

ALL_INTERRUPT_BLOCKING : All interrupts should be blocked as this API’s can be called in the interrupts

4.18.8.2. Multi-core support

Not supported

4.18.9. Configuration

4.18.9.1. LinDemEventParameterRefs

Item

Name

LinDemEventParameterRefs

Description

Reference to the DemEventParameter which shall be issued when the error “Timeout caused by hardware error” has occurred. If the reference is not configured the error shall be reported as DET error.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.18.9.2. LinGeneral

This container contains the parameters related to each LIN Driver Unit.

4.18.9.2.1. LinDevErrorDetect

Item

Name

LinDevErrorDetect

Description

Switches the development error detection and notification on or off.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.18.9.2.2. LinIndex

Item

Name

LinIndex

Description

Specifies the InstanceId of this module instance. If only one instance is present it shall have the Id 0.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

4.18.9.2.3. LinWakeupId

Item

Name

LinWakeupId

Description

Specifies the LIN ID used to transmit a header instead of a wakeup signal due to hardware constraints. The hardware enters an undefined state when a standard wakeup signal is transmitted. To mitigate this limitation, an unused header frame is utilized as the wakeup signal, which conforms to the LIN 2.1 specification

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

63

Max-value

63

Min-value

0

4.18.9.2.4. LinVersionInfoApi

Item

Name

LinVersionInfoApi

Description

Switches the Lin_GetVersionInfo function ON or OFF.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.18.9.2.5. LinEnableRegisterReadbackApi

Item

Name

LinEnableRegisterReadbackApi

Description

Switch to indicate that the Lin_RegisterReadBack is supported

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.18.9.3. LinGlobalConfig

This container contains the global configuration parameter of the Lin driver.

4.18.9.3.1. LinChannel

This container contains the configuration (parameters) of the LIN Controller(s).

4.18.9.3.1.1. LinChannelBaudRate

Item

Name

LinChannelBaudRate

Description

Specifies the baud rate of the LIN channel

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

19200

Max-value

20000

Min-value

1000

4.18.9.3.1.2. LinChannelId

Item

Name

LinChannelId

Description

Identifies the LIN channel. Replaces LIN_CHANNEL_INDEX_NAME from the LIN SWS.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

2

Min-value

0

4.18.9.3.1.3. LinInstance

Item

Name

LinInstance

Description

Selects Lin Instance.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

LIN_INSTANCE_0

Range

LIN_INSTANCE_0
LIN_INSTANCE_1
LIN_INSTANCE_2

4.18.9.3.1.4. LinLoopbackMode

Item

Name

LinLoopbackMode

Description

Select loopback mode to be used for this Lin instance.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

LIN_LOOPBACK_DISABLED

Range

LIN_LOOPBACK_DISABLED
LIN_LOOPBACK_INTERNAL
LIN_LOOPBACK_EXTERNAL

4.18.9.3.1.5. LinChannelWakeupSupport

Item

Name

LinChannelWakeupSupport

Description

Specifies if the LIN hardware channel supports wake up functionality

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.18.9.3.1.6. LinISRType

Item

Name

LinISRType

Description

Select ISR type to be used for this Lin instance.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

LIN_ISR_CAT2

Range

LIN_ISR_VOID
LIN_ISR_CAT1
LIN_ISR_CAT2

4.18.9.3.1.7. LinInterruptLineSelect

Item

Name

LinInterruptLineSelect

Description

Select interrupt line to be used for this Lin instance.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

LIN_INTERRUPT_LINE_NUM_0

Range

LIN_INTERRUPT_LINE_NUM_0
LIN_INTERRUPT_LINE_NUM_1

4.18.9.3.1.8. LinChannelEcuMWakeupSource

Item

Name

LinChannelEcuMWakeupSource

Description

This parameter contains a reference to the Wakeup Source for this controller as defined in the ECU State Manager.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.18.9.3.1.9. LinClockRef

Item

Name

LinClockRef

Description

Reference to the LIN clock source configuration, which is set in the MCU driver configuration.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.18.9.3.2. LinBaudrateConfig

This container contains the baudrate configuration parameter of the Lin driver.

4.18.9.3.2.1. LinChannelPrescalar

Item

Name

LinChannelPrescalar

Description

Prescalar to derive LINCLK from VCLK

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

16777215

Min-value

0

4.18.10. Examples

4.18.10.1. Overview

  1. For AM261x SOM board (ZCZ package):

    • LIN1 pins are exposed and LIN1 is configured with a 19200 baud.

  2. While running the example code :

    • First, it asks to select the example to run.

    • For Master Response example 8 Lin Frames are transmitted with varying PIDs, length and data.

    • For Slave Response example LIN1 will transmit header with PID (0x20h) and slave will respond with data. Received data will be printed on screen and user can confirm if the data is correct.

    • For Slave to Slave example LIN1 will transmit header with PID (0x30h); then one of the slaves will send response with data which should be received by the other slave connected on same cluster. User can confirm if the second slave receives the data.

    • User can also select ‘a’ in console to run all examples sequentially.

4.18.10.2. Hardware Software Setup and Tools

  1. Locate A9 and B9 GPIO pins which are out on the HSEC board.

  2. Since there is no inbuilt transceiver, external transceiver needs to be connected. User can use TLIN1021DEVM as external transceiver.

  3. Locate the LIN, LIN-GND and VBat-LIN pins on both the PLIN device and the transceiver. Refer to the documentation or user manual for both the PLIN device and the board to find the correct pins.

  4. Select appropriate cables with the necessary connectors to connect between the PLIN device, transceiver and the board. Ensure the cables have the correct connectors to fit securely into both the PLIN device and board’s connectors.

  5. For reference, user can follow the connection as per the image.

LIN Hardware Connectivity with PLIN USB

Fig. 4.81 LIN Hardware Connectivity with PLIN USB

  1. Open the PLIN configuration software on your PC. The software is usually provided by the manufacturer of the PLIN device.

  2. Locate the settings for baud rate configuration.

  3. Set the baud rate to 19200 and select mode as Slave.

  4. Apply the changes and save the configuration.

  5. Ensure all connections are secure and properly plugged into their respective connectors on both the PLIN device and the board.

  6. Before powering on the system, double-check all connections to ensure they are correctly made, and there are no loose or improperly connected cables.

  7. After making the connections and configuring the PLIN device, power on both the board and the PLIN device.

  8. Once the system is powered on, verify that the LIN communication is established between the board and the PLIN device.

  9. If Slave to Slave mode example needs to be run; we would need 2 PLIN channels to be connected to the same LIN bus.

  10. Reference PLIN configs are placed at path (mcal/examples/Lin/Peak_PLIN_Config); these can be loaded for ease of use.

4.18.10.3. Steps to build and run example

  1. LIN example application demonstrating the MCAL LIN driver features is in folder <MCAL_ROOT>/examples/Lin.

  2. This application can be built from the build folder by giving “gmake –s lin_app PLATFORM=am261.”

  3. Once the build is completed we get a binary file, which is loaded in our controller and executed.

4.18.10.4. Configuration used to test this example

  1. LIN1 instance is configured as Channel_1.

  2. Baudrate of 19200 is configured.

4.18.10.5. Example Logs


    LIN_APP: Sample Application - STARTS !!!
  
    LIN_APP: LIN MCAL Version Info
    ---------------------
    LIN_APP: Vendor ID: 44
    LIN_APP: Module ID: 82
    LIN_APP: SW Major Version: 10
    LIN_APP: SW Minor Version: 1
    LIN_APP: SW Patch Version: 0
    
    LIN_APP: Variant - Post Build being used !!!
    
    LIN_APP: Using LinChannel_1 -> LIN_INSTANCE_1 
    LIN_APP: Waking LinChannel_1 from sleep 
    LIN_APP: LinChannel_1 Wakeup Successful 
    
    LIN_APP: Enter one of the following
    LIN_APP: m - Send Master Response Lin Request
    LIN_APP: s - Send Slave Response Lin Request
    LIN_APP: x - Send Slave to Slave Lin Request
    LIN_APP: a - Send all types Lin Request
    LIN_APP: q - to quit the application

    LIN_APP: LinChannel_1 operating in Master Response mode 
    LIN_APP: LinChannel_1 Transmission successful for 0 data frame 
    LIN_APP: LinChannel_1 Transmission successful for 1 data frame 
    LIN_APP: LinChannel_1 Transmission successful for 2 data frame 
    LIN_APP: LinChannel_1 Transmission successful for 3 data frame 
    LIN_APP: LinChannel_1 Transmission successful for 4 data frame 
    LIN_APP: LinChannel_1 Transmission successful for 5 data frame 
    LIN_APP: LinChannel_1 Transmission successful for 6 data frame 
    LIN_APP: LinChannel_1 Transmission successful for 7 data frame 
    
    LIN_APP: Enter one of the following
    LIN_APP: m - Send Master Response Lin Request
    LIN_APP: s - Send Slave Response Lin Request
    LIN_APP: x - Send Slave to Slave Lin Request
    LIN_APP: a - Send all types Lin Request
    LIN_APP: q - to quit the application

    LIN_APP: LinChannel_1 operating in Slave Response mode 
    LIN_APP: Received Data :  0xa5  0x55  0xaa  0x55  0xaa  0x55  0xaa  0x55  
    
    LIN_APP: Does the data received match the data sent by the Slave? (y/n) 
    
    LIN_APP: LinChannel_1 Reception successful 
    LIN_APP: Enter one of the following
    LIN_APP: m - Send Master Response Lin Request
    LIN_APP: s - Send Slave Response Lin Request
    LIN_APP: x - Send Slave to Slave Lin Request
    LIN_APP: a - Send all types Lin Request
    LIN_APP: q - to quit the application

    LIN_APP:All sample test case pass 

4.18.10.6. File Structure

📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Lin
┃ ┃ ┃ ┣ 📂Peak_PLIN_Config
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜LinApp.c : Contains LIN test example.
┃ ┃ ┃ ┣ 📜LinApp.h : Contains LIN test example headers.
┃ ┃ ┃ ┣ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Lin_Demo_Cfg
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am261
┃ ┃ ┃ ┃ ┃ ┣ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Lin_Cfg.h : Contains the Precompile switches, Macros for LIN controllers, Hardware Objects etc.
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Lin_Cfg.c : Contains all controllers Pre-Compile Configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Lin_PBcfg.c : Contains all controllers Post-Build Configuration parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┣ 📜README.txt

4.18.11. FAQ’s

None

4.18.12. References

AUTOSAR_SWS_LINDriver
Technical Reference Manual