4.16. GPT Module

4.16.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

GPT

General Purpose Timer

BSW

Basic Software

MCAL

Micro Controller Abstraction Layer

API

Application Programming Interface

DET

Default Error Tracer

SW

Software

MCU

Micro Controller Unit

OS

Operating System

Definitions

Descriptions

Timer channel

Represents a logical timer entity assigned to a timer hardware

Target Time

Something as per requirement occurs once this time value reached

Ticks

Defines the timer resolution, the duration of a timer increment

4.16.2. Introduction

This document describes the functionality, API and configuration of the AUTOSAR BSW module GPT.

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Pre-Compile & Post Build

Vendor ID

GPT_VENDOR_ID (44)

Module ID

GPT_MODULE_ID (100)

Supported Platform

AM261x

4.16.3. Functional Overview

The GPT module initializes and controls the internal General Purpose Timer(s) (GPT) of the microcontroller. The GPT driver provides services and configuration parameters for

  1. Starting and stopping hardware timers

  2. Getting timer values

  3. Controlling time triggered interrupt notifications

Note that the conversion between timer ticks provided by GPT and actual time value is not done by GPT. User software must take care of it. The tick duration of a timer channel depends on channel specific settings (part of GPT driver) as well as on system clock and settings of the clock tree controlled by the MCU module. The brief overview on GPT module is given below:

4.16.3.1. GPT Driver Architecture

The following figure shows where the GPT is in the AUTOSAR architecture.

GPT in AUTOSAR architecture

Fig. 4.73 GPT in AUTOSAR architecture

4.16.3.2. Initialization

The driver GPT is initialized by calling Gpt_Init(), with parameter ConfigPtr referencing a runtime configuration set. After de-initializing the module, that is calling Gpt_DeInit(), it can be initialized again.

4.16.3.3. States

Each GPT channel has up to five different states, depending on its configuration and running state as described below

  1. GPT_UNINITIALIZED: GPT channel is not initialized and not counting.

  2. GPT_INITIALIZED: GPT channel is initialized with Gpt_Init() and not counting.

  3. GPT_RUNNING: GPT channel is initialized and running (counting).

  4. GPT_STOPPED: GPT channel is initialized but not counting (stopped).

  5. GPT_EXPIRED: GPT channel is expired (timer overflowed). This state will be applicable in timer one shot mode where after encountering overflow timer stops.

The figure below taken from the AUTOSAR specification shows the state transitions for different function calls and events:

GPT channel states and state transitions

Fig. 4.74 GPT channel states and state transitions

4.16.3.4. GPT channel modes

The GPT channel can be configured in “one-shot mode” or in “continuous mode”.

  1. One-shot mode: In one-shot mode timer stops counting after overflow (when timer value matches to target value set by Gpt_StartTimer).

  2. Continuous mode: In continuous mode if the timer has reached the target time (timer value = target time), the timer will continue running with the value “0” at next timer tick.

GPT channel mode can be selected through configuration structure Gpt_ConfigType.

4.16.3.5. GPT operating modes

The GPT channels can be configured in normal mode. In this mode, GPT channel will be initialized with Gpt_Init(). In this mode, interrupt notifications will be allowed if enabled through configuration.

GPT driver modes

Fig. 4.75 GPT driver modes

4.16.3.6. GPT starting/stopping channel counting and reading count

The GPT channel starts counting after calling Gpt_Init() . The count value (target time in ticks) is passed to Gpt_StartTimer() function. GPT channel will start counting till target time is reached. Depending on channel mode it will stop (one-shot mode) or roll over (continuous mode) after target time is reached. GPT channel can be explicitly stopped by calling function Gpt_StopTimer(). This will stop channel from counting and disable all its interrupts notifications.

To read channel count when channel is running functions Gpt_GetTimeElapsed() and Gpt_GetTimeRemaining() can be used. As name suggests these give time elapsed after starting timer and time remaining to reach target time respectively. Below snapshot from GPT MCAL spec shows working of these two functions.

Please note that general-purpose timers doesn’t keep track on amount of time that has overflowed by above two functions and the time overflow is always considered absolute and not relative.

Time Elapsed and Time remaining for a timer channel

Fig. 4.76 Time Elapsed and Time remaining for a timer channel

4.16.3.7. GPT interrupt notifications

GPT driver supports enabling and disabling interrupt notifications for GPT channels through Gpt_EnableNotification() and Gpt_DisableNotification() functions. For getting notification from channel, a pointer to notification function should be passed through configuration structure during initialization. In case notification function not available Gpt_EnableNotification() will return an error. Also, it is important to note that interrupt notifications are only enabled when device is in normal mode. In sleep mode interrupt notifications are disabled if they are not wakeup capable (and not enabled for wakeup).

Once interrupt notifications are enabled GPT channel after counting till target time will generate interrupt and channel ISR will be called. This ISR will determine whether to call notification function or wakeup function depending on which one is enabled beforehand. It is responsibility of user software to register these ISR with MCU before starting channel.

4.16.3.8. Assumptions

None

4.16.3.9. Limitations

None

4.16.3.10. Design overview

Will be updated in future releases:

4.16.4. Hardware Features

4.16.4.1. IP Supported Features

  • Free running 32 bit up counter

  • Auto reload mode (can be used for continuous counter operation)

  • Support dynamic Start / Stop counter operation

  • Programmable clock dividers (2n, where n = [0-8])

  • 2 timers modules could be operated in cascaded mode to provide 64bit counter

  • Programmable interrupt generation on overflow, compare and capture

  • Programmable clock source

  • Supports 3 basic functional modes Timer mode, Capture mode & Compare mode

4.16.4.2. AUTOSAR Supported Features

  • Initialization and de-initialization of all GPT channels.

  • Starting and stopping of counting for individual channels.

  • Getting elapsed and remaining counter value

  • Enabling/disabling counter triggered interrupt notifications

  • One shot and continuous mode.

4.16.4.3. Not supported Features

  • Predefined timers are not supported

  • Sleep and wakeup is not supported.

4.16.5. Source files

Description of static files is provided below:

📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Gpt
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Gpt.h : Contains the API’s of the GPT driver to be used by upper layers
┃ ┃ ┃ ┗ 📜Gpt_Irq.h : Contains ISR function declaration
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Gpt.c : Implementation of the API’s for GPT driver
┃ ┃ ┃ ┗ 📜Gpt_Irq.c : Contains ISR function definitions
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┣ 📜Gpt_Priv.h : Contains data structures and Internal function declarations
┃ ┃ ┃ ┗ 📜Gpt_Priv.c : Contains Internal Functions Definitions
┃ ┃ ┗ 📜Makefile
┣ 📂mcal_config
┣ 📂mcal_docs
┗ 📜README.txt

Description of generated files is provided below:

Plugin Files

Description

Gpt_Cfg.h

Contains the base addresses, Precompile switches, Macros for channels, counters etc

Gpt_PBcfg.c

Contains all channels Post-Build Configuration parameters

Gpt_Cfg.c

Contains all channels Pre-Compile Configuration parameters

The below diagram shows the files structure for the GPT driver.

GPT header file include structure

Fig. 4.77 GPT header file include structure

4.16.6. Module requirements

Will be updated in future release:

4.16.6.1. Memory Mapping

Memory Mapping Sections

GPT_CODE

GPT_VAR

GPT_VAR_NOINIT

GPT_CONST

GPT_APPL_CODE

GPT_PBCFG

GPT_START_SEC_VAR_INIT_UNSPECIFIED (.data)

x

GPT_STOP_SEC_VAR_INIT_UNSPECIFIED

x

GPT_START_SEC_CODE (.text)

x

GPT_STOP_SEC_CODE

x

GPT_START_SEC_VAR_NO_INIT_UNSPECIFIED (.bss)

x

GPT_STOP_SEC_VAR_NO_INIT_UNSPECIFIED

x

GPT_START_SEC_CONST_UNSPECIFIED(.rodata)

x

GPT_STOP_SEC_CONST_UNSPECIFIED

x

GPT_START_SEC_ISR_CODE (.text)

x

GPT_STOP_SEC_ISR_CODE

x

GPT_START_SEC_CONST_PTR (.rodata)

x

GPT_STOP_SEC_CONST_PTR

x

GPT_START_SEC_VAR_INIT_PTR (.data)

x

GPT_STOP_SEC_VAR_INIT_PTR

x

For application code used by GPT (like callback functions)

x

4.16.6.2. Scheduling

There is no scheduling functions in Gpt.

4.16.6.3. Error handling

4.16.6.3.1. Development Error Reporting

The module GPT depends on the DET (by default) to report development errors. The DET can be replaced optionally by an equivalent component which is responsible to recognize development errors, if no DET component is available.

AUTOSAR requires that API functions shall check the validity of their respective parameters. These checks are for development error reporting and can be enabled or disabled.

4.16.6.4. Error codes

4.16.6.4.1. Development Errors

Type of Error

Related Error code

Value (Hex)

API service called without module initialization

GPT_E_UINIT

0x0A

API service for initialization is called when already initialized

GPT_E_ALREADY_INITIALIZED

0x0D

API error return code: Init function failed

GPT_E_INIT_FAILED

0x0E

API parameter checking: invalid channel

GPT_E_PARAM_CHANNEL

0x14

API parameter checking: invalid value

GPT_E_PARAM_VALUE

0x15

API parameter checking: invalid pointer

GPT_E_PARAM_POINTER

0x16

API parameter checking: invalid Predef Time

GPT_E_PARAM_PREDEF_TIMER

0x17

API parameter checking: invalid mode

GPT_E_PARAM_MODE

0x1F

4.16.6.4.2. Runtime Errors

Type of Error

Related Error code

Value (Hex)

API service called when timer channel is still busy (running)

GPT_E_BUSY

0x0B

API service called when driver is in wrong mode

GPT_E_MODE

0x0C

4.16.6.4.3. DEM Errors

The errors reported to DEM are described in the following table:

Error Code

Description

Assigned by DEM

GPT_E_HARDWARE_ERROR

This error is raised when issued when GPT Timer register reset fails

4.16.7. Used resources

4.16.7.1. Interrupt Handling

For interrupt notification and wakeup, ISR are provided in GPT driver. There is one ISR for each timer channel. Depending on mode of timer it will call notify function. The interrupt service routines shall be mapped to the interrupt sources of the respective GPT unit interrupt. The supported ISR’s are part of the Gpt_Irq.h file.

Following are timer modules with its respective ISRs and counter blocks for each channel in AM261x:

Timer

ISR

Counter Blocks

GptChannelTickFrequency(Prescaler value)

RTI0

Gpt_Ch0Isr()

GPT_RTI_COUNTER0

GptModule0CounterBlk0Frequency

RTI0

Gpt_Ch1Isr()

GPT_RTI_COUNTER0

GptModule0CounterBlk0Frequency

RTI0

Gpt_Ch2Isr()

GPT_RTI_COUNTER1

GptModule0CounterBlk1Frequency

RTI0

Gpt_Ch3Isr()

GPT_RTI_COUNTER1

GptModule0CounterBlk1Frequency

RTI1

Gpt_Ch4Isr()

GPT_RTI_COUNTER0

GptModule1CounterBlk0Frequency

RTI1

Gpt_Ch5Isr()

GPT_RTI_COUNTER0

GptModule1CounterBlk0Frequency

RTI1

Gpt_Ch6Isr()

GPT_RTI_COUNTER1

GptModule1CounterBlk1Frequency

RTI1

Gpt_Ch7Isr()

GPT_RTI_COUNTER1

GptModule1CounterBlk1Frequency

RTI2

Gpt_Ch8Isr()

GPT_RTI_COUNTER0

GptModule2CounterBlk0Frequency

RTI2

Gpt_Ch9Isr()

GPT_RTI_COUNTER0

GptModule2CounterBlk0Frequency

RTI2

Gpt_Ch10Isr()

GPT_RTI_COUNTER1

GptModule2CounterBlk1Frequency

RTI2

Gpt_Ch11Isr()

GPT_RTI_COUNTER1

GptModule2CounterBlk1Frequency

RTI3

Gpt_Ch12Isr()

GPT_RTI_COUNTER0

GptModule3CounterBlk0Frequency

RTI3

Gpt_Ch13Isr()

GPT_RTI_COUNTER0

GptModule3CounterBlk0Frequency

RTI3

Gpt_Ch14Isr()

GPT_RTI_COUNTER1

GptModule3CounterBlk1Frequency

RTI3

Gpt_Ch15Isr()

GPT_RTI_COUNTER1

GptModule3CounterBlk1Frequency

Gpt-channel tick frequency is considered to be as prescaler value.It needs to be configured under GptDriverConfiguration container of configuration file. It is defined as GptModule<module_number>CounterBlk0Frequency and GptModule<module_number>CounterBlk1Frequency. Here “module_number” defines the rti register number.

There are 2 counter blocks GPT_RTI_COUNTER0 and GPT_RTI_COUNTER1 which can be mapped as shown above. Detailed description on the above parameters are explained in Configuration Section.

For example,if we are configuring 5th channel,then channel id shall be 4 and it belongs to RTI1 timer section and counter block is GPT_RTI_COUNTER0. So the respective prescaler value,i.e.,GptChannelTickFrequency shall be “GptModule1CounterBlk0Frequency” in configuration file.Here ‘Module1’ defined for RTI1 timer and ‘CounterBlk0’ defined for GPT_RTI_COUNTER0 counter block.

4.16.8. Integration description

4.16.8.1. Dependent modules

4.16.8.1.1. MCU

The module MCU powers up the microcontroller’s peripherals at startup time and initializes the PLL as well as the internal clock domains which is connected to the GPT unit. The GPT module also supports an internal divider which can be changed at configuration time using the ‘prescale’ member of Gpt_ChannelConfigType structure to configure the actual GPT functional clock.

Note that Module GPT will not take care of settings which configure the clock and PLL for channels in its init function. This must be done by the MCU module.

4.16.8.1.2. PORT

The GPT module does not require any PORT configuration. Hence there is no dependency on PORT module.

4.16.8.1.3. OS

An operating system can be used for task scheduling, interrupt handling, global suspend and restore of interrupts and creating of the Interrupt Vector Table.The GPT module may use AUTOSAR OS to suspend and restore global interrupts.

4.16.8.1.4. DET

This implementation depends on the DET in order to report development errors The detection of development errors is configurable (ON / OFF), The switch GPT_CFG_DEV_ERROR_DETECT will activate or deactivate the detection of all development errors.

4.16.8.1.5. DEM

By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus().

Note

Dem Event is enable only if $(Module_Name)DemEventParameterRefs is enabled.

4.16.8.1.6. SchM

If multiple AUTOSAR runnables have access to the same Data Store Memory block, the exported AUTOSAR specification enforces data consistency by using an AUTOSAR exclusive area. With this specification, the runnables have mutually exclusive access to the per-instance memory global data, which prevents data corruption. Beside the OS, the BSW Scheduler provides functions that GPT module calls at begin and end of critical sections. This implementation requires 1 level of exclusive access to guard critical sections.

The data consistency mechanism that has to be applied to an ExclusiveArea might be domain, ECU or even project specific. The decision which mechanism has to be applied by RTE / Basic Software Scheduler is taken during ECU integration by setting the Exclusive Area configuration parameter RteExclusiveAreaImplMechanism. This parameter is an input for RTE generator.

For GPT Module, data consistency and exclusive access to critical sections are required for the following sections as shown in the table below:

Exclusive Area Functions used

GPT Function calling Exclusive Area

Need for Exclusive Area

Recommended Exclusive Area Mapping

GPT_EXCLUSIVE_AREA_0

Gpt_StartTimer
Gpt_StopTimer
Gpt_EnableNotification
Gpt_DisableNotification

To protect against multiple access for shared resources

ALL_INTERRUPT_BLOCKING : All interrupts should be blocked as this API’s can be called in the interrupts

4.16.8.1.7. Callback Notification

This section describes notification functions which are passed to GPT driver as a target function. The target function is usually a call-back function. The names of these functions are not fixed and can be changed. At its configurable interfaces the GPT defines notifications that can be mapped to callback functions to respective channels. Function pointer to callback function (for non-wakeup notification) should be defined in Gpt.h with Gpt_NotifyType datatype. There should be separate notification call back function for each timer channel which is configured as Gpt_Channel_Notify<channelnumber>. Example: Gpt_Channel_Notify5 for channel 5

4.16.8.2. Multi-core support

Not Supported

4.16.9. Configuration

4.16.9.1. GptChannelConfigSet

This container is the base of a Configuration Set which contains the configured GPT channels. This way, different configuration sets can be defined for post-build process.

4.16.9.1.1. GptChannelConfiguration

Configuration of an individual GPT channel.

4.16.9.1.1.1. GptChannelId

Item

Name

GptChannelId

Description

Channel Id of the GPT channel. This value will be assigned to the symbolic name derived of the GptChannelConfiguration container short name. Channel 0 -Channel 3 are associated with RTI Module A, Channel 4 -Channel 7 are associated with RTI Module B, Channel 8 -Channel 11 are associated with RTI Module C, Channel 12 -Channel 15 are associated with RTI Module D

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

15

Min-value

0

4.16.9.1.1.2. GptChannelMode

Item

Name

GptChannelMode

Description

Specifies the behavior of the timer channel after the target time is reached.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

GPT_CH_MODE_CONTINUOUS

Range

GPT_CH_MODE_CONTINUOUS
GPT_CH_MODE_ONESHOT

4.16.9.1.1.3. GptCounterBlkId

Item

Name

GptCounterBlkId

Description

This is the Counter block ID for the RTI modules. Each RTI module has 2 counter blocks that are defined in this configuration parameter.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

GPT_RTI_COUNTER1

Range

GPT_RTI_COUNTER0
GPT_RTI_COUNTER1

4.16.9.1.1.4. GptEnableWakeup

Item

Name

GptEnableWakeup

Description

Enables wakeup capability of MCU for a channel.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.16.9.1.1.5. GptNotification

Item

Name

GptNotification

Description

Function pointer to callback function (for non-wakeup notification)

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

4.16.9.1.1.6. GptChannelClkSrcRef

Item

Name

GptChannelClkSrcRef

Description

Reference to the GptClockReferencePoint from which the channel

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.16.9.1.2. GptWakeupConfiguration

Function pointer to callback function (for wakeup notification).

4.16.9.1.2.1. GptWakeupSourceRef

Item

Name

GptWakeupSourceRef

Description

In case the wakeup-capability is true this value is transmitted to the Ecu State Manager.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.16.9.2. GptConfigurationOfOptApiServices

This container contains all configuration switches for configuring optional API services of the GPT driver.

4.16.9.2.1. GptDeinitApi

Item

Name

GptDeinitApi

Description

Adds / removes the service Gpt_DeInit() from the code.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.16.9.2.2. GptEnableDisableNotificationApi

Item

Name

GptEnableDisableNotificationApi

Description

Adds / removes the services Gpt_EnableNotification() and Gpt_DisableNotification from the code.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.16.9.2.3. GptTimeElapsedApi

Item

Name

GptTimeElapsedApi

Description

Adds / removes the service Gpt_GetTimeElapsed() from the code

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.16.9.2.4. GptTimeRemainingApi

Item

Name

GptTimeRemainingApi

Description

Adds / removes the service Gpt_GetTimeRemaining() from the code.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.16.9.2.5. GptVersionInfoApi

Item

Name

GptVersionInfoApi

Description

Adds / removes the service Gpt_GetVersionInfo() from the code.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.16.9.2.6. GptRegisterReadback

Item

Name

GptRegisterReadback

Description

Adds / removes the service Gpt_ConfigRegReadBack() from the code.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.16.9.2.7. GptWakeupFunctionalityApi

Item

Name

GptWakeupFunctionalityApi

Description

Adds / removes the services Gpt_SetMode(), Gpt_EnableWakeup() Gpt_DisableWakeup() and Gpt_CheckWakeup() from the code.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.16.9.3. GptDriverConfiguration

This container contains the module-wide configuration (parameters) of the GPT Driver

4.16.9.3.1. GptDevErrorDetect

Item

Name

GptDevErrorDetect

Description

Enables/Disables development error detection.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.16.9.3.2. GptPredefTimer100us32bitEnable

Item

Name

GptPredefTimer100us32bitEnable

Description

Enables/disables the GPT Predef Timer 100us32bit.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.16.9.3.3. GptPredefTimer1usEnablingGrade

Item

Name

GptPredefTimer1usEnablingGrade

Description

Specifies the grade of enabling the GPT Predef Timers with 1us tick duration.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

GPT_PREDEF_UNDEFINED

Range

GPT_PREDEF_UNDEFINED

4.16.9.3.4. GptReportWakeupSource

Item

Name

GptReportWakeupSource

Description

Enables/Disables wakeup source reporting.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.16.9.3.5. GptTypeofInterruptFunction

Item

Name

GptTypeofInterruptFunction

Description

Type of ISR function

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

GPT_ISR_CAT1

Range

GPT_ISR_VOID
GPT_ISR_CAT1
GPT_ISR_CAT2

4.16.9.3.6. GptPrescaler

Item

Name

GptPrescaler

Description

Prescaler value defined to get the desired frequency.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

2147483647

Min-value

0

4.16.9.3.7. GptModule0CounterBlk0Frequency

Item

Name

GptModule0CounterBlk0Frequency

Description

Specifies the tick frequency of the timer channel in Hz.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

2147483647

Min-value

0

4.16.9.3.8. GptModule0CounterBlk1Frequency

Item

Name

GptModule0CounterBlk1Frequency

Description

Specifies the tick frequency of the timer channel in Hz.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

2147483647

Min-value

0

4.16.9.3.9. GptModule1CounterBlk0Frequency

Item

Name

GptModule1CounterBlk0Frequency

Description

Specifies the tick frequency of the timer channel in Hz.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

2147483647

Min-value

0

4.16.9.3.10. GptModule1CounterBlk1Frequency

Item

Name

GptModule1CounterBlk1Frequency

Description

Specifies the tick frequency of the timer channel in Hz.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

2147483647

Min-value

0

4.16.9.3.11. GptModule2CounterBlk0Frequency

Item

Name

GptModule2CounterBlk0Frequency

Description

Specifies the tick frequency of the timer channel in Hz.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

2147483647

Min-value

0

4.16.9.3.12. GptModule2CounterBlk1Frequency

Item

Name

GptModule2CounterBlk1Frequency

Description

Specifies the tick frequency of the timer channel in Hz.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

2147483647

Min-value

0

4.16.9.3.13. GptModule3CounterBlk0Frequency

Item

Name

GptModule3CounterBlk0Frequency

Description

Specifies the tick frequency of the timer channel in Hz.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

2147483647

Min-value

0

4.16.9.3.14. GptModule3CounterBlk1Frequency

Item

Name

GptModule3CounterBlk1Frequency

Description

Specifies the tick frequency of the timer channel in Hz.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

2147483647

Min-value

0

4.16.9.3.15. GptDefaultOSCounterId

Item

Name

GptDefaultOSCounterId

Description

Default Os Counter Id if node reference to OsCounter ref GptOsCounterRef is not set

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

16

Min-value

0

4.16.9.3.16. GptTimeoutDuration

Item

Name

GptTimeoutDuration

Description

GPT timeout - used in GPT busy wait

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

32000

Max-value

4294967295

Min-value

1

4.16.9.3.17. GptOsCounterRef

Item

Name

GptOsCounterRef

Description

This parameter contains a reference to the OsCounter, which is used by the GPT driver.

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.16.9.3.18. GptClockReferencePoint

This container contains a parameter, which represents a reference to a container of the type McuClockReferencePoint (defined in module MCU).

4.16.9.3.18.1. GptClockReference

Item

Name

GptClockReference

Description

Reference to a container of the type McuClockReferencePoint, to select an input clock.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.16.9.4. Steps To Configure Gpt Module

  1. Open EB Tresos configurator tool, load Gpt. Select the Config Variant ( Precompile/Post-Build)

  2. Go to GptChannelConfiguration Container tab and create a new container.

  3. Configure the channels parameters for all channels.

  4. Save the configuration and generate the configuration.

4.16.10. Examples

The example applications demonstrates use of Gpt module, the list below identifies key steps performed in the example.

4.16.10.1. Overview

  • Gpt Example:

    • Initialize clock using Mcu_Init()

    • Initialize port using Port_Init()

    • Get Gpt Version using Gpt_GetVersionInfo()

    • Initialize Gpt using Gpt_Init()

    • Configure GPT interrupt using GptApp_interruptConfig()

    • Start Gpt timer using Gpt_StartTimer()

    • Enable channel notification for a GPT channel using Gpt_EnableNotification()

    • Read the time already elapsed using Gpt_GetTimeElapsed()

    • Read the time remaining until the target time is reached using Gpt_GetTimeRemaining()

4.16.10.1.1. Flow of the example application

  1. After initialization of timer followed by starting of timer, a channel waits until the interrupt is received. Interrupt indicates that 2sec is completed for respective channel.

  2. After receiving interrupt notification, it stops the current channel and starts next channel to execute the same process.

  3. The provided example application of GPT is configured with a preload value of 1 which equates to around 10ns/tick for a 200 MHz RTI Clock input.

4.16.10.2. Setup required to run example

None

4.16.10.3. How to run examples

4.16.10.3.1. Steps to build and run example

  1. GPT example application demonstrates the MCAL GPT driver features, which is referred from folder <MCAL_ROOT>/examples/Gpt.

  2. This application can be built from the build folder by giving “gmake –s gpt_app PLATFORM=am261”.

  3. Once the build is completed we get a binary file,which is loaded in our controller and executed.

4.16.10.3.2. Configuration used to test this example

  1. In Example program,total 12 channels are configured in AM263x.

  2. Channels 5, 6, 9, 12, 13, 16 are configured in Continuous mode in AM263x

  3. Channels 7, 8, 10, 11, 14, 15 are configured in one-shot mode in AM263x

  4. Channels 1, 2, 3, 4 are not configured as RTI0 timer is being used for delay and OS counter purpose.

  5. Each channel is configured to run for 2sec.

Assuming Source Clock Signal input for RTI is 200MHz and the preload value is set as '1', to achieve the desired tick frequency for the particular gpt channel, use the below mentioned formula: 
 Tick Frequency = RTI Clock Input/(1 + Preload Value)
 
 Here as the RTI Clock Input = 200 MHz = 200 * (10^6) Hz
 
 Hence the Tick frequency shall be,
 
 Tick frequency = (200*10^6)/(1+1) = (200*10^6)/2 = 100 * 10^6 
 
 Tick frequency = 100MHz
  
 Accordingly, the time Period shall be,
 
 Time period = 1/Tick Frequency = 1/100Mhz =10ns 
 
 This defines that for every 10 ns time period, counter will increase by 1 tick.
 
 In order to get 1 sec time period,the number of ticks can be defined in counter upto 1/10ns times, i.e., 100*10^6 ticks.
 
 So, 100*10^6 = 0x05F5E100 shall be passed to Gpt_StartTimer in order to produce 1 sec delay.

4.16.10.4. Sample Log

GPT_APP: Sample Application - STARTS !!!

GPT_APP: Sample Application - STARTS !!!
 
GPT MCAL Version Info
---------------------
Vendor ID           : 44
Module ID           : 100
SW Major Version    : 10
SW Minor Version    : 1
SW Patch Version    : 0
 
----------------------------------------------------------------------------------
GPT_APP: GPTIMER Test Configuration
----------------------------------------------------------------------------------
Initializing channels
Post-Build variant is being used .. 
------------------------------------------
GPT_APP: Running GPT Test for channel 4
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 4f
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 5 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27be95
GPT_APP: Time Remaining Value = 0xba07184
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =4 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 5
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 6 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27be3e
GPT_APP: Time Remaining Value = 0xba07250
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =5 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 6
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 7 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =6 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 7
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 8 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =7 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 8
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 9 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27be4f
GPT_APP: Time Remaining Value = 0xba07238
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =8 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 9
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 10 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =9 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 10
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 11 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =10 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 11
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 12 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27e052
GPT_APP: Time Remaining Value = 0xba05035
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =11 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 12
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 13 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27e04f
GPT_APP: Time Remaining Value = 0xba05031
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =12 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 13
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 14 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =13 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 14
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 15 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =14 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 15
------------------------------------------
GPT_APP: Starting timer for 2 s 
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 16 :)!!!

GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27e05e
GPT_APP: Time Remaining Value = 0xba05027
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer 
GPT Test Passed for channel =15 !!!
GPT Test Passed for configuration!!
GPT Test Completed, njoy life!!!
GPT_APP: Sample Application - DONE !!!
 GPT Stack Usage: 832 bytes
 All tests have Passed!!!

4.16.10.5. File Structure

📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Gpt
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜GptApp.c : Contains GPT test example
┃ ┃ ┃ ┣ 📜GptApp.h : Contains GPT test example header file
┃ ┃ ┃ ┗ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Gpt_Demo_Cfg
┃ ┃ ┃ ┗ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am261
┃ ┃ ┃ ┃ ┃ ┗ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Gpt_Cfg.h : Contains the configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┗ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣📜Gpt_Cfg.c : Contains all Pre-Compile Configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗ 📜Gpt_PBcfg.c : contains all Post build configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┗ 📜README.txt

4.16.11. References

AUTOSAR_SWS_GPTDriver
Technical Reference Manual