5.14. ICU
5.14.1. Types
Base type |
Type Name |
Brief |
|---|---|---|
enum |
This type defines a range of mode type. |
|
enum |
This type defines a input state of ICU driver. |
|
enum |
This type defines Activation range. |
|
enum |
This type defines Input XBAR. |
|
enum |
This type defines ECAP selection. |
|
enum |
This type defines available measurement modes. |
|
enum |
This type defines Signal Measurement Property range. |
|
enum |
This type defines TimeStamp Property range. |
|
typedef uint16 |
This type defines Value type. |
|
typedef uint32 |
This type defines return value Icu_GetTimeStampIndex. |
|
typedef uint32 |
This type defines return value of Icu-Icu_GetEdgeNumbers. |
|
typedef void(*)(void) |
Notification callback function pointer |
|
typedef uint8 |
This type defines Channel type. |
|
typedef uint8 |
This type defines Prescaler type. |
5.14.1.1. enum Icu_ModeType
Enumerator |
Value |
Description |
|---|---|---|
ICU_MODE_NORMAL |
Normal Mode. |
|
ICU_MODE_SLEEP |
Sleep Mode. |
Brief: This type defines a range of mode type.
5.14.1.2. enum Icu_InputStateType
Enumerator |
Value |
Description |
|---|---|---|
ICU_ACTIVE |
Module is in active state. |
|
ICU_IDLE |
Module is in idle state. |
Brief: This type defines a input state of ICU driver.
5.14.1.3. enum Icu_ActivationType
Enumerator |
Value |
Description |
|---|---|---|
ICU_RISING_EDGE |
Rising Edge Activation type. |
|
ICU_FALLING_EDGE |
Falling Edge Activation type. |
|
ICU_BOTH_EDGES |
Both Edge Activation type. |
Brief: This type defines Activation range.
5.14.1.4. enum Icu_XbarSelect
Enumerator |
Value |
Description |
|---|---|---|
INPUT_XBAR_0 |
=202 |
XBAR 0. |
INPUT_XBAR_1 |
XBAR 1. |
|
INPUT_XBAR_2 |
XBAR 2. |
|
INPUT_XBAR_3 |
XBAR 3. |
|
INPUT_XBAR_4 |
XBAR 4. |
|
INPUT_XBAR_5 |
XBAR 5. |
|
INPUT_XBAR_6 |
XBAR 6. |
|
INPUT_XBAR_7 |
XBAR 7. |
|
INPUT_XBAR_8 |
XBAR 8. |
|
INPUT_XBAR_9 |
XBAR 9. |
|
INPUT_XBAR_10 |
XBAR 10. |
|
INPUT_XBAR_11 |
XBAR 11. |
|
INPUT_XBAR_12 |
XBAR 12. |
|
INPUT_XBAR_13 |
XBAR 13. |
|
INPUT_XBAR_14 |
XBAR 14. |
|
INPUT_XBAR_15 |
XBAR 15. |
|
INPUT_XBAR_16 |
XBAR 16. |
|
INPUT_XBAR_17 |
XBAR 17. |
|
INPUT_XBAR_18 |
XBAR 18. |
|
INPUT_XBAR_19 |
XBAR 19. |
|
INPUT_XBAR_20 |
XBAR 20. |
|
INPUT_XBAR_21 |
XBAR 21. |
|
INPUT_XBAR_22 |
XBAR 22. |
|
INPUT_XBAR_23 |
XBAR 23. |
|
INPUT_XBAR_24 |
XBAR 24. |
|
INPUT_XBAR_25 |
XBAR 25. |
|
INPUT_XBAR_26 |
XBAR 26. |
|
INPUT_XBAR_27 |
XBAR 27. |
|
INPUT_XBAR_28 |
XBAR 28. |
|
INPUT_XBAR_29 |
XBAR 29. |
|
INPUT_XBAR_30 |
XBAR 30. |
|
INPUT_XBAR_31 |
XBAR 31. |
Brief: This type defines Input XBAR.
5.14.1.5. enum Icu_IntrCapSelect
Enumerator |
Value |
Description |
|---|---|---|
ECAP_CEVT1_INT |
CSL_ECAP_ECEINT_ECFLG_CEVT1_MASK |
|
ECAP_CEVT2_INT |
CSL_ECAP_ECEINT_ECFLG_CEVT2_MASK |
|
ECAP_CEVT3_INT |
CSL_ECAP_ECEINT_ECFLG_CEVT3_MASK |
|
ECAP_CEVT4_INT |
CSL_ECAP_ECEINT_ECFLG_CEVT4_MASK |
|
ECAP_CEVT1_CEVT2_INT |
CSL_ECAP_ECEINT_ECFLG_CEVT1_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT2_MASK |
|
ECAP_CEVT1_CEVT3_INT |
CSL_ECAP_ECEINT_ECFLG_CEVT1_MASK| CSL_ECAP_ECEINT_ECFLG_CEVT3_MASK |
|
ECAP_CEVT1_CEVT4_INT |
CSL_ECAP_ECEINT_ECFLG_CEVT1_MASK| CSL_ECAP_ECEINT_ECFLG_CEVT4_MASK |
|
ECAP_CEVT2_CEVT3_INT |
CSL_ECAP_ECEINT_ECFLG_CEVT2_MASK| CSL_ECAP_ECEINT_ECFLG_CEVT3_MASK |
|
ECAP_CEVT2_CEVT4_INT |
CSL_ECAP_ECEINT_ECFLG_CEVT2_MASK| CSL_ECAP_ECEINT_ECFLG_CEVT4_MASK |
|
ECAP_CEVT3_CEVT4_INT |
CSL_ECAP_ECEINT_ECFLG_CEVT3_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT4_MASK |
|
ECAP_CEVT1_CEVT2_CEVT3_INT |
CSL_ECAP_ECEINT_ECFLG_CEVT1_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT2_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT3_MASK |
|
ECAP_CEVT1_CEVT2_CEVT4_INT |
=CSL_ECAP_ECEINT_ECFLG_CEVT1_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT2_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT4_MASK |
|
ECAP_CEVT1_CEVT3_CEVT4_INT |
=CSL_ECAP_ECEINT_ECFLG_CEVT1_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT3_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT4_MASK |
|
ECAP_CEVT2_CEVT3_CEVT4_INT |
=CSL_ECAP_ECEINT_ECFLG_CEVT2_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT3_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT4_MASK |
|
ECAP_INT_ALLCAPS |
CSL_ECAP_ECEINT_ECFLG_CEVT1_MASK|CSL_ECAP_ECEINT_ECFLG_CEVT2_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT3_MASK | CSL_ECAP_ECEINT_ECFLG_CEVT4_MASK |
Brief: This type defines ECAP selection.
5.14.1.6. enum Icu_MeasurementModeType
Enumerator |
Value |
Description |
|---|---|---|
ICU_MODE_SIGNAL_EDGE_DETECT |
Signal Edge Detect Mode. |
|
ICU_MODE_SIGNAL_MEASUREMENT |
Signal measurement Mode. |
|
ICU_MODE_TIMESTAMP |
Signal Timestamp Mode. |
|
ICU_MODE_EDGE_COUNTER |
Signal Edge counter Mode. |
Brief: This type defines available measurement modes.
5.14.1.7. enum Icu_SignalMeasurementPropertyType
Enumerator |
Value |
Description |
|---|---|---|
ICU_LOW_TIME |
Signal Low time. |
|
ICU_HIGH_TIME |
Signal High time. |
|
ICU_PERIOD_TIME |
Signal Period time. |
|
ICU_DUTY_CYCLE |
Signal Duty Cycle time. |
Brief: This type defines Signal Measurement Property range.
5.14.1.8. enum Icu_TimestampBufferType
Enumerator |
Value |
Description |
|---|---|---|
ICU_LINEAR_BUFFER |
Linear Buffer to be used in Timestamp. |
|
ICU_CIRCULAR_BUFFER |
Circular Buffer to be used in Timestamp. |
Brief: This type defines TimeStamp Property range.
5.14.1.9. typedef Icu_ValueType
typedef uint16 Icu_ValueType;
Brief: This type defines Value type.
5.14.1.10. typedef Icu_IndexType
typedef uint32 Icu_IndexType;
Brief: This type defines return value Icu_GetTimeStampIndex.
5.14.1.11. typedef Icu_EdgeNumberType
typedef uint32 Icu_EdgeNumberType;
Brief: This type defines return value of Icu-Icu_GetEdgeNumbers.
5.14.1.12. typedef Icu_NotifyFuncType
typedef void(* Icu_NotifyFuncType) (void);
Brief: Notification callback function pointer
5.14.1.13. typedef Icu_ChannelType
typedef uint8 Icu_ChannelType;
Brief: This type defines Channel type.
5.14.1.14. typedef Icu_ChannelPrescalerType
typedef uint8 Icu_ChannelPrescalerType;
Brief: This type defines Prescaler type.
5.14.2. Structures
Name |
Brief |
|---|---|
This type defines Duty Cycle struct. |
|
ICU Channel Config Structure of Pre-Compile only. |
|
ICU Config Structure of Pre-Compile only. |
|
ICU Channel Config Structure. |
|
ICU Config Structure. |
5.14.3. Defines
Name |
Brief |
|---|---|
ICU_VENDOR_ID |
Texas Instruments Vendor ID. |
ICU_MODULE_ID |
ICU Driver Module ID. |
ICU_INSTANCE_ID |
ICU Driver Instance ID. |
ICU_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
ICU_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
ICU_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
ICU_AR_RELEASE_MAJOR_VERSION |
AUTOSAR Major version specification implemented by ICU Driver. |
ICU_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by ICU Driver. |
ICU_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by ICU Driver. |
ICU_ISR_VOID |
void ISR type |
ICU_ISR_CAT1 |
Category 1 ISR type. |
ICU_ISR_CAT2 |
Category 2 ISR type. |
ICU_INIT_ID |
Icu_Init() API Service ID. |
ICU_DEINIT_ID |
Icu_DeInit() API Service ID. |
ICU_SETMODE_ID |
Icu_SetMode() API Service ID. |
ICU_SETACTIVATIONCONDITION_ID |
Icu_SetActivationCondition() API Service ID. |
ICU_DISABLENOTIFICATION_ID |
Icu_DisableNotification() API Service ID. |
ICU_ENABLENOTIFICATION_ID |
Icu_EnableNotification() API Service ID. |
ICU_GETINPUTSTATE_ID |
Icu_GetInputState() API Service ID. |
ICU_STARTTIMESTAMP_ID |
Icu_StartTimestamp() API Service ID. |
ICU_STOPTIMESTAMP_ID |
Icu_StopTimestamp() API Service ID. |
ICU_GETTIMESTAMPINDEX_ID |
Icu_GetTimeStampIndex() API Service ID. |
ICU_RESETEDGECOUNT_ID |
Icu_ResetEdgeCount() API Service ID. |
ICU_ENABLEEDGECOUNT_ID |
Icu_EnableEdgeCount() API Service ID. |
ICU_ENABLEEDGEDETECTION_ID |
Icu_EnableEdgeDetection() API Service ID. |
ICU_DISABLEEDGEDETECTION_ID |
Icu_DisableEdgeDetection() API Service ID. |
ICU_DISABLEEDGECOUNT_ID |
Icu_DisableEdgeCount() API Service ID. |
ICU_GETEDGENUMBERS_ID |
Icu_GetEdgeNumbers() API Service ID. |
ICU_STARTSIGNALMEASUREMENT_ID |
Icu_StartSignalMeasurement() API Service ID. |
ICU_STOPSIGNALMEASUREMENT_ID |
Icu_StopSignalMeasurement() API Service ID. |
ICU_GETTIMEELAPSED_ID |
Icu_GetTimeElapsed() API Service ID. |
ICU_GETDUTYCYCLEVALUES_ID |
Icu_GetDutyCycleValues() API Service ID. |
ICU_GETVERSIONINFO_ID |
Icu_GetVersionInfo() API Service ID. |
ICU_REGISTERREADBACK_ID |
Icu_RegisterReadback() API Service ID. |
ICU_E_PARAM_POINTER |
API service called with invalid pointer. |
ICU_E_PARAM_CHANNEL |
API service called with invalid channel identifier or channel not configured. |
ICU_E_PARAM_ACTIVATION |
API service calleed with an invalid or not feasible activation. |
ICU_E_INIT_FAILED |
Init Function Failed. |
ICU_E_PARAM_BUFFER_SIZE |
API service used with invalid Buffer size. |
ICU_E_PARAM_MODE |
API service called with invalid mode. |
ICU_E_UNINIT |
API service calleed without module initialisation. |
ICU_E_NOT_STARTED |
Icu_StopTimestamp called on channel not started or already stopped. |
ICU_E_BUSY_OPERATION |
API service called while a running operation. |
ICU_E_ALREADY_INITIALIZED |
API service Icu_Init called when module already initialized. |
ICU_E_PARAM_NOTIFY_INTERVAL |
API service called when notify interval is invalid. |
ICU_E_PARAM_VINFO |
API service Icu_GetVersionInfo called and parameter is invalid. |
ICU_STATUS_UNINIT |
ICU driver Status uninitialized. |
ICU_STATUS_INIT |
ICU driver Status Initialized. |
ICU_FALLING |
Capture regsiter configuration for FALLING edge |
ICU_RISING |
Capture regsiter configuration for RISING edge |
5.14.4. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Icu_Init(const Icu_ConfigType * ConfigPtr) |
Service for ICU initialization. |
void |
Icu_DeInit(void ) |
Service for ICU de-initialization. |
void |
Icu_SetActivationCondition(Icu_ChannelType Channel, Icu_ActivationType Activation) |
Service for setting Activation Condition. |
void |
Icu_DisableNotification(Icu_ChannelType Channel) |
Service for disabling notification. |
void |
Icu_EnableNotification(Icu_ChannelType Channel) |
Service for enabling notification. |
Icu_GetInputState(Icu_ChannelType Channel) |
Service for getting the ICU input status. |
|
void |
Icu_StartTimestamp(Icu_ChannelType Channel, Icu_ValueType * BufferPtr, uint16 BufferSize, uint16 NotifyInterval) |
Service for starts the captuing of timer values on the edges. |
void |
Icu_StopTimestamp(Icu_ChannelType Channel) |
Service for stopping the timestamp measurement. |
Icu_GetTimestampIndex(Icu_ChannelType Channel) |
Service for reading the timestamp index of a givem channel. |
|
void |
Icu_ResetEdgeCount(Icu_ChannelType Channel) |
Service for resets the value of the counted edges to zero. |
void |
Icu_EnableEdgeCount(Icu_ChannelType Channel) |
Service enabling the counting of edges of a given channel. |
void |
Icu_DisableEdgeCount(Icu_ChannelType Channel) |
Service for disabling the couting of edges of the given channel. |
Icu_GetEdgeNumbers(Icu_ChannelType Channel) |
Service for reading the number of counted edges. |
|
void |
Icu_EnableEdgeDetection(Icu_ChannelType Channel) |
Service for enabling/re-enabling the detection of edges of the given channel. |
void |
Icu_DisableEdgeDetection(Icu_ChannelType Channel) |
Service for disabling the detection of edges of the given channel. |
void |
Service for starting the measurement of signals. |
|
void |
Icu_StopSignalMeasurement(Icu_ChannelType Channel) |
Service for stopping the measurement of signals. |
Icu_GetTimeElapsed(Icu_ChannelType Channel) |
Service for reading the elasped time for the given channel. |
|
void |
Icu_GetDutyCycleValues(Icu_ChannelType Channel, Icu_DutyCycleType * DutyCycleValues) |
Service for reading the coherent active time and period time of given channel. |
void |
Icu_CheckWakeup(EcuM_WakeupSourceType WakeupSource) |
This function checks if a wakeup capable ICU channel is the source for a wakeup event and calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid ICU channel wakeup event. |
void |
Icu_DisableWakeup(Icu_ChannelType Channel) |
This function disables the wakeup capability of a single ICU channel. |
void |
Icu_EnableWakeup(Icu_ChannelType Channel) |
This function (re-)enables the wakeup capability of the given ICU channel. |
void |
Icu_SetMode(Icu_ModeType Mode) |
This function sets the ICU mode. |
Std_ReturnType |
Icu_RegisterReadback(Icu_ChannelType Channel, Icu_RegisterReadbackType * RegRbPtr) |
This function reads the important registers of the hardware unit and returns the value in the structure. |
5.14.4.1. function Icu_Init
void Icu_Init(
const Icu_ConfigType * ConfigPtr
)
Brief: Service for ICU initialization.
Initializes internal variables and the ECAP unit of the micro controller. The function can be called on task level.
Service ID[hex] - 0x00
Sync/Async - Synchronous
Reentrancy - Non Reentrant
Parameters:
CfgPtr Pointer to configuration
Returns:
None
Return: None
5.14.4.2. function Icu_DeInit
void Icu_DeInit(
void
)
Brief: Service for ICU de-initialization.
DeInit ECAP module
Service ID[hex] - 0x01
Sync/Async - Synchronous
Reentrancy - Non Reentrant
Returns:
None
Return: None
5.14.4.3. function Icu_SetActivationCondition
void Icu_SetActivationCondition(
Icu_ChannelType Channel,
Icu_ActivationType Activation
)
Brief: Service for setting Activation Condition.
This service sets the Activation edge for channel Type of activation (if supported by hardware) ICU_RISING_EDGE, ICU_FALLING_EDGE, ICU_BOTH_EDGES.
Service ID[hex] - 0x05
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Activation - activation edge to be used by ICU module
Returns:
None
Return: None
5.14.4.4. function Icu_DisableNotification
void Icu_DisableNotification(
Icu_ChannelType Channel
)
Brief: Service for disabling notification.
This service disables the notificaiton of a channel
Service ID[hex] - 0x06
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.5. function Icu_EnableNotification
void Icu_EnableNotification(
Icu_ChannelType Channel
)
Brief: Service for enabling notification.
This service enables the notificaiton of a channel
Service ID[hex] - 0x07
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.6. function Icu_GetInputState
Icu_InputStateType Icu_GetInputState(
Icu_ChannelType Channel
)
Brief: Service for getting the ICU input status.
This service returns the status of the ICU input
Service ID[hex] - 0x08
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
ICU_ACTIVE - Module is in active state
ICU_IDLE - Module is in idle state
Return: Icu_InputStateType
5.14.4.7. function Icu_StartTimestamp
void Icu_StartTimestamp(
Icu_ChannelType Channel,
Icu_ValueType * BufferPtr,
uint16 BufferSize,
uint16 NotifyInterval
)
Brief: Service for starts the captuing of timer values on the edges.
This service starts the capturing of timer values on the edges
Service ID[hex] - 0x09
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel
BufferSize
NotifyInterval
BufferPtr
Returns:
None
Return: None
5.14.4.8. function Icu_StopTimestamp
void Icu_StopTimestamp(
Icu_ChannelType Channel
)
Brief: Service for stopping the timestamp measurement.
This service stops timestamp measurement of the given channel.
Service ID[hex] - 0x0A
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.9. function Icu_GetTimestampIndex
Icu_IndexType Icu_GetTimestampIndex(
Icu_ChannelType Channel
)
Brief: Service for reading the timestamp index of a givem channel.
This service reads the timestamp index of a given channel.
Service ID[hex] - 0x0B
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
timestamp index value
Return: Icu_IndexType
5.14.4.10. function Icu_ResetEdgeCount
void Icu_ResetEdgeCount(
Icu_ChannelType Channel
)
Brief: Service for resets the value of the counted edges to zero.
This service resets the value of the counted edges to zero.
Service ID[hex] - 0x0C
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.11. function Icu_EnableEdgeCount
void Icu_EnableEdgeCount(
Icu_ChannelType Channel
)
Brief: Service enabling the counting of edges of a given channel.
This service enables the couting of edges of the given channel.
Service ID[hex] - 0x0D
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.12. function Icu_DisableEdgeCount
void Icu_DisableEdgeCount(
Icu_ChannelType Channel
)
Brief: Service for disabling the couting of edges of the given channel.
This service disables the couting of edges of a given channel.
Service ID[hex] - 0x0E
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.13. function Icu_GetEdgeNumbers
Icu_EdgeNumberType Icu_GetEdgeNumbers(
Icu_ChannelType Channel
)
Brief: Service for reading the number of counted edges.
This service reads the number of counted edges.
Service ID[hex] - 0x0F
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
Number of counted edges
Return: Icu_EdgeNumberType
5.14.4.14. function Icu_EnableEdgeDetection
void Icu_EnableEdgeDetection(
Icu_ChannelType Channel
)
Brief: Service for enabling/re-enabling the detection of edges of the given channel.
This service enables/re-enables the detection of edges of a channel.
Service ID[hex] - 0x16
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.15. function Icu_DisableEdgeDetection
void Icu_DisableEdgeDetection(
Icu_ChannelType Channel
)
Brief: Service for disabling the detection of edges of the given channel.
This service disables the detection of edges of a channel.
Service ID[hex] - 0x17
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.16. function Icu_StartSignalMeasurement
void Icu_StartSignalMeasurement(
Icu_ChannelType Channel
)
Brief: Service for starting the measurement of signals.
This service starts the measurement of signals of a given channel.
Service ID[hex] - 0x13
Sync/Async - Asynchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.17. function Icu_StopSignalMeasurement
void Icu_StopSignalMeasurement(
Icu_ChannelType Channel
)
Brief: Service for stopping the measurement of signals.
This service stops the measurement of signals of a given channel.
Service ID[hex] - 0x14
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.18. function Icu_GetTimeElapsed
Icu_ValueType Icu_GetTimeElapsed(
Icu_ChannelType Channel
)
Brief: Service for reading the elasped time for the given channel.
This service reads elasped time for a given channel.
Service ID[hex] - 0x10
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
Elapsed time for the given channel
Return: Icu_ValueType
5.14.4.19. function Icu_GetDutyCycleValues
void Icu_GetDutyCycleValues(
Icu_ChannelType Channel,
Icu_DutyCycleType * DutyCycleValues
)
Brief: Service for reading the coherent active time and period time of given channel.
This service reads active time and period of given channel.
Service ID[hex] - 0x11
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Channel - Numeric identifier of the ICU channel
DutyCycleValues - pointer to store dutycycle
Returns:
None
Return: None
5.14.4.20. function Icu_CheckWakeup
void Icu_CheckWakeup(
EcuM_WakeupSourceType WakeupSource
)
Brief: This function checks if a wakeup capable ICU channel is the source for a wakeup event and calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid ICU channel wakeup event.
Service ID[hex] - 0x15
Sync/Async - Synchronous
Reentrancy - Reentrant(limited according to ICU050)
Parameters:
WakeupSource - Informatin on wakeup source to be checked. The associated ICU channel can be determined from configuration data
Returns:
None
Return: None
5.14.4.21. function Icu_DisableWakeup
void Icu_DisableWakeup(
Icu_ChannelType Channel
)
Brief: This function disables the wakeup capability of a single ICU channel.
Service ID[hex] - 0x03
Sync/Async - Synchronous
Reentrancy - Reentrant(limited according to ICU050)
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.22. function Icu_EnableWakeup
void Icu_EnableWakeup(
Icu_ChannelType Channel
)
Brief: This function (re-)enables the wakeup capability of the given ICU channel.
Service ID[hex] - 0x04
Sync/Async - Synchronous
Reentrancy - Reentrant(limited according to ICU050)
Parameters:
Channel - Numeric identifier of the ICU channel
Returns:
None
Return: None
5.14.4.23. function Icu_SetMode
void Icu_SetMode(
Icu_ModeType Mode
)
Brief: This function sets the ICU mode.
Service ID[hex] - 0x02
Sync/Async - Synchronous
Reentrancy - Non Reentrant
Parameters:
Mode - ICU_MODE_NORMAL: Normal operation, all used interrupts are enabled according to the notification requests, ICU_MODE_SLEEP: Reduced power mode. In sleep mode only those notifications are available which are configured as wakeup capable.
Returns:
None
Return: None
5.14.4.24. function Icu_RegisterReadback
Std_ReturnType Icu_RegisterReadback(
Icu_ChannelType Channel,
Icu_RegisterReadbackType * RegRbPtr
)
Brief: This function reads the important registers of the hardware unit and returns the value in the structure.
This API is used to check the status of critical registers which donot change during program execution.
Service ID[hex] - 0x15
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
ChannelNumber - Numeric identifier of the ICU channel
RegRbPtr - Pointer to where to store the readback values. If this pointer is NULL, then the API will return E_NOT_OK.
Returns:
E_OK - Register read back has been done successfully
E_NOT_OK - Register read back failed
Return: Std_ReturnType