5.2. CAN
5.2.1. Types
Base type |
Type Name |
Brief |
|---|---|---|
enum |
Can Mailbox direction enum. |
|
enum |
Can Handle Type enum. |
|
enum |
Can Tx/Rx processing enum. |
|
enum |
Can Controller Error Types. |
|
enum |
Can Controller instance enum. |
|
typedef void(*)(uint32 canErrorType) |
Typedef for error notification function pointer. |
|
typedef uint8 |
Can Controller State enum type. |
|
typedef uint32 |
Can Interrupt Mask type. |
5.2.1.1. enum Can_MailBoxDirectionType
Enumerator |
Value |
Description |
|---|---|---|
CAN_MAILBOX_DIRECTION_RX |
0x0U |
Mailbox is for receive. |
CAN_MAILBOX_DIRECTION_TX |
0x1U |
Mailbox is for transmit. |
Brief: Can Mailbox direction enum.
5.2.1.2. enum Can_HandleType
Enumerator |
Value |
Description |
|---|---|---|
CAN_FULL |
0x0U |
For only one L-PDU (identifier) is handled by the hardware object. |
CAN_BASIC |
0x1U |
For several L-PDUs are handled by the hardware object. |
Brief: Can Handle Type enum.
5.2.1.3. enum Can_TxRxProcessingType
Enumerator |
Value |
Description |
|---|---|---|
CAN_TX_RX_PROCESSING_INTERRUPT |
0x0U |
Interrupt Mode of operation. |
CAN_TX_RX_PROCESSING_MIXED |
0x1U |
Mixed Mode of operation. |
CAN_TX_RX_PROCESSING_POLLING |
0x2U |
Polling Mode of operation. |
Brief: Can Tx/Rx processing enum.
5.2.1.4. enum Can_ECCErrorType
Enumerator |
Value |
Description |
|---|---|---|
CAN_ECC_ERROR_TYPE_PARITY |
0x0U |
Parity Error. |
CAN_ECC_ERROR_TYPE_SEC |
0x1U |
Single Bit Error Detected and corrected. |
CAN_ECC_ERROR_TYPE_DED |
0x2U |
Double Bit Error Detected. |
Brief: Can Controller Error Types.
5.2.1.5. enum Can_ControllerInstance
Enumerator |
Value |
Description |
|---|---|---|
CAN_CONTROLLER_INSTANCE_MCAN0 |
0x0U |
MCAN0 Controller Instance. |
CAN_CONTROLLER_INSTANCE_MCAN1 |
0x1U |
MCAN1 Controller Instance. |
Brief: Can Controller instance enum.
5.2.1.6. typedef Can_ErrNotifyType
typedef void(* Can_ErrNotifyType) (uint32 canErrorType);
Brief: Typedef for error notification function pointer.
5.2.1.7. typedef CanControllerState_Type
typedef uint8 CanControllerState_Type;
Brief: Can Controller State enum type.
5.2.1.8. typedef Can_InterruptMask_Type
typedef uint32 Can_InterruptMask_Type;
Brief: Can Interrupt Mask type.
5.2.2. Structures
Name |
Brief |
|---|---|
Structure defining the filter mask to be used |
|
Structure defining the HW filter to be used. |
|
Structure defining the CAN FD data phase baud rate configuration. |
|
Structure defining the CAN baud rate configuration. |
|
Can Controller Configuration definition. |
|
Can Controller Pre Compile Configuration definition. |
|
Can mailbox configuration definition. |
|
Can mailox Pre compile configuration definition. |
|
Can MCAL root configuration structure. |
|
Register Readback Structure The Safety API to readback CAN register vales will populate this structure. |
5.2.3. Defines
Name |
Brief |
|---|---|
CAN_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
CAN_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
CAN_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
CAN_AR_RELEASE_MAJOR_VERSION |
AUTOSAR Major version specification implemented by CanDriver. |
CAN_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by CanDriver. |
CAN_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by CanDriver. |
CAN_VENDOR_ID |
Texas Instruments Vendor ID. |
CAN_MODULE_ID |
Can Driver Module ID |
CAN_INSTANCE_ID |
CAN Driver Instance ID. |
CAN_UNINIT |
CAN Driver is NOT initialized. |
CAN_READY |
CAN Driver is initialized. |
CAN_INIT_ID |
Can_Init() |
CAN_MAINFCT_WRITE_ID |
Can_MainFunction_Write() |
CAN_SETCTR_ID |
Can_SetControllerMode() |
CAN_DIINT_ID |
Can_DisableControllerInterrupts() |
CAN_ENINT_ID |
Can_EnableControllerInterrupts() |
CAN_WRITE_ID |
Can_Write() |
CAN_VERSION_ID |
Can_GetVersionInfo() |
CAN_MAINFCT_READ_ID |
Can_MainFunction_Read() |
CAN_MAINFCT_BO_ID |
Can_MainFunction_BusOff() |
CAN_MAINFCT_WU_ID |
Can_MainFunction_Wakeup() |
CAN_CKWAKEUP_ID |
Can_CheckWakeup() |
CAN_MAINFCT_MODE_ID |
Can_MainFunction_Mode() |
CAN_SETBAUDRATE_ID |
Can_SetBaudrate() |
CAN_DEINIT_ID |
Can_DeInit() |
CAN_GETCTRERRST_ID |
Can_GetControllerErrorState() |
CAN_GETCTRMODE_ID |
Can_GetControllerMode() |
CAN_RXPROCESS_ID_INTERRUPT |
Can_RxProcess_Interrupt() |
CAN_RXPROCESS_ID_POLLING |
Can_RxProcess_Polling() |
CAN_REGISTER_READBACK_ID |
Can_RegisterReadback() |
CAN_LOOPBACK_ENABLE_ID |
Can_TestLoopBackModeEnable() |
CAN_LOOPBACK_DISABLE_ID |
Can_TestLoopBackModeDisable() |
CAN_ZERO |
Numerical value. |
CAN_RXINDI_ID |
CanIf_RxIndication callback. |
CAN_TXCNF_ID |
CanIf_TxConfirmation callback. |
CAN_CTRWAKEUP_ID |
Controller Wakeup indication callback. |
CAN_CTRBUSOFF_ID |
Controller Off indication callback. |
CAN_E_PARAM_POINTER |
ERROR:NULL_PTR passed as parameter. |
CAN_E_PARAM_HANDLE |
ERROR:Invalid Controller Handle. |
CAN_E_PARAM_DATA_LENGTH |
ERROR:Invalid length of msg. |
CAN_E_PARAM_CONTROLLER |
ERROR:Invalid controller id. |
CAN_E_UNINIT |
ERROR:Error due to API invoked without performing Can_Init() |
CAN_E_TRANSITION |
ERROR:Error during Controller state transition. |
CAN_E_PARAM_BAUDRATE |
ERROR:Invalid Baudrate configuration. |
CAN_E_ICOM_CONFIG_INVALID |
ERROR:Invalid config ID. |
CAN_E_INIT_FAILED |
ERROR:Timeout occured. |
CAN_E_DATALOST |
ERROR:Data lost/dropped . Runtime Error. |
CAN_CFG_ID_0 |
Config 0 (All configurations ON) |
CAN_CFG_ID_1 |
Config 1 (All configurations OFF). CAN_CFG_ID_1 is used only for compile check. |
CAN_CFG_ID_2 |
Config 2 (All configurations ON except DET OFF) |
CAN_CFG_ID_3 |
Config 3 (Configurator auto generated file) |
CAN_CFG_ID_4 |
Config 4 (Configurator auto generated file MCAN with pre-compile variant ON) |
CAN_CFG_ID_5 |
Config 5 (All configurations ON but used only for testing WakeUp by external HW event and Performance tests) |
CAN_CFG_ID_6 |
Config 6 (Used for MCAN Testing) |
CAN_CFG_ID_7 |
Config 7 (Used for MCAN Testing) |
5.2.4. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Can_GetVersionInfo(Std_VersionInfoType * Can_VersionInfo) |
Function returns the version information of this module. |
void |
Can_Init(const Can_ConfigType * CfgPtr) |
This function initializes the module. All the required initialization for the CAN driver and hardware is performed in this function. |
Std_ReturnType |
Can_SetControllerMode(uint8 Controller, Can_ControllerStateType Transition) |
This function performs software triggered state transitions of the CAN controller State machine. |
Std_ReturnType |
Can_Write(Can_HwHandleType Hth, const Can_PduType * PduInfo) |
This function is called by CanIf to pass a CAN message to CanDrv for transmission. |
Std_ReturnType |
Can_CheckWakeup(uint8 Controller) |
This function checks if a wakeup has occurred for the given controller. |
void |
Can_DisableControllerInterrupts(uint8 Controller) |
This function disables all interrupts for this CAN controller Basically it will Disable the CAN interrupts(reset bit 1 in CTL reg(IE0=0)). |
void |
Can_EnableControllerInterrupts(uint8 Controller) |
This function will Enable the interrupts for the Controller desired. It will restore the interrupts that were defined in the configuration. Basically it will enable the CAN interrupts. |
void |
Can_MainFunction_Write(void ) |
This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING. |
void |
Can_MainFunction_BusOff(void ) |
This function performs the polling of bus-off events that are configured statically as ‘to be polled’. |
void |
Can_MainFunction_Read(void ) |
This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING. |
void |
Can_MainFunction_Wakeup(void ) |
This function performs the polling of wake-up events that are configured statically as ‘to be polled. |
void |
Can_MainFunction_Mode(void ) |
This function performs the polling of CAN controller mode transitions This will indicate only the CanController SW state and cannot indicate any HW state as there is no HW state exposed from the Can Controller. |
Std_ReturnType |
Can_TestLoopBackModeEnable(uint8 controller, uint8 mode) |
This service will enable CAN loopback mode. |
Std_ReturnType |
Can_TestLoopBackModeDisable(uint8 controller, uint8 mode) |
This service will disable CAN loopback mode. |
void |
Can_0_Int0ISR_Fun(void ) |
This function is the ISR for CAN controller 0/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR. |
void |
Can_0_Int1ISR_Fun(void ) |
This function is the ISR for CAN controller 0/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR. |
void |
Can_1_Int0ISR_Fun(void ) |
This function is the ISR for CAN controller 1/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR. |
void |
Can_1_Int1ISR_Fun(void ) |
This function is the ISR for CAN controller 1/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR. |
void |
Can_2_Int0ISR_Fun(void ) |
This function is the ISR for CAN controller 2/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR. |
void |
Can_2_Int1ISR_Fun(void ) |
This function is the ISR for CAN controller 2/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR. |
void |
Can_3_Int0ISR_Fun(void ) |
This function is the ISR for CAN controller 3/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR. |
void |
Can_3_Int1ISR_Fun(void ) |
This function is the ISR for CAN controller 3/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR. |
Std_ReturnType |
Can_SetBaudrate(uint8 Controller, uint16 BaudRateConfigID) |
This function Sets Can controller baud rate selected by BaudRateConfigID. |
Std_ReturnType |
Can_RegisterReadback(uint8 Controller, Can_RegisterReadbackType * RegRbPtr) |
This service will readback CAN registers This is the function for checking the configuration registers. This API can be called by higher layers to check if configuration is correct. |
Std_ReturnType |
Can_EccParityEnable(uint8 controller, uint8 flag, uint8 ramInitEnable) |
This function Enables/Disables Parity This function used to test ECC/Parity error. ramInitEnable should be set to TRUE if ECC enabled for normal operations otherwise pass false if it is diagnostic purpose. |
Std_ReturnType |
Can_EccDiagnosticGetErrMsgBoxNum(uint8 controller, uint8 * msgBox) |
This function returns corrupted mailbox number This function returns mailbox number whose RAM is Corrupted. |
Std_ReturnType |
Can_EccDiagnosticModeEnable(uint8 controller, uint8 flag) |
This function Sets ECC diagnostic mode This function used to test Single bit ECC correction. |
Std_ReturnType |
Can_EccGetErrStatus(uint8 controller, uint32 * ecccErrStatus) |
This API will read the ECC error status information of MCAN controller This function used to test Double bit error detection. |
Std_ReturnType |
Can_EccClrErrStatus(uint8 controller) |
This API clears the ECC error status register. |
void |
Can_DeInit(void ) |
This service is only used for UT testing and not for app use. This API is not standard AUTOSAR API. This service sets the internal Can Controller state to UNINIT state so that Can_Init can be invoked again. This is required for UT test cases with diff Config. |
Std_ReturnType |
Can_GetControllerErrorState(uint8 ControllerId, Can_ErrorStateType * ErrorStatePtr) |
This function get the error state of the controller. |
Std_ReturnType |
Can_GetControllerMode(uint8 Controller, Can_ControllerStateType * ControllerModePtr) |
This service reports about the current status of the requested CAN controller. |
5.2.4.1. function Can_GetVersionInfo
void Can_GetVersionInfo(
Std_VersionInfoType * Can_VersionInfo
)
Brief: Function returns the version information of this module.
Service ID[hex] : 0x07
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
versioninfo Pointer to where to store the version information of this module.
Returns:
None
Return: None
5.2.4.2. function Can_Init
void Can_Init(
const Can_ConfigType * CfgPtr
)
Brief: This function initializes the module. All the required initialization for the CAN driver and hardware is performed in this function.
Service ID[hex] : 0x00
Sync/Async : Synchronous
Reentrancy : Non Reentrant
Parameters:
CfgPtr Pointer to driver configuration.
Returns:
None
Return: None
5.2.4.3. function Can_SetControllerMode
Std_ReturnType Can_SetControllerMode(
uint8 Controller,
Can_ControllerStateType Transition
)
Brief: This function performs software triggered state transitions of the CAN controller State machine.
Service ID[hex] : 0x03
Sync/Async : Asynchronous
Reentrancy : Non Reentrant
Parameters:
Controller - CAN controller for which the status shall be changed
Transition - Transition value to request new CAN controller state
Returns:
E_OK request accepted
E_NOT_OK request not accepted, a development error occurred
Return: Std_ReturnType
5.2.4.4. function Can_Write
Std_ReturnType Can_Write(
Can_HwHandleType Hth,
const Can_PduType * PduInfo
)
Brief: This function is called by CanIf to pass a CAN message to CanDrv for transmission.
Service ID[hex] : 0x06
Sync/Async : Synchronous
Reentrancy : Reentrant (thread-safe)
Parameters:
Hth - Information which HW-transmit handle shall be used for transmit. Implicitly this is also the information about the controller to use because the Hth numbers are unique inside one hardware unit.
PduInfo - Pointer to SDU user memory, DLC and Identifier.
Returns:
E_OK Write command has been accepted
E_NOT_OK development error occurred
CAN_BUSY No TX hardware buffer available or pre-emptive call of Can_Write that can’t be implemented re-entrant
Return: Std_ReturnType
5.2.4.5. function Can_CheckWakeup
Std_ReturnType Can_CheckWakeup(
uint8 Controller
)
Brief: This function checks if a wakeup has occurred for the given controller.
Service ID[hex] : 0x0b
Sync/Async : Synchronous
Reentrancy : Non Reentrant
Parameters:
Controller - Controller to be checked for a wakeup.
Returns:
E_OK if wakeup is detected.
E_NOT_OK if Wakeup is not detected
Return: Std_ReturnType
5.2.4.6. function Can_DisableControllerInterrupts
void Can_DisableControllerInterrupts(
uint8 Controller
)
Brief: This function disables all interrupts for this CAN controller Basically it will Disable the CAN interrupts(reset bit 1 in CTL reg(IE0=0)).
Service ID[hex] : 0x04
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
None
Returns:
None
Return: None
5.2.4.7. function Can_EnableControllerInterrupts
void Can_EnableControllerInterrupts(
uint8 Controller
)
Brief: This function will Enable the interrupts for the Controller desired. It will restore the interrupts that were defined in the configuration. Basically it will enable the CAN interrupts.
Service ID[hex] : 0x05
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
Controller - CAN controller for which interrupts shall be enabled.
Returns:
None
Return: None
5.2.4.8. function Can_MainFunction_Write
void Can_MainFunction_Write(
void
)
Brief: This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING.
Service ID[hex] : 0x01
Parameters:
None
Returns:
None
Return: None
5.2.4.9. function Can_MainFunction_BusOff
void Can_MainFunction_BusOff(
void
)
Brief: This function performs the polling of bus-off events that are configured statically as ‘to be polled’.
Service ID[hex] : 0x09
Parameters:
None
Returns:
None
Return: None
5.2.4.10. function Can_MainFunction_Read
void Can_MainFunction_Read(
void
)
Brief: This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.
Service ID[hex] : 0x08
Parameters:
None
Returns:
None
Return: None
5.2.4.11. function Can_MainFunction_Wakeup
void Can_MainFunction_Wakeup(
void
)
Brief: This function performs the polling of wake-up events that are configured statically as ‘to be polled.
Service ID[hex] : 0x0A
Parameters:
None
Returns:
None
Return: None
5.2.4.12. function Can_MainFunction_Mode
void Can_MainFunction_Mode(
void
)
Brief: This function performs the polling of CAN controller mode transitions This will indicate only the CanController SW state and cannot indicate any HW state as there is no HW state exposed from the Can Controller.
Service ID[hex] : 0x0C
Parameters:
None
Returns:
None
Return: None
5.2.4.13. function Can_TestLoopBackModeEnable
Std_ReturnType Can_TestLoopBackModeEnable(
uint8 controller,
uint8 mode
)
Brief: This service will enable CAN loopback mode.
Service ID[hex] : 0x0f
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
Controller - CAN Controller to enable loopback mode
Loopback mode - # 0 - Digital Loopback, # 1 - Analog Loopback
Returns:
E_OK Loopback mode enabled in the CAN Controller
E_NOT_OK Loopback mode enable failed
Return: Std_ReturnType
5.2.4.14. function Can_TestLoopBackModeDisable
Std_ReturnType Can_TestLoopBackModeDisable(
uint8 controller,
uint8 mode
)
Brief: This service will disable CAN loopback mode.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
Controller - CAN Controller to disable loopback mode
Loopback mode - # 0 - Digital Loopback, # 1 - Analog Loopback
Returns:
E_OK Loopback mode disabled in the CAN Controller
E_NOT_OK Loopback mode disable failed
Return: Std_ReturnType
5.2.4.15. function Can_0_Int0ISR_Fun
void Can_0_Int0ISR_Fun(
void
)
Brief: This function is the ISR for CAN controller 0/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.
This is the ISR function for the MCAN controller 0. All the Interrupts are hooked to MCAN0INT. This ISR sends the TX confirmation for the successful tx msg. This ISR will call the RX processing function for the received message. This ISR will call the Error processing function in case of any error interrupts.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
None
Returns:
None
Return: None
5.2.4.16. function Can_0_Int1ISR_Fun
void Can_0_Int1ISR_Fun(
void
)
Brief: This function is the ISR for CAN controller 0/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.
This is the ISR function for the MCAN controller 0 ECC Error. This ISR will clear and report the ECC Error through call back function.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
None
Returns:
None
Return: None
5.2.4.17. function Can_1_Int0ISR_Fun
void Can_1_Int0ISR_Fun(
void
)
Brief: This function is the ISR for CAN controller 1/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.
This is the ISR function for the MCAN controller 1. All the Interrupts are hooked to MCAN1INT. This ISR sends the TX confirmation for the successful tx msg. This ISR will call the RX processing function for the received message. This ISR will call the Error processing function in case of any error interrupts.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
None
Returns:
None
Return: None
5.2.4.18. function Can_1_Int1ISR_Fun
void Can_1_Int1ISR_Fun(
void
)
Brief: This function is the ISR for CAN controller 1/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.
This is the ISR function for the MCAN controller 1 ECC Error. This ISR will clear and report the ECC Error through call back function.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
None
Returns:
None
Return: None
5.2.4.19. function Can_2_Int0ISR_Fun
void Can_2_Int0ISR_Fun(
void
)
Brief: This function is the ISR for CAN controller 2/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.
This is the ISR function for the MCAN controller 2. All the Interrupts are hooked to MCAN2INT. This ISR sends the TX confirmation for the successful tx msg. This ISR will call the RX processing function for the received message. This ISR will call the Error processing function in case of any error interrupts.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
None
Returns:
None
Return: None
5.2.4.20. function Can_2_Int1ISR_Fun
void Can_2_Int1ISR_Fun(
void
)
Brief: This function is the ISR for CAN controller 2/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.
This is the ISR function for the MCAN controller 2 ECC Error. This ISR will clear and report the ECC Error through call back function.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
None
Returns:
None
Return: None
5.2.4.21. function Can_3_Int0ISR_Fun
void Can_3_Int0ISR_Fun(
void
)
Brief: This function is the ISR for CAN controller 3/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.
This is the ISR function for the MCAN controller 3. All the Interrupts are hooked to MCAN3INT. This ISR sends the TX confirmation for the successful tx msg. This ISR will call the RX processing function for the received message. This ISR will call the Error processing function in case of any error interrupts.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
None
Returns:
None
Return: None
5.2.4.22. function Can_3_Int1ISR_Fun
void Can_3_Int1ISR_Fun(
void
)
Brief: This function is the ISR for CAN controller 3/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.
This is the ISR function for the MCAN controller 4 ECC Error. This ISR will clear and report the ECC Error through call back function.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
None
Returns:
None
Return: None
5.2.4.23. function Can_SetBaudrate
Std_ReturnType Can_SetBaudrate(
uint8 Controller,
uint16 BaudRateConfigID
)
Brief: This function Sets Can controller baud rate selected by BaudRateConfigID.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
Controller - Controller whose Baud Rate is being set
BaudRateConfigID - ID number corresponding to a Baud Rate Configuration
Returns:
E_OK Service request accepted, setting of (new) baud rate started
E_NOT_OK Service request not accepted
Return: Std_ReturnType
5.2.4.24. function Can_RegisterReadback
Std_ReturnType Can_RegisterReadback(
uint8 Controller,
Can_RegisterReadbackType * RegRbPtr
)
Brief: This service will readback CAN registers This is the function for checking the configuration registers. This API can be called by higher layers to check if configuration is correct.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
Controller - CAN Controller to readback registers
RegRbPtr - Pointer to where to store the readback values. If this pointer is NULL_PTR, then the API will return E_NOT_OK.
Returns:
E_OK Register readback successful
E_NOT_OK Register readback failed
Return: Std_ReturnType
5.2.4.25. function Can_EccParityEnable
Std_ReturnType Can_EccParityEnable(
uint8 controller,
uint8 flag,
uint8 ramInitEnable
)
Brief: This function Enables/Disables Parity This function used to test ECC/Parity error. ramInitEnable should be set to TRUE if ECC enabled for normal operations otherwise pass false if it is diagnostic purpose.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
Controller - Controller Id
flag - Enable/Disable Parity
ramInitEnable - Enable/Disable Ram Init
Returns:
E_OK Parity enabled
E_NOT_OK Parity enable failed
Return: Std_ReturnType
5.2.4.26. function Can_EccDiagnosticGetErrMsgBoxNum
Std_ReturnType Can_EccDiagnosticGetErrMsgBoxNum(
uint8 controller,
uint8 * msgBox
)
Brief: This function returns corrupted mailbox number This function returns mailbox number whose RAM is Corrupted.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
controller - Controller Id
msgBox - Message number which caused ECC error.
Returns:
E_OK Request successful
E_NOT_OK Request failed
Return: Std_ReturnType
5.2.4.27. function Can_EccDiagnosticModeEnable
Std_ReturnType Can_EccDiagnosticModeEnable(
uint8 controller,
uint8 flag
)
Brief: This function Sets ECC diagnostic mode This function used to test Single bit ECC correction.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
controller - Controller Id
flag - Enable/Disable Parity
Returns:
E_OK ECC diagnostic mode enabled
E_NOT_OK ECC diagnostic mode failed
Return: Std_ReturnType
5.2.4.28. function Can_EccGetErrStatus
Std_ReturnType Can_EccGetErrStatus(
uint8 controller,
uint32 * ecccErrStatus
)
Brief: This API will read the ECC error status information of MCAN controller This function used to test Double bit error detection.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
controller - Controller Id
ecccErrStatus - ECC error status
Returns:
E_OK Get ECC error status successful
E_NOT_OK Get ECC error status failed
Return: Std_ReturnType
5.2.4.29. function Can_EccClrErrStatus
Std_ReturnType Can_EccClrErrStatus(
uint8 controller
)
Brief: This API clears the ECC error status register.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
controller - Controller Id
Returns:
E_OK Clear ECC error status successful
E_NOT_OK Clear ECC error status failed
Return: Std_ReturnType
5.2.4.30. function Can_DeInit
void Can_DeInit(
void
)
Brief: This service is only used for UT testing and not for app use. This API is not standard AUTOSAR API. This service sets the internal Can Controller state to UNINIT state so that Can_Init can be invoked again. This is required for UT test cases with diff Config.
Service ID[hex] : N/A
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
None
Returns:
None
Return: None
5.2.4.31. function Can_GetControllerErrorState
Std_ReturnType Can_GetControllerErrorState(
uint8 ControllerId,
Can_ErrorStateType * ErrorStatePtr
)
Brief: This function get the error state of the controller.
Service ID[hex] : 0x11
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
ControllerId - ID of the CAN controller whose error state is requested.
ErrorStatePtr - Pointer where the error state is updated.
Returns:
E_OK Error state request accepted
E_NOT_OK Error state request not accepted
Return: Std_ReturnType
5.2.4.32. function Can_GetControllerMode
Std_ReturnType Can_GetControllerMode(
uint8 Controller,
Can_ControllerStateType * ControllerModePtr
)
Brief: This service reports about the current status of the requested CAN controller.
Service ID[hex] : 0x12
Sync/Async : Synchronous
Reentrancy : Non-Reentrant
Parameters:
Controller - CAN controller for which the status shall be changed
ControllerModePtr - Pointer to a memory location where the current mode of the CAN controller will be stored.
Returns:
E_OK request accepted
E_NOT_OK request not accepted
Return: Std_ReturnType