UDMA utility API to make TR, get TR descriptor memory requirement.
Go to the source code of this file.
Functions | |
| uint32_t | UdmaUtils_getRingMemSize (uint8_t mode, uint32_t elemCnt, uint8_t elemSize) |
| UDMA get ring size utility API. More... | |
| void | UdmaUtils_makeTrpdTr15 (uint8_t *trpdMem, uint32_t trCnt, uint32_t cqRingNum) |
| UDMA utility API to make TRPD with TR15 TR type. Other TRPD make APIs should be called only after this API. More... | |
| void | UdmaUtils_makeTrpd (uint8_t *trpdMem, uint32_t trType, uint32_t trCnt, uint32_t cqRingNum) |
| UDMA utility API to make TRPD. Other TRPD make APIs should be called only after this API. More... | |
| uint32_t | UdmaUtils_getTrSizeEncoded (uint32_t trType) |
| Returns the size of TR (encoded) based on the type. More... | |
| uint32_t | UdmaUtils_getTrSizeBytes (uint32_t trType) |
| Returns the size of TR in bytes based on the type. More... | |
| static uint32_t | UdmaUtils_getTrpdTr15Response (const uint8_t *trpdMem, uint32_t trCnt, uint32_t trIndex) |
| Returns the TR response in the TRPD memory based on the index. More... | |
| static CSL_UdmapTR15 * | UdmaUtils_getTrpdTr15Pointer (uint8_t *trpdMem, uint32_t trIndex) |
| Returns the TR15 pointer in the TRPD memory based on the index. More... | |