Go to the source code of this file.
|
| typedef void * | UART_DmaHandle |
| | Handle to the UART DMA Config Object returned by UART_dmaOpen. More...
|
| |
| typedef int32_t(* | UART_dmaOpenFxn) (UART_Handle uartHandle, void *uartDmaArgs) |
| | Driver implementation to open a specific DMA driver channel - UDMA, EDMA etc. More...
|
| |
| typedef int32_t(* | UART_dmaTransferReadFxn) (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction) |
| | Driver implementation to do a DMA read using a specific DMA driver - UDMA, EDMA etc. More...
|
| |
| typedef int32_t(* | UART_dmaTransferWriteFxn) (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction) |
| | Driver implementation to do a DMA write using a specific DMA driver - UDMA, EDMA etc. More...
|
| |
| typedef int32_t(* | UART_dmaCloseFxn) (UART_Handle handle) |
| | Driver implementation to close a specific DMA driver channel - UDMA, EDMA etc. More...
|
| |
| typedef int32_t(* | UART_dmaDisableChannelFxn) (UART_Handle handle, uint32_t isChannelTx) |
| | Driver implementation to diisable a specific DMA driver channel - UDMA, EDMA etc. More...
|
| |