Go to the source code of this file.
Data Structures | |
| struct | tisci_msg_fwl_change_owner_info_req |
| This file contains: More... | |
| struct | tisci_msg_fwl_change_owner_info_resp |
| Response for a change owner operation. More... | |
| struct | tisci_msg_fwl_set_firewall_region_req |
| Request for configuring the firewall permissions. More... | |
| struct | tisci_msg_fwl_set_firewall_region_resp |
| Response for configuring the firewall permissions. More... | |
| struct | tisci_msg_fwl_get_firewall_region_req |
| Request for retrieving the firewall permissions. More... | |
| struct | tisci_msg_fwl_get_firewall_region_resp |
| Response for retrieving the firewall permissions. More... | |
Functions | |
| struct tisci_msg_fwl_change_owner_info_req | __attribute__ ((__packed__)) |
Variables | |
| struct tisci_header | hdr |
| uint16_t | fwl_id |
| uint16_t | region |
| uint8_t | owner_index |
| uint8_t | owner_privid |
| uint16_t | owner_permission_bits |
| uint32_t | n_permission_regs |
| uint32_t | control |
| uint32_t | permissions [FWL_MAX_PRIVID_SLOTS] |
| uint64_t | start_address |
| uint64_t | end_address |
| struct tisci_header hdr |
| uint16_t fwl_id |
| uint16_t region |
| uint8_t owner_index |
| uint8_t owner_privid |
| uint16_t owner_permission_bits |
| uint32_t n_permission_regs |
| uint32_t control |
| uint32_t permissions |
| uint64_t start_address |
| uint64_t end_address |