Go to the source code of this file.
Data Structures | |
| struct | tisci_msg_sa2ul_set_dkek_req |
| TISCI Request for setting DKEK in SA2UL registers. More... | |
| struct | tisci_msg_sa2ul_set_dkek_resp |
| TISCI Response for setting DKEK in SA2UL registers. More... | |
| struct | tisci_msg_sa2ul_release_dkek_req |
| TISCI Request for releasing DKEK. More... | |
| struct | tisci_msg_sa2ul_release_dkek_resp |
| TISCI Response for Releasing DKEK. More... | |
| struct | tisci_msg_sa2ul_get_dkek_req |
| TISCI Request for getting DKEK via TISCI. More... | |
| struct | tisci_msg_sa2ul_get_dkek_resp |
| TISCI Response for requesting DKEK. More... | |
Macros | |
| #define | SA2UL_DKEK_KEY_LEN (32U) |
| This file contains: More... | |
| #define | KDF_LABEL_AND_CONTEXT_LEN_MAX 41U |
| key derivation label and context length More... | |
Functions | |
| struct tisci_msg_sa2ul_set_dkek_req | __attribute__ ((__packed__)) |
Variables | |
| struct tisci_header | hdr |
| uint8_t | sa2ul_instance |
| uint8_t | kdf_label_len |
| uint8_t | kdf_context_len |
| uint8_t | kdf_label_and_context [KDF_LABEL_AND_CONTEXT_LEN_MAX] |
| uint8_t | dkek [SA2UL_DKEK_KEY_LEN] |
| struct tisci_header hdr |
| uint8_t sa2ul_instance |
| uint8_t kdf_label_len |
| uint8_t kdf_context_len |
| uint8_t kdf_label_and_context |
| uint8_t dkek[SA2UL_DKEK_KEY_LEN] |