I2C Parameters.
I2C parameters are used to with the I2C_open() call. Default values for these parameters are set using I2C_Params_init().
If I2C_TransferMode is set to I2C_MODE_BLOCKING then I2C_transfer function calls will block thread execution until the transaction has completed.
If I2C_TransferMode is set to I2C_MODE_CALLBACK then I2C_transfer will not block thread execution and it will call the function specified by transferCallbackFxn. Sequential calls to I2C_transfer in I2C_MODE_CALLBACK mode will put the designated transaction onto an internal queue that automatically starts queued transactions after the previous transaction has completed. (regardless of error state).
I2C_BitRate specifies the I2C bus rate used for I2C communications.
Data Fields | |
| uint8_t | transferMode |
| void(* | transferCallbackFxn )(I2C_Handle i2cHnd, I2C_Transaction *msg, int32_t transferStatus) |
| uint8_t | bitRate |
| uint8_t I2C_Params::transferMode |
Blocking or Callback mode
| void(* I2C_Params::transferCallbackFxn) (I2C_Handle i2cHnd, I2C_Transaction *msg, int32_t transferStatus) |
I2C_CallbackFxn transferCallbackFxn; Callback function pointer
| uint8_t I2C_Params::bitRate |
I2C bus bit rate