ClockP module config, set as part of SysConfig, not to be set by end-users directly.
Data Fields | |
| uint32_t | timerBaseAddr |
| uint32_t | timerHwiIntNum |
| uint32_t | timerInputClkHz |
| uint32_t | timerInputPreScaler |
| uint32_t | usecPerTick |
| uint32_t ClockP_Config::timerBaseAddr |
HW Timer MMR base address
| uint32_t ClockP_Config::timerHwiIntNum |
CPU interrupt number for this timer
| uint32_t ClockP_Config::timerInputClkHz |
Timer clock in units of Hz
| uint32_t ClockP_Config::timerInputPreScaler |
Timer divider to apply to the input clock
| uint32_t ClockP_Config::usecPerTick |
period of one timer tick in units of usecs