Data Fields | |
| uint32_t | tdIndicator |
| uint32_t | chId |
| uint32_t | forced |
| uint32_t CSL_UdmapTdResponse::tdIndicator |
TRUE: Indicates that a teardown has completed.
| uint32_t CSL_UdmapTdResponse::chId |
Indicates which channel the teardown completed on.
| uint32_t CSL_UdmapTdResponse::forced |
FALSE: Indicates that the teardown was graceful and data was not lost. TRUE : Indicates that the teardown was not graceful and data was potentially lost