Region config structure, this is used by SysConfig and not to be used by end-users directly.
Data Fields | |
| uint64_t | systemAddr |
| uint32_t | localAddr |
| uint32_t | size |
| uint64_t AddrTranslateP_RegionConfig::systemAddr |
translated 48b system addr as seen by the SOC, MUST align to region size
| uint32_t AddrTranslateP_RegionConfig::localAddr |
region start address as seen by the CPU, MUST align to region size
| uint32_t AddrTranslateP_RegionConfig::size |
region size, see AddrTranslateP_RegionSize