|
| void | RPMessage_Params_init (RPMessage_Params *params) |
| | Set default values to RPMessage_Params. More...
|
| |
| void | RPMessage_CreateParams_init (RPMessage_CreateParams *params) |
| | Set default values to RPMessage_CreateParams. More...
|
| |
| int32_t | RPMessage_init (const RPMessage_Params *params) |
| | Initialize RPMessage module. More...
|
| |
| void | RPMessage_deInit (void) |
| | De-Initialize RPMessage module. More...
|
| |
| int32_t | RPMessage_waitForLinuxReady (uint32_t timeout) |
| | Wait for linux side RPMessage to be ready. More...
|
| |
| void | RPMessage_controlEndPtCallback (RPMessage_ControlEndPtCallback controlEndPtCallback, void *controlEndPtCallbackArgs) |
| | Callback to call when a control message is received on a control end point. More...
|
| |
| int32_t | RPMessage_construct (RPMessage_Object *obj, const RPMessage_CreateParams *createParams) |
| | Create a RPMessage object to receive messages at a specified end-point. More...
|
| |
| void | RPMessage_destruct (RPMessage_Object *obj) |
| | Delete a previously created RPMessage object. More...
|
| |
| void | RPMessage_unblock (RPMessage_Object *obj) |
| | Unblocks RPMessage_recv, for the input object, if it is blocked waiting on messages and users want to exit that task. More...
|
| |
| uint16_t | RPMessage_getLocalEndPt (const RPMessage_Object *obj) |
| | Return local end point of a RPMessage_Object. More...
|
| |
| int32_t | RPMessage_announce (uint16_t remoteProcId, uint16_t localEndPt, const char *name) |
| | Announce a local end point at which a service is created to a remote core. More...
|
| |
| int32_t | RPMessage_send (void *data, uint16_t dataLen, uint16_t remoteCoreId, uint16_t remoteEndPt, uint16_t localEndPt, uint32_t timeout) |
| | Send a message to a remote core at a specified remote end point. More...
|
| |
| int32_t | RPMessage_recv (RPMessage_Object *obj, void *data, uint16_t *dataLen, uint16_t *remoteCoreId, uint16_t *remoteEndPt, uint32_t timeout) |
| | Blocking API to wait till a message is received from any CPU at the specified local end point. More...
|
| |