DMSC controls the power management, security and resource management of the device.
|
| static uint32_t | get_field (uint32_t val, uint32_t end, uint32_t start) |
| | extract the specified bit field from a 32 bit unsigned integer. More...
|
| |
| static uint32_t | set_field (uint32_t tgt, uint32_t end, uint32_t start, uint32_t val) |
| | set the specified bit field from a 32 bit unsigned integer to provided value More...
|
| |
| static uint32_t | get_mask (uint32_t end, uint32_t start) |
| | Generate a mask for the give bit field [end:start]. More...
|
| |
◆ TISCI_BIT
| #define TISCI_BIT |
( |
|
n | ) |
(((uint32_t) 1U) << (n)) |
This file contains:
WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!!
System Firmware
Functions for bit and bitfield operations TISCI_BIT macro for easily calculating a bit at offset (n)
◆ get_field()
| static uint32_t get_field |
( |
uint32_t |
val, |
|
|
uint32_t |
end, |
|
|
uint32_t |
start |
|
) |
| |
|
inlinestatic |
extract the specified bit field from a 32 bit unsigned integer.
- Parameters
-
| val | input from which the bitfield is extracted |
| end | upper bit index of the bitfield |
| start | lower bit index of the bitfield |
- Returns
- extracted bit field, right shifted by start bits.
◆ set_field()
| static uint32_t set_field |
( |
uint32_t |
tgt, |
|
|
uint32_t |
end, |
|
|
uint32_t |
start, |
|
|
uint32_t |
val |
|
) |
| |
|
inlinestatic |
set the specified bit field from a 32 bit unsigned integer to provided value
- Parameters
-
| tgt | input in which the bitfield is to be set |
| end | upper bit index of the bitfield |
| start | lower bit index of the bitfield |
| val | value to which the bit field is to be set. |
- Returns
- input value with bitfield updated as specified.
◆ get_mask()
| static uint32_t get_mask |
( |
uint32_t |
end, |
|
|
uint32_t |
start |
|
) |
| |
|
inlinestatic |
Generate a mask for the give bit field [end:start].
All the bits between the two specified bit indices including the specified indices are set to 1. Rest of the bits are set to zero.
- Parameters
-
| end | upper bit index of the mask |
| start | lower bit index of the mask |
- Returns
- generated mask