Go to the source code of this file.
Data Structures | |
| struct | TaskP_Load |
| Task load statistics. More... | |
| struct | TaskP_Object |
| Opaque task object used with the task APIs. More... | |
| struct | TaskP_Params |
| Parameters passed during TaskP_construct. More... | |
Macros | |
| #define | TaskP_PRIORITY_LOWEST (0u) |
| Value to be used for lowest priority task. More... | |
| #define | TaskP_PRIORITY_HIGHEST (31u) |
| Value to be used for highest priority task. More... | |
| #define | TaskP_LOAD_UPDATE_WINDOW_MSEC (500u) |
| The update rate at which TaskP_loadUpdateAll() is called. More... | |
| #define | TaskP_OBJECT_SIZE_MAX (160u) |
| Max size of task object across all OS's. More... | |
Typedefs | |
| typedef void(* | TaskP_FxnMain) (void *args) |
| Entry point to the task. More... | |
Functions | |
| void | TaskP_Params_init (TaskP_Params *params) |
| Set default values to TaskP_Params. More... | |
| int32_t | TaskP_construct (TaskP_Object *obj, TaskP_Params *params) |
| Create a task object. More... | |
| void | TaskP_destruct (TaskP_Object *obj) |
| Cleanup, delete, destruct a task object. More... | |
| void * | TaskP_getHndl (TaskP_Object *obj) |
| Return OS defined task handle. More... | |
| void | TaskP_yield (void) |
| Yield current task. More... | |
| void | TaskP_exit (void) |
| Exit current task. More... | |
| void | TaskP_loadGet (TaskP_Object *obj, TaskP_Load *taskLoad) |
| Get task load. More... | |
| void | TaskP_loadUpdateAll (void) |
| Updated task load statistics. More... | |
| void | TaskP_loadResetAll (void) |
| Reset task load statistics. More... | |
| uint32_t | TaskP_loadGetTotalCpuLoad (void) |
| Get total CPU load including all task and ISR execution time. More... | |