Go to the source code of this file.
Data Structures | |
| struct | SemaphoreP_Object |
| Opaque semaphore object used with the semaphore APIs. More... | |
Macros | |
| #define | SemaphoreP_OBJECT_SIZE_MAX (152U) |
| Max size of semaphore object across no-RTOS and all OS's. More... | |
Functions | |
| int32_t | SemaphoreP_constructMutex (SemaphoreP_Object *obj) |
| Create a mutex semaphore object. More... | |
| int32_t | SemaphoreP_constructBinary (SemaphoreP_Object *obj, uint32_t initValue) |
| Create a binary semaphore object. More... | |
| int32_t | SemaphoreP_constructCounting (SemaphoreP_Object *obj, uint32_t initValue, uint32_t maxValue) |
| Create a counting semaphore object. More... | |
| void | SemaphoreP_destruct (SemaphoreP_Object *obj) |
| Cleanup, delete, destruct a semaphore object. More... | |
| void | SemaphoreP_post (SemaphoreP_Object *obj) |
| Post a semaphore object or unlock a mutex. More... | |
| int32_t | SemaphoreP_pend (SemaphoreP_Object *obj, uint32_t timeToWaitInTicks) |
| Pend on a semaphore object or lock a mutex. More... | |