- Attention
- This document contains the details for AM65X-IDK board setup under each section. User should select the right board setup in the sections.
Cable Connections
AM65X-IDK
- The figure below shows some important cable connections, ports and switches.
- Take note of the location of the "BOOTMODE" switch, this is used to switch between different boot modes like OSPI, UART, SD, NOBOOT mode
AM65X-IDK
Setup UART Terminal
AM65X-IDK
- Many examples use a standard UART terminal to log the output from the examples. You can use any UART terminal program for the same. Below steps show how to setup the UART terminal from CCS.
- First identify the UART port as enumerated on the host machine.
- Make sure that the IDK and UART cable connected as shown in Cable Connections
- In windows, you can use the "Device Manager" to see the detected UART ports
- Search "Device Manager" in Windows Search Box in the Windows taskbar.
- If dont see any USB serial ports listed in "Device Manager" under "Ports (COM & LPT)", then make sure you have installed the UART to USB driver from FTDI, https://www.ftdichip.com/FTDrivers.htm.
Identify UART Port in Windows Device Manager
- In CCS, goto "View > Terminal"
UART Terminal Menu
Open New UART Terminal
- Select the UART port, keep other options to default, i.e 115200 baud rate - 8 data bits - No parity - 1 stop bit,
- We use the 1st USB serial port, as seen in the device manager, for below in the SDK
- Flashing application via UART
- Booting application via UART
- Console output for examples which run from R5F
- We use the 2nd USB serial port, as seen in the device manager, as terminal output for examples which run from M3F
Connect to UART port
- In this screenshot this happens to be COM13 and COM14 however on your machine this could be different. One tip to make sure there is no mistake in identifying the UART port is to disconnect all other UART to USB devices other than this IDK before checking in device manager.
Additional Details
- Note
- This section has more details on AM65X-IDK. This is mainly for reference and can be skiped unless referred to by other pages in this user guide.
SOC Initialization Using CCS Scripting
- Note
- We have mentioned the steps for GP device.
Set Environment Variable
- Note
- This step needs to be done once and is needed for the SOC initialization script
load_dmsc.js/load_dmsc_hsfs.js to find certain initialization files within the SDK folder. This variable is not used otherwise in the build process. If you dont like adding variables in the environment, then you need to edit the file ${SDK_INSTALL_PATH}/tools/ccs_load/am65x/load_dmsc.js/${SDK_INSTALL_PATH}/tools/ccs_load/am65x/load_dmsc_hsfs.js and specify the SDK path in the file itself.
- Add path to the SDK folder as a environment variable in the host machine.
- In windows, goto "Windows Task Bar Search" and search for "environment variables for your account"
Environment Variables For Your Account
- Add a new variable named
MCU_PLUS_SDK_AM65X_PATH and point it to the path where the SDK is installed
Add New Environment Variable For Your Account
Run the SOC Initialization Script
AM65X-IDK
- Attention
- This step needs to be done every time the IDK is power-cycled.
- POWER-OFF the IDK
- Make sure below cables are connected as shown in Cable Connections
- Set IDK in NOBOOT mode as shown below
NO BOOT MODE
- POWER-ON the IDK
- Launch the target configuration created with Create Target Configuration
Launch Target Configuration
- You will see the AM65X target configuration in the "Debug" window as shown below
Target Configuration After Launch
- Goto "CCS Toolbar > View > Scripting Console"
- Type the below command in the scripting console and press "enter", to load DMSC FW and initialize the SOC
Scripting Console
- In Linux, run the same command, only the path would be a Linux path like
/home/{username}/ti/mcu_plus_sdk_{soc}_{sdk version}/tools/ccs_load/am65x/load_dmsc.js
- After successful execution of this script one would see logs as below
- In the scripting console, this is log from the script itself.
Scripting Console Log
- In the AM65X "CIO" console, this is log from the R5F.
AM65X CIO Console R5F Log
- In the AM65X console, this is log from the GEL scripts.
Select AM65X GEL Console
AM65X Console GEL Log
- For success, all the three consoles should have no errors in their logs.
- If the script is run without providing power to the IDK or if the IDK BOOTMODE is not set to NOBOOT MODE then you will see errors in the console and/or unexpected behaviour and error messages.
- SOLUTION: Power cycle IDK and repeat the steps.
BOOT MODE
NOBOOT MODE
AM65X-IDK
This mode is used in conjunction with the load_dmsc.js script described here SOC Initialization Using CCS Scripting,
BOOTMODE [ 0 : 7 ] (SW2) = 0010 0000
BOOTMODE [ 8 : 15 ] (SW3) = 0000 0000
BOOTMODE [0:1] (SW4) = 00
NO BOOT MODE
Troubleshooting IDK issues
- JTAG connection fails on some IDKs with the following error. Need to connect the JTAG cable after board is powered on.
JTAG Connection Error Dialog