- Attention
- It is strongly recommended to begin development by following the steps in the order listed below.
- Note
- The steps in this user guide show screen shots and descriptions based on Windows. However the steps in Linux would remain the same, unless mentioned otherwise.
-
${SDK_INSTALL_PATH} refers to the path where the SDK is installed. Recommend to install in
C:/ti in Windows, and ${HOME}/ti in Linux. To install to other locations, refer Installing SDK at non-default location
-
{some text} refers to a variable string that should be replaced by user and {some text} should not be typed verbatim on the command prompt.
-
In Windows, use the
cmd.exe as command prompt and in Linux, use the bash shell as the command prompt.
Introduction
Getting Started Goals
On successful completion of below steps, you would have achieved the following
- All tools needed for development are installed
- IDK setup needed for development is verified
- CCS IDE setup needed for development is verified
- One SDK example has been built using makefile as well as CCS project
- One SDK example has been loaded and run on the IDK
- Output console logs on CCS and UART are working as expected
Terms and Abbreviations
| Term | Description |
| I2C Controller | I2C device generates the SCL clock and initiates communication |
| I2C Target | I2C device which responds to I2C Controller |
Getting Started Steps
- Step 1: Download, install SDK and related tools, see Download, Install and Setup SDK and Tools [NEEDS TO BE DONE ONCE when SDK is installed]
- Step 2: Download, install and setup CCS for development, see Download, Install and Setup CCS [NEEDS TO BE DONE ONCE when SDK is installed]
- Step 3: Setup IDK for program execution, see IDK Setup
- Step 4: Build a "hello world" example for the IDK, see Build a Hello World example
- Step 5: Load and run the "hello world" example on the IDK, see CCS Launch, Load and Run
Next Steps
Now you can explore the SDK by running more examples (see Examples and Demos) and browsing through various developer notes (see Developer Guides), to understand the SDK better and develop your own applications with the SDK.