Introduction
This is a special example which sends the sciclient boardcfg to the SYSFW running on Cortex M3. This example is mainly used in conjunction with the NO BOOT MODE, refer to SOC Initialization Using CCS Scripting for more information on this.
The boardcfg is a SOC specific configuration data regarding the various system attributes controlled by the SYSFW. These include resources, power and clock, security etc.
If the SYSFW accepts the boardcfg sent, the test result is passed otherwise failed.
- Note
- Please note that this example is valid only in cases where Cortex-M3 is already loaded with SYSFW. If SYSFW is not loaded, the example would fail. Typically this example is used for SOC initialization via CCS in GP devices.
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 freertos |
r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am65x-idk |
Example folder | examples/drivers/sciclient/sciclient_set_boardcfg |
Steps to Run the Example
See Also
SCICLIENT
Sample Output
DMSC Firmware Version 22.1.1--v2022.01a (Terrific Lla
DMSC Firmware revision 0x15
DMSC ABI revision 3.1
[SCICLIENT] ABI check PASSED
[SCICLIENT] Board Configuration with Debug enabled ...
[SCICLIENT] Common Board Configuration PASSED
[SCICLIENT] PM Board Configuration PASSED
[SCICLIENT] RM Board Configuration PASSED
[SCICLIENT] Security Board Configuration PASSED
DMSC Firmware Version 22.1.1--v2022.01a (Terrific Lla
DMSC Firmware revision 0x15
DMSC ABI revision 3.1
All tests have passed!!