The UDMA driver provides API to program the DMA module of the NAVSS subsystem to setup and initiate DMA transfers.
The DMA architecture specifies the data structures used by Texas Instruments standard communications modules to facilitate direct memory access (DMA) and to provide a consistent application programming interface (API) to the host software in multi-core devices. The data structures and the API used to manipulate them will be jointly referred to as NAVSS. Frequent tasks are commonly offloaded from the host processor to peripheral hardware to increase system performance. Significant performance gains may result from careful design of the host software and communication module interface. In networking systems, packet transmission and reception are critical tasks. Texas Instruments has developed the NAVSS standard, which is aimed at maximizing the efficiency of interaction between the host software and communications modules.
The Navigator Subsystem (NAVSS hardware) is a container which groups together as much as possible the components which provide the Hardare to Software boundary for data movement control in the system. All of the components which control work handoff (queuing, interrupts, monitoring and debugging) are included in the NAVSS which in turn is located as close as possible to the various host processors to which services are provided. Other DMA components such as DRUs, UTC, and PDMAs exist outside the NAVSS but all are controlled by the root complexes provided in NAVSS.
The Unified DMA 3rd-Party Channel Controller is intended to perform similar (but significantly upgraded) functions to the EDMA Channel Controller engine on previous SoC devices. The UDMA-C module supports the transmission of Transfer Request packets from memory mapped data structures to data channels within UTCs in the system and reception of Transfer Response packets from data channels in UTCs in the system into memory mapped data structures. Up to 512 (configuration specific) third-party.DMA control channels are provided within the UDMA-C. Each control channel corresponds to a single third party DMA data channel in a separate UTC. Transfer Request messages provide transfer parameters which are to be used by the UTC channels to move data in the system (previously implemented as PARAM entries). Transfer Response messages are sent back from the UTC in a one to one relationship with Transfer Request packets and provide an indication of both completion of a data transfer and whether or not any exception or error occurred during the data transfer.
The UDMA-C controller maintains state information for each of its channels which allows Transfer Request packet transmission and Transfer Response packet reception operations to be time division multiplexed between channels in order to share the underlying DMA hardware. An internal DMA scheduler is used to control the ordering and rate at which this multiplexing occurs for the transmission of Transfer Request packets. The ordering and rate of Transfer Response receive operations is directly controlled by the order in which those packets are received on the Rx PSI-L interface.
The UDMA-P is intended to perform similar (but significantly upgraded) functions as the packet-oriented DMA used on previous SoC devices. The UDMA-P module supports the transmission and reception of various packet types. The UDMA-P is architected to facilitate the segmentation and reassembly of SoC DMA data structure compliant packets to/from smaller data blocks that are natively compatible with the specific requirements of each connected peripheral. Multiple Tx and Rx channels are provided within the DMA which allow multiple segmentation or reassembly operations to be ongoing. The DMA controller maintains state information for each of the channels which allows packet segmentation and reassembly operations to be time division multiplexed between channels in order to share the underlying DMA hardware. An external DMA scheduler is used to control the ordering and rate at which this multiplexing occurs for Transmit operations. The ordering and rate of Receive operations is indirectly controlled by the order in which blocks are pushed into the DMA on the Rx PSI-L interface.
The UDMA-P also supports acting as both a UTC and UDMA-C for its internal channels. Channels in the UDMA-P can be configured to be either Packet-Based or Third-Party channels on a channel by channel basis.
Below section describes the high level flow of the driver for the data transfer
Transfer configuration is specified in the TR record. Size of TR is variable from 16 bytes to 64 bytes. Specified via TR Type in FLAGS field
Below table summarizes different TR types and the transfer type for which they are used
| TR Type | Descriptrion |
|---|---|
| Type 0 | 1D (word0-3) |
| Type 1 | 2D (word0-4) |
| Type 2 | 3D (word0-6) |
| Type 3 | 4D (word0-8) |
| Type 5 | Cache warm (word0-15) (MSMC DRU ONLY) |
| Type 8 | 4D Block Copy (word0-15) |
| Type 9 | 4D Block Copy with reformatting (word0-15) (MSMC DRU ONLY) |
| Type 10 | 2D Block Copy (word0-15) |
| Type 11 | 2D Block Copy with reformatting (word0-15) (MSMC DRU ONLY) |
| Type 15 | 4D Block Copy with reformatting and indirection (word0-15) (MSMC DRU ONLY) |
Below diagram shows the high level flow for the transfer requests from application and driver
Below diagram shows the UDMA transfer API flow
Include the below file to access the APIs
Channel Open Example
Channel Close Example