Go to the source code of this file.
Functions | |
| void | CycleCounterP_init (const uint64_t cpuFreqHz) |
| initialize PMU Cycle Counter More... | |
| uint32_t | CycleCounterP_getCount32 (void) |
| Get 32b CPU cycle counter value. More... | |
| void | CycleCounterP_reset (void) |
| Enable, reset, clear overflow for CPU cycle counter. More... | |
| uint64_t | CycleCounterP_getCount64 (void) |
| Get 64b CPU cycle counter value. More... | |
| uint64_t | CycleCounterP_nsToTicks (const uint64_t nanosecs) |
| API function to convert nanosecs to PMU counter ticks. More... | |