AM64x MCU+ SDK  12.00.00

Detailed Description

Set the desired frequency for a clock.

This set the desired frequency for a clock within an allowable range. This message will fail on an enabled clock unless TISCI_MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE is set for the clock. Additionally, if other clocks have their frequency modified due to this message, they also must have the TISCI_MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE or be disabled.

Calling set frequency on a clock input to the SoC psuedo-device will inform the PMMC of that clock's frequency. Setting a frequency of zero will indicate the clock is disabled.

Calling set frequency on clock outputs from the SoC pseudo-device will function similarly to setting the clock frequency on a device.

Parameters
hdrTISCI header
deviceThe device ID that the clock is connected to.
min_freq_hzThe minimum allowable frequency in Hz. This is the minimum allowable programmed frequency and does not account for clock tolerances and jitter.
target_freq_hzThe target clock frequency. The clock will be programmed at a rate as close to this target frequency as possible.
max_freq_hzThe maximum allowable frequency in Hz. This is the maximum allowable programmed frequency and does not account for clock tolerances and jitter. The firmware will actually accept any frequency up to but not including max + 1.
clkEach device has its own set of clock inputs. This indexes which clock input to modify.

If the clock index is 255 or greater, this field should be set to 255 and the full value placed in the clk32 field. This is kept for backwards compatibility with older firmwares.

Parameters
clk32Stores the actual clock index if clk field is set to 255. This field is ignored otherwise. This field can hold the full range of possible clock indexes, but for compatibility with older firmwares should only be used when the index is 255 or greater.

Data Fields

struct tisci_header hdr
 
uint32_t device
 
uint64_t min_freq_hz
 
uint64_t target_freq_hz
 
uint64_t max_freq_hz
 
uint8_t clk
 
uint32_t clk32
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_set_freq_req::hdr

◆ device

uint32_t tisci_msg_set_freq_req::device

◆ min_freq_hz

uint64_t tisci_msg_set_freq_req::min_freq_hz

◆ target_freq_hz

uint64_t tisci_msg_set_freq_req::target_freq_hz

◆ max_freq_hz

uint64_t tisci_msg_set_freq_req::max_freq_hz

◆ clk

uint8_t tisci_msg_set_freq_req::clk

◆ clk32

uint32_t tisci_msg_set_freq_req::clk32