AM64x MCU+ SDK  12.01.00

Detailed Description

Slave TOG Static Registers.

This structure contains Slave TOG static registers The register values are not expected to change until a new configuration is done.

Data Fields

uint32_t PID
 
uint32_t CFG
 
uint32_t ENABLE
 
uint32_t FLUSH
 
uint32_t TIMEOUT
 
uint32_t ERR
 

Field Documentation

◆ PID

uint32_t SDL_TOG_staticRegs::PID

Revision Register

◆ CFG

uint32_t SDL_TOG_staticRegs::CFG

Configuration Register

◆ ENABLE

uint32_t SDL_TOG_staticRegs::ENABLE

Enable Register

◆ FLUSH

uint32_t SDL_TOG_staticRegs::FLUSH

Flush Register

◆ TIMEOUT

uint32_t SDL_TOG_staticRegs::TIMEOUT

Timeout Value Register

◆ ERR

uint32_t SDL_TOG_staticRegs::ERR

Error Interrupt Enabled Status/Set Register