AM64x MCU+ SDK  12.01.00
SDL_POK_staticRegs Struct Reference

Detailed Description

POK Static Registers structure.

This structure defines the POK static configuration registers

POK Function to enable or disable ping/pong mode for a specified PRG. Only supported for v1 version of the IP.

Parameters
instanceInstance of PRG
enableEnable or disable the ping/pong mode
Returns
SDL_PASS for success. SDL Error Code for failure.

Data Fields

uint8_t hystCtrl
 
uint8_t hystCtrlOV
 
uint8_t voltDetMode
 
uint8_t trim
 
uint8_t trimOV
 
uint8_t deglitch
 
bool porBGapOK
 
uint8_t porModuleStatus
 

Field Documentation

◆ hystCtrl

uint8_t SDL_POK_staticRegs::hystCtrl

Hysteresis control value

◆ hystCtrlOV

uint8_t SDL_POK_staticRegs::hystCtrlOV

Hysteresis control for OV

◆ voltDetMode

uint8_t SDL_POK_staticRegs::voltDetMode

Voltage Detection Mode value

◆ trim

uint8_t SDL_POK_staticRegs::trim

trim value

◆ trimOV

uint8_t SDL_POK_staticRegs::trimOV

trim value for OV

◆ deglitch

uint8_t SDL_POK_staticRegs::deglitch

deglitch value

◆ porBGapOK

bool SDL_POK_staticRegs::porBGapOK

POR Band Gap OK status

◆ porModuleStatus

uint8_t SDL_POK_staticRegs::porModuleStatus

POR Module Status