AM64x MCU+ SDK  12.01.00

Detailed Description

Unicast entry type info apart from MAC address that can be set.

Data Fields

uint32_t portNum
 
bool blocked
 
bool secure
 
bool super
 
bool ageable
 
bool trunk
 

Field Documentation

◆ portNum

uint32_t CpswAle_UcastEntryInfo::portNum

Port number that the packet with a unicast destination address is forwarded to

◆ blocked

bool CpswAle_UcastEntryInfo::blocked

Indicates that packet with a matching source or destination address should be dropped

◆ secure

bool CpswAle_UcastEntryInfo::secure

Indicates that packet with a matching source address should be dropped, if the received port number is not equal to the port number in the table entry

◆ super

bool CpswAle_UcastEntryInfo::super

Indicates that this address can be received in port state other than Forwarding state

◆ ageable

bool CpswAle_UcastEntryInfo::ageable

Indicates if the unicast entry is subject to aging

◆ trunk

bool CpswAle_UcastEntryInfo::trunk

Indicates if the portNum refers to trunk number of port number