AM64x MCU+ SDK  12.01.00

Detailed Description

Data Fields

uint32_t policerMatchEnMask
 
uint32_t port
 
bool portIsTrunk
 
uint32_t priority
 
uint32_t ouiAleEntryIdx
 
uint32_t srcMacAleEntryIdx
 
uint32_t dstMacAleEntryIdx
 
uint32_t ivlanAleEntryIdx
 
uint32_t ovlanAleEntryIdx
 
uint32_t etherTypeAleEntryIdx
 
uint32_t srcIpAleEntryIdx
 
uint32_t dstIpAleEntryIdx
 
bool threadIdEn
 
uint32_t threadId
 
uint32_t peakRateInBitsPerSec
 
uint32_t commitRateInBitsPerSec
 
uint32_t policerEntryIdx
 
bool egressOpEn
 
uint32_t egressOpcode
 
bool ttlCheckEn
 
uint32_t egressTrunkIdx
 
uint32_t dstPortMask
 

Field Documentation

◆ policerMatchEnMask

uint32_t CpswAle_PolicerEntryOutArgs::policerMatchEnMask

Bitmask selecting classifier types to be enabled for this policer.

See also
ALE classifier match types

◆ port

uint32_t CpswAle_PolicerEntryOutArgs::port

Port number to match. Valid if bit CPSW_ALE_POLICER_MATCH_PORT in policerMatchEnMask is set

◆ portIsTrunk

bool CpswAle_PolicerEntryOutArgs::portIsTrunk

Flag indicating port number is a trunk group. Valid if bit CPSW_ALE_POLICER_MATCH_PORT in policerMatchEnMask is set

◆ priority

uint32_t CpswAle_PolicerEntryOutArgs::priority

Received packet priority to match. Valid if bit CPSW_ALE_POLICER_MATCH_PRIORITY in policerMatchEnMask is set

◆ ouiAleEntryIdx

uint32_t CpswAle_PolicerEntryOutArgs::ouiAleEntryIdx

OUI ALE table entry index to match. Valid if bit CPSW_ALE_POLICER_MATCH_OUI in policerMatchEnMask is set

◆ srcMacAleEntryIdx

uint32_t CpswAle_PolicerEntryOutArgs::srcMacAleEntryIdx

MAC address ALE table entry index to match source MAC address. Valid if bit CPSW_ALE_POLICER_MATCH_MACSRC in policerMatchEnMask is set

◆ dstMacAleEntryIdx

uint32_t CpswAle_PolicerEntryOutArgs::dstMacAleEntryIdx

MAC address ALE table entry index to match destination MAC address. Valid if bit CPSW_ALE_POLICER_MATCH_MACDST in policerMatchEnMask is set

◆ ivlanAleEntryIdx

uint32_t CpswAle_PolicerEntryOutArgs::ivlanAleEntryIdx

Inner VLAN ALE table entry index to match. Valid if bit CPSW_ALE_POLICER_MATCH_IVLAN in policerMatchEnMask is set

◆ ovlanAleEntryIdx

uint32_t CpswAle_PolicerEntryOutArgs::ovlanAleEntryIdx

Outer VLAN ALE table entry index to match. Valid if bit CPSW_ALE_POLICER_MATCH_OVLAN in policerMatchEnMask is set

◆ etherTypeAleEntryIdx

uint32_t CpswAle_PolicerEntryOutArgs::etherTypeAleEntryIdx

EtherType ALE table entry index to match. It's valid if bit CPSW_ALE_POLICER_MATCH_ETHERTYPE in policerMatchEnMask is set

◆ srcIpAleEntryIdx

uint32_t CpswAle_PolicerEntryOutArgs::srcIpAleEntryIdx

IP address ALE table entry index to match as source IP address. Valid if bit CPSW_ALE_POLICER_MATCH_IPSRC in policerMatchEnMask is set

◆ dstIpAleEntryIdx

uint32_t CpswAle_PolicerEntryOutArgs::dstIpAleEntryIdx

IP address ALE table entry index to match as destination IP address. Valid if bit CPSW_ALE_POLICER_MATCH_IPDST in policerMatchEnMask is set

◆ threadIdEn

bool CpswAle_PolicerEntryOutArgs::threadIdEn

Flag indicating if thread id setting is enabled for this policer entry

◆ threadId

uint32_t CpswAle_PolicerEntryOutArgs::threadId

Thread Id which will be enabled for this policer match. Valid if threadIdEn is true.

◆ peakRateInBitsPerSec

uint32_t CpswAle_PolicerEntryOutArgs::peakRateInBitsPerSec

Peak rate in bits per second. 0 indicates rate limit is disabled

◆ commitRateInBitsPerSec

uint32_t CpswAle_PolicerEntryOutArgs::commitRateInBitsPerSec

Commit rate in bits per second. 0 indicates rate limit is disabled

◆ policerEntryIdx

uint32_t CpswAle_PolicerEntryOutArgs::policerEntryIdx

ALE policer table entry index

◆ egressOpEn

bool CpswAle_PolicerEntryOutArgs::egressOpEn

Egress Op enabled

◆ egressOpcode

uint32_t CpswAle_PolicerEntryOutArgs::egressOpcode

Egress Op code:

◆ ttlCheckEn

bool CpswAle_PolicerEntryOutArgs::ttlCheckEn

TTL check enabled for the interVLAN route. Valid only if egress op code has interVLan route enabled

◆ egressTrunkIdx

uint32_t CpswAle_PolicerEntryOutArgs::egressTrunkIdx

Trunk index to be used if detPort for interVLAN route is a trunk. Valid only if egress op code has interVLAN route enabled

◆ dstPortMask

uint32_t CpswAle_PolicerEntryOutArgs::dstPortMask

Port mask to which the packet is to be routed. Valid only if egress op code has interVLAN route enabled