|
AM64x MCU+ SDK
12.01.00
|
|
Go to the documentation of this file.
66 #include <drivers/hw_include/csl_types.h>
67 #include <drivers/hw_include/cslr_gpmc.h>
68 #include <drivers/gpmc/v0/dma/gpmc_dma.h>
84 #define GPMC_CHIP_SELECT_CS0 (0U)
85 #define GPMC_CHIP_SELECT_CS1 (1U)
86 #define GPMC_CHIP_SELECT_CS2 (2U)
87 #define GPMC_CHIP_SELECT_CS3 (3U)
98 #define GPMC_FIFOEVENT_STATUS (0U)
99 #define GPMC_TERMINALCOUNT_STATUS (1U)
100 #define GPMC_WAIT0EDGEDETECTION_STATUS (2U)
101 #define GPMC_WAIT1EDGEDETECTION_STATUS (3U)
112 #define GPMC_FIFOEVENT_INT (0U)
113 #define GPMC_TERMINALCOUNT_INT (1U)
114 #define GPMC_WAIT0EDGEDETECTION_INT (2U)
115 #define GPMC_WAIT1EDGEDETECTION_INT (3U)
126 #define GPMC_PREFETCH_ACCESSMODE_READ (0U)
127 #define GPMC_PREFETCH_ACCESSMODE_WRITE (1U)
138 #define GPMC_ECC_ALGORITHM_HAMMINGCODE (0U)
139 #define GPMC_ECC_ALGORITHM_BCH (1U)
149 #define GPMC_ECC_BCH_ERRCORRCAP_UPTO_4BITS (0U)
150 #define GPMC_ECC_BCH_ERRCORRCAP_UPTO_8BITS (1U)
151 #define GPMC_ECC_BCH_ERRCORRCAP_UPTO_16BITS (2U)
162 #define GPMC_ECCPOINTER_RESULT_1 (1U)
163 #define GPMC_ECCPOINTER_RESULT_2 (2U)
164 #define GPMC_ECCPOINTER_RESULT_3 (3U)
165 #define GPMC_ECCPOINTER_RESULT_4 (4U)
166 #define GPMC_ECCPOINTER_RESULT_5 (5U)
167 #define GPMC_ECCPOINTER_RESULT_6 (6U)
168 #define GPMC_ECCPOINTER_RESULT_7 (7U)
169 #define GPMC_ECCPOINTER_RESULT_8 (8U)
170 #define GPMC_ECCPOINTER_RESULT_9 (9U)
179 #define GPMC_ECC_SIZE_0 (0U)
180 #define GPMC_ECC_SIZE_1 (1U)
189 #define GPMC_ECC_RESULT_1 (1U)
190 #define GPMC_ECC_RESULT_2 (2U)
191 #define GPMC_ECC_RESULT_3 (3U)
192 #define GPMC_ECC_RESULT_4 (4U)
193 #define GPMC_ECC_RESULT_5 (5U)
194 #define GPMC_ECC_RESULT_6 (6U)
195 #define GPMC_ECC_RESULT_7 (7U)
196 #define GPMC_ECC_RESULT_8 (8U)
197 #define GPMC_ECC_RESULT_9 (9U)
206 #define GPMC_BCH_RESULT0 (0U)
207 #define GPMC_BCH_RESULT1 (1U)
208 #define GPMC_BCH_RESULT2 (2U)
209 #define GPMC_BCH_RESULT3 (3U)
210 #define GPMC_BCH_RESULT4 (4U)
211 #define GPMC_BCH_RESULT5 (5U)
212 #define GPMC_BCH_RESULT6 (6U)
221 #define GPMC_CS_MASK_ADDR_SIZE_256MB (0x00U)
222 #define GPMC_CS_MASK_ADDR_SIZE_128MB (0x08U)
223 #define GPMC_CS_MASK_ADDR_SIZE_64MB (0x0cU)
224 #define GPMC_CS_MASK_ADDR_SIZE_32MB (0x0eU)
225 #define GPMC_CS_MASK_ADDR_SIZE_16MB (0x0fU)
251 #define GPMC_CS_TIMING_CONFIG(CSWrOffTime, CSRdOffTime, CSExtDelayFlag, \
253 ((uint32_t) (((CSWrOffTime) << CSL_GPMC_CONFIG2_CSWROFFTIME_SHIFT) \
254 & CSL_GPMC_CONFIG2_CSWROFFTIME_MASK) | \
255 (((CSRdOffTime) << CSL_GPMC_CONFIG2_CSRDOFFTIME_SHIFT) \
256 & CSL_GPMC_CONFIG2_CSRDOFFTIME_MASK) | \
257 (((CSExtDelayFlag) << CSL_GPMC_CONFIG2_CSEXTRADELAY_SHIFT) \
258 & CSL_GPMC_CONFIG2_CSEXTRADELAY_MASK) | \
259 (((CSOnTime) << CSL_GPMC_CONFIG2_CSONTIME_SHIFT) \
260 & CSL_GPMC_CONFIG2_CSONTIME_MASK))
298 #define GPMC_ADV_TIMING_CONFIG(ADVAADMuxWrOffTime, ADVAADMuxRdOffTime, \
299 ADVWrOffTime, ADVRdOffTime, ADVExtDelayFlag, \
302 ((uint32_t) (((ADVAADMuxWrOffTime) << \
303 CSL_GPMC_CONFIG3_ADVAADMUXWROFFTIME_SHIFT) & \
304 CSL_GPMC_CONFIG3_ADVAADMUXWROFFTIME_MASK) | \
305 (((ADVAADMuxRdOffTime) << CSL_GPMC_CONFIG3_ADVAADMUXRDOFFTIME_SHIFT) & \
306 CSL_GPMC_CONFIG3_ADVAADMUXRDOFFTIME_MASK) | \
307 (((ADVWrOffTime) << CSL_GPMC_CONFIG3_ADVWROFFTIME_SHIFT) & \
308 CSL_GPMC_CONFIG3_ADVWROFFTIME_MASK) | \
309 (((ADVRdOffTime) << CSL_GPMC_CONFIG3_ADVRDOFFTIME_SHIFT) & \
310 CSL_GPMC_CONFIG3_ADVRDOFFTIME_MASK) | \
311 (((ADVExtDelayFlag) << CSL_GPMC_CONFIG3_ADVEXTRADELAY_SHIFT) & \
312 CSL_GPMC_CONFIG3_ADVEXTRADELAY_MASK) | \
313 (((ADVAADMuxOnTime) << CSL_GPMC_CONFIG3_ADVAADMUXONTIME_SHIFT) & \
314 CSL_GPMC_CONFIG3_ADVAADMUXONTIME_MASK) | \
315 (((ADVOnTime) << CSL_GPMC_CONFIG3_ADVONTIME_SHIFT) & \
316 CSL_GPMC_CONFIG3_ADVONTIME_MASK))
362 #define GPMC_WE_OE_TIMING_CONFIG(WEOffTime, WEExtDelayFlag, WEOnTime, \
363 OEAADMuxOffTime, OEOffTime, OEExtDelayFlag, \
364 OEAADMuxOnTime, OEOnTime) \
365 ((uint32_t) (((WEOffTime) << \
366 CSL_GPMC_CONFIG4_WEOFFTIME_SHIFT) & \
367 CSL_GPMC_CONFIG4_WEOFFTIME_MASK) | \
368 (((WEExtDelayFlag) << \
369 CSL_GPMC_CONFIG4_WEEXTRADELAY_SHIFT) & CSL_GPMC_CONFIG4_WEEXTRADELAY_MASK) | \
371 CSL_GPMC_CONFIG4_WEONTIME_SHIFT) & CSL_GPMC_CONFIG4_WEONTIME_MASK) | \
372 (((OEAADMuxOffTime) << \
373 CSL_GPMC_CONFIG4_OEAADMUXOFFTIME_SHIFT) & \
374 CSL_GPMC_CONFIG4_OEAADMUXOFFTIME_MASK) | \
376 CSL_GPMC_CONFIG4_OEOFFTIME_SHIFT) & CSL_GPMC_CONFIG4_OEOFFTIME_MASK) | \
377 (((OEExtDelayFlag) << \
378 CSL_GPMC_CONFIG4_OEEXTRADELAY_SHIFT) & CSL_GPMC_CONFIG4_OEEXTRADELAY_MASK) | \
379 (((OEAADMuxOnTime) << \
380 CSL_GPMC_CONFIG4_OEAADMUXONTIME_SHIFT) & \
381 CSL_GPMC_CONFIG4_OEAADMUXONTIME_MASK) | \
383 CSL_GPMC_CONFIG4_OEONTIME_SHIFT) & CSL_GPMC_CONFIG4_OEONTIME_MASK))
403 #define GPMC_RDACCESS_CYCLETIME_TIMING_CONFIG(rdCycleTime, wrCycleTime, \
405 pageBurstAccessTime) \
406 ((uint32_t) (((rdCycleTime) << \
407 CSL_GPMC_CONFIG5_RDCYCLETIME_SHIFT) & \
408 CSL_GPMC_CONFIG5_RDCYCLETIME_MASK) | \
410 CSL_GPMC_CONFIG5_WRCYCLETIME_SHIFT) & CSL_GPMC_CONFIG5_WRCYCLETIME_MASK) | \
411 (((rdAccessTime) << \
412 CSL_GPMC_CONFIG5_RDACCESSTIME_SHIFT) & CSL_GPMC_CONFIG5_RDACCESSTIME_MASK) | \
413 (((pageBurstAccessTime) << \
414 CSL_GPMC_CONFIG5_PAGEBURSTACCESSTIME_SHIFT) & \
415 CSL_GPMC_CONFIG5_PAGEBURSTACCESSTIME_MASK))
448 #define GPMC_CYCLE2CYCLE_BUSTURNAROUND_TIMING_CONFIG(cycle2CycleDelay, \
449 cycle2CycleDelaySameCSCfg, \
450 cycle2CycleDelayDiffCSCfg, \
452 ((uint32_t) (((cycle2CycleDelay) << \
453 CSL_GPMC_CONFIG6_CYCLE2CYCLEDELAY_SHIFT) & \
454 CSL_GPMC_CONFIG6_CYCLE2CYCLEDELAY_MASK) | \
455 (((cycle2CycleDelaySameCSCfg) << \
456 CSL_GPMC_CONFIG6_CYCLE2CYCLESAMECSEN_SHIFT) & \
457 CSL_GPMC_CONFIG6_CYCLE2CYCLESAMECSEN_MASK) | \
458 (((cycle2CycleDelayDiffCSCfg) << \
459 CSL_GPMC_CONFIG6_CYCLE2CYCLEDIFFCSEN_SHIFT) & \
460 CSL_GPMC_CONFIG6_CYCLE2CYCLEDIFFCSEN_MASK) | \
462 CSL_GPMC_CONFIG6_BUSTURNAROUND_SHIFT) & CSL_GPMC_CONFIG6_BUSTURNAROUND_MASK))
465 #define GPMC_DMA_COPY_LOWER_LIMIT (512U)
467 #define GPMC_CS_BASE_ADDR_SHIFT (24U)
469 #define GPMC_ECC_WRAP_MODE1 (1)
471 #define GPMC_CMD_INVALID (0xFFFFFFFFU)
473 #define GPMC_MEM_TYPE_NAND (0)
474 #define GPMC_MEM_TYPE_PSRAM (1)
475 #define GPMC_MEM_TYPE_NORLIKE (1) //Same as pSRAM
485 typedef enum GPMC_v1_nandEccAlgo_s
500 typedef enum GPMC_OperatingMode_s {
516 typedef enum GPMC_TransferMode_s {
534 typedef enum GPMC_TransactionType_e {
549 typedef enum GPMC_TransactionStatus_s {
588 typedef struct GPMC_Transaction_s {
614 typedef struct GPMC_Params_s
658 typedef struct GPMC_Object_s {
683 typedef struct GPMC_timingParams_s
745 typedef struct GPMC_HwAttrs_s
801 typedef struct GPMC_Config_s {
1206 params->
devType = CSL_GPMC_CONFIG1_DEVICETYPE_NANDLIKE;
1207 params->
devType = CSL_GPMC_CONFIG1_DEVICESIZE_EIGHTBITS;
GPMC driver object.
Definition: gpmc.h:658
int32_t GPMC_writeNandCommand(GPMC_Handle handle, GPMC_nandCmdParams *cmdParams)
Function to write NAND command parameters.
uint32_t waitPinPol
Definition: gpmc.h:772
int32_t GPMC_configureTimingParameters(GPMC_Handle handle)
Function to configure GPMC timing parameters.
uint32_t waitPinNum
Definition: gpmc.h:770
int32_t GPMC_eccBchConfigureElm(GPMC_Handle handle, uint8_t numSectors)
Function to configure ELM module for error correction.
int32_t GPMC_configurePrefetchPostWriteEngine(GPMC_Handle handle)
Function to configure GPMC PREFETCH read and POST write engine.
void GPMC_norMakeCmd(uint8_t busWidth, uint32_t cmd, uint8_t *cmdBuf)
Function to create correct NOR cmd based on bus width.
uint32_t cycleDelaySameChipSel
Definition: gpmc.h:729
@ GPMC_TRANSACTION_TYPE_WRITE_CMDREG
Definition: gpmc.h:541
uint32_t isOpen
Definition: gpmc.h:666
uint32_t intrPriority
Definition: gpmc.h:758
uint32_t dataBaseAddr
Definition: gpmc.h:750
@ GPMC_TRANSFER_CSN_DEASSERT
Definition: gpmc.h:554
uint32_t writeType
Definition: gpmc.h:780
void GPMC_init(void)
This function initializes the GPMC module.
uint32_t csOnTime
Definition: gpmc.h:685
uint32_t intrNum
Definition: gpmc.h:756
uint32_t rdCycleTime
Definition: gpmc.h:721
@ GPMC_TRANSACTION_TYPE_READ_CMDREG
Definition: gpmc.h:539
uint32_t rdAccessTime
Definition: gpmc.h:717
int32_t GPMC_nandWriteData(GPMC_Handle handle, GPMC_Transaction *trans)
Function to write data to NANDflash using CPU prefetch/post write engine.
int32_t GPMC_nandReadData(GPMC_Handle handle, GPMC_Transaction *trans)
Function to read data from NAND flash using DMA or CPU prefetch/post write engine.
uint16_t index
Definition: tisci_rm_proxy.h:3
uint32_t oeOffTime
Definition: gpmc.h:709
@ GPMC_TRANSFER_FAILED
Definition: gpmc.h:553
uint32_t busTurnAroundTime
Definition: gpmc.h:735
int32_t GPMC_norReadData(GPMC_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Function to read data from norlike device.
uint32_t advAadMuxOnTime
Definition: gpmc.h:697
GPMC Driver configuration structure.
Definition: gpmc.h:801
const GPMC_HwAttrs * attrs
Definition: gpmc.h:803
uint32_t optimisedAccess
Definition: gpmc.h:786
uint32_t gpmcBaseAddr
Definition: gpmc.h:748
GPMC_Object * object
Definition: gpmc.h:805
uint32_t regionSize
Definition: gpmc.h:649
uint8_t * GPMC_norMakeAddr(uint8_t busWidth, uint32_t blkAddr, uint32_t offset)
Function to create correct address based on bus width.
uint32_t csExDelay
Definition: gpmc.h:782
GPMC_TransferMode transferMode
Definition: gpmc.h:631
Data structure to set transaction type parameters.
Definition: gpmc.h:588
void GPMC_transactionInit(GPMC_Transaction *trans)
Function to initialise GPMC_Transaction structure to default values.
GPMC instance attributes.
Definition: gpmc.h:746
uint32_t inputClkFreq
Definition: gpmc.h:754
void * Buf
Definition: gpmc.h:594
uint32_t cycle2CycleDelay
Definition: gpmc.h:727
int32_t GPMC_setDeviceType(GPMC_Handle handle)
Function to set device type (NANDLIKE OR NORLIKE) for GPMC instance connected to external device.
@ GPMC_NAND_ECC_ALGO_HAMMING_1BIT
Definition: gpmc.h:488
uint32_t transferTimeout
Definition: gpmc.h:598
int32_t GPMC_eccCalculateBchSyndromePolynomial(GPMC_Handle handle, uint8_t *pEccdata, uint32_t sector)
Function to compute BCH syndrome polynomial for NAND write operation.
uint32_t timeLatency
Definition: gpmc.h:764
void GPMC_eccResultRegisterClear(GPMC_Handle handle)
Function to clear GPMC ECC result register.
uint32_t cycleOptimisation
Definition: gpmc.h:788
GPMC_OperatingMode
GPMC driver operating modes.
Definition: gpmc.h:500
@ GPMC_OPERATING_MODE_POLLING
Definition: gpmc.h:506
uint32_t chipSelAddrSize
Definition: gpmc.h:768
uint32_t devType
Definition: gpmc.h:621
GPMC_TransactionType transType
Definition: gpmc.h:590
int32_t GPMC_enableFlashWriteProtect(GPMC_Handle handle)
Function to disable WRITE protect line.
uint32_t numRowAddrCycles
Definition: gpmc.h:571
@ GPMC_NAND_ECC_ALGO_BCH_8BIT
Definition: gpmc.h:490
SemaphoreP_Object mutex
Definition: gpmc.h:670
uint32_t cmdCycle2
Definition: gpmc.h:567
@ GPMC_NAND_ECC_ALGO_BCH_16BIT
Definition: gpmc.h:491
uint32_t wrCycleTime
Definition: gpmc.h:723
@ GPMC_TRANSACTION_TYPE_READ
Definition: gpmc.h:535
HwiP_Object hwi
Definition: gpmc.h:668
@ GPMC_OPERATING_MODE_BLOCKING
Definition: gpmc.h:502
GPMC_Config * GPMC_Handle
Definition: gpmc.h:816
static void GPMC_Params_init(GPMC_Params *params)
Function to initialize the GPMC_Params struct to its defaults.
Definition: gpmc.h:1199
int32_t GPMC_setDeviceSize(GPMC_Handle handle)
Function to set device width for GPMC instance connected to external device.
uint32_t oeOnTime
Definition: gpmc.h:707
uint32_t oeAadMuxOffTime
Definition: gpmc.h:713
GPMC_TransferMode
GPMC data transfer modes.
Definition: gpmc.h:516
int32_t GPMC_eccGetBchSyndromePolynomial(GPMC_Handle handle, uint32_t sector, uint32_t *bchData)
Function to get BCH syndrome polynomial per sector NAND read operation.
void GPMC_close(GPMC_Handle handle)
Function to close a GPMC peripheral specified by the GPMC handle.
GPMC_timingParams timingParams
Definition: gpmc.h:774
uint32_t weOffTime
Definition: gpmc.h:705
uint32_t waitTimeout
Definition: gpmc.h:577
uint32_t intrEnable
Definition: gpmc.h:627
GPMC_Params params
Definition: gpmc.h:659
uint32_t advOnTime
Definition: gpmc.h:691
uint32_t colAddress
Definition: gpmc.h:573
uint32_t weOnTtime
Definition: gpmc.h:703
int32_t GPMC_disableFlashWriteProtect(GPMC_Handle handle)
Function to disable WRITE protect line.
@ GPMC_TRANSFER_MODE_BLOCKING
Definition: gpmc.h:518
@ GPMC_NAND_ECC_ALGO_BCH_4BIT
Definition: gpmc.h:489
GPMC_Handle GPMC_open(uint32_t index, const GPMC_Params *prms)
This function opens a given GPMC peripheral.
int32_t GPMC_eccValueSizeSet(GPMC_Handle handle, uint32_t eccSize, uint32_t eccSizeVal)
Function to set ECC used and unused bytes size in nibbles.
uint32_t oeAadMuxOnTime
Definition: gpmc.h:711
uint32_t elmBaseAddr
Definition: gpmc.h:752
@ GPMC_NAND_ECC_ALGO_NONE
Definition: gpmc.h:487
uint32_t csWrOffTime
Definition: gpmc.h:689
Gpmc_DmaArgs * gpmcDmaHandle
Definition: gpmc.h:676
GPMC_nandEccAlgo eccAlgo
Definition: gpmc.h:776
uint32_t advAadMuxRdOffTime
Definition: gpmc.h:699
@ GPMC_TRANSFER_CANCELED
Definition: gpmc.h:552
uint32_t regionStartAddr
Definition: gpmc.h:647
uint32_t cycleDelayDiffChipSel
Definition: gpmc.h:732
uint32_t advWrOffTime
Definition: gpmc.h:695
GPMC timing parameters.
Definition: gpmc.h:684
@ GPMC_TRANSFER_TIMEOUT
Definition: gpmc.h:555
uint32_t numColAddrCycles
Definition: gpmc.h:575
@ GPMC_TRANSFER_STARTED
Definition: gpmc.h:551
SemaphoreP_Object transferComplete
Definition: gpmc.h:672
uint32_t gGpmcConfigNum
Externally defined driver configuration array size.
int32_t GPMC_eccBchFillSyndromeValue(GPMC_Handle handle, uint32_t sector, uint32_t *bchData)
Function to fill BCH syndrome value per sector to ELM module.
uint32_t advAadMuxWrOffTime
Definition: gpmc.h:701
int32_t GPMC_norWriteData(GPMC_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Function to write data to norlike device.
@ GPMC_OPERATING_MODE_CALLBACK
Definition: gpmc.h:504
int32_t GPMC_eccBchSectorGetError(GPMC_Handle handle, uint32_t sector, uint32_t *errCount, uint32_t *errLoc)
Function to get number of errors per sector by ELM module.
const GPMC_AddrRegion * dmaRestrictedRegions
Definition: gpmc.h:790
uint32_t cmdCycle1
Definition: gpmc.h:565
uint32_t csRdOffTime
Definition: gpmc.h:687
uint32_t rowAddress
Definition: gpmc.h:569
int32_t GPMC_eccEngineEnable(GPMC_Handle handle)
Function to enable GPMC ECC engine.
void * arg
Definition: gpmc.h:596
GPMC driver instance parameters.
Definition: gpmc.h:615
@ GPMC_TRANSFER_MODE_CALLBACK
Definition: gpmc.h:523
uint32_t accessType
Definition: gpmc.h:784
int32_t GPMC_eccBchCheckErrorProcessingStatus(GPMC_Handle handle, uint32_t sector)
Function to get error processing status for a sector by ELM module.
uint32_t count
Definition: gpmc.h:592
uint32_t readType
Definition: gpmc.h:778
GPMC_Handle GPMC_getHandle(uint32_t driverInstanceIndex)
This function returns the handle of an open GPMC Instance from the instance index.
uint32_t GPMC_getInputClk(GPMC_Handle handle)
This function returns the input clk frequency GPMC was programmed at.
Opaque Hwi object used with the Hwi APIs.
Definition: HwiP.h:142
uint32_t chipSelBaseAddr
Definition: gpmc.h:766
uint32_t wrAcessTime
Definition: gpmc.h:719
@ GPMC_TRANSFER_COMPLETED
Definition: gpmc.h:550
GPMC_OperatingMode operMode
Definition: gpmc.h:661
Data structure to set NAND command parameters.
Definition: gpmc.h:564
int32_t gpmcDmaChIndex
Definition: gpmc.h:619
uint32_t clkDivider
Definition: gpmc.h:760
uint32_t chipSel
Definition: gpmc.h:625
uint32_t pageBurstAccess
Definition: gpmc.h:715
uint32_t dmaEnable
Definition: gpmc.h:629
GPMC_TransactionStatus status
Definition: gpmc.h:600
uint32_t checkReadypin
Definition: gpmc.h:579
GPMC_TransactionType
Type of the GPMC transaction for read and write.
Definition: gpmc.h:534
GPMC_nandEccAlgo
GPMC ECC engine algoritms.
Definition: gpmc.h:486
uint32_t advRdOffTime
Definition: gpmc.h:693
GPMC Address Region.
Definition: gpmc.h:646
GPMC_Transaction * transaction
Definition: gpmc.h:674
void GPMC_writeNandCommandParamsInit(GPMC_nandCmdParams *cmdParams)
Function to initialise GPMC_nandCmdParams structure to default values.
@ GPMC_TRANSACTION_TYPE_WRITE
Definition: gpmc.h:537
uint32_t wrDataOnMuxBusTime
Definition: gpmc.h:725
uint32_t addrDataMux
Definition: gpmc.h:762
GPMC_Config gGpmcConfig[]
Externally defined driver configuration array.
void GPMC_deinit(void)
This function de-initializes the GPMC module.
uint32_t memDevice
Definition: gpmc.h:633
int32_t GPMC_eccBchStartErrorProcessing(GPMC_Handle handle, uint8_t sector)
Function to start error processing for a sector by ELM module.
int32_t GPMC_eccEngineBCHConfig(GPMC_Handle handle, uint32_t eccSteps)
Function to configure GPMC ECC engine for BCH algorithm.
GPMC_TransactionStatus
Transaction status codes that are set by the GPMC driver.
Definition: gpmc.h:549
uint32_t devSize
Definition: gpmc.h:623