AM64x MCU+ SDK  12.01.00
SemaphoreP.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2018-2021 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33  #ifndef SEMAPHOREP_H
34  #define SEMAPHOREP_H
35 
36  #ifdef __cplusplus
37  extern "C" {
38  #endif
39 
40  #include <stdint.h>
41  #include <kernel/dpl/SystemP.h>
42 
52  #if defined(OS_NORTOS)
53 
56  typedef struct SemaphoreP_Object_ {
57  uint32_t type;
58  uint32_t maxCount;
59  volatile uint32_t count;
60  volatile uint32_t nestCount;
61  } SemaphoreP_Object;
62 
63  #elif defined (OS_FREERTOS) || defined (OS_FREERTOS_SMP) || defined (OS_FREERTOS_MPU)
64 
67  #include <FreeRTOS.h>
68  #include <task.h>
69  #include <semphr.h>
70  typedef struct SemaphoreP_Object_ {
71  StaticSemaphore_t semObj;
72  SemaphoreHandle_t semHndl;
73  uint32_t isRecursiveMutex;
74  } SemaphoreP_Object;
75 
76  #elif defined(OS_SAFERTOS)
77 
80  #include <SafeRTOS.h>
81  #include <queue.h>
82  #include <semaphore.h>
83  #include <mutex.h>
84  typedef struct SemaphoreP_Object_ {
85  uint64_t semObj[(safertosapiQUEUE_OVERHEAD_BYTES / sizeof(uint64_t) + 1)];
86  xSemaphoreHandle semHndl;
87  uint32_t isRecursiveMutex;
88  } SemaphoreP_Object;
89 
90  #else
91  #error "Define OS_NORTOS, OS_FREERTOS, or OS_SAFERTOS"
92  #endif
93 
101  int32_t SemaphoreP_constructMutex(SemaphoreP_Object *obj);
102 
111  int32_t SemaphoreP_constructBinary(SemaphoreP_Object *obj, uint32_t initValue);
112 
122  int32_t SemaphoreP_constructCounting(SemaphoreP_Object *obj, uint32_t initValue, uint32_t maxValue);
123 
129  void SemaphoreP_destruct(SemaphoreP_Object *obj);
130 
136  void SemaphoreP_post(SemaphoreP_Object *obj);
137 
148  int32_t SemaphoreP_pend(SemaphoreP_Object *obj, uint32_t timeToWaitInTicks);
149 
158  int32_t SemaphoreP_getCount(SemaphoreP_Object *obj);
161  #ifdef __cplusplus
162  }
163  #endif
164 
165  #endif /* SEMAPHOREP_H */
166 
SystemP.h
type
uint16_t type
Definition: tisci_rm_core.h:1
SemaphoreP_constructCounting
int32_t SemaphoreP_constructCounting(SemaphoreP_Object *obj, uint32_t initValue, uint32_t maxValue)
Create a counting semaphore object.
count
uint16_t count
Definition: tisci_pm_device.h:1
SemaphoreP_destruct
void SemaphoreP_destruct(SemaphoreP_Object *obj)
Cleanup, delete, destruct a semaphore object.
SemaphoreP_constructMutex
int32_t SemaphoreP_constructMutex(SemaphoreP_Object *obj)
Create a mutex semaphore object.
SemaphoreP_getCount
int32_t SemaphoreP_getCount(SemaphoreP_Object *obj)
Function to return the count of a semaphore.
SemaphoreP_post
void SemaphoreP_post(SemaphoreP_Object *obj)
Post a semaphore object or unlock a mutex.
SemaphoreP_constructBinary
int32_t SemaphoreP_constructBinary(SemaphoreP_Object *obj, uint32_t initValue)
Create a binary semaphore object.
SemaphoreP_pend
int32_t SemaphoreP_pend(SemaphoreP_Object *obj, uint32_t timeToWaitInTicks)
Pend on a semaphore object or lock a mutex.