AM64x MCU+ SDK  11.02.00
Release Notes 09.00.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
A53 support is applicable for AM64x only. It is NOT applicable for AM243x.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless noted otherwise, the SW modules would work in both FreeRTOS and NORTOS environment.
Unless noted otherwise, the SW modules would work on any of the R5F's present on the SOC.
Unless noted otherwise, the SW modules would work on all supported EVMs
M4F drivers support only MCU domain peripheral and peripheral instance while R5/A53 supports MAIN domain peripheral and peripheral instance.
Attention
Industrial Protocol and Motor control libraries and examples are no longer part of MCU+ SDK and will be available as separate release

New in this Release

Feature Module
RNDIS device class support USB
NCM device class support USB
GPMC support for NAND Flash GPMC
EMMC high speed support MMCSD
Interrupt profiling support and example DPL
Smart placement support Common
MbedTLS MQTT example Networking
Support added for Single Packet reception from DMA Networking
Integrated with industry grade with TSN gPTP protocol stack with example Networking
Descoped GP support Common

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM64x R5F, M4F, A53 AM64x GP EVM (referred to as am64x-evm in code) Windows 10 64b or Ubuntu 18.04 64b
AM64x SK EVM (Limited examples are added) (referred to as am64x-sk in code)

Tools, Compiler and Other Open Source SW Module Information

Tools / SW module Supported CPUs Version
Code Composer Studio R5F, M4F, A53 12.4.0
SysConfig R5F, M4F, A53 1.17.0, build 3128
TI ARM CLANG R5F, M4F 2.1.3.LTS
GCC AARCH64 A53 9.2-2019.12
GCC ARM R5F 7-2017-q4-major (AM64x only)
FreeRTOS Kernel R5F, M4F, A53 10.4.3
FreeRTOS SMP Kernel A53 202110.00-SMP
Tiny USB R5F 0.14.0
LwIP R5F STABLE-2_1_2_RELEASE
Mbed-TLS R5F mbedtls-2.13.1
Attention
TI ARM CLANG 2.1.3.LTS is not part of CCS by default, Follow steps at TI CLANG Compiler Toolchain to install the compiler

Key Features

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
A53 NORTOS support and A53 NORTOS examples DPL, NORTOS
A53 FreeRTOS (single core) support and A53 FreeRTOS examples DPL, FreeRTOS
SBL booting A53 NORTOS Bootloader
GCC support for R5F for limited examples R5F
A53 FreeRTOS dual core in SMP mode and A53 SMP FreeRTOS examples DPL, FreeRTOS
GUI for UART Uniflash Tool (No support for EMMC flashing) Bootloader

Features not supported in release

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F, M4F, A53 NA Task, Task notification, interrupts, semaphores, mutexes, timers, event groups. ROV views in CCS IDE, Task load measurement using FreeRTOS run time statistics APIs. Only single core A53 FreeRTOS is supported. Second core is NOT used.
FreeRTOS SMP Kernel A53 NA Task, Task notification, interrupts, semaphores, mutexes, timers, event groups. ROV views in CCS IDE, Task load measurement using FreeRTOS run time statistics APIs. -
FreeRTOS POSIX R5F, M4F, A53 NA pthread, mqueue, semaphore, clock -
NO RTOS R5F, M4F, A53 NA See Driver Porting Layer (DPL) below Only single core A53 NORTOS is supported. Second core is NOT used.

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Address Translate M4F YES FreeRTOS, NORTOS Use RAT to allow M4F access to peripheral address space -
Cache R5F, A53 YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F, M4F, A53 YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CpuId R5F NA FreeRTOS, NORTOS Verify Core ID and Cluster ID that application is running -
CycleCounter R5F, M4F, A53 NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F, M4F, A53 YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F, M4F, A53 NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F, M4F, A53 YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore -
MPU R5F, M4F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
MMU A53 YES NORTOS Setup MMU and control access to address space -
Semaphore R5F, M4F, A53 NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F, M4F, A53 NA FreeRTOS Create, delete tasks -
Timer R5F, M4F, A53 YES FreeRTOS, NORTOS Configure arbitrary timers -
Event R5F, M4F YES FreeRTOS Setting, getting, clearing, and waiting of Event bits -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: OSPI, OSPI XIP, UART, SD. All R5F's, M4F, A53 NORTOS/FreeRTOS/Linux boot. RPRC, multi-core image format, DDR init SBL OSPI XIP for A53

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
ADC R5F YES Yes Single conversion (one-shot mode), interrupt mode, DMA mode Continuous conversion not tested
CRC R5F YES No CRC in full CPU mode -
DDR R5F YES No Tested LPDDR4 at 400MHz frequency. -
ECAP R5F YES No Frequency, Duty cycle, interrupt mode -
EPWM R5F YES No Different Frequency, Duty cycle, interrupt mode, Deadband and chopper module Tripzone module not tested
EQEP R5F YES No Signal Frequency and Direction, interrupt mode -
FSI (RX/TX) R5F YES No RX, TX, polling, interrupt mode, single/dual lanes -
GPIO R5F, M4F, A53 YES No Basic input/output, GPIO as interrupt GPIO as interrupt is not tested for A53.
GTC R5F, A53 NA No Enable GTC, setting FID (Frequency indicator) -
I2C R5F, M4F, A53 YES No Controller mode, basic read/write, polling and interrupt mode Target mode not supported. M4F not tested due to EVM limitation
IPC Notify R5F, M4F, A53 YES No Low latency IPC between RTOS/NORTOS CPUs -
IPC Rpmsg R5F, M4F, A53 YES No RPMessage protocol based IPC for all R5F, M4F, A53 running NORTOS/FreeRTOS/Linux -
MCAN R5F YES No RX, TX, interrupt and polling mode -
MCSPI R5F, M4F YES Yes Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode -
MDIO R5F NA No Register read/write, link status and link interrupt enable API -
MMCSD R5F YES Yes Raw read/write and file I/O on MMCSD0 eMMC, and MMCSD1 SD. eMMC tested till HS SDR mode (8-bit data, 52 MHz), SD tested till SD HS mode (4-bit, 25 MHz) Interrupt mode not tested
OSPI R5F YES Yes Read direct, Write indirect, Read/Write commands, DMA for read, PHY Mode Interrupt mode not supported
PCIe R5F YES No Buffer Transfer between EP and RC modes. Legacy interrupt MSI and MSIx capability
Pinmux R5F, M4F, A53 YES No Tested with multiple peripheral pinmuxes -
PRUICSS R5F YES No Tested with Ethercat, EtherNet/IP, IO-Link, ICSS-EMAC, HDSL, EnDat -
SOC R5F, M4F, A53 YES No lock/unlock MMRs, get CPU clock, CPU name, clock enable, set frequency, SW Warm/POR Reset, Address Translation -
Sciclient R5F, M4F, A53 YES No Tested with clock setup, module on/off -
SPINLOCK R5F, M4F, A53 NA No Lock, unlock HW spinlocks -
UART R5F, M4F, A53 YES Yes Basic read/write, polling, interrupt mode, HW flow control not tested. DMA mode not supported
UDMA R5F, A53 YES Yes Basic memory copy, SW trigger, Chaining -
WDT R5F, A53 YES No Interrupt after watchdog expiry Reset not supported

Software Diagnostic Library (SDL)

SDL Module Supported CPUs SysConfig Support
ESM M4F, R5F NO
MCRC M4F, R5F NO
RTI M4F, R5F NO
DCC M4F, R5F NO
VTM M4F, R5F NO
STOG M4F, R5F NO
PBIST M4F, R5F NO
MTOG M4F NO
POK M4F, R5F NO
ECC M4F, R5F NO

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES I2C based EEPROM -
ETHPHY R5F YES Ethernet Phy configuration for EtherCAT SubDevice example -
Flash R5F YES XSPI, OSPI, QSPI based flash, Octal, Quad mode, DDR mode All vendor flash types not tested
LED R5F, A53 YES GPIO , I2C IO expander based LED control, I2C based industrial LEDs(TPIC2810) -

File System

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
FreeRTOS+FAT R5F YES NORTOS File read, write, create. FAT partition and mounting File I/O with FreeRTOS

CMSIS

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
CMSIS DSP R5F NA FreeRTOS, NORTOS Basic math, complex math, controller, fast math, filtering, Matrix, statistics, transform -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
TSN R5F NO FreeRTOS gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration Multi-Clock Domain
LwIP R5F YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, TCP iperf, scatter-gather, DSCP priority mapping Other LwIP features
Ethernet driver (ENET) R5F YES FreeRTOS Ethernet as port using CPSW, MAC loopback and PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, Policer and Classifier, MDIO Manual Mode, CBS (IEEE 802.1Qav) on CPSW, IET (IEEE 802.1Qbu) on CPSW, Strapped PHY (Early Ethernet), cut through switch on CPSW RMII mode
Mbed-TLS R5F NO FreeRTOS Tested software cryptography after porting, used mbedTLS with LwIP to implement HTTPS server Hardware offloaded cryptography

USB

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
USB SoC Porting Layer R5F YES FreeRTOS, NORTOS USB 2.0 device mode USB 3.0
USB Device Driver R5F NO FreeRTOS, NORTOS USB 2.0 device mode USB Host driver
TinyUSB Core and CDC Driver R5F NO FreeRTOS, NORTOS USB device with CDC class USB Host, other USB device class drivers
TinyUSB Core and DFU Driver R5F NO FreeRTOS, NORTOS USB device with DFU class USB Host, other USB device class drivers

SECURITY

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
SA2UL AES R5F YES NORTOS AES CBC-128 encryption and decryption, AES CBC-256 encryption and decryption, AES ECB-128 encryption and decryption, AES ECB-256 encryption and decryption, AES CMAC-128, AES CMAC-256 -
SA2UL SHA R5F YES NORTOS SHA 512 single shot and multi-shot, SHA 256 single shot and multi-shot, HMAC SHA-256, HMAC SHA-512, HMAC SHA-1 -
SA2UL RNG R5F YES NORTOS RNG generate random number with size of 4 words(128 bit) -
SA2UL PKA R5F YES NORTOS RSA Encryption and Decryption support upto 4k bit, RSA Signing and Verification support upto 4k bit, ECDSA Signing and Verification support with P-256 and P-384 curves -

Demos

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Benchmark demo 4xR5F's YES NORTOS CFFT, FIR and FOC benchmarks ADC/PWM benchmark

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
MCUSDK-9811 IPC Notify unregister client always returns success IPC 8.05.00 onwards Added status variable check -
MCUSDK-10213 GPIO interrrupt resource allocation is not happening for m4 core GPIO 8.05.00 onwards Updated RM config to DEVGRP_APP -
MCUSDK-10551 UDMA_ALIGN_SIZE macro implementation is incorrect UDMA 8.06.00 onwards - -
MCUSDK-10577 PIN_OSPI0_LBCLKO is not defined in pinmux.h Pinmux 8.05.00 onwards Added pinmux definition -
MCUSDK-10704 SocId parser is not working with python3 SBL 8.06.00 onwards Migrated the script to python 3 -
MCUSDK-10841 SBL needs to copy the vector table for self core right before the self-core reset release SBL 8.06.00 onwards Move the image load for self core just before the release reset instead of doing it early -
MCUSDK-10895 Baud Rate of MCU_UART limited to 3.7 Mbps but SysConfig shows no warning UART 8.06.00 onwards Enabled warning in Sysconfig -
MCUSDK-10904 DFU Uniflash gives TIMEOUT on sending a file of 1MB USB 8.06.00 onwards - -
MCUSDK-10905 Python Uniflash scripts (UART & DFU) generates exception at the end on trying to send a file of size more than 1MB SBL 8.06.00 onwards - -
MCUSDK-11178 CCS is not generating a encrypted SBL image for HS-SE device SBL 8.06.00 onwards ENC_SBL_ENABLED condition was missing from the ccs bootimage gen makefile -
MCUSDK-11264 UART syscfg DMA mode defaults to BCDMA instead of PKT DMA causes assert UDMA 8.06.00 onwards Sysconfig update to use PKT DMA instead of BCDMA -
MCUSDK-8361 ENET Layer 2 CPSW Switch Port 2 does not link up for AM64x-SK baord Networking 8.4.0 - -
MCUSDK-11207 Incorrect IOCTL params for CPSW ENET_TIMESYNC_IOCTL_SET_TIMESTAMP Networking 8.5.0 - -
MCUSDK-10775 Example build failing on enabling External Phy Management Networking 8.6.0 - -
PROC_SDL-6010 ECCerror injection is not supported for 2 instances. These are SDL_ECC_AGGR1 Ram ID 4 fails on interconnect ram ID 4 checker group 4-14 and SDL_PCIE0_PCIE_G2X1_64_CORE_CORE_ECC_AGGR. SDL 8.6.0 AM64x, AM243x

-

MCUSDK-10715 Conflict between the flashing address of linux.appimage & u-boot.img in OSPI SBL 8.05.00 onwards - -
MCUSDK-10840 SBL-to-Linux Boot Flow must leave control MMRs unlocked - Just like U-Boot/SPL SBL 8.06.00 onwards -

-

Known Issues

ID Head Line Module Applicable Releases Applicable Devices Workaround
MCUSDK-626 DMA not working with ADC FIFO 1 ADC 7.3.0 onwards AM64x, AM243x Use ADC FIFO 0
MCUSDK-1900 UART Hardware Flow Control is not working UART 7.3.0 onwards AM243x -
MCUSDK-2113 [Docs] Sysfw RM/PM documentation doesn't specify AM243x Docs 8.0.0 onwards AM243x -
MCUSDK-6262 [AM243X] : MMCSD read io example is not functional on eMMC if the APP_MMCSD_START_BLK is changed for MMCSD_write and MMCSD_read MMCSD 8.3.0 owards AM243x, AM64x -
MCUSDK-8842 OSPI Writes fail with multi threaded applications OSPI 8.4.0 AM64x, AM243x -
MCUSDK-8938 Last 512KB of memory is not accessible in dev boot mode flow SBL 8.4.0 AM64x, AM243x Use other boot modes
MCUSDK-8945 Boot Time Degradation is observed for HS-FS device SBL 8.5.0 AM64x, AM243x Skip the authentication of application Image using SysConfig
mbedTLS-advisory
MCUSDK-9082
MbedTLS - RSA exploit by kernel-privileged cache side-channel attackers Mbed-TLS 8.6.0 AM64x, AM243x, AM263X, AM273X -
MCUSDK-2715 PKA ECDSA sign verify is not working for P-521 and BrainPool P-512R1 curves SECURITY 8.2.0 onwards AM64x, AM243x -
MCUSDK-10691 flash sequence does not work for MX25U51245G (4-4-4 mode) Flash 8.6.0 AM64x, AM243x -
MCUSDK-10781 Flash Re-Init is not supported Flash 8.6.0 AM64x, AM243x -
MCUSDK-10783 Flash Driver is not supported with XIP Flash 8.6.0 AM64x, AM243x -
MCUSDK-10939 PCIe MSI error when connected to Linux Root Complex PCIe 8.6.0 AM64x, AM243x -
MCUSDK-11028 PCIe as End Point throwing error when changing BAR aperture PCIe 8.6.0 AM64x, AM243x -
MCUSDK-3626 Enet: Phy tuning is not done correctly on AM64x/AM243x and AM263x platforms Enet 8.1.0 onwards AM64x, AM243x PHY delay is not tuned but set to value based on limited testing on a small set of boards.If packet drops are still seen, we can force the phy to set to 100mbps.Make below change in application code: linkCfg->speed = ENET_SPEED_100MBIT; linkCfg->duplexity = ENET_DUPLEX_FULL;
MCUSDK-8376 LWIP web server application crashes in server stress test Enet, LWIP 8.3.0 onwards AM64x, AM243x -
MCUSDK-9739 AM64B SK loss of packet on using CPSW switch Networking 8.5.0 AM64x -
MCUSDK-10679 CPSW UDP Iperf test instability on AM243x Networking 8.6.0 AM64x, AM243x -
MCUSDK-11507 ENET: CPSW MAC port is stuck forever and dropping all the Rx/Tx packets with reception of corrupts preamble. CPSW 8.2.0 onwards AM64x, AM243x Disable hostRxTimestampEn flag in CPSW CPST configuration. This does not impact the CPTS Rx or Tx Timestamp Events for PTP packets and is orthogonal feature.
MCUSDK-11518 IPC: Firewalling error due to Alignment not being per core pair. IPC 09.00.00 AM243x Firewalling should not be enabled for SafeIPC.
PROC_SDL-6445 ECC error injection test fails for VTM aggregator from R5F domain. SDL 8.6.0 AM64x, AM243x For VTM ECC aggregator, use M4F for error injection.

Errata

ID Head Line Module SDK Status
i2311 USART: Spurious DMA Interrupts UART Implemented
i2313 GPMC: Sub-32-bit read issue with NAND and FPGA/FIFO GPMC Implemented
i2331 CPSW: Device lockup when reading CPSW registers CPSW, SBL Implemented
i2345 CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks CPSW Implemented
i2326 PCIe: MAIN_PLLx operating in fractional mode, which is required for enabling SSC, is not compliant with PCIe Refclk jitter limits PCIe Open
i2312 MMCSD: HS200 and SDR104 Command Timeout Window Too Small MMCSD Open
i2310 USART: Erroneous clear/trigger of timeout interrupt UART Open
i2279 MCAN: Specification Update for dedicated Tx Buffers and Tx Queues configured with same Message ID MCAN Open
i2278 MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID MCAN Open

Limitations

ID Head Line Module Reported in Release Applicable Devices Workaround
MCUSDK-208 gmake with -j can sometimes lock up Windows command prompt Build 7.3.0 AM64x, AM243x Use bash for windows as part of git for windows or don't use -j option

Upgrade and Compatibility Information

Attention
When migrating from Processor SDK RTOS, see Migration Guides for more details

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

Compiler Options

Module Affected API Change Additional Remarks

Examples

Module Affected API Change Additional Remarks

OS Kernel

Module Affected API Change Additional Remarks

SOC Device Drivers

Module Affected API Change Additional Remarks
ECAP ECAP_continousModeConfig Spell corrected to "ECAP_continuousmodeConfig" -
IPC Notify IpcNotify_init IntrPriority added as an element in IpcNotify_Params structure to make interrupt priority configurable. This field is automatically updated by sysconfig
ClockP ClockP_init IntrPriority added as an element in ClockP_Params structure to make Tick interrupt priority configurable. This field is automatically updated by sysconfig

Networking

Module Affected API Change Additional Remarks