AM64x MCU+ SDK  12.00.00
Intercore Ethernet Packet Exchange With ICSSG, Using LwIP Bridge

Introduction

Note
LwIP features are made available as is from public lwIP project. SDK configuration may only enable and exercise a subset of these features.

This example shows how to use the shared memory-based Intercore driver for data traffic sharing across, coupled with the Ethernet driver (ENET) and LwIP bridge.

On AM64X, we can do Ethernet-based communication using ICSSG Hardware peripheral.

  • ICSS
    • This is a firmware enabled Ethernet switch + port HW
    • This HW can be used with industrial communication protocols as well
    • In this example we use ICSS as a standard Ethernet port

It uses ENET ethernet driver underneath with LwIP TCP/IP networking stack.

The example demonstrates the driver feature to exchange Ethernet (IEEE 802.1) packets between r5fss0-0 and r5fss0-1 cores, via shared memory and an Ethernet bridge (LwIP software bridge). CPU core r5fss0-0 fully owns & configures ICSSG1 peripheral resources and the corresponding DMA channels to handle packet reception/transmission directly from/to ICSSG1. It steers the traffic to core r5fss0-1 based on MAC address, using the LwIP bridge. Separate MAC addresses are used to differentiate different CPU core traffic. Both the MAC addresses are added to ICSSG host port FDB entry so that HW accepts the traffic with those MAC addresses. Separate TCP/IP (LiWP) stack instances are set up in each core, with an independent DHCP client, thus different IP addresses for each core. Furthermore, at application level, TCP echo servers are initialized on socket port 8888, in each core to handle the TCP traffic.

Core r5fss0-1 get the packet form ICSSG1 via LwIP bridge running on core r5fss0-0, using shared memory driver.

Few details on the operating sequence of this example is mentioned below:

  • CPU r5fss0-0 initializes ICSSG ethernet driver (LwIP netif 0) and the shared memory enet (LwIP netif 1) driver. Setups LwIP bridge with bridgeIF, linked to netif0 and netif1.
  • CPU r5fss0-1 initializes shared memory enet driver and links to LwIP netif. Prints of r5fss0-1 is directed to CCS console and Prints of r5fss0-0 is directed to UART terminal.
  • CPU cores r5fss0-0 and r5fss0-1 are referred respectively as main core and remote core in the example.
  • Both r5fss0-0 and r5fss0-1 use RPMsg to exchange control messages, in addition to the shared memory interface (which is used to communicate packet data).
  • TCP Server task running on each core awaits for connection from external client on port 8888. When connection is established, it waits for a message from the connected client.
  • In response to external clients message. TCP Server task sends back "Greetings from Texas Instruments!" message back to the client and closes the connection.
  • Supports iPerf TCP performance tests, ping (ICMP) applications across both the cores.

Application Block Diagram

Supported Combinations

Parameter Value
CPU + OS r5fss0-0_freertos, r5fss0-1_freertos
Toolchain ti-arm-clang
Board am64x-evm
Example folder source/networking/enet/core/examples/lwip/enet_intercore_icssg

Note: To configure any core other than r5fss0-0 as the main core, user needs to change the DMA channel resource allocation to the respective core, so that the ICSSG DMA channels for packet transfer are available to the configured main core. Please refer to Modifying resource allocation to modify the resource allocation.

Configuring Syscfg

  • Following Syscfg option allows flexibility to configure memory footprint based on the required use case like: Gigabit Ethernet Support Enable, preemption support, McM Support and QoS level required.
  • Supported Options with default configuration
Feature Description

Remarks/Default Setting

Pkt Pool Enable Flag nable Flag Flag to enable packet allocation from enet utils library.
It should be disabled to avoid utils memory wastage, in case application allots packet via other mechanism. (Ex- Lwip pools)

Default is true. It is disabled for lwip based examples.
If enabled, size of pkt pool size depends on Number of Tx Packet and Number of Rx Packet.

Number of Tx Packet No of Tx packets required for DMA channel

Default is 16.
It contributes to the size of Pkt Mem Pool, DMA ring buffer and accessories.

Number of Rx Packet No of Rx packets required for DMA channel

Default is 32.
It contributes to the size of Pkt Mem Pool, DMA ring buffer and accessories size.

QoS Level No of QoS level required

Can be in between 1-8. Higher QoS level will be serviced by adding more number of buffers.

Premption Enable Flag to enable premption

Default is false.
If enabled, it will add premption buffer to service the feature.

Gigabit Support Decides buffer pool allocation based on interface speed selected

Default is true.
Enabling this option will increase buffer requirement as more buffering required at gigabit speed.

Netif instance TI Networking / Enet (ICSSG) / LWIP Interface config No of netifs allocated by the example.
Only one netif should be set to default when more than one netif is allocated.

TCP Client using ncat tool

Ncat is a general-purpose command-line tool for reading, writing, redirecting, and encrypting data across a network. It aims to be your network Swiss Army knife, handling a wide variety of security testing and administration tasks. Ncat is suitable for interactive use or as a network-connected back end for other tools.

  • Ncat is started as server to which EVM connects.
  • Version used for this example Version 7+ ( https://nmap.org/ncat )

Intercore driver setup

  1. Intercore driver is a shared memory based data routing layer used to send data traffic across cores.
  2. This needs two unique channels open between a given pair of cores.
  3. This needs shared memory space, which is placed in a commonly accessible region.
  4. The region and the channel depth can be adjusted through application code.
  5. This uses custom pBufs which helps in decreasing the memory footprint on other dependent libraries.
  6. This example can be modified to work in tandem with Linux. Refer to TI academy (or TI E2E forums) for more details.

Steps to Run the Example

To Configure Static IP

Please refer to Ethernet LwIP TCP/IP Static IP.

Build the example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

HW Setup

Note
Make sure you have setup the EVM with cable connections as shown here, EVM Setup. In addition do below steps.

AM64X-EVM

For ICSSG based example

  • Connect an Ethernet cable to the EVM from host PC as shown below

Ethernet cable for CPSW based ethernet

Create a network between EVM and host PC

  • The EVM will get an IP address using DHCP, so make sure to connect the other end of the cable to a network which has a DHCP server running.
  • To get started, one can create a simple local network between the EVM and the host PC by using a home broadband/wifi router as shown below. Most such routers run a DHCP server

Local network between PC and EVM
  • To check the router connection with host PC, recommend to disconnect all other networking connections on the PC, sometimes you may need to disable firewall SW, and make sure the routeuter is able to assign a IP address to your host PC
  • After we run the example on the EVM (next step), the EVM will similarly be assigned a IP address, and then host can communicate with the EVM using the assigned IP address.
  • To enable static IP, set the static IP in the ipAddr variable in the App_setupNetif() before passing it as arguement to initiate the netif, and stop the dhcp from starting in the App_allocateIPAddress() function.

Run the example

Attention
If you need to reload and run again, a CPU power-cycle is MUST
  • Launch a CCS debug session and run the example executable, see CCS Launch, Load and Run
  • You will see logs in the UART terminal as shown in the next section.
  • Note the IP address seen in the log, this is what we will use to communicate with the EVM.

Sample output

Steps to execute

  1. Run example on EVM
  2. Try to reach the EVM using ping as shown below, using a command shell on the host PC
    $ping 192.168.1.10
    "192.168.1.10" should be replaced with IP of EVM.
  3. Start TCP client using 'ncat' cmds as shown below. Below steps have been tried with a Linux Ubuntu 18.04 host PC running bash shell

    Install 'ncat' if not installed by doing below

    $sudo apt install ncat

    Invoke 'ncat' to connect to EVM IP

    $ncat 192.168.1.10 8888
    $

    "192.168.1.10" should be replaced with EVM IP.

  4. Send any msg in ncat terminal and wait for reply from EVM.
  5. Close the connection using Ctrl + C.

iPerf Performance

UDP Throughput

Direction Main core Remote Core
From Networt; To core 200 Mbps @ 100% CPU load 150 Mbps @ 85% CPU load
From Core; To Network 200 Mbps @ 100% CPU load 160 Mbps @ 75% CPU load

TCP Throughput

Direction Main core Remote Core
From Networt; To core 93 Mbps @ 60% CPU load 46.6 Mbps @ 25% CPU load
From Core; To Network 93 Mbps @ 80% CPU load 46.6 Mbps @ 20% CPU load

Troubleshooting issues

  • If you see MAC address as 00:00:00:00:00:00, likely you are using a very early Si sample which does not have MAC address "fused" in. In this case, do the below steps
    • Use manual MAC address populate option from sysconfig GUI
  • If you see a valid, non-zero MAC address and continuously see "Waiting for network UP..." prints in UART terminal
    • Make sure you see Enet IF UP Event. message, if not check the ethernet cable
    • Check the local network and check if the DHCP server is indeed running as expected
    • When using a home broadband/wifi router, its possible to check the clients connected to the DHCP server via a web browser. Check your router user manual for more details.

See Also

Ethernet And Networking