Request for exporting the entire keystore contents.
The host will make the request to encrypt and export the entire keystore contents for saving to some storage mechanism to be made available for future re-import. Only the host who owns the keystore structure may execute this operation. The host is responsible for pre-allocating enough memory to fit the keystore structure and all encryption parameters.
- Parameters
-
hdr | Common TI-SCI header |
keystore_lo | Lower 32-bit memory location where the encrypted keystore contents will be placed to pass back to the host |
keystore_hi | Higher 32-bit memory location where the encrypted keystore contents will be placed to pass back to the host |