AM64x MCU+ SDK  10.00.00
sdl_ecc.h File Reference

Introduction

Header file contains enumerations, structure definitions and function.

declarations for SDL ECC interface.

Go to the source code of this file.

Data Structures

struct  SDL_ECC_InitConfig_t
 
struct  SDL_ECC_InjectErrorConfig_t
 
struct  SDL_ECC_ErrorInfo_t
 

Typedefs

typedef uint32_t SDL_ECC_MemSubType
 This enumerator indicate ECC memory Sub Type. More...
 
typedef uint32_t SDL_ECC_MemType
 This enumerator indicate ECC memory type. More...
 
typedef void(* SDL_ECC_ErrorCallback_t) (uint32_t errorSrc, uint32_t address)
 
typedef void(* SDL_ECC_VIMDEDVector_t) (void)
 

Enumerations

enum  SDL_ECC_AggregatorType { SDL_ECC_AGGR_TYPE_INJECT_ONLY = 1, SDL_ECC_AGGR_TYPE_FULL_FUNCTION = 2 }
 
enum  SDL_ECC_InjectErrorType {
  SDL_INJECT_ECC_NO_ERROR = 0, SDL_INJECT_ECC_ERROR_FORCING_1BIT_ONCE = 1, SDL_INJECT_ECC_ERROR_FORCING_2BIT_ONCE = 2, SDL_INJECT_ECC_ERROR_FORCING_1BIT_N_ROW_ONCE = 3,
  SDL_INJECT_ECC_ERROR_FORCING_2BIT_N_ROW_ONCE = 4, SDL_INJECT_ECC_ERROR_FORCING_1BIT_REPEAT = 5, SDL_INJECT_ECC_ERROR_FORCING_2BIT_REPEAT = 6, SDL_INJECT_ECC_ERROR_FORCING_1BIT_N_ROW_REPEAT = 7,
  SDL_INJECT_ECC_ERROR_FORCING_2BIT_N_ROW_REPEAT = 8
}
 ECC Inject error types. More...
 
enum  SDL_ECC_RamIdType { SDL_ECC_RAM_ID_TYPE_WRAPPER = 0, SDL_ECC_RAM_ID_TYPE_INTERCONNECT = 1 }
 

Functions

int32_t SDL_ECC_initEsm (const SDL_ESM_Inst esmInstType)
 Initializes an module for usage with ECC module. More...
 
int32_t SDL_ECC_init (SDL_ECC_MemType eccMemType, const SDL_ECC_InitConfig_t *pECCInitConfig)
 Initializes ECC module for ECC detection. More...
 
int32_t SDL_ECC_initMemory (SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType)
 Initializes Memory to be ready for ECC error detection. Assumes ECC is already enabled. More...
 
int32_t SDL_ECC_selfTest (SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_ECC_InjectErrorType errorType, const SDL_ECC_InjectErrorConfig_t *pECCErrorConfig, uint32_t selfTestTimeOut)
 Runs self test by injecting and error and monitor response Assumes ECC is already enabled. More...
 
int32_t SDL_ECC_injectError (SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_ECC_InjectErrorType errorType, const SDL_ECC_InjectErrorConfig_t *pECCErrorConfig)
 Injects ECC error at specified location Assumes ECC is already enabled. More...
 
int32_t SDL_ECC_getStaticRegisters (SDL_ECC_MemType eccMemType, SDL_ECC_staticRegs *pStaticRegs)
 Gets the static registers for the specified ECC instance. More...
 
int32_t SDL_ECC_getErrorInfo (SDL_ECC_MemType eccMemType, SDL_Ecc_AggrIntrSrc intrSrc, SDL_ECC_ErrorInfo_t *pErrorInfo)
 Retrieves the ECC error information for the specified memtype and interrupt source. More...
 
int32_t SDL_ECC_ackIntr (SDL_ECC_MemType eccMemType, SDL_Ecc_AggrIntrSrc intrSrc)
 Acknowledge the ECC interrupt. More...
 
int32_t SDL_ECC_getESMErrorInfo (SDL_ESM_Inst instance, uint32_t intSrc, SDL_ECC_MemType *eccMemType, SDL_Ecc_AggrIntrSrc *intrSrcType)
 Retrieves the ECC error information for the specified ESM error. If it isn't an ECC error or the ECC error is not supported an error is returned. More...
 
int32_t SDL_ECC_clearNIntrPending (SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_Ecc_AggrIntrSrc intrSrc, SDL_Ecc_AggrEDCErrorSubType subType, uint32_t numEvents)
 Clears N pending interrupts for the specified memtype, subtype and interrupt source. More...
 
void SDL_ECC_applicationCallbackFunction (SDL_ECC_MemType eccMemType, uint32_t errorSrc, uint32_t address, uint32_t ramId, uint64_t bitErrorOffset, uint32_t bitErrorGroup)
 Application provided external callback function for ECC handling Called inside the reference functions when ECC errors occur. NOTE: This is application supplied and not part of the SDL If not supplied by application this will result in an linker error. More...
 
int32_t SDL_ECC_tpccParity (SDL_ECC_MemType eccMemType, uint32_t bitValue, uint32_t paramregvalue, uint32_t regval)
 Injects TPCC Parity error. More...
 

Typedef Documentation

◆ SDL_ECC_ErrorCallback_t

typedef void(* SDL_ECC_ErrorCallback_t) (uint32_t errorSrc, uint32_t address)

/brief Format of ECC error Call back function

◆ SDL_ECC_VIMDEDVector_t

typedef void(* SDL_ECC_VIMDEDVector_t) (void)

/brief Format of VIM DED vector function