AM64x MCU+ SDK  10.00.00

Introduction

This module contains APIs to program and use the I2C LLD module. The APIs can be used by other drivers to get access to I2C and also by application to initiate transaction operations.

The I2C LLD header file should be included in an application as follows:

Files

file  i2c_lld.h
 I2C LLD Driver API/interface file.
 

Data Structures

struct  I2CLLD_Transaction
 I2C Transaction. More...
 
struct  I2CLLD_Message
 I2C Message. More...
 
struct  I2C_ExtendedParams
 Data structure used with I2C_lld_write(), I2C_lld_writeIntr(), I2C_lld_read(), I2C_lld_readIntr() More...
 
struct  I2C_Memory_ExtendedParams
 Data structure used with I2C_lld_mem_write(), I2C_lld_mem_writeIntr(), I2C_lld_mem_read(), I2C_lld_mem_readIntr() More...
 
struct  I2CLLD_targetTransaction
 I2C Target Transaction. More...
 
struct  I2CLLD_Object
 I2C Driver Object. More...
 

Functions

int32_t I2C_lld_init (I2CLLD_Handle handle)
 This API Initializes the I2C instance. More...
 
int32_t I2C_lld_deInit (I2CLLD_Handle handle)
 This API De-Initializes the I2C instance. More...
 
int32_t I2C_lld_Transaction_init (I2CLLD_Transaction *transaction)
 API to set default values of I2CLLD_Transaction in transaction. More...
 
int32_t I2C_lld_Message_init (I2CLLD_Message *msg)
 API to set default values of I2CLLD_Message in msg. More...
 
int32_t I2C_lld_write (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams, uint32_t timeout)
 API to initiate the write transaction in polled mode. More...
 
int32_t I2C_lld_writeIntr (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams)
 API to initiate the write transaction in Interrupt mode. More...
 
int32_t I2C_lld_read (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams, uint32_t timeout)
 API to initiate the read transaction in polled mode. More...
 
int32_t I2C_lld_readIntr (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams)
 API to initiate the read transaction in Interrupt mode. More...
 
int32_t I2C_lld_mem_write (I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams, uint32_t timeout)
 Function to initiate a transfer from I2C in interrupt mode. More...
 
int32_t I2C_lld_mem_writeIntr (I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams)
 Function to initiate a transfer from I2C in interrupt mode. More...
 
int32_t I2C_lld_mem_read (I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams, uint32_t timeout)
 Function to initiate a transfer from I2C in interrupt mode. More...
 
int32_t I2C_lld_mem_readIntr (I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams)
 Function to initiate a transfer from I2C in interrupt mode. More...
 
int32_t I2C_lld_transferPoll (I2CLLD_Handle handle, I2CLLD_Message *msg)
 Function to initiate a transfer from I2C in polled mode. More...
 
int32_t I2C_lld_transferIntr (I2CLLD_Handle handle, I2CLLD_Message *msg)
 Function to initiate a transfer from I2C in interrupt mode. More...
 
int32_t I2C_lld_targetTransferIntr (I2CLLD_Handle handle, I2CLLD_targetTransaction *txn)
 Function to initiate a transfer from I2C in target mode. More...
 
int32_t I2C_lld_probe (I2CLLD_Handle handle, uint32_t targetAddr)
 Function to probe I2C. More...
 
int32_t I2C_lld_setBusFrequency (I2CLLD_Handle handle, uint32_t busFrequency)
 Function to set the bus frequency. More...
 
int32_t I2C_lld_recoverBus (I2CLLD_Handle handle, uint32_t i2cDelay)
 Function to recover the bus in case of lockup. More...
 
void I2C_lld_controllerIsr (void *args)
 This is the I2C Controller ISR and can be used as IRQ handler in Controller mode. More...
 
void I2C_lld_targetIsr (void *args)
 This is the I2C Target ISR and can be used as IRQ handler in Target mode. More...
 

Typedefs

typedef uint32_t(* I2C_Clock_getTicks) (void)
 The definition of a get System Tick function used by the I2C driver to keep track of time. More...
 
typedef uint32_t(* I2C_Clock_usecToTicks) (uint64_t usecs)
 The definition of a micro seconds to ticks function used by the I2C driver to get ticks from microseconds. More...
 
typedef void(* I2C_Clock_uSleep) (uint32_t usec)
 The definition of a sleep function used by the I2C driver for delay. More...
 
typedef void(* I2C_lld_transferCompleteCallback) (void *args, const I2CLLD_Message *msg, int32_t transferStatus)
 The definition of a transfer completion callback function used by the I2C driver when used in Controller Callback Mode. More...
 
typedef void(* I2C_lld_targetTransferCompleteCallback) (void *args, const I2CLLD_targetTransaction *targetTxn, int32_t transferStatus)
 The definition of a transfer completion callback function used by the I2C driver when used in Target Mode. More...
 
typedef struct I2CLLD_ObjectI2CLLD_Handle
 

Macros

#define I2C_MAX_NUM_OWN_TARGET_ADDR   (4U)
 

Return status

#define I2C_STS_SUCCESS   ((int32_t) 0)
 Return status when the API execution was successful. More...
 
#define I2C_STS_ERR   ((int32_t)-1)
 Return status when the API execution was not successful due to a generic Error. More...
 
#define I2C_STS_ERR_TIMEOUT   ((int32_t)-2)
 Return status when the API execution was not successful due to a time out. More...
 
#define I2C_STS_ERR_INVALID_PARAM   ((int32_t)-3)
 Return status when the API execution failed due invalid parameters. More...
 
#define I2C_STS_ERR_BUS_BUSY   ((int32_t)-4)
 Return status when the API execution failed due to driver busy. More...
 
#define I2C_STS_ERR_NO_ACK   ((int32_t)-5)
 Return status when the API execution failed due to no Acknowledgement from target. More...
 
#define I2C_STS_ERR_ARBITRATION_LOST   ((int32_t)-6)
 Return status when the API execution failed due to loss in arbitration during transmission. More...
 
#define I2C_STS_ERR_ACCESS_ERROR   ((int32_t)-7)
 

Timeout values

#define I2C_NO_WAIT   ((uint32_t)0)
 Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available. More...
 
#define I2C_WAIT_FOREVER   ((uint32_t)-1)
 Value to use when needing a timeout of infinity or wait forver until resource is available. More...
 

I2C Driver states

#define I2C_STATE_RESET   ((uint8_t) 0U)
 I2C driver is in Reset State prior to driver init and post driver deinit. More...
 
#define I2C_STATE_IDLE   ((uint8_t) 1U)
 I2C driver accepts runtime APIs only Ready State, otherwise return error. More...
 
#define I2C_STATE_BUSY   ((uint8_t) 2U)
 I2C driver is busy performing operation with peripherals, return error when APIs are invoked. More...
 
#define I2C_STATE_ERROR   ((uint8_t) 3U)
 I2C driver ran into error, returns error for all APIs other than deinit in this state. More...
 

MACROS used to select one of the standardized bus bit rates for

I2C communication. Deafults to I2C_400KHZ

#define I2C_100KHZ   ((uint8_t) 0U)
 I2C bus frequency : 100KHz. More...
 
#define I2C_400KHZ   ((uint8_t) 1U)
 I2C bus frequency : 400KHz. More...
 
#define I2C_1P0MHZ   ((uint8_t) 2U)
 I2C bus frequency : 1.0MHz. More...
 
#define I2C_3P4MHZ   ((uint8_t) 3U)
 I2C bus frequency : 3.4MHz. More...
 

MACROS for the possible values of Memory Write/Read API parameter.

#define I2C_MEM_ADDR_SIZE_8_BITS   ((uint8_t) 1U)
 I2C Target Internal Memory address 8 bits. More...
 
#define I2C_MEM_ADDR_SIZE_16_BITS   ((uint8_t) 2U)
 I2C Target Internal Memory address 16 bits. More...
 

MACROS used to define the state of the I2C Driver State Machine

#define I2C_WRITE_STATE   ((uint8_t) 10U)
 I2C is in Write state. More...
 
#define I2C_READ_STATE   ((uint8_t) 11U)
 I2C is in Write state. More...
 
#define I2C_TARGET_XFER_STATE   ((uint8_t) 12U)
 I2C is trasferring in target mode. More...
 
#define I2C_TARGET_RESTART_STATE   ((uint8_t) 13U)
 I2C is restarting trasfer in target mode. More...
 

Macro Definition Documentation

◆ I2C_MAX_NUM_OWN_TARGET_ADDR

#define I2C_MAX_NUM_OWN_TARGET_ADDR   (4U)

◆ I2C_STS_SUCCESS

#define I2C_STS_SUCCESS   ((int32_t) 0)

Return status when the API execution was successful.

◆ I2C_STS_ERR

#define I2C_STS_ERR   ((int32_t)-1)

Return status when the API execution was not successful due to a generic Error.

◆ I2C_STS_ERR_TIMEOUT

#define I2C_STS_ERR_TIMEOUT   ((int32_t)-2)

Return status when the API execution was not successful due to a time out.

◆ I2C_STS_ERR_INVALID_PARAM

#define I2C_STS_ERR_INVALID_PARAM   ((int32_t)-3)

Return status when the API execution failed due invalid parameters.

◆ I2C_STS_ERR_BUS_BUSY

#define I2C_STS_ERR_BUS_BUSY   ((int32_t)-4)

Return status when the API execution failed due to driver busy.

◆ I2C_STS_ERR_NO_ACK

#define I2C_STS_ERR_NO_ACK   ((int32_t)-5)

Return status when the API execution failed due to no Acknowledgement from target.

◆ I2C_STS_ERR_ARBITRATION_LOST

#define I2C_STS_ERR_ARBITRATION_LOST   ((int32_t)-6)

Return status when the API execution failed due to loss in arbitration during transmission.

◆ I2C_STS_ERR_ACCESS_ERROR

#define I2C_STS_ERR_ACCESS_ERROR   ((int32_t)-7)

◆ I2C_NO_WAIT

#define I2C_NO_WAIT   ((uint32_t)0)

Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available.

◆ I2C_WAIT_FOREVER

#define I2C_WAIT_FOREVER   ((uint32_t)-1)

Value to use when needing a timeout of infinity or wait forver until resource is available.

◆ I2C_STATE_RESET

#define I2C_STATE_RESET   ((uint8_t) 0U)

I2C driver is in Reset State prior to driver init and post driver deinit.

◆ I2C_STATE_IDLE

#define I2C_STATE_IDLE   ((uint8_t) 1U)

I2C driver accepts runtime APIs only Ready State, otherwise return error.

◆ I2C_STATE_BUSY

#define I2C_STATE_BUSY   ((uint8_t) 2U)

I2C driver is busy performing operation with peripherals, return error when APIs are invoked.

◆ I2C_STATE_ERROR

#define I2C_STATE_ERROR   ((uint8_t) 3U)

I2C driver ran into error, returns error for all APIs other than deinit in this state.

◆ I2C_100KHZ

#define I2C_100KHZ   ((uint8_t) 0U)

I2C bus frequency : 100KHz.

◆ I2C_400KHZ

#define I2C_400KHZ   ((uint8_t) 1U)

I2C bus frequency : 400KHz.

◆ I2C_1P0MHZ

#define I2C_1P0MHZ   ((uint8_t) 2U)

I2C bus frequency : 1.0MHz.

◆ I2C_3P4MHZ

#define I2C_3P4MHZ   ((uint8_t) 3U)

I2C bus frequency : 3.4MHz.

◆ I2C_MEM_ADDR_SIZE_8_BITS

#define I2C_MEM_ADDR_SIZE_8_BITS   ((uint8_t) 1U)

I2C Target Internal Memory address 8 bits.

◆ I2C_MEM_ADDR_SIZE_16_BITS

#define I2C_MEM_ADDR_SIZE_16_BITS   ((uint8_t) 2U)

I2C Target Internal Memory address 16 bits.

◆ I2C_WRITE_STATE

#define I2C_WRITE_STATE   ((uint8_t) 10U)

I2C is in Write state.

◆ I2C_READ_STATE

#define I2C_READ_STATE   ((uint8_t) 11U)

I2C is in Write state.

◆ I2C_TARGET_XFER_STATE

#define I2C_TARGET_XFER_STATE   ((uint8_t) 12U)

I2C is trasferring in target mode.

◆ I2C_TARGET_RESTART_STATE

#define I2C_TARGET_RESTART_STATE   ((uint8_t) 13U)

I2C is restarting trasfer in target mode.

Typedef Documentation

◆ I2C_Clock_getTicks

typedef uint32_t(* I2C_Clock_getTicks) (void)

The definition of a get System Tick function used by the I2C driver to keep track of time.

Returns
Returns system ticks in 32-bit unsigned int format

◆ I2C_Clock_usecToTicks

typedef uint32_t(* I2C_Clock_usecToTicks) (uint64_t usecs)

The definition of a micro seconds to ticks function used by the I2C driver to get ticks from microseconds.

Parameters
usecsMicro Seconds
Returns
Returns system ticks in 32-bit unsigned int format

◆ I2C_Clock_uSleep

typedef void(* I2C_Clock_uSleep) (uint32_t usec)

The definition of a sleep function used by the I2C driver for delay.

Parameters
usecMicro Seconds

◆ I2C_lld_transferCompleteCallback

typedef void(* I2C_lld_transferCompleteCallback) (void *args, const I2CLLD_Message *msg, int32_t transferStatus)

The definition of a transfer completion callback function used by the I2C driver when used in Controller Callback Mode.

Parameters
argsVoid Pointer
msgPointer to I2CLLD_Message Object
transferStatusTransfer Status

◆ I2C_lld_targetTransferCompleteCallback

typedef void(* I2C_lld_targetTransferCompleteCallback) (void *args, const I2CLLD_targetTransaction *targetTxn, int32_t transferStatus)

The definition of a transfer completion callback function used by the I2C driver when used in Target Mode.

Parameters
argsVoid Pointer
targetTxnPointer to I2CLLD_targetTransaction Object
transferStatusTransfer Status

◆ I2CLLD_Handle

typedef struct I2CLLD_Object * I2CLLD_Handle

Function Documentation

◆ I2C_lld_init()

int32_t I2C_lld_init ( I2CLLD_Handle  handle)

This API Initializes the I2C instance.

Parameters
handle[IN] Handle to the I2C instance used
Returns
I2C_StatusCode

◆ I2C_lld_deInit()

int32_t I2C_lld_deInit ( I2CLLD_Handle  handle)

This API De-Initializes the I2C instance.

Parameters
handle[IN] Handle to the I2C instance used
Returns
I2C_StatusCode

◆ I2C_lld_Transaction_init()

int32_t I2C_lld_Transaction_init ( I2CLLD_Transaction transaction)

API to set default values of I2CLLD_Transaction in transaction.

Parameters
transaction[IN] Pointer to the structure to be initialized
Returns
I2C_StatusCode

◆ I2C_lld_Message_init()

int32_t I2C_lld_Message_init ( I2CLLD_Message msg)

API to set default values of I2CLLD_Message in msg.

Parameters
msg[IN] Pointer to the structure to be initialized
Returns
I2C_StatusCode

◆ I2C_lld_write()

int32_t I2C_lld_write ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams,
uint32_t  timeout 
)

API to initiate the write transaction in polled mode.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
timeout[IN] Timeout for read operation in Micro Seconds I2cTimeoutValues
Returns
I2C_StatusCode

◆ I2C_lld_writeIntr()

int32_t I2C_lld_writeIntr ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams 
)

API to initiate the write transaction in Interrupt mode.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
Returns
I2C_StatusCode

◆ I2C_lld_read()

int32_t I2C_lld_read ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams,
uint32_t  timeout 
)

API to initiate the read transaction in polled mode.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
timeout[IN] Timeout for read operation in Micro Seconds I2cTimeoutValues
Returns
I2C_StatusCode

◆ I2C_lld_readIntr()

int32_t I2C_lld_readIntr ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams 
)

API to initiate the read transaction in Interrupt mode.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
Returns
I2C_StatusCode

◆ I2C_lld_mem_write()

int32_t I2C_lld_mem_write ( I2CLLD_Handle  handle,
I2C_Memory_ExtendedParams mem_extendedParams,
uint32_t  timeout 
)

Function to initiate a transfer from I2C in interrupt mode.

Parameters
handle[IN] Handle to the I2C instance used
mem_extendedParams[IN] Pointer to structure containing transfer parameters
timeout[IN] Timeout for read operation in Micro Seconds I2cTimeoutValues
Returns
I2C_StatusCode

◆ I2C_lld_mem_writeIntr()

int32_t I2C_lld_mem_writeIntr ( I2CLLD_Handle  handle,
I2C_Memory_ExtendedParams mem_extendedParams 
)

Function to initiate a transfer from I2C in interrupt mode.

Parameters
handle[IN] Handle to the I2C instance used
mem_extendedParams[IN] Pointer to structure containing transfer parameters
Returns
I2C_StatusCode

◆ I2C_lld_mem_read()

int32_t I2C_lld_mem_read ( I2CLLD_Handle  handle,
I2C_Memory_ExtendedParams mem_extendedParams,
uint32_t  timeout 
)

Function to initiate a transfer from I2C in interrupt mode.

Parameters
handle[IN] Handle to the I2C instance used
mem_extendedParams[IN] Pointer to structure containing transfer parameters
timeout[IN] Timeout for read operation in Micro Seconds I2cTimeoutValues
Returns
I2C_StatusCode

◆ I2C_lld_mem_readIntr()

int32_t I2C_lld_mem_readIntr ( I2CLLD_Handle  handle,
I2C_Memory_ExtendedParams mem_extendedParams 
)

Function to initiate a transfer from I2C in interrupt mode.

Parameters
handle[IN] Handle to the I2C instance used
mem_extendedParams[IN] Pointer to structure containing transfer parameters
Returns
I2C_StatusCode

◆ I2C_lld_transferPoll()

int32_t I2C_lld_transferPoll ( I2CLLD_Handle  handle,
I2CLLD_Message msg 
)

Function to initiate a transfer from I2C in polled mode.

Parameters
handle[IN] Handle to the I2C instance used
msg[IN] Pointer to the I2CLLD_Message structure that contains values for this specific transfer
Returns
I2C_StatusCode

◆ I2C_lld_transferIntr()

int32_t I2C_lld_transferIntr ( I2CLLD_Handle  handle,
I2CLLD_Message msg 
)

Function to initiate a transfer from I2C in interrupt mode.

Parameters
handle[IN] Handle to the I2C instance used
msg[IN] Pointer to the I2CLLD_Message structure that contains values for this specific transfer
Returns
I2C_StatusCode

◆ I2C_lld_targetTransferIntr()

int32_t I2C_lld_targetTransferIntr ( I2CLLD_Handle  handle,
I2CLLD_targetTransaction txn 
)

Function to initiate a transfer from I2C in target mode.

Parameters
handle[IN] Handle to the I2C instance used
txn[IN] Poiter to the I2CLLD_targetTransaction structure that contains values for this specific transfer
Returns
I2C_StatusCode

◆ I2C_lld_probe()

int32_t I2C_lld_probe ( I2CLLD_Handle  handle,
uint32_t  targetAddr 
)

Function to probe I2C.

Parameters
handle[IN] handle to the I2C instance used
targetAddr[IN] address of the target to probe
Returns
I2C_StatusCode

◆ I2C_lld_setBusFrequency()

int32_t I2C_lld_setBusFrequency ( I2CLLD_Handle  handle,
uint32_t  busFrequency 
)

Function to set the bus frequency.

Parameters
handle[IN] handle to the I2C instance used
busFrequency[IN] frequency value to be set I2cBitRates
Returns
I2C_StatusCode

◆ I2C_lld_recoverBus()

int32_t I2C_lld_recoverBus ( I2CLLD_Handle  handle,
uint32_t  i2cDelay 
)

Function to recover the bus in case of lockup.

Parameters
handle[IN] handle to the I2C
i2cDelay[IN] the length of delay for sending clock pulses to target
Returns
I2C_StatusCode

◆ I2C_lld_controllerIsr()

void I2C_lld_controllerIsr ( void *  args)

This is the I2C Controller ISR and can be used as IRQ handler in Controller mode.

Parameters
args[IN] Argument to the ISR

◆ I2C_lld_targetIsr()

void I2C_lld_targetIsr ( void *  args)

This is the I2C Target ISR and can be used as IRQ handler in Target mode.

Parameters
args[IN] Argument to the ISR
i2c_lld.h
I2C LLD Driver API/interface file.