AM64x MCU+ SDK  09.02.01
Flash_NandConfig Struct Reference

Detailed Description

Flash device config. This will be part of the flash config, so has to be filled by sysconfig or otherwise before invoking Flash_open.

Data Fields

uint8_t cmdWrsr
 
uint8_t cmdPageLoad
 
uint8_t cmdPageProg
 
uint32_t srWipReg
 
uint32_t xspiRdsrDummy
 
uint32_t progStatusReg
 
uint32_t xspiProgStatusReg
 
uint32_t eraseStatusReg
 
uint32_t xspiEraseStatusReg
 
uint8_t srProgStatus
 
uint8_t srEraseStatus
 
uint8_t srWriteProtectReg
 
uint8_t srWriteProtectMask
 

Field Documentation

◆ cmdWrsr

uint8_t Flash_NandConfig::cmdWrsr

◆ cmdPageLoad

uint8_t Flash_NandConfig::cmdPageLoad

◆ cmdPageProg

uint8_t Flash_NandConfig::cmdPageProg

◆ srWipReg

uint32_t Flash_NandConfig::srWipReg

◆ xspiRdsrDummy

uint32_t Flash_NandConfig::xspiRdsrDummy

◆ progStatusReg

uint32_t Flash_NandConfig::progStatusReg

◆ xspiProgStatusReg

uint32_t Flash_NandConfig::xspiProgStatusReg

◆ eraseStatusReg

uint32_t Flash_NandConfig::eraseStatusReg

◆ xspiEraseStatusReg

uint32_t Flash_NandConfig::xspiEraseStatusReg

◆ srProgStatus

uint8_t Flash_NandConfig::srProgStatus

◆ srEraseStatus

uint8_t Flash_NandConfig::srEraseStatus

◆ srWriteProtectReg

uint8_t Flash_NandConfig::srWriteProtectReg

◆ srWriteProtectMask

uint8_t Flash_NandConfig::srWriteProtectMask