AM64x MCU+ SDK  09.02.01
sdl_exception.h File Reference

Introduction

Header file contains enumerations, structure definitions and function declarations for SDL EXCEPTION interface.

The SDL exception data structures include:

  1. Structure of call back functions for various exception events

The SDL exception APIs include:

  1. API to execute SDL Exception module initialization
  2. APIs to handle various exceptions

Go to the source code of this file.

Data Structures

struct  SDL_EXCEPTION_CallbackFunctions_t
 Structure of call back functions for various exception events. More...
 

Typedefs

typedef void(* SDL_EXCEPTION_ECCCallback_t) (uint32_t intSource, uint32_t errorAddr, uint32_t ramId, uint64_t bitErrorOffset, uint32_t bitErrorGroup)
 Format of Call back function for ECC error events. More...
 
typedef void(* SDL_EXCEPTION_Callback_t) (void)
 Format of Call back function for exception. More...
 

Functions

void SDL_EXCEPTION_init (const SDL_EXCEPTION_CallbackFunctions_t *callbackFunctions)
 Initialise Exception module. More...
 
void SDL_EXCEPTION_registerECCHandler (SDL_EXCEPTION_ECCCallback_t ECCCallBackFunctionPtr)
 Function to register ECC exception handler. More...
 
void SDL_EXCEPTION_undefInstructionExptnHandler (void *param)
 Undefined Instruction Exception Handler. More...
 
void SDL_EXCEPTION_swIntrExptnHandler (void *param)
 SW Interrupt Exception Handler. More...
 
void SDL_EXCEPTION_prefetchAbortExptnHandler (void *param)
 Prefetch Abort Exception Handler. More...
 
void SDL_EXCEPTION_dataAbortExptnHandler (void *param)
 Data Abort Exception Handler. More...
 
void SDL_EXCEPTION_irqExptnHandler (void *param)
 IRQ Exception Handler. More...
 
void SDL_EXCEPTION_fiqExptnHandler (void *param)
 FIQ Exception Handler. More...
 

Typedef Documentation

◆ SDL_EXCEPTION_ECCCallback_t

typedef void(* SDL_EXCEPTION_ECCCallback_t) (uint32_t intSource, uint32_t errorAddr, uint32_t ramId, uint64_t bitErrorOffset, uint32_t bitErrorGroup)

Format of Call back function for ECC error events.

◆ SDL_EXCEPTION_Callback_t

typedef void(* SDL_EXCEPTION_Callback_t) (void)

Format of Call back function for exception.

Function Documentation

◆ SDL_EXCEPTION_init()

void SDL_EXCEPTION_init ( const SDL_EXCEPTION_CallbackFunctions_t callbackFunctions)

Initialise Exception module.

============================================================================

Parameters
callbackFunctionsPointer to callback Functions structure

◆ SDL_EXCEPTION_registerECCHandler()

void SDL_EXCEPTION_registerECCHandler ( SDL_EXCEPTION_ECCCallback_t  ECCCallBackFunctionPtr)

Function to register ECC exception handler.

============================================================================

Parameters
ECCCallBackFunctionPtrcallback function to register

◆ SDL_EXCEPTION_undefInstructionExptnHandler()

void SDL_EXCEPTION_undefInstructionExptnHandler ( void *  param)

Undefined Instruction Exception Handler.

============================================================================

Parameters
paramParameter pointer

◆ SDL_EXCEPTION_swIntrExptnHandler()

void SDL_EXCEPTION_swIntrExptnHandler ( void *  param)

SW Interrupt Exception Handler.

============================================================================

Parameters
paramParameter pointer

◆ SDL_EXCEPTION_prefetchAbortExptnHandler()

void SDL_EXCEPTION_prefetchAbortExptnHandler ( void *  param)

Prefetch Abort Exception Handler.

============================================================================

Parameters
paramParameter pointer

◆ SDL_EXCEPTION_dataAbortExptnHandler()

void SDL_EXCEPTION_dataAbortExptnHandler ( void *  param)

Data Abort Exception Handler.

============================================================================

Parameters
paramParameter pointer

◆ SDL_EXCEPTION_irqExptnHandler()

void SDL_EXCEPTION_irqExptnHandler ( void *  param)

IRQ Exception Handler.

============================================================================

Parameters
paramParameter pointer

◆ SDL_EXCEPTION_fiqExptnHandler()

void SDL_EXCEPTION_fiqExptnHandler ( void *  param)

FIQ Exception Handler.

============================================================================

Parameters
paramParameter pointer