AM64x MCU+ SDK  09.02.00

Introduction

For more details and example usage, see Queue

Data Structures

struct  QueueP_Elem
 Opaque QueueP element. More...
 
struct  QueueP_Object
 Opaque task object used with the task APIs. More...
 

Functions

QueueP_Handle QueueP_create (QueueP_Object *obj)
 Function to create a queue. More...
 
int32_t QueueP_delete (QueueP_Handle handle)
 Function to delete a queue. More...
 
void * QueueP_get (QueueP_Handle handle)
 Function to Get the element at the front of the queue. This function removes an element from the front of a queue and returns it. More...
 
int32_t QueueP_put (QueueP_Handle handle, void *elem)
 Function to Put an element at end of queue. More...
 
uint32_t QueueP_isEmpty (QueueP_Handle handle)
 Function to perform queue empty check. More...
 

Typedefs

typedef void * QueueP_Handle
 Opaque client reference to an instance of a QueueP. More...
 

Macros

#define QueueP_OBJECT_SIZE_MAX   (8u)
 Max size of task object across all OS's. More...
 

State codes for current queue state

#define QueueP_NOTEMPTY   (0U)
 
#define QueueP_EMPTY   (1U)
 

Macro Definition Documentation

◆ QueueP_NOTEMPTY

#define QueueP_NOTEMPTY   (0U)

◆ QueueP_EMPTY

#define QueueP_EMPTY   (1U)

◆ QueueP_OBJECT_SIZE_MAX

#define QueueP_OBJECT_SIZE_MAX   (8u)

Max size of task object across all OS's.

Typedef Documentation

◆ QueueP_Handle

typedef void* QueueP_Handle

Opaque client reference to an instance of a QueueP.

A QueueP_Handle returned from the QueueP_create represents that instance and is used in the other instance based functions

Function Documentation

◆ QueueP_create()

QueueP_Handle QueueP_create ( QueueP_Object obj)

Function to create a queue.

Parameters
obj[in] Pointer to QueueP_Object.
Returns
A QueueP_Handle on success or a NULL on an error

◆ QueueP_delete()

int32_t QueueP_delete ( QueueP_Handle  handle)

Function to delete a queue.

Parameters
handle[in] A QueueP_Handle returned from QueueP_create
Returns
Status of the functions
  • QueueP_OK: Deleted the queue instance
  • QueueP_FAILURE: Failed to delete the queue instance

◆ QueueP_get()

void* QueueP_get ( QueueP_Handle  handle)

Function to Get the element at the front of the queue. This function removes an element from the front of a queue and returns it.

Parameters
handle[in] A QueueP_Handle returned from QueueP_create
Returns
pointer to the element or pointer to queue itself incase of empty queue

◆ QueueP_put()

int32_t QueueP_put ( QueueP_Handle  handle,
void *  elem 
)

Function to Put an element at end of queue.

Parameters
handle[in] A QueueP_Handle returned from QueueP_create
elem[in] Pointer to new queue element
Returns
Status of the functions
  • QueueP_OK: Put the element at end of queue
  • QueueP_FAILURE: Failed to Put the element at end of queue

◆ QueueP_isEmpty()

uint32_t QueueP_isEmpty ( QueueP_Handle  handle)

Function to perform queue empty check.

Parameters
handle[in] A QueueP_Handle returned from QueueP_create
Returns
Current state of the Queue
  • QueueP_NOTEMPTY: queue is not empty
  • QueueP_EMPTY: queue is empty