This file contains the prototype of UART driver APIs.
Go to the source code of this file.
Data Structures | |
struct | UART_ExtendedParams |
struct | UART_Transaction |
Data structure used with UART_read() and UART_write() More... | |
struct | UARTLLD_InitObject |
UART driver initialization object. More... | |
struct | UARTLLD_Object |
UART driver object. More... | |
Macros | |
#define | UART_FIFO_SIZE (64U) |
Uart FIFO Size. More... | |
#define | UART_TRANSMITEMPTY_TRIALCOUNT (3000U) |
Timeout in ms used for TX FIFO empty at the time of delete. Three seconds is more than sufficient to transfer 64 bytes (FIFO size) at the lowest baud rate of 2400. More... | |
#define | UART_ERROR_COUNT (0x00FFFFFFU) |
Count Value to check error in the recieved byte More... | |
#define | UART_NOT_IN_USE(x) (void) 0 |
NOT_IN_USE macro to highlight unused parameters. More... | |
#define | UART_STATE_RX_DISABLED (0x0U) |
#define | UART_STATE_RX_ENABLED (0x1U) |
Transfer Status Code | |
#define | UART_STATUS_SUCCESS ((int32_t)0) |
Transaction success. More... | |
#define | UART_STATUS_FAILURE ((int32_t)-1) |
Transaction failure. More... | |
#define | UART_TRANSFER_STATUS_SUCCESS ((int32_t)0) |
Transaction success. More... | |
#define | UART_TRANSFER_STATUS_FAILURE ((int32_t)-1) |
Transaction failure. More... | |
#define | UART_WAIT_FOREVER ((int32_t)-1) |
Value to use when needing a timeout of infinity or wait forver until resource is available. More... | |
#define | UART_INVALID_PARAM ((int32_t)-3) |
Return status when the API execution failed due invalid parameters. More... | |
#define | UART_TRANSFER_BUSY ((int32_t)-4) |
Return status when the API execution failed due to driver busy. More... | |
#define | UART_TRANSFER_TIMEOUT ((int32_t)-2) |
Return status when the API execution was not successful due to a time out. More... | |
#define | UART_TRANSFER_INVALID_STATE ((int32_t)-5) |
Return status when the API execution failed due to invalid LLD state. More... | |
#define | UART_TRANSFER_STATUS_TIMEOUT (1U) |
Time out error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_BI (2U) |
Break condition error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_FE (3U) |
Framing error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_PE (4U) |
Parity error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_OE (5U) |
Overrun error. More... | |
#define | UART_TRANSFER_STATUS_CANCELLED (6U) |
Cancelled. More... | |
#define | UART_TRANSFER_STATUS_STARTED (7U) |
Transaction started. More... | |
#define | UART_TRANSFER_STATUS_READ_TIMEOUT (8U) |
Read timeout error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_INUSE (9U) |
UART is currently in use. More... | |
#define | UART_TRANSFER_STATUS_ERROR_OTH (10U) |
Other errors. More... | |
#define | UART_STATE_RESET (0U) |
#define | UART_STATE_READY (1U) |
#define | UART_STATE_BUSY (2U) |
#define | UART_STATE_ERROR (3U) |
UART Read length | |
This enumeration defines the return modes for UART_read(). UART_READ_RETURN_MODE_FULL unblocks or performs a callback when the read buffer has been filled with the number of bytes passed to UART_read(). UART_READ_RETURN_MODE_PARTIAL unblocks or performs a callback whenever a read timeout error occurs on the UART peripheral. The read timeout occurs if the read FIFO is non-empty and no new data has been received for a specific device/baudrate dependent number of clock cycles. This mode can be used when the exact number of bytes to be read is not known. | |
#define | UART_READ_RETURN_MODE_FULL (0U) |
Unblock/callback when buffer is full. More... | |
#define | UART_READ_RETURN_MODE_PARTIAL (1U) |
Unblock/callback when no new data comes in. More... | |
UART data length | |
#define | UART_LEN_5 (0U) |
#define | UART_LEN_6 (1U) |
#define | UART_LEN_7 (2U) |
#define | UART_LEN_8 (3U) |
UART stop bits | |
#define | UART_STOPBITS_1 (0U) |
#define | UART_STOPBITS_2 (1U) |
#define | UART_STOPBITS_1P5 (UART_STOPBITS_1) |
UART Parity | |
#define | UART_PARITY_NONE (0x00U) |
#define | UART_PARITY_ODD (0x01U) |
#define | UART_PARITY_EVEN (0x03U) |
#define | UART_PARITY_FORCED0 (0x07U) |
#define | UART_PARITY_FORCED1 (0x05U) |
UART Flow Control Type | |
#define | UART_FCTYPE_NONE (0x00U) |
#define | UART_FCTYPE_HW (0x02U) |
UART Flow Control Params for RX | |
#define | UART_FCPARAM_RXNONE (0x00U) |
#define | UART_FCPARAM_RXXONXOFF_2 (0x01U) |
#define | UART_FCPARAM_RXXONXOFF_1 (0x02U) |
#define | UART_FCPARAM_RXXONXOFF_12 (0x03U) |
#define | UART_FCPARAM_AUTO_RTS (0x40U) |
UART Flow Control Params for TX | |
#define | UART_FCPARAM_TXNONE (0x00U) |
#define | UART_FCPARAM_TXXONXOFF_2 (0x04U) |
#define | UART_FCPARAM_TXXONXOFF_1 (0x08U) |
#define | UART_FCPARAM_TXXONXOFF_12 (0x0CU) |
#define | UART_FCPARAM_AUTO_CTS (0x80U) |
UART RX trigger level | |
#define | UART_RXTRIGLVL_1 (1U) |
#define | UART_RXTRIGLVL_8 (8U) |
#define | UART_RXTRIGLVL_16 (16U) |
#define | UART_RXTRIGLVL_56 (56U) |
#define | UART_RXTRIGLVL_60 (60U) |
UART TX trigger level | |
#define | UART_TXTRIGLVL_1 (1U) |
#define | UART_TXTRIGLVL_8 (8U) |
#define | UART_TXTRIGLVL_16 (16U) |
#define | UART_TXTRIGLVL_32 (32U) |
#define | UART_TXTRIGLVL_56 (56U) |
UART Operational Mode | |
#define | UART_OPER_MODE_16X (0U) |
#define | UART_OPER_MODE_SIR (1U) |
#define | UART_OPER_MODE_16X_AUTO_BAUD (2U) |
#define | UART_OPER_MODE_13X (3U) |
#define | UART_OPER_MODE_MIR (4U) |
#define | UART_OPER_MODE_FIR (5U) |
#define | UART_OPER_MODE_CIR (6U) |
#define | UART_OPER_MODE_DISABLED (7U) |
Values indicating the filled status of TX FIFO | |
#define | UART_TX_FIFO_NOT_FULL |
#define | UART_TX_FIFO_FULL |
Values related to status of Interrupt souces. | |
#define | UART_INTID_MODEM_STAT |
Values pertaining to status of UART Interrupt sources. More... | |
#define | UART_INTID_TX_THRES_REACH |
#define | UART_INTID_RX_THRES_REACH |
#define | UART_INTID_RX_LINE_STAT_ERROR |
#define | UART_INTID_CHAR_TIMEOUT |
#define | UART_INTID_XOFF_SPEC_CHAR_DETECT |
#define | UART_INTID_MODEM_SIG_STATE_CHANGE |
#define | UART_INTR_PENDING (0U) |
Values indicating the UART Interrupt pending status. More... | |
#define | UART_N0_INTR_PENDING (1U) |
Values related to enabling/disabling of Interrupts. | |
#define | UART_INTR_CTS (UART_IER_CTS_IT_MASK) |
Values for enabling/disabling the interrupts of UART. More... | |
#define | UART_INTR_RTS (UART_IER_RTS_IT_MASK) |
#define | UART_INTR_XOFF (UART_IER_XOFF_IT_MASK) |
#define | UART_INTR_SLEEPMODE (UART_IER_SLEEP_MODE_MASK) |
#define | UART_INTR_MODEM_STAT (UART_IER_MODEM_STS_IT_MASK) |
#define | UART_INTR_LINE_STAT (UART_IER_LINE_STS_IT_MASK) |
#define | UART_INTR_THR (UART_IER_THR_IT_MASK) |
#define | UART_INTR_RHR_CTI (UART_IER_RHR_IT_MASK) |
#define | UART_INTR2_RX_EMPTY (UART_IER2_EN_RXFIFO_EMPTY_MASK) |
#define | UART_INTR2_TX_EMPTY (UART_IER2_EN_TXFIFO_EMPTY_MASK) |
Values related to Line Status information. | |
#define | UART_FIFO_PE_FE_BI_DETECTED (UART_LSR_RX_FIFO_STS_MASK) |
Values pertaining to UART Line Status information. More... | |
#define | UART_BREAK_DETECTED_ERROR (UART_LSR_RX_BI_MASK) |
#define | UART_FRAMING_ERROR (UART_LSR_RX_FE_MASK) |
#define | UART_PARITY_ERROR (UART_LSR_RX_PE_MASK) |
#define | UART_OVERRUN_ERROR (UART_LSR_RX_OE_MASK) |
Values related to Register Mode Configuration. | |
#define | UART_REG_CONFIG_MODE_A ((uint32_t) 0x0080) |
Values to be used while switching between register configuration modes. More... | |
#define | UART_REG_CONFIG_MODE_B ((uint32_t) 0x00BF) |
#define | UART_REG_OPERATIONAL_MODE ((uint32_t) 0x007F) |
UART Configration Mode | |
#define | UART_CONFIG_MODE_POLLED (0x00U) |
#define | UART_CONFIG_MODE_INTERRUPT (0x01U) |
#define | UART_CONFIG_MODE_USER_INTR (0x02U) |
#define | UART_CONFIG_MODE_DMA (0x03U) |
Typedefs | |
typedef void * | UART_DmaHandle |
A handle that is returned from a UART_open() call. More... | |
typedef void * | UART_DmaChConfig |
typedef uint32_t(* | UART_clockGet) (void) |
typedef uint32_t(* | UART_clockUsecToTick) (uint64_t usecs) |
typedef void(* | UART_readCompCallbackFxn) (void *hUart) |
The definition of a read complete callback function used by the UART driver when used in UART_TRANSFER_MODE_CALLBACK. More... | |
typedef void(* | UART_writeCompCallbackFxn) (void *hUart) |
The definition of a write complete callback function used by the UART driver when used in UART_TRANSFER_MODE_CALLBACK. More... | |
typedef void(* | UART_errorCallbackFxn) (void *hUart) |
The definition of a error callback function used by the UART driver when used in UART_TRANSFER_MODE_CALLBACK. More... | |
typedef struct UARTLLD_InitObject * | UARTLLD_InitHandle |
typedef struct UARTLLD_Object * | UARTLLD_Handle |
Functions | |
uint32_t | UART_operatingModeSelect (uint32_t baseAddr, uint32_t modeFlag) |
uint32_t | UART_spaceAvail (uint32_t baseAddr) |
int32_t | UART_writeCancelNoCB (UARTLLD_Handle hUart) |
int32_t | UART_readCancelNoCB (UARTLLD_Handle hUart) |
uint32_t | UART_getBaseAddr_lld (UARTLLD_Handle handle) |
Function to get base address of UART instance of a particular handle. More... | |
void | UART_enableLoopbackMode (uint32_t baseAddr) |
Function to enable loopback mode. This function is for internal use. Not recommended for customers to use. More... | |
void | UART_disableLoopbackMode (uint32_t baseAddr) |
Function to disable loopback mode. This function is for internal use. Not recommended for customers to use. More... | |
int32_t | UART_lld_init (UARTLLD_Handle hUart) |
This API Initializes the UART instance. More... | |
int32_t | UART_lld_initDma (UARTLLD_Handle hUart) |
This API Initializes the UART instance in DMA mode. More... | |
int32_t | UART_lld_deInit (UARTLLD_Handle hUart) |
This API De-Initializes the UART instance. More... | |
int32_t | UART_lld_deInitDma (UARTLLD_Handle hUart) |
This API De-Initializes the UART instance in DMA mode. More... | |
int32_t | UART_lld_write (UARTLLD_Handle hUart, void *txBuf, uint32_t size, uint32_t timeout, const UART_ExtendedParams *extendedParams) |
This API writes data to the UART instance in Polling mode. More... | |
int32_t | UART_lld_writeIntr (UARTLLD_Handle hUart, void *txBuf, uint32_t size, const UART_ExtendedParams *extendedParams) |
This API writes data to the UART instance in Interrupt mode. More... | |
int32_t | UART_lld_writeDma (UARTLLD_Handle hUart, void *txBuf, uint32_t size, const UART_ExtendedParams *extendedParams) |
This API writes data to the UART instance in DMA mode. More... | |
int32_t | UART_lld_read (UARTLLD_Handle hUart, void *rxBuf, uint32_t size, uint32_t timeout, const UART_ExtendedParams *extendedParams) |
This API writes data to the UART instance in Polling mode. More... | |
int32_t | UART_lld_readIntr (UARTLLD_Handle hUart, void *rxBuf, uint32_t size, const UART_ExtendedParams *extendedParams) |
This API writes data to the UART instance in Interrupt mode. More... | |
int32_t | UART_lld_readDma (UARTLLD_Handle hUart, void *rxBuf, uint32_t size, const UART_ExtendedParams *extendedParams) |
This API writes data to the UART instance in DMA mode. More... | |
int32_t | UART_lld_writeCancel (UARTLLD_Handle hUart, UART_Transaction *trans) |
This API cancels current UART Write. More... | |
int32_t | UART_lld_readCancel (UARTLLD_Handle hUart, UART_Transaction *trans) |
This API cancels current UART Read. More... | |
int32_t | UART_lld_flushTxFifo (UARTLLD_Handle hUart) |
Function to flush a TX FIFO of peripheral specified by the UART handle. More... | |
int32_t | UART_procLineStatusErr (UARTLLD_Handle hUart) |
Function to check various error conditions in uart. More... | |
int32_t | UART_lld_setRxState (UARTLLD_Handle hUart, uint32_t state) |
Function to enable/disable UART RX. More... | |
void | UART_lld_controllerIsr (void *args) |
This is the UART ISR and can be used as IRQ handler. More... | |
void | UART_intrDisable (uint32_t baseAddr, uint32_t intrFlag) |
This API disables the specified interrupts in the UART mode of operation. More... | |
void | UART_intr2Disable (uint32_t baseAddr, uint32_t intrFlag) |
This API disables the specified interrupts in the UART mode of operation for IER2. More... | |
uint32_t | UART_checkCharsAvailInFifo (uint32_t baseAddr) |
This API checks if the RX FIFO (or RHR in non-FIFO mode) has atleast one byte of data to be read. More... | |
uint32_t | UART_readLineStatus (uint32_t baseAddr) |
This API reads the line status register value. More... | |
uint8_t | UART_getCharFifo (uint32_t baseAddr, uint8_t *readBuf) |
This API reads the data present at the top of the RX FIFO, that is, the data in the Receive Holding Register(RHR). However before reading the data from RHR, it checks for RX error. More... | |
void | UART_putChar (uint32_t baseAddr, uint8_t byteTx) |
This API writes a byte to the Transmitter FIFO without checking for the emptiness of the Transmitter FIFO or the Transmitter Shift Register(TSR). More... | |
void | UART_intrEnable (uint32_t baseAddr, uint32_t intrFlag) |
This API enables the specified interrupts in the UART mode of operation. More... | |
uint32_t | UART_getChar (uint32_t baseAddr, uint8_t *pChar) |
This API reads a byte from the Receiver Buffer Register (RBR). It checks once if any character is ready to be read. More... | |
uint32_t | UART_getIntr2Status (uint32_t baseAddr) |
This API determines the UART Interrupt Status 2. More... | |
uint32_t | UART_getIntrIdentityStatus (uint32_t baseAddr) |
This API determines the UART Interrupt Status. More... | |
void | UART_intr2Enable (uint32_t baseAddr, uint32_t intrFlag) |
This API enables the specified interrupts in the UART mode of operation for IER2. More... | |
void | UART_lld_Transaction_init (UART_Transaction *trans) |
Function to initialize the UART_Transaction struct to its defaults. More... | |
void | UART_lld_Transaction_deInit (UART_Transaction *trans) |
Function to de-initialize the UART_Transaction struct to its defaults. More... | |