This module contains APIs to program and use the MCSPI LLD module. The APIs can be used by other drivers to get access to MCSPI and also by application to initiate data transfer operation.
Files | |
file | mcspi_lld.h |
MCSPI LLD Driver API/interface file. | |
Data Structures | |
struct | MCSPI_Transaction |
Data structure used with MCSPI_transfer() More... | |
struct | MCSPI_ExtendedParams |
Data structure used with MCSPI_lld_read(), MCSPI_lld_readIntr(), MCSPI_lld_readDma(), MCSPI_lld_write(), MCSPI_lld_writeIntr, MCSPI_lld_writeDma, MCSPI_lld_readWrite(), MCSPI_lld_readWriteIntr(), MCSPI_lld_readWriteDma(). MCSPI ExtendedParams to be used in case, one's don't want to use default parameters, else pass NULL. More... | |
struct | MCSPI_ChConfig |
MCSPI configuration parameters for the channel. More... | |
struct | MCSPI_ChObject |
MCSPI channel object. More... | |
struct | MCSPILLD_InitObject |
MCSPI driver initialization object. More... | |
struct | MCSPILLD_Object |
MCSPI driver object. More... | |
Functions | |
void | MCSPI_reset (uint32_t baseAddr) |
void | MCSPI_clearAllIrqStatus (uint32_t baseAddr) |
void | MCSPI_stop (MCSPILLD_Handle hMcspi, MCSPI_ChObject *chObj, uint32_t chNum) |
void | MCSPI_setChDataSize (uint32_t baseAddr, MCSPI_ChObject *chObj, uint32_t dataSize, uint32_t csDisable) |
static void | MCSPI_intrStatusClear (const MCSPI_ChObject *chObj, uint32_t baseAddr, uint32_t intFlags) |
int32_t | MCSPI_lld_init (MCSPILLD_Handle hMcspi) |
This API Initializes the McSPI instance. More... | |
int32_t | MCSPI_lld_initDma (MCSPILLD_Handle hMcspi) |
This API Initializes the McSPI instance in DMA Mode. More... | |
int32_t | MCSPI_lld_deInit (MCSPILLD_Handle hMcspi) |
This API De-Initializes the McSPI instance. More... | |
int32_t | MCSPI_lld_deInitDma (MCSPILLD_Handle hMcspi) |
This API De-Initializes the McSPI instance in DMA mode. More... | |
int32_t | MCSPI_lld_write (MCSPILLD_Handle hMcspi, void *txBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API writes data to the McSPI instance in Polling mode. More... | |
int32_t | MCSPI_lld_writeIntr (MCSPILLD_Handle hMcspi, void *txBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API writes data to the McSPI instance in Interrupt mode. More... | |
int32_t | MCSPI_lld_writeDma (MCSPILLD_Handle hMcspi, void *txBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API writes data to the McSPI instance in DMA mode. More... | |
int32_t | MCSPI_lld_read (MCSPILLD_Handle hMcspi, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads data from the McSPI instance in Polling mode. More... | |
int32_t | MCSPI_lld_readIntr (MCSPILLD_Handle hMcspi, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads data from the McSPI instance in Interrupt mode. More... | |
int32_t | MCSPI_lld_readDma (MCSPILLD_Handle hMcspi, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads data from the McSPI instance in DMA mode. More... | |
int32_t | MCSPI_lld_readWrite (MCSPILLD_Handle hMcspi, void *txBuf, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads writes data from the McSPI instance in polling mode. More... | |
int32_t | MCSPI_lld_readWriteIntr (MCSPILLD_Handle hMcspi, void *txBuf, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads writes data from the McSPI instance in Interrupt mode. More... | |
int32_t | MCSPI_lld_readWriteDma (MCSPILLD_Handle hMcspi, void *txBuf, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads writes data from the McSPI instance in DMA mode. More... | |
int32_t | MCSPI_lld_readWriteCancel (MCSPILLD_Handle hMcspi) |
This API cancels current McSPI transfer. More... | |
int32_t | MCSPI_lld_readWriteDmaCancel (MCSPILLD_Handle hMcspi) |
This API cancels current McSPI transfer in DMA mode. More... | |
int32_t | MCSPI_lld_transfer (MCSPILLD_Handle hMcspi, MCSPI_Transaction *transaction) |
This API transfers data from the McSPI instance in Polling mode. More... | |
int32_t | MCSPI_lld_transferIntr (MCSPILLD_Handle hMcspi, MCSPI_Transaction *transaction) |
This API reads data from the McSPI instance in Interrupt mode. More... | |
int32_t | MCSPI_lld_transferDma (MCSPILLD_Handle hMcspi, MCSPI_Transaction *transaction) |
This API reads data from the McSPI instance in DMA mode. More... | |
void | MCSPI_lld_controllerIsr (void *args) |
This is the McSPI Controller ISR and can be used as IRQ handler in Controller mode. More... | |
void | MCSPI_lld_peripheralIsr (void *args) |
This is the McSPI Peripheral ISR and can be used as IRQ handler in Peripheral mode. More... | |
int32_t | MCSPI_lld_getState (MCSPILLD_Handle hMcspi) |
This API returns the driver state. More... | |
int32_t | MCSPI_lld_transferCancel (MCSPILLD_Handle hMcspi) |
This API cancels current McSPI transfer. More... | |
int32_t | MCSPI_lld_transferDmaCancel (MCSPILLD_Handle hMcspi) |
This API cancels current McSPI transfer in DMA mode. More... | |
static void | MCSPI_lld_ChConfig_init (MCSPI_ChConfig *chConfig) |
Function to initialize the MCSPI_ChConfig struct to its defaults. More... | |
static void | MCSPI_lld_Transaction_init (MCSPI_Transaction *trans) |
Function to initialize the MCSPI_Transaction struct to its defaults. More... | |
uint32_t | MCSPI_lld_getBaseAddr (MCSPILLD_Handle handle) |
Function to get base address of MCSPI instance of a particular handle. More... | |
int32_t | MCSPI_lld_reConfigFifo (MCSPILLD_Handle handle, uint32_t chNum, uint32_t numWordsRxTx) |
Function to re-configure Effective FIFO Words. More... | |
static uint8_t | MCSPI_getBufWidthShift (uint32_t dataSize) |
This API will return the buffer width in bytes based on dataSize. More... | |
static uint32_t | MCSPI_readChStatusReg (uint32_t baseAddr, uint32_t chNum) |
This API will return the status of the McSPI channel currently in use. More... | |
static uint32_t | MCSPI_readChCtrlReg (uint32_t baseAddr, uint32_t chNum) |
This API returns Channel control register value. More... | |
static void | MCSPI_writeChCtrlReg (uint32_t baseAddr, uint32_t chNum, uint32_t regVal) |
This API sets Channel control register value. More... | |
static uint32_t | MCSPI_readChConf (uint32_t baseAddr, uint32_t chNum) |
This API returns Channel Config register value. More... | |
static void | MCSPI_writeChConfReg (uint32_t baseAddr, uint32_t chNum, uint32_t regVal) |
This API sets Channel Config register value. More... | |
static void | MCSPI_writeTxDataReg (uint32_t baseAddr, uint32_t txData, uint32_t chNum) |
This API will put the data on to the McSPI Channel transmit register. More... | |
static void | MCSPI_enableTxFIFO (uint32_t baseAddr, uint32_t chNum, uint32_t enableFlag) |
This API will enable/disable the Tx FIFOs of McSPI peripheral. More... | |
static void | MCSPI_enableRxFIFO (uint32_t baseAddr, uint32_t chNum, uint32_t enableFlag) |
This API will enable/disable the Rx FIFOs of McSPI peripheral. More... | |
static uint32_t | MCSPI_readRxDataReg (uint32_t baseAddr, uint32_t chNum) |
This API will return the data present in the MCSPI_RX register. More... | |
static void | MCSPI_setDataWidth (uint32_t baseAddr, uint32_t chNum, uint32_t dataWidth) |
This API will set the data width in the channel config register. More... | |
Typedefs | |
typedef void * | MCSPI_DmaHandle |
typedef void * | MCSPI_DmaChConfig |
typedef uint32_t(* | MCSPI_clockGet) (void) |
typedef void(* | MCSPI_transferCallbackFxn) (void *args, uint32_t tansferStatus) |
The definition of a transfer completion callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK. More... | |
typedef void(* | MCSPI_errorCallbackFxn) (void *args) |
The definition of a error callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK. More... | |
typedef struct MCSPILLD_InitObject * | MCSPILLD_InitHandle |
typedef struct MCSPILLD_Object * | MCSPILLD_Handle |
Macros | |
#define | MCSPI_MAX_NUM_CHANNELS (4U) |
Max number of channels/Chip Select (CS) supported. More... | |
#define | MCSPI_ERROR_TX_UNDERFLOW (0x00000001U) |
McSPI error macro's. More... | |
#define | MCSPI_ERROR_RX_OVERFLOW (0x00000002U) |
#define | MCSPI_MAX_CLK_DIVIDER_SUPPORTED (4096U) |
#define | MCSPI_FIFO_LENGTH (64U) |
Total length of FIFO for both TX/RX. More... | |
#define | MCSPI_RX_FIFO_ENABLE |
McSPI peripheral Rx FIFO is enabled. More... | |
#define | MCSPI_RX_FIFO_DISABLE |
McSPI peripheral Rx FIFO is disabled. More... | |
#define | MCSPI_TX_FIFO_ENABLE |
McSPI peripheral Tx FIFO is enabled. More... | |
#define | MCSPI_TX_FIFO_DISABLE |
McSPI peripheral Tx FIFO is disabled. More... | |
#define | MCSPI_REG_OFFSET (0x14U) |
McSPI Register Offset for MCSPI_CHxCONF, MCSPI_CHxSTAT, MCSPI_CHxCTRL, MCSPI_TXx and MCSPI_RXx register set. More... | |
#define | MCSPI_CHCONF(x) |
Base address of McSPI_CHCONF(x) More... | |
#define | MCSPI_CHSTAT(x) |
Base address of McSPI_CHSTAT(x) More... | |
#define | MCSPI_CHCTRL(x) |
Base address of McSPI_CHCTRL(x) More... | |
#define | MCSPI_CHTX(x) |
Base address of McSPI_CHTX(x) More... | |
#define | MCSPI_CHRX(x) |
Base address of McSPI_CHRX(x) More... | |
#define | MCSPI_CLKD_MASK (0x0FU) |
#define | MCSPI_IRQSTATUS_CLEAR_ALL |
Bit mask to clear all status bits. More... | |
Return status | |
#define | MCSPI_STATUS_SUCCESS ((int32_t)0) |
Return status when the API execution was successful. More... | |
#define | MCSPI_STATUS_FAILURE ((int32_t)-1) |
Return status when the API execution was not successful due to a failure. More... | |
#define | MCSPI_TIMEOUT ((int32_t)-2) |
Return status when the API execution was not successful due to a time out. More... | |
#define | MCSPI_INVALID_PARAM ((int32_t)-3) |
Return status when the API execution failed due invalid parameters. More... | |
#define | MCSPI_STATUS_BUSY ((int32_t)-4) |
Return status when the API execution failed due to driver busy. More... | |
#define | MCSPI_INVALID_STATE ((int32_t)-5) |
Return status when the API execution failed due to invalid state. More... | |
Timeout values | |
#define | MCSPI_NO_WAIT ((uint32_t)0) |
Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available. More... | |
#define | MCSPI_WAIT_FOREVER ((uint32_t)-1) |
Value to use when needing a timeout of infinity or wait forver until resource is available. More... | |
MCSPI Driver states | |
#define | MCSPI_STATE_RESET ((uint32_t)0U) |
MCSPI driver is in Reset State prior to driver init and post driver deinit. More... | |
#define | MCSPI_STATE_READY ((uint32_t)1U) |
MCSPI driver accepts runtime APIs only Ready State, otherwise return error. More... | |
#define | MCSPI_STATE_BUSY ((uint32_t)2U) |
MCSPI driver is busy performing operation with peripherals, return error when APIs are invoked. More... | |
#define | MCSPI_STATE_ERROR ((uint32_t)3U) |
MCSPI driver ran into error, returns error for all APIs other than deinit in this state. More... | |
Channel Id | |
Values used to determine the channel number used for McSPI communication. This determines which Chip Select (CS) line to use | |
#define | MCSPI_CHANNEL_0 (0U) |
#define | MCSPI_CHANNEL_1 (1U) |
#define | MCSPI_CHANNEL_2 (2U) |
#define | MCSPI_CHANNEL_3 (3U) |
Operating Mode | |
Values used to determine the McSPI driver operation. | |
#define | MCSPI_OPER_MODE_POLLED (0U) |
#define | MCSPI_OPER_MODE_INTERRUPT (1U) |
#define | MCSPI_OPER_MODE_DMA (2U) |
Transfer Status Code | |
Status codes that are set by the MCSPI driver | |
#define | MCSPI_TRANSFER_COMPLETED ((int32_t)0U) |
#define | MCSPI_TRANSFER_STARTED ((int32_t)1U) |
#define | MCSPI_TRANSFER_CANCELLED ((int32_t)2U) |
#define | MCSPI_TRANSFER_FAILED ((int32_t)3U) |
#define | MCSPI_TRANSFER_CSN_DEASSERT ((int32_t)4U) |
#define | MCSPI_TRANSFER_TIMEOUT ((int32_t)5U) |
Modes of Operation | |
Definitions for various MCSPI modes of operation The MCSPI driver operates in both controller and SPI peripheral modes. Logically, the implementation is identical, however the difference between these two modes is driven by hardware. The default mode is MCSPI_MS_MODE_CONTROLLER, but can be set to peripheral mode by setting MCSPI_OpenParams.msMode to MCSPI_MS_MODE_PERIPHERAL in the parameters passed to MCSPI_open(). | |
#define | MCSPI_MS_MODE_CONTROLLER (CSL_MCSPI_MODULCTRL_MS_MASTER) |
The module generates the clock and CS. More... | |
#define | MCSPI_MS_MODE_PERIPHERAL (CSL_MCSPI_MODULCTRL_MS_SLAVE) |
The module receives the clock and CS. More... | |
Frame Format | |
Definitions for various SPI data frame formats POL0 = SPICLK is held low during the INACTIVE state POL1 = SPICLK is held high during the INACTIVE state PHA0 = Data are latched on odd-numbered edges of SPICLK PHA1 = Data are latched on even-numbered edges of SPICLK | |
#define | MCSPI_FF_POL0_PHA0 (0U) |
#define | MCSPI_FF_POL0_PHA1 (1U) |
#define | MCSPI_FF_POL1_PHA0 (2U) |
#define | MCSPI_FF_POL1_PHA1 (3U) |
Chip-select Polarity | |
#define | MCSPI_CS_POL_HIGH (CSL_MCSPI_CH0CONF_EPOL_ACTIVEHIGH) |
SPIEN (CS) is held high during the ACTIVE state. More... | |
#define | MCSPI_CS_POL_LOW (CSL_MCSPI_CH0CONF_EPOL_ACTIVELOW) |
SPIEN (CS) is held low during the ACTIVE state. More... | |
Transmit-Receive Modes | |
#define | MCSPI_TR_MODE_TX_RX (CSL_MCSPI_CH0CONF_TRM_TRANSRECEI) |
#define | MCSPI_TR_MODE_RX_ONLY (CSL_MCSPI_CH0CONF_TRM_RECEIVONLY) |
#define | MCSPI_TR_MODE_TX_ONLY (CSL_MCSPI_CH0CONF_TRM_TRANSONLY) |
Input Select | |
#define | MCSPI_IS_D0 (CSL_MCSPI_CH0CONF_IS_LINE0) |
Data line 0 (SPIDAT[0]) selected for reception. More... | |
#define | MCSPI_IS_D1 (CSL_MCSPI_CH0CONF_IS_LINE1) |
Data line 1 (SPIDAT[1]) selected for reception. More... | |
Transmission Enable for Data Line | |
#define | MCSPI_DPE_ENABLE (CSL_MCSPI_CH0CONF_DPE0_ENABLED) |
Data line selected for transmission. More... | |
#define | MCSPI_DPE_DISABLE (CSL_MCSPI_CH0CONF_DPE0_DISABLED) |
No transmission on Data Line. More... | |
Peripheral Chip-select Signal Select | |
#define | MCSPI_SLV_CS_SELECT_0 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN0) |
#define | MCSPI_SLV_CS_SELECT_1 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN1) |
#define | MCSPI_SLV_CS_SELECT_2 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN2) |
#define | MCSPI_SLV_CS_SELECT_3 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN3) |
Start-bit Polarity | |
#define | MCSPI_SB_POL_HIGH (CSL_MCSPI_CH0CONF_SBPOL_HIGHLEVEL) |
SStart-bit polarity is held to 1 during MCSPI transfer. More... | |
#define | MCSPI_SB_POL_LOW (CSL_MCSPI_CH0CONF_SBPOL_LOWLEVEL) |
Start-bit polarity is held to 0 during MCSPI transfer. More... | |
Chip-select Idle Time | |
Values used to configure the chip select time control (TCS) | |
#define | MCSPI_TCS0_0_CLK (CSL_MCSPI_CH0CONF_TCS0_ZEROCYCLEDLY) |
0.5 clock cycles delay More... | |
#define | MCSPI_TCS0_1_CLK (CSL_MCSPI_CH0CONF_TCS0_ONECYCLEDLY) |
1.5 clock cycles delay More... | |
#define | MCSPI_TCS0_2_CLK (CSL_MCSPI_CH0CONF_TCS0_TWOCYCLEDLY) |
2.5 clock cycles delay More... | |
#define | MCSPI_TCS0_3_CLK (CSL_MCSPI_CH0CONF_TCS0_THREECYCLEDLY) |
3.5 clock cycles delay More... | |
Channel Mode | |
#define | MCSPI_CH_MODE_SINGLE (CSL_MCSPI_MODULCTRL_SINGLE_SINGLE) |
Only one channel will be used in controller mode. This should be used when CS is used in forced enable mode. More... | |
#define | MCSPI_CH_MODE_MULTI (CSL_MCSPI_MODULCTRL_SINGLE_MULTI) |
More than one channel will be used in controller mode. More... | |
Pin Mode | |
#define | MCSPI_PINMODE_3PIN (CSL_MCSPI_MODULCTRL_PIN34_3PINMODE) |
SPIEN (CS) is not used. In this mode all related options to chip-select have no meaning. More... | |
#define | MCSPI_PINMODE_4PIN (CSL_MCSPI_MODULCTRL_PIN34_4PINMODE) |
Init Delay | |
Values used to enable initial delay for first transfer | |
#define | MCSPI_INITDLY_0 (CSL_MCSPI_MODULCTRL_INITDLY_NODELAY) |
No delay. More... | |
#define | MCSPI_INITDLY_4 (CSL_MCSPI_MODULCTRL_INITDLY_4CLKDLY) |
4 SPI bus clock delays More... | |
#define | MCSPI_INITDLY_8 (CSL_MCSPI_MODULCTRL_INITDLY_8CLKDLY) |
8 SPI bus clock delays More... | |
#define | MCSPI_INITDLY_16 (CSL_MCSPI_MODULCTRL_INITDLY_16CLKDLY) |
16 SPI bus clock delays More... | |
#define | MCSPI_INITDLY_32 (CSL_MCSPI_MODULCTRL_INITDLY_32CLKDLY) |
32 SPI bus clock delays More... | |
#define MCSPI_STATUS_SUCCESS ((int32_t)0) |
Return status when the API execution was successful.
#define MCSPI_STATUS_FAILURE ((int32_t)-1) |
Return status when the API execution was not successful due to a failure.
#define MCSPI_TIMEOUT ((int32_t)-2) |
Return status when the API execution was not successful due to a time out.
#define MCSPI_INVALID_PARAM ((int32_t)-3) |
Return status when the API execution failed due invalid parameters.
#define MCSPI_STATUS_BUSY ((int32_t)-4) |
Return status when the API execution failed due to driver busy.
#define MCSPI_INVALID_STATE ((int32_t)-5) |
Return status when the API execution failed due to invalid state.
#define MCSPI_NO_WAIT ((uint32_t)0) |
Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available.
#define MCSPI_WAIT_FOREVER ((uint32_t)-1) |
Value to use when needing a timeout of infinity or wait forver until resource is available.
#define MCSPI_STATE_RESET ((uint32_t)0U) |
MCSPI driver is in Reset State prior to driver init and post driver deinit.
#define MCSPI_STATE_READY ((uint32_t)1U) |
MCSPI driver accepts runtime APIs only Ready State, otherwise return error.
#define MCSPI_STATE_BUSY ((uint32_t)2U) |
MCSPI driver is busy performing operation with peripherals, return error when APIs are invoked.
#define MCSPI_STATE_ERROR ((uint32_t)3U) |
MCSPI driver ran into error, returns error for all APIs other than deinit in this state.
#define MCSPI_CHANNEL_0 (0U) |
#define MCSPI_CHANNEL_1 (1U) |
#define MCSPI_CHANNEL_2 (2U) |
#define MCSPI_CHANNEL_3 (3U) |
#define MCSPI_OPER_MODE_POLLED (0U) |
#define MCSPI_OPER_MODE_INTERRUPT (1U) |
#define MCSPI_OPER_MODE_DMA (2U) |
#define MCSPI_MAX_NUM_CHANNELS (4U) |
Max number of channels/Chip Select (CS) supported.
#define MCSPI_TRANSFER_COMPLETED ((int32_t)0U) |
#define MCSPI_TRANSFER_STARTED ((int32_t)1U) |
#define MCSPI_TRANSFER_CANCELLED ((int32_t)2U) |
#define MCSPI_TRANSFER_FAILED ((int32_t)3U) |
#define MCSPI_TRANSFER_CSN_DEASSERT ((int32_t)4U) |
#define MCSPI_TRANSFER_TIMEOUT ((int32_t)5U) |
#define MCSPI_MS_MODE_CONTROLLER (CSL_MCSPI_MODULCTRL_MS_MASTER) |
The module generates the clock and CS.
#define MCSPI_MS_MODE_PERIPHERAL (CSL_MCSPI_MODULCTRL_MS_SLAVE) |
The module receives the clock and CS.
#define MCSPI_FF_POL0_PHA0 (0U) |
#define MCSPI_FF_POL0_PHA1 (1U) |
#define MCSPI_FF_POL1_PHA0 (2U) |
#define MCSPI_FF_POL1_PHA1 (3U) |
#define MCSPI_CS_POL_HIGH (CSL_MCSPI_CH0CONF_EPOL_ACTIVEHIGH) |
SPIEN (CS) is held high during the ACTIVE state.
#define MCSPI_CS_POL_LOW (CSL_MCSPI_CH0CONF_EPOL_ACTIVELOW) |
SPIEN (CS) is held low during the ACTIVE state.
#define MCSPI_TR_MODE_TX_RX (CSL_MCSPI_CH0CONF_TRM_TRANSRECEI) |
#define MCSPI_TR_MODE_RX_ONLY (CSL_MCSPI_CH0CONF_TRM_RECEIVONLY) |
#define MCSPI_TR_MODE_TX_ONLY (CSL_MCSPI_CH0CONF_TRM_TRANSONLY) |
#define MCSPI_IS_D0 (CSL_MCSPI_CH0CONF_IS_LINE0) |
Data line 0 (SPIDAT[0]) selected for reception.
#define MCSPI_IS_D1 (CSL_MCSPI_CH0CONF_IS_LINE1) |
Data line 1 (SPIDAT[1]) selected for reception.
#define MCSPI_DPE_ENABLE (CSL_MCSPI_CH0CONF_DPE0_ENABLED) |
Data line selected for transmission.
#define MCSPI_DPE_DISABLE (CSL_MCSPI_CH0CONF_DPE0_DISABLED) |
No transmission on Data Line.
#define MCSPI_SLV_CS_SELECT_0 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN0) |
#define MCSPI_SLV_CS_SELECT_1 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN1) |
#define MCSPI_SLV_CS_SELECT_2 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN2) |
#define MCSPI_SLV_CS_SELECT_3 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN3) |
#define MCSPI_SB_POL_HIGH (CSL_MCSPI_CH0CONF_SBPOL_HIGHLEVEL) |
SStart-bit polarity is held to 1 during MCSPI transfer.
#define MCSPI_SB_POL_LOW (CSL_MCSPI_CH0CONF_SBPOL_LOWLEVEL) |
Start-bit polarity is held to 0 during MCSPI transfer.
#define MCSPI_TCS0_0_CLK (CSL_MCSPI_CH0CONF_TCS0_ZEROCYCLEDLY) |
0.5 clock cycles delay
#define MCSPI_TCS0_1_CLK (CSL_MCSPI_CH0CONF_TCS0_ONECYCLEDLY) |
1.5 clock cycles delay
#define MCSPI_TCS0_2_CLK (CSL_MCSPI_CH0CONF_TCS0_TWOCYCLEDLY) |
2.5 clock cycles delay
#define MCSPI_TCS0_3_CLK (CSL_MCSPI_CH0CONF_TCS0_THREECYCLEDLY) |
3.5 clock cycles delay
#define MCSPI_CH_MODE_SINGLE (CSL_MCSPI_MODULCTRL_SINGLE_SINGLE) |
Only one channel will be used in controller mode. This should be used when CS is used in forced enable mode.
#define MCSPI_CH_MODE_MULTI (CSL_MCSPI_MODULCTRL_SINGLE_MULTI) |
More than one channel will be used in controller mode.
#define MCSPI_PINMODE_3PIN (CSL_MCSPI_MODULCTRL_PIN34_3PINMODE) |
SPIEN (CS) is not used. In this mode all related options to chip-select have no meaning.
#define MCSPI_PINMODE_4PIN (CSL_MCSPI_MODULCTRL_PIN34_4PINMODE) |
#define MCSPI_INITDLY_0 (CSL_MCSPI_MODULCTRL_INITDLY_NODELAY) |
No delay.
#define MCSPI_INITDLY_4 (CSL_MCSPI_MODULCTRL_INITDLY_4CLKDLY) |
4 SPI bus clock delays
#define MCSPI_INITDLY_8 (CSL_MCSPI_MODULCTRL_INITDLY_8CLKDLY) |
8 SPI bus clock delays
#define MCSPI_INITDLY_16 (CSL_MCSPI_MODULCTRL_INITDLY_16CLKDLY) |
16 SPI bus clock delays
#define MCSPI_INITDLY_32 (CSL_MCSPI_MODULCTRL_INITDLY_32CLKDLY) |
32 SPI bus clock delays
#define MCSPI_ERROR_TX_UNDERFLOW (0x00000001U) |
McSPI error macro's.
#define MCSPI_ERROR_RX_OVERFLOW (0x00000002U) |
#define MCSPI_MAX_CLK_DIVIDER_SUPPORTED (4096U) |
Maximuum Clock Divider supported
#define MCSPI_FIFO_LENGTH (64U) |
Total length of FIFO for both TX/RX.
#define MCSPI_RX_FIFO_ENABLE |
McSPI peripheral Rx FIFO is enabled.
#define MCSPI_RX_FIFO_DISABLE |
McSPI peripheral Rx FIFO is disabled.
#define MCSPI_TX_FIFO_ENABLE |
McSPI peripheral Tx FIFO is enabled.
#define MCSPI_TX_FIFO_DISABLE |
McSPI peripheral Tx FIFO is disabled.
#define MCSPI_REG_OFFSET (0x14U) |
McSPI Register Offset for MCSPI_CHxCONF, MCSPI_CHxSTAT, MCSPI_CHxCTRL, MCSPI_TXx and MCSPI_RXx register set.
#define MCSPI_CHCONF | ( | x | ) |
Base address of McSPI_CHCONF(x)
#define MCSPI_CHSTAT | ( | x | ) |
Base address of McSPI_CHSTAT(x)
#define MCSPI_CHCTRL | ( | x | ) |
Base address of McSPI_CHCTRL(x)
#define MCSPI_CHTX | ( | x | ) |
Base address of McSPI_CHTX(x)
#define MCSPI_CHRX | ( | x | ) |
Base address of McSPI_CHRX(x)
#define MCSPI_CLKD_MASK (0x0FU) |
#define MCSPI_IRQSTATUS_CLEAR_ALL |
Bit mask to clear all status bits.
typedef void* MCSPI_DmaHandle |
typedef void* MCSPI_DmaChConfig |
typedef uint32_t(* MCSPI_clockGet) (void) |
typedef void(* MCSPI_transferCallbackFxn) (void *args, uint32_t tansferStatus) |
The definition of a transfer completion callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK.
void* | void pointer |
typedef void(* MCSPI_errorCallbackFxn) (void *args) |
The definition of a error callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK.
void* | void pointer |
typedef struct MCSPILLD_InitObject * MCSPILLD_InitHandle |
typedef struct MCSPILLD_Object * MCSPILLD_Handle |
void MCSPI_reset | ( | uint32_t | baseAddr | ) |
void MCSPI_clearAllIrqStatus | ( | uint32_t | baseAddr | ) |
void MCSPI_stop | ( | MCSPILLD_Handle | hMcspi, |
MCSPI_ChObject * | chObj, | ||
uint32_t | chNum | ||
) |
void MCSPI_setChDataSize | ( | uint32_t | baseAddr, |
MCSPI_ChObject * | chObj, | ||
uint32_t | dataSize, | ||
uint32_t | csDisable | ||
) |
|
inlinestatic |
int32_t MCSPI_lld_init | ( | MCSPILLD_Handle | hMcspi | ) |
This API Initializes the McSPI instance.
hMcspi | Handle to the McSPI instance used |
int32_t MCSPI_lld_initDma | ( | MCSPILLD_Handle | hMcspi | ) |
This API Initializes the McSPI instance in DMA Mode.
hMcspi | Handle to the McSPI instance used |
int32_t MCSPI_lld_deInit | ( | MCSPILLD_Handle | hMcspi | ) |
This API De-Initializes the McSPI instance.
hMcspi | Handle to the McSPI instance used |
int32_t MCSPI_lld_deInitDma | ( | MCSPILLD_Handle | hMcspi | ) |
This API De-Initializes the McSPI instance in DMA mode.
hMcspi | Handle to the McSPI instance used |
int32_t MCSPI_lld_write | ( | MCSPILLD_Handle | hMcspi, |
void * | txBuf, | ||
uint32_t | count, | ||
uint32_t | timeout, | ||
const MCSPI_ExtendedParams * | extendedParams | ||
) |
This API writes data to the McSPI instance in Polling mode.
hMcspi | Handle to the McSPI instance used |
txBuf | Pointer to write data buffer |
count | Number of frames for this transaction |
timeout | Write timeout value |
extendedParams | Pointer to structure that contains the transfer data. |
int32_t MCSPI_lld_writeIntr | ( | MCSPILLD_Handle | hMcspi, |
void * | txBuf, | ||
uint32_t | count, | ||
uint32_t | timeout, | ||
const MCSPI_ExtendedParams * | extendedParams | ||
) |
This API writes data to the McSPI instance in Interrupt mode.
hMcspi | Handle to the McSPI instance used |
txBuf | Pointer to write data buffer |
count | Number of frames for this transaction |
timeout | write timeout value |
extendedParams | Pointer to structure that contains the transfer data. |
int32_t MCSPI_lld_writeDma | ( | MCSPILLD_Handle | hMcspi, |
void * | txBuf, | ||
uint32_t | count, | ||
uint32_t | timeout, | ||
const MCSPI_ExtendedParams * | extendedParams | ||
) |
This API writes data to the McSPI instance in DMA mode.
hMcspi | Handle to the McSPI instance used |
txBuf | Pointer to write data buffer |
count | Number of frames for this transaction |
timeout | write timeout value |
extendedParams | Pointer to structure that contains the transfer data. |
int32_t MCSPI_lld_read | ( | MCSPILLD_Handle | hMcspi, |
void * | rxBuf, | ||
uint32_t | count, | ||
uint32_t | timeout, | ||
const MCSPI_ExtendedParams * | extendedParams | ||
) |
This API reads data from the McSPI instance in Polling mode.
hMcspi | Handle to the McSPI instance used |
rxBuf | Pointer to Read data buffer |
count | Number of frames for this transaction |
timeout | Read timeout value |
extendedParams | Pointer to structure that contains the transfer data. |
int32_t MCSPI_lld_readIntr | ( | MCSPILLD_Handle | hMcspi, |
void * | rxBuf, | ||
uint32_t | count, | ||
uint32_t | timeout, | ||
const MCSPI_ExtendedParams * | extendedParams | ||
) |
This API reads data from the McSPI instance in Interrupt mode.
hMcspi | Handle to the McSPI instance used |
rxBuf | Pointer to Read data buffer |
count | Number of frames for this transaction |
timeout | Read timeout value |
extendedParams | Pointer to structure that contains the transfer data. |
int32_t MCSPI_lld_readDma | ( | MCSPILLD_Handle | hMcspi, |
void * | rxBuf, | ||
uint32_t | count, | ||
uint32_t | timeout, | ||
const MCSPI_ExtendedParams * | extendedParams | ||
) |
This API reads data from the McSPI instance in DMA mode.
hMcspi | Handle to the McSPI instance used |
rxBuf | Pointer to Read data buffer |
count | Number of frames for this transaction |
timeout | Read timeout value |
extendedParams | Pointer to structure that contains the transfer data. extendedParams |
int32_t MCSPI_lld_readWrite | ( | MCSPILLD_Handle | hMcspi, |
void * | txBuf, | ||
void * | rxBuf, | ||
uint32_t | count, | ||
uint32_t | timeout, | ||
const MCSPI_ExtendedParams * | extendedParams | ||
) |
This API reads writes data from the McSPI instance in polling mode.
hMcspi | Handle to the McSPI instance used |
txBuf | Pointer to write data buffer |
rxBuf | Pointer to Read data buffer |
count | Number of frames for this transaction |
timeout | Read write timeout value |
extendedParams | Pointer to structure that contains the transfer data. |
int32_t MCSPI_lld_readWriteIntr | ( | MCSPILLD_Handle | hMcspi, |
void * | txBuf, | ||
void * | rxBuf, | ||
uint32_t | count, | ||
uint32_t | timeout, | ||
const MCSPI_ExtendedParams * | extendedParams | ||
) |
This API reads writes data from the McSPI instance in Interrupt mode.
hMcspi | Handle to the McSPI instance used |
txBuf | Pointer to write data buffer |
rxBuf | Pointer to Read data buffer |
count | Number of frames for this transaction |
timeout | Read write timeout value |
extendedParams | Pointer to structure that contains the transfer data. |
int32_t MCSPI_lld_readWriteDma | ( | MCSPILLD_Handle | hMcspi, |
void * | txBuf, | ||
void * | rxBuf, | ||
uint32_t | count, | ||
uint32_t | timeout, | ||
const MCSPI_ExtendedParams * | extendedParams | ||
) |
This API reads writes data from the McSPI instance in DMA mode.
hMcspi | Handle to the McSPI instance used |
txBuf | Pointer to write data buffer |
rxBuf | Pointer to Read data buffer |
count | Number of frames for this transaction |
timeout | Read write timeout value |
extendedParams | Pointer to structure that contains the transfer data. |
int32_t MCSPI_lld_readWriteCancel | ( | MCSPILLD_Handle | hMcspi | ) |
This API cancels current McSPI transfer.
hMcspi | Handle to the McSPI instance used |
int32_t MCSPI_lld_readWriteDmaCancel | ( | MCSPILLD_Handle | hMcspi | ) |
This API cancels current McSPI transfer in DMA mode.
hMcspi | Handle to the McSPI instance used |
int32_t MCSPI_lld_transfer | ( | MCSPILLD_Handle | hMcspi, |
MCSPI_Transaction * | transaction | ||
) |
This API transfers data from the McSPI instance in Polling mode.
hMcspi | Handle to the McSPI instance used |
transaction | Pointer to structure that contains the transfer data. |
int32_t MCSPI_lld_transferIntr | ( | MCSPILLD_Handle | hMcspi, |
MCSPI_Transaction * | transaction | ||
) |
This API reads data from the McSPI instance in Interrupt mode.
hMcspi | Handle to the McSPI instance used |
transaction | Pointer to structure that contains the transfer data. |
int32_t MCSPI_lld_transferDma | ( | MCSPILLD_Handle | hMcspi, |
MCSPI_Transaction * | transaction | ||
) |
This API reads data from the McSPI instance in DMA mode.
hMcspi | Handle to the McSPI instance used |
transaction | Pointer to structure that contains the transfer data. |
void MCSPI_lld_controllerIsr | ( | void * | args | ) |
This is the McSPI Controller ISR and can be used as IRQ handler in Controller mode.
args | Argument to the ISR. |
void MCSPI_lld_peripheralIsr | ( | void * | args | ) |
This is the McSPI Peripheral ISR and can be used as IRQ handler in Peripheral mode.
args | Argument to the ISR. |
int32_t MCSPI_lld_getState | ( | MCSPILLD_Handle | hMcspi | ) |
This API returns the driver state.
hMcspi | Handle to the McSPI instance used |
int32_t MCSPI_lld_transferCancel | ( | MCSPILLD_Handle | hMcspi | ) |
This API cancels current McSPI transfer.
hMcspi | Handle to the McSPI instance used |
int32_t MCSPI_lld_transferDmaCancel | ( | MCSPILLD_Handle | hMcspi | ) |
This API cancels current McSPI transfer in DMA mode.
hMcspi | Handle to the McSPI instance used |
|
inlinestatic |
Function to initialize the MCSPI_ChConfig struct to its defaults.
chConfig | Pointer to MCSPI_ChConfig structure for initialization |
|
inlinestatic |
Function to initialize the MCSPI_Transaction struct to its defaults.
trans | Pointer to MCSPI_Transaction structure for initialization |
uint32_t MCSPI_lld_getBaseAddr | ( | MCSPILLD_Handle | handle | ) |
Function to get base address of MCSPI instance of a particular handle.
handle | MCSPILLD_Handle returned from MCSPI_open() |
int32_t MCSPI_lld_reConfigFifo | ( | MCSPILLD_Handle | handle, |
uint32_t | chNum, | ||
uint32_t | numWordsRxTx | ||
) |
Function to re-configure Effective FIFO Words.
handle | MCSPILLD_Handle returned from MCSPI_open() |
chNum | Channel used for communication. |
numWordsRxTx | Number of words to transfer |
|
inlinestatic |
This API will return the buffer width in bytes based on dataSize.
dataSize | MCSPI data frame size in bits - valid values: 4 bits to 32 bits |
|
inlinestatic |
This API will return the status of the McSPI channel currently in use.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel used for communication.'chNum' can take the following values.\n MCSPI_CHANNEL_n - Channel n is used for communication.\n |
|
inlinestatic |
This API returns Channel control register value.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
|
inlinestatic |
This API sets Channel control register value.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
regVal | register value to set in channel control register. |
|
inlinestatic |
This API returns Channel Config register value.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
|
inlinestatic |
This API sets Channel Config register value.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
regVal | register value to set in channel Config register. |
|
inlinestatic |
This API will put the data on to the McSPI Channel transmit register.
baseAddr | Memory Address of the McSPI instance used. |
txData | 32 bit data sent by the user which is put on to the MCSPI_TX register. |
chNum | Channel number of the McSPI instance used.'chNum' can take the following values.\n MCSPI_CHANNEL_n - Channel n is used for communication.\n For chNum n can range from 0-3.\n |
|
inlinestatic |
This API will enable/disable the Tx FIFOs of McSPI peripheral.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
enableFlag | Flag to enable/diable FIFO transmit mode. 'enableFlag' can take the following values.\n MCSPI_TX_FIFO_ENABLE - Enables the receiver FIFO of McSPI.\n MCSPI_TX_FIFO_DISABLE - Disables the receiver FIFO of McSPI.\n 'chNum' can take the following values.\n MCSPI_CHANNEL_n - Channel n is used for communication.\n For chNum n can range from 0-3.\n |
|
inlinestatic |
This API will enable/disable the Rx FIFOs of McSPI peripheral.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
enableFlag | Flag to enable/diable FIFO receive mode. 'enableFlag' can take the following values.\n MCSPI_RX_FIFO_ENABLE - Enables the receiver FIFO of McSPI.\n MCSPI_RX_FIFO_DISABLE - Disables the receiver FIFO of McSPI.\n 'chNum' can take the following values.\n MCSPI_CHANNEL_n - Channel n is used for communication.\n For chNum n can range from 0-3.\n |
|
inlinestatic |
This API will return the data present in the MCSPI_RX register.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. 'chNum' can take the following values.\n MCSPI_CHANNEL_n - Channel n is used for communication.\n For chNum n can range from 0-3.\n |
|
inlinestatic |
This API will set the data width in the channel config register.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
dataWidth | MCSPI data frame width in bits. 'chNum' can take the following values.\n MCSPI_CHANNEL_n - Channel n is used for communication.\n For chNum n can range from 0-3.\n For dataWidth valid values: 4 bits to 32 bits |